Skip to content

Generate

The generate command creates source code from configuration files.

Generate code

cfsutil generate -i <value> [-o <value>] [-v] [-s <value>]

Generates source code from a .cfsconfig file. The -i <filename> switch is required. Additional switches are optional. The following switches are available:

Switch Effect
-i=<file> Required. The .cfsconfig file to generate from
-o=<directory> The output directory for the generated code
-s=<path> Adds a directory to search for plugins. Can be used multiple times
-v Generate verbose output

Example

 cfsutil generate -i=max32690-wlp.cfsconfig -v