Device tree
The device tree provides a command to parse device tree files (*.dts,*.dtsi, or *.overlay). The output is in JSON format.
Parse
cfsutil dt parse <FILEPATH> [-I <value>...] [-o <value>] [-v]
| Switch | Effect |
|---|---|
-I, --includeDirs=<value>... |
Specifies directories to include when parsing the Devicetree file. Can be used multiple times, e.g., -Idir1 -Idir2 -Idir3 |
-o, --output=<value> |
Specifies the output file in JSON format. |
-v, --verbose |
Enables verbose mode for additional details during parsing. |
Example
cfsutil dt parse myfile.dts -o output.json