Skip to content

Profile

The cfsutil ai profile command estimates memory usage, hardware performance, per-layer efficiency, and optimization opportunities for a model on the target device. Unlike cfsutil ai compat (which flags unsupported features), it focuses on performance characteristics and optimization opportunities. You can apply the suggested optimizations to improve efficiency and better fit the model to your hardware.

Note

This is an early version of the reporting feature, and it may evolve in future releases. Currently, only TFLM models are supported. CNN accelerator models on MAX78002, which use PyTorch (izer backend), are not supported for reporting.

Tip

The cfsutil ai profile logic is located in profile_resources.py. This script can be adapted or extended to suit your own use cases.

cfsutil ai profile [--format text|json] [-s <value>] [-p <value>] [-c <value>] [-a <value>] [-m <value>] [--report-file <value>] [--report-format text|json] [-x <value>...] [--ignore-cache]

To run the cfsutil ai profile command, you must provide:

  • The model path with --model (or -m)
  • The target SoC with --soc (or -s)

--core is optional for SoCs with a single AI-capable core — it is inferred automatically.

cfsutil ai profile --soc <soc> --model <path/to/model_file>

Tip

If the SoC has exactly one AI-capable core, --core is inferred automatically. If the SoC has multiple cores but only one supports AI, it is still inferred — but a warning is shown confirming which core was selected. If multiple AI-capable cores are available, you must specify --core. Run cfsutil socs info <soc> --cores to see available cores for a given SoC.

Example

# --core inferred (MAX32657 has one AI-capable core)
cfsutil ai profile --soc MAX32657 --model model.tflite

# --core required (ADSP-SC835 has two AI-capable cores)
cfsutil ai profile --soc ADSP-SC835 --core FX --model model.tflite

Flags

Flag Short Description
--acc -a Target accelerator.
--core -c Target core (optional when only one AI-capable core exists for the SoC — inferred automatically).
--model -m Path or URL to the model file.
--package -p SoC package.
--soc -s Target SoC.
--search-path -x Additional search path for templates and data models. Can be repeated.
--ignore-cache Bypass cache and fetch latest remote files.
--format Output format: text (default) or json.
--report-file Path to output report file.
--report-format Report output format: json (default) or text.

Check for a specific SoC package variant

cfsutil ai profile --soc MAX32690 --core CM4 --package WLP --model model.tflite

Output in JSON format

cfsutil ai profile --soc MAX32690 --core CM4 --model model.tflite --format json

Report output

The Resource Profiling report provides resource and performance estimates for your model on the target hardware. The report progressively drills down from high-level summaries to detailed layer-by-layer analysis across five key categories:

  • Model summary — Basic details about the model file and its size.
  • Memory analysis — Peak RAM usage, utilization, and whether it fits in the target hardware (includes optional memory issues and recommendations when problems are detected).
  • Hardware performance — Overall compute cycles, latency, and acceleration metrics.
  • Per-layer performance — Detailed cycles, energy, and memory usage for each layer, highlighting bottlenecks.
  • Optimization opportunities — Suggested strategies such as quantization, pruning, and layer-level alternatives for large or compute-heavy layers.

Report formats

The examples below show the terminal output. Use --report-format json with --report-file to generate machine-readable JSON output for programmatic analysis or integration with other tools.

Model summary

The model summary provides a high-level overview of the analyzed model before detailed profiling.

Field Description
Model name Filename of the model under test.
Model path Path to the model file on disk.
Framework ML framework type. Currently only TensorFlow Lite is supported.
Model size Memory required to store the model.
Data type Numerical precision defined in the model file.
Layer count Total number of layers parsed from the model.

Sample output

== MODEL SUMMARY ===
| Metric               | Value                                    |
| -------------------- | ---------------------------------------- |
| Model Name           | resnet.tflite                            |
| Model Path           | /Users/.../resnet.tflite                 |
| Framework            | TensorFlow Lite                          |
| Model Size           | 5787.48 KB                               |
| Data Type            | float32                                  |
| Layer Count          | 54                                       |

Memory analysis

Memory analysis shows how much RAM the model requires at runtime and compares it to the available RAM defined in the target hardware profile.

Field Description
Peak RAM Required Maximum RAM usage observed during model execution.
RAM Status Indicates whether RAM usage fits the target hardware constraints.
Available RAM Total RAM available on the target hardware, from the hardware profile.
RAM Utilization Percentage of available RAM consumed by peak usage. Formula: (Peak RAM Required ÷ Available RAM) × 100.

In the example below, the model requires 576 KB of RAM at runtime, which fits comfortably within the target hardware's 1 MB RAM. This corresponds to 56.2% utilization, so the RAM status is marked as OK.

Sample output

=== MEMORY ANALYSIS ===
| Memory Metric             | Value                               |
| ------------------------- | ----------------------------------- |
| Peak RAM Required         | 576.00 KB (0.56 MB)                 |
| RAM Status                | OK                                  |
| Available RAM             | 1024.00 KB (1.00 MB)                |
| RAM Utilization           | 56.2%                               |

Memory issues

Lists the critical problems identified. This section appears only if the profiler detects over-usage or excessive utilization. For example, model peak RAM exceeds target RAM.

Sample output

Memory Issues:
    • Peak RAM usage (5880.0 KB) exceeds available RAM (1024.0 KB)

Memory recommendations

Provides recommendations tailored to the model and target hardware. The set of recommendations varies depending on the severity level, model architecture, computational complexity and memory usage patterns.

Sample output

Memory Recommendations:
    • URGENT: Model requires 4856 KB (474%) more RAM than available
    • Evaluate quantization potential with representative dataset

Hardware performance

This section estimates how the model performs on the target hardware. Metrics are aggregated from per-layer analysis and the hardware profile.

Field Description
Total cycles Total number of compute cycles required for full model execution.
Estimated latency End-to-end inference time in milliseconds, derived from cycles and max CPU clock frequency.
Peak memory Maximum RAM required during inference.
Accelerated layers Number of layers executed using hardware accelerators (such as DSP, NPU).
CPU-only layers Number of layers that must run on the CPU because no hardware acceleration is available.

For example, in the sample output below, the model runs in about 1.8 seconds (1802.62 ms), requires 576 KB of RAM at peak, and executes 37 layers on accelerators with 17 layers falling back to the CPU.

Sample output

=== HARDWARE PERFORMANCE ===
| Metric               | Value                               |
| -------------------- | ------------------------------------|
| Total Cycles         | 180,261,962                         |
| Estimated Latency    | 1802.62 ms                          |
| Peak Memory          | 576.00 KB                           |
| Accelerated Layers   | 37                                  |
| CPU-Only Layers      | 17                                  |

Per-layer performance

This section provides a detailed breakdown of compute and memory requirements for each model layer. It helps identify which specific layers are the performance bottlenecks.

Field Description
Layer Index of the layer in the model (e.g. 0, 1, 2). Matches the parser output.
Operator Operator type used in this layer (e.g. CONV_2D, ADD, SOFTMAX).
Cycles Total compute cycles required to execute the layer.
Latency Estimated runtime of the layer in milliseconds.
Energy Estimated energy consumption of the layer in microjoules (µJ).
Power Average power draw while executing the layer in milliwatts (mW). Currently disabled and shows -.
MACs Number of multiply-accumulate operations performed by the layer.
Memory Memory footprint of the layer in KB (if available).
Accel Whether the layer is executed on hardware acceleration (Yes) or CPU only (No).

For example, in the sample output below, layers 2 and 5 (CONV_2D) have significantly higher cycles and latency than the other layers, making them the primary performance bottlenecks.

Sample output

=== PER-LAYER PERFORMANCE ===
| Layer    | Operator        |     Cycles | Latency (ms) | Energy (uJ) |  Power (mW) |       MACs |  Memory (KB) | Accel  |
| -------- | --------------- | ---------- | ------------ | ----------- | ----------- | ---------- | ------------ | ------ |
| 0        | CONV_2D         |    442,368 |       4.4237 |      110.59 |           - |    442,368 |         1.75 |  Yes   |
| (CONV_2… |                 |            |              |             |             |            |              |        |
| 1        | CONV_2D         |  7,077,888 |      70.7789 |     1769.47 |           - |  7,077,888 |        27.19 |  Yes   |
| (CONV_2… |                 |            |              |             |             |            |              |        |
| 2        | CONV_2D         | 21,233,664 |     212.3366 |     5308.42 |           - | 21,233,664 |        81.19 |  Yes   |
| (CONV_2… |                 |            |              |             |             |            |              |        |
| 3        | CONV_2D         |    786,432 |       7.8643 |      196.61 |           - |    786,432 |         3.19 |  Yes   |
| (CONV_2… |                 |            |              |             |             |            |              |        |
| 4 (ADD)  | ADD             |     49,152 |       0.4915 |       12.29 |           - |     49,152 |            - |   No   |
| 5        | CONV_2D         | 21,233,664 |     212.3366 |     5308.42 |           - | 21,233,664 |        81.19 |  Yes   |
| (CONV_2… |                 |            |              |             |             |            |              |        |

Optimization opportunities

The Optimization Opportunities section provides baseline metrics about your model's resource requirements. These summary values help you understand the overall optimization potential before diving into layer-specific recommendations.

Field Description
Total parameter memory Size of all model parameters (weights) in KB, as parsed from the model.
Total MACs Multiply–accumulate operations required to run the model. Higher values indicate more compute demand.

These baseline metrics serve as reference points for measuring optimization impact. The actual optimization suggestions appear in the layerwise sections that follow.

Sample output

=== OPTIMIZATION OPPORTUNITIES ===
| Metric                 | Value       |
| ---------------------- | ----------- |
| Total Parameter Memory | 5787.48 KB  |
| Total MACs             | 180,261,962 |

Layerwise memory optimization opportunities

This section highlights individual layers with high parameter memory (weights), which are the most likely to benefit from targeted optimizations.

Field Description
Layer index Index of the layer in the model (e.g. 34).
Operation type Operator type, usually CONV_2D, comes from the model.
Parameter memory Estimated parameter memory footprint of the layer (in KB), if applicable.
MACs Number of multiply–accumulate operations for this layer.
Kernel info Kernel tensor shape information for the layer (e.g. [128, 3, 3, 128]), if available.
Suggestion Context-aware optimization hint (such as depthwise separable convolution, low-rank factorization).

The report lists only layers that exceed certain thresholds, such as large CONV_2D layers with floating-point weights. For these layers, suggestions are generated dynamically. For example, a convolution layer with 576 KB of parameters might receive a recommendation to use depthwise separable convolution or low-rank factorization to reduce memory usage on constrained hardware.

Sample output

|          |                 |     Param Mem |            |              |                      |
| Layer    | Op Type         |          (KB) |       MACs | Kernel Info  | Suggestion           |
| -------- | --------------- | ------------- | ---------- | ------------ | ---------------------|
| 34       | CONV_2D         |        576.50 |    147,456 | [[128, 3, 3, | Consider depthwise   |
|          |                 |               |            | 128], [128]] | separable            |
|          |                 |               |            |              | convolution or       |
|          |                 |               |            |              | low-rank             |
|          |                 |               |            |              | factorization        |
| 37       | CONV_2D         |        576.50 |    147,456 | [[128, 3, 3, | Consider depthwise   |
|          |                 |               |            | 128], [128]] | separable            |
|          |                 |               |            |              | convolution or       |
|          |                 |               |            |              | low-rank             |
|          |                 |               |            |              | factorization        |

Layerwise MAC optimization opportunities

This section highlights layers with very high multiply–accumulate operations (MACs), which often dominate the overall compute cost. The report lists only layers that exceed certain thresholds and provides targeted suggestions for reducing total cycles, latency, and energy usage. For example, large CONV_2D layers may be flagged with a recommendation to use depthwise convolution as a more efficient alternative.

Sample output

|          |                 |     Param Mem |            |              |                      |
| Layer    | Op Type         |          (KB) |       MACs | Kernel Info  | Suggestion           |
| -------- | --------------- | ------------- | ---------- | ------------ | -------------------- |
| 2        | CONV_2D         |         81.19 | 21,233,664 | [[48, 3, 3,  | Replace with         |
|          |                 |               |            | 48], [48]]   | depthwise            |
|          |                 |               |            |              | convolution to       |
|          |                 |               |            |              | reduce MACs          |
| 5        | CONV_2D         |         81.19 | 21,233,664 | [[48, 3, 3,  | Replace with         |
|          |                 |               |            | 48], [48]]   | depthwise            |
|          |                 |               |            |              | convolution to       |
|          |                 |               |            |              | reduce MACs          |

Next steps

Apply the recommended optimizations (such as quantization, pruning, or layer restructuring), then re-run cfsutil ai profile to verify improved efficiency and hardware compatibility.