2.3.0 Release Notes
Source
CodeFusion Studio source can be found on GitHub under tag V2.3.0
About this release
CodeFusion Studio 2.3.0 expands AI-assisted embedded development. A new Model Zoo helps you discover and deploy models. Documentation-backed AI assistant skills answer product questions directly in your editor. Zephelin profiling now captures traces over USB as well as UART, giving deeper insight into AI inference performance on hardware.
This release also includes a graphical Package Manager that puts browsing, filtering, and installing packages in one place, alongside workspace template expansion and usability improvements across the Workspace Creation Wizard, System Planner, and debug tools.
What's new
The following are some of the new features and enhancements introduced in version 2.3.0.
-
Workspace templates — expanded template library: This release adds new templates and extends existing templates to additional processors (SoCs).
Templates added or updated in this release include:
Template Supported processors MSDK Single Core AES MAX32655, MAX32672, MAX78000 MSDK Single Core Coremark MAX32655, MAX32690 MSDK Single Core CRC MAX32655, MAX32672, MAX32690, MAX78000 MSDK Single Core CTB AES MAX32672, MAX32690 MSDK Single Core ECC MAX78000 MSDK Single Core Flash MAX32655, MAX32672, MAX32690, MAX78000 MSDK Single Core GPIO MAX32655, MAX32672, MAX32690, MAX78000 MSDK Single Core Hash MAX32690 MSDK Single Core RTC Backup MAX32655, MAX32672, MAX32690, MAX78000 MSDK Single Core SPI MAX32655, MAX32672, MAX32690, MAX78000 Zephyr Single Core ADC Devicetree MAX32655, MAX32666, MAX32672, MAX32690, MAX78000 Zephyr Single Core CRC MAX32655, MAX32657, MAX32658, MAX32666, MAX32672, MAX32690, MAX78000 Zephyr Single Core Eventfd MAX32655, MAX32657, MAX32658, MAX32666, MAX32672, MAX32690, MAX78000 Zephyr Single Core Hello World User MAX32655, MAX32657, MAX32658, MAX32666, MAX32672, MAX32690, MAX78000 Zephyr Single Core LVGL Basic MAX32672, MAX32690 Zephyr Single Core UART Async API MAX32655, MAX32657, MAX32658, MAX32666, MAX32672, MAX32690, MAX78000 Templates are shown in the Workspace Creation wizard based on your selected device — choose your processor and board to see available templates for your hardware.
Note
The Zephyr Single Core Hello World User template builds a Zephyr userspace application (
CONFIG_USERSPACE=y), which requires thegperfpackage (gperf/3.1.0). When you create a workspace from this template, CFS detects thatgperfis required and prompts you to install it. See Commonly available packages.Processor support expanded for existing templates:
Template Processors added MSDK Single Core ICC (Instruction Cache Controller) MAX32672, MAX78000 Zephyr Single Core Basic Synchronization MAX32657, MAX32658, MAX32666, MAX32672, MAX78000 Zephyr Single Core Counter Alarm MAX32657, MAX32658, MAX32666, MAX32672, MAX78000 Zephyr Single Core Dining Philosophers MAX32657, MAX32658, MAX32666, MAX32672, MAX78000 Zephyr Single Core Hello World C++ MAX32657, MAX32658, MAX32666, MAX32672, MAX78000 Zephyr Single Core Synchronization C++ MAX32657, MAX32658, MAX32666, MAX32672, MAX78000 -
Quick Access Panel: The CFS sidebar now includes a Help and Support section with links to the Getting Started walkthrough, online documentation, Engineer Zone, and technical support.
-
Workspace Creation Wizard — template usability improvements:
- Templates in the Workspace Template section of the Workspace Creation Options step are now listed in alphabetical order.
- A search bar lets you filter templates by name or description, making it faster to find the right starting point.
-
Peripheral Allocation — automatic signal assignment: When you allocate a peripheral to a project, CFS automatically assigns each required signal (if it has a single possible pin), reducing manual setup.
-
Memory Viewer — go to symbol: The Go to field now accepts symbol names in addition to hex and decimal addresses. Enter a variable or function name to jump directly to its location in memory without looking up the address first.
-
Package Manager UI — new graphical package management: A new graphical interface for managing packages directly in VS Code. Browse and filter packages by name, status, SoC, or type; view package details including version history, license, and supported processors; and install or uninstall packages - all without leaving the editor. Open it by clicking Manage Packages in the Home section of the CFS sidebar, or by running (CFS) Open Package Manager from the Command Palette.
-
Telemetry — expanded usage insights: Anonymous, opt-in telemetry covers System Planner configuration, code generation, build, flash, debug, and artificial intelligence (AI) model workflows. Telemetry remains disabled by default and collects no personally identifying information.
Enabling telemetry is one of the most direct ways to influence what we build next — it tells us which features matter most so we can prioritize them. If you'd like to help shape the roadmap, you can turn it on at any time in Settings by searching for
cfs.telemetry. For more information about what is collected, view Telemetry. -
API key authentication for
cfsutil: CLI commands that access restricted cloud resources — includingcatalog update,ai build,docker pull, and package manager commands — can now authenticate using an API key. Set theCFS_API_KEYenvironment variable to your key value before running a command. This is particularly useful in CI/CD pipelines and other automated workflows where interactive login is not possible.Use the following commands under the
cfsutil myanalog apikeytopic to create and manage API keys. These commands require an active myAnalog session:Command Description cfsutil myanalog apikey createCreates a new API key. cfsutil myanalog apikey listLists all API keys for your account. cfsutil myanalog apikey delete <key-id>Deletes an API key by ID. -
Registers-Only Plugin deprecated: The Registers-Only (bare-metal) Plugin is deprecated and will be removed in a future release. It remains available in this release for advanced workflows that generate code accessing memory-mapped registers (MMRs) directly.
-
AI-Assisted Development Skills — doc-backed answers in your AI assistant: New
cfs-docsandcfs-cliskills give your AI assistant product-specific answers about CodeFusion Studio. They are bundled with the VS Code extension for GitHub Copilot, and follow the open Agent Skills standard so they also work in Claude Code, OpenAI Codex, and other supported agents. -
Model Zoo — browse and select AI models: When you add a model in the Embedded AI Tools or create a workspace from an AI model, the Browse button opens the Model Zoo — a library of AI models hosted by Analog Devices. Search and filter by platform, core, and category, compare model sizes across quantizations, and select a model to populate its file and, when available, sample data fields. You can still select a local model file, or point the Model Zoo at a custom source.
-
Profiling — USB trace capture: Capture Zephelin profiling traces over a USB interface in addition to UART. Select USB as the trace interface in System Planner, then select the connected USB device in the Trace Capture panel.
-
Machine-readable documentation (
llms.txt): The User Guide is available in an AI-friendly format that follows the llms.txt standard. Point your AI assistant at llms.txt for an indexed list of documentation sections, or llms-full.txt for the full documentation content in a single file. -
Build command output: Build commands display output in a new format. Underlying build behavior is unchanged.
Development platforms and tools
- Support for Zephyr RTOS 4.3 Get started with Zephyr RTOS 4.3
- Support for the MSDK Get started with MSDK
- Support for the ADSP-2183x/SC83x SHARC-FX family (Windows only), which requires the Xtensa SHARC-FX toolchain to build and the ADI ICE drivers to debug through ADI ICE probes. For setup and debugging instructions, see Debugging a SHARC-FX application.
- Compiler and debug support is available for Zephyr (Arm Cortex-M only) and MSDK (Arm Cortex-M and RISC-V) on supported MAX32xxx and MAX78xxx microcontrollers, and SHARC-FX (ADSP-2183x/SC83x family).
Software component versions installed with CFS 2.3.0
| Component | Version | Notes |
|---|---|---|
| Bare-metal ARM toolchain | 14.3.Rel1 | GCC toolchain for 32-bit Arm® targets |
| Bare-metal RISC-V toolchain | 14.2.0 | GCC toolchain for RISC-V targets |
| MSDK | 2.3.0 | Part support and examples for MAX32xxx and MAX78xxx microcontrollers |
| SHARC-FX SDK | 3.0.3 | SDK for the Cortex-M33 core on SHARC-FX targets |
| Zephyr RTOS | 4.3.0 | Real-time operating system for MAX32xxx and MAX78xxx microcontrollers |
| Zephyr SDK | 0.17.4 | GCC-based toolchain for 32-bit Arm® development with Zephyr RTOS |
Host architecture support
CodeFusion Studio is supported on the following host operating systems:
- Windows 11 (64-bit)
- macOS 15 and macOS 26 (ARM64)
- Ubuntu 22.04 and 24.04 (64-bit)
Earlier or newer OS versions might work but are not officially supported.
Target architecture support
Processor support is unchanged in this release. For the full list of supported processors and their feature support, see supported processors.
Known issues and limitations
- Profiling — USB trace capture on Windows: USB trace capture does not work reliably on Windows hosts. The device is usually not detected and does not appear in the USB Device list, and capture can fail even when the device is detected. Capturing through WSL2 is also unreliable, because USB device sharing is inconsistent. To capture profiling traces over USB, use a macOS or Linux host.
- Profiling — USB trace capture for run-once applications: USB capture cannot record traces from applications whose traced activity runs once at startup, including the Zephyr Single Core TensorFlow AI Inference Profiling template. Periodic metrics such as CPU Load remain available. Use UART to capture run-once traces. See Profiling.
- Profiling — USB trace capture fails to build on MAX78002, MAX32650, and MAX32666: On MAX78002, MAX32650, and MAX32666 Zephyr projects, selecting USB as the trace interface generates code that fails to build, because the High-Speed USB peripheral on these processors is not yet supported in the Zephyr devicetree. The build stops with
warning: The High-Speed USB peripheral is not currently supported in devicetreefollowed byerror: '__device_dts_ord_DT_N_NODELABEL_zephyr_udc0_ORD' undeclared. In this release, USB trace capture is supported on MAX32690 only, and on macOS and Linux hosts only (see the Windows limitation in this section). Use UART to capture profiling traces on MAX78002, MAX32650, and MAX32666. See Profiling. - Profiling — trace capture not supported on MAX32675C: On MAX32675C Zephyr projects, Zephelin profiling trace capture is not supported over UART or USB.
- Model Zoo — default catalog coverage: The Model Zoo displays models from the default catalog for the ADSP-SC835 / SC835W and MAX32690. For other processors, point the Model Zoo at a custom source or select a local model file instead.
- Package Manager UI — Type filter: The Type filter may not always return the correct package results. To find a specific package, search by name using the search field instead.