MAX32657/MAX32658 Zephyr 4.4.0
This tutorial gets you up and running with MAX32657 or MAX32658 development on Zephyr 4.4.0 using CodeFusion Studio. You install the required packages, run the Blinky example to verify your board, and then run the low power mode example.
Prerequisites
Before you begin:
-
Install the
zephyr/4.4.0-b.1package (zephyr_arm_toolchain/1.0.1is installed automatically as a dependency):- Command Palette: Open the Command Palette and run (CFS) Install Package. Find
zephyr/4.4.0-b.1in the list and install it. See Install packages using the Command Palette. -
Command line: Run the following from the CFS Terminal. See Install packages using cfsutil.
cfsutil pkg install zephyr/4.4.0-b.1
- Command Palette: Open the Command Palette and run (CFS) Install Package. Find
-
Install J-Link drivers V8.94 or later and configure your CFS J-Link (
cfs.jlink.path) path to point to the J-Link installation directory — see Install J-Link drivers. -
Connect your EV Kit — see Connect hardware.
Tutorials
Run the tutorials in order — low power mode builds on the setup from Blinky.
- Blinky — Flash an LED and verify your board.
- Low power mode — Step the device through its supported low power states.