Docker
The CLI can be used to pull Docker images from the Analog Devices registry. If you are logged in to myAnalog or have set the CFS_API_KEY environment variable with a valid API key, your credentials are used for authentication. See myAnalog authentication and API key authentication for more information.
Requirements
The CLI will invoke Docker or Podman to perform the pull, so one of these applications must be installed and found on PATH.
- Docker
- Podman
Pull image
cfsutil docker pull IMAGE [-n] [-q] [-u]
| Flag | Description |
|---|---|
-n, --nocredential |
Do not use credentials when pulling the image. |
-u, --update |
Pull the Docker image even if it already exists locally. |
-q, --quiet |
Suppress output from the pull command. |
Example
cfsutil docker pull docker.cloudsmith.io/adi/codefusion-public/EXAMPLE -q