Skip to content

2.0.2 Release Notes

Source

CodeFusion Studio source can be found on GitHub under tag V2.0.2

About this release

CodeFusion Studio 2.0.2 is a patch release that fixes a regression affecting CFS Telemetry.

In CodeFusion Studio 2.0.1, telemetry events were not collected due to this regression. This impacted the following event types:

  • Workspace creation events
  • Extension activation events

Ensure that you are running the CodeFusion Studio 2.0.2 VS Code extension to resolve this issue.

If extension auto-updates are enabled, no action is required. For installation or upgrade steps, refer to Install the CodeFusion Studio VS Code extension.

Note

CodeFusion Studio 2.0.2 is distributed only through the Visual Studio Code Marketplace. A standalone installer is not provided for this release, so manual installation using a VSIX file is not supported.

What's new

Bug fixes

  • Fixed an issue where CFS telemetry events were not correctly emitted in version 2.0.1
  • Updated release notes and CHANGELOG.md

Known Issues

See 2.0.1 known issues for other issues.