AD—- HDL Project (template)

Overview

Supported boards

Supported devices

Supported carriers

Evaluation board

Carrier

FMC slot

EVAL-AD9081

A10SoC

FMCA

VCK190

FMC0

VCU118

FMC+

ZCU102

FMC HPC0

ZC706

FMC HPC

Block design

Block diagram

The data path and clock domains are depicted in the below diagram:

AD-QUADMXFE1-EBZ/VCU118 JESD204B block diagram

Important

This configuration was built using the make command with the following parameters:

/hdl/projects/ad_quadmxfe1_ebz$
make JESD_MODE=8B10B \
     RX_JESD_L=4 \
     RX_JESD_M=8 \
     RX_JESD_NP=16 \
     RX_NUM_LINKS=4 \
     TX_JESD_L=4 \
     TX_JESD_M=8 \
     TX_JESD_NP=16 \
     TX_NUM_LINKS=4

Block name

IP name

Documentation

Additional info

AXI_ADXCVR

axi_adxcvr

AXI ADXCVR

2 instances, one for RX and one for TX

AXI_DMAC

axi_dmac

AXI DMAC

2 instances, one for RX and one for TX

DATA_OFFLOAD

data_offload

Data Offload

2 instances, one for RX and one for TX

RX JESD LINK

axi_mxfe_rx_jesd

JESD204B/C Link Receive Peripheral

Instantiaded by adi_axi_jesd204_rx_create procedure

RX JESD TPL

rx_mxfe_tpl_core

ADC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_rx_create procedure

TX JESD LINK

axi_mxfe_tx_jesd

JESD204B/C Link Transmit Peripheral

Instantiaded by adi_axi_jesd204_tx_create procedure

TX JESD TPL

tx_mxfe_tpl_core

DAC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_tx_create procedure

UTIL_ADXCVR

util_adxcvr

UTIL_ADXCVR core for AMD Xilinx devices

Used for both AXI ADXCVR instances

UTIL_CPACK

util_cpack2

Channel CPACK Utility

—

UTIL_UPACK

util_upack2

Channel UPACK Utility

—

Clock scheme

  • External clock source AD-SYNCHRONA14-EBZ

  • SYSREF clocks are LVDS

  • ADCCLK and REFCLK are LVPECL

Only the channels presented in the clocking selection are relevant. For the rest, you can either disable them or just put a divided frequency of the source clock.

Limitations

The design has one JESD receive chain with 4 lanes at rate of 13Gbps. The JESD receive chain consists of a physical layer represented by an XCVR module, a link layer represented by an RX JESD LINK module and transport layer represented by a RX JESD TPL module. The link operates in Subclass 1.

The link is set for full bandwidth mode and operate with the following parameters:

Deframer paramaters: L=4, M=2, F=1, S=1, NP=16

SYSREF - 5.078125 MHZ
REFCLK - 325MHz (Lane Rate/40)
DEVICECLK - 325 MHz
ADCCLK - 1300MHz
JESD204B Lane Rate - 13Gbps

The transport layer component presents on its output 128 bits at once on every clock cycle, representing 4 samples per converter. The two receive chains are merged together and transferred to the DDR with a single DMA.

Configuration modes

The following are the parameters of this project that can be configured:

  • JESD_MODE: used link layer encoder mode

    • 64B66B - 64b66b link layer defined in JESD204C, uses AMD IP as Physical Layer

    • 8B10B - 8b10b link layer defined in JESD204B, uses ADI IP as Physical Layer

  • RX_LANE_RATE: lane rate of the Rx link (MxFE to FPGA)

  • TX_LANE_RATE: lane rate of the Tx link (FPGA to MxFE)

  • REF_CLK_RATE: the rate of the reference clock

  • [RX/TX]_JESD_M: number of converters per link

  • [RX/TX]_JESD_L: number of lanes per link

  • [RX/TX]_JESD_S: number of samples per frame

  • [RX/TX]_JESD_NP: number of bits per sample

  • [RX/TX]_NUM_LINKS: number of links

  • [RX/TX]_TPL_WIDTH

  • TDD_SUPPORT: set to 1, adds the TDD; enables external synchronization through TDD. Must be set to 1 when SHARED_DEVCLK=1

  • SHARED_DEVCLK

  • TDD_CHANNEL_CNT

  • TDD_SYNC_WIDTH

  • TDD_SYNC_INT

  • TDD_SYNC_EXT

  • TDD_SYNC_EXT_CDC: if enabled, the CDC circuitry for the external sync signal is added

  • [RX/TX]_KS_PER_CHANNEL: Number of samples stored in internal buffers in kilosamples per converter (M)

  • [ADC/DAC]_DO_MEM_TYPE

  • Check out this guide on more details regarding these parameters: AXI TDD

Detailed description

The design has one JESD204B receive chain and one transmit chain, each with 8 lanes.

Each chain consists of a transport layer represented by a JESD TPL module, a link layer represented by a JESD LINK module, and a shared among chains physical layer, represented by an XCVR module. The HDL project in its current state, has the link operating in subclass 0.

  • Rx device clock - 122.88 MHz

  • Tx device clock - 245.76 MHz

  • JESD204B Rx Lane Rate - 4.9152 Gbps

  • JESD204B Tx Lane Rate - 9.8304 Gbps

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Depending on the values of parameters $INTF_CFG, $ADI_PHY_SEL and $TDD_SUPPORT, some IPs are instantiated and some are not.

Check-out the table below to find out the conditions.

Instance

Depends on parameter

Zynq/Microblaze

ZynqMP

Versal

axi_mxfe_rx_xcvr

$INTF_CFG!=”TX” & $ADI_PHY_SEL==1

0x44A6_0000

0x84A6_0000

0xA4A6_00000

rx_mxfe_tpl_core

$INTF_CFG!=”TX”

0x44A1_0000

0x84A1_0000

0xA4A1_00000

axi_mxfe_rx_jesd

$INTF_CFG!=”TX”

0x44A9_0000

0x84A9_0000

0xA4A9_00000

axi_mxfe_rx_dma

$INTF_CFG!=”TX”

0x7C42_0000

0x9C42_0000

0xBC42_00000

mxfe_rx_data_offload

$INTF_CFG!=”TX”

0x7C45_0000

0x9C45_0000

0xBC45_00000

axi_mxfe_tx_xcvr

$INTF_CFG!=”RX” & $ADI_PHY_SEL==1

0x44B6_0000

0x84B6_0000

0xA4B6_00000

tx_mxfe_tpl_core

$INTF_CFG!=”RX”

0x44B1_0000

0x84B1_0000

0xA4B1_00000

axi_mxfe_tx_jesd

$INTF_CFG!=”RX”

0x44B9_0000

0x84B9_0000

0xA4B9_00000

axi_mxfe_tx_dma

$INTF_CFG!=”RX”

0x7C43_0000

0x9C43_0000

0xBC43_00000

mxfe_tx_data_offload

$INTF_CFG!=”RX”

0x7C44_0000

0x9C44_0000

0xBC44_00000

axi_tdd_0

$TDD_SUPPORT==1

0x7C46_0000

0x9C46_0000

0xBC46_00000

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PS

SPI 0

ADXYZT

0

PS

SPI 1

AD0000

0

PL

axi_spi_bus_1

AD23456

0

GPIOs

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

Software GPIO

(from FPGA view)

Zynq-7000

Zynq MP

signal_name[31:0]

IN/OUT/INOUT

127:96

181:150

205:174

signal_name[31:0]

IN/OUT/INOUT

95:64

149:118

173:142

signal_name[31:0]

IN/OUT/INOUT

63:32

117:86

141:110

Interrupts

Below are the Programmable Logic interrupts used in this project.

You have many ways of writing this table: as a list-table or really to draw it. Take a look in the .rst of this page to see how they’re written and which suits best your case.

Instance name

HDL

Linux Zynq

Actual Zynq

Linux ZynqMP

Actual ZynqMP

S10SoC

Linux Cyclone V

Actual Cyclone V

—

15

59

91

111

143

32

55

87

—

14

58

90

110

142

31

54

86

—

13

57

89

109

141

30

53

85

—

12

56

88

108

140

29

52

84

—

11

55

87

107

139

28

51

83

—

10

54

86

106

138

27

50

82

—

9

53

85

105

137

26

49

81

—

8

52

84

104

136

25

48

80

—

7

36

68

96

128

24

47

79

—

6

35

67

95

127

23

46

78

—

5

34

66

94

126

22

45

77

—

4

33

65

93

125

21

44

76

—

3

32

64

92

124

20

43

75

—

2

31

63

91

123

19

42

74

—

1

30

62

90

122

18

41

73

—

0

29

61

89

121

17

40

72

Resource utilization

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.

Then go to the hdl/projects/$eval_board/$carrier location and run the make command.

Linux/Cygwin/WSL

Example of running the make command without parameters (using the default configuration):

~$
cd hdl/projects/ad9081_fmca_ebz/zcu102
~/hdl/projects/ad9081_fmca_ebz/zcu102$
make

Example of running the make command with parameters:

~$
cd hdl/projects/ad9081_fmca_ebz/a10soc
~/hdl/projects/ad9081_fmca_ebz/a10soc$
make RX_LANE_RATE=2.5 TX_LANE_RATE=2.5 RX_JESD_L=8 RX_JESD_M=4 RX_JESD_S=1 RX_JESD_NP=16 TX_JESD_L=8 TX_JESD_M=4 TX_JESD_S=1 TX_JESD_NP=16

The following dropdowns contain tables with the parameters that can be used to configure this project, depending on the carrier used. Where a cell contains a — (dash) it means that the parameter doesn’t exist for that project (ad9081_fmca_ebz/$carrier or ad9082_fmca_ebz/$carrier).

Parameter

Default value of the parameters

depending on carrier

VCK190

VCU118

ZC706

ZCU102

JESD_MODE

64B66B

8B10B

8B10B*

8B10B*

RX_LANE_RATE

24.75

15

10

15

TX_LANE_RATE

24.75

15

10

15

REF_CLK_RATE

375

—

—

—

RX_JESD_M

4

4

8

4

RX_JESD_L

8

8

4

8

RX_JESD_S

4

1

1

1

RX_JESD_NP

12

16

16

16

RX_NUM_LINKS

1

1

1

1

RX_TPL_WIDTH

—

—

—

{}

TX_JESD_M

4

4

8

4

TX_JESD_L

8

8

4

8

TX_JESD_S

8

1

1

1

TX_JESD_NP

12

16

16

16

TX_NUM_LINKS

1

1

1

1

TX_TPL_WIDTH

—

—

—

{}

RX_KS_PER_CHANNEL

64

64

—

—

TX_KS_PER_CHANNEL

64

64

—

—

Legend

* — for this carrier only the 8B10B mode is supported

The result of the build, if parameters were used, will be in a folder named by the configuration used:

if the following command was run

make RX_LANE_RATE=2.5 TX_LANE_RATE=2.5 RX_JESD_L=8 RX_JESD_M=4 RX_JESD_S=1 RX_JESD_NP=16 TX_JESD_L=8 TX_JESD_M=4 TX_JESD_S=1 TX_JESD_NP=16

then the folder name will be:

RXRATE2_5_TXRATE2_5_RXL8_RXM4_RXS1_RXNP16_TXL8_TXM4_TXS1_TXNP16 because of truncation of some keywords so the name will not exceed the limits of the Operating System (JESD, LANE, etc. are removed) of 260 characters.

A more comprehensive build guide can be found in the Build an HDL project user guide.

Software considerations

ADC - crossbar config *** EXAMPLE ***

Due to physical constraints, Rx lanes are reordered as described in the following table.

e.g physical lane 2 from ADC connects to logical lane 7 from the FPGA. Therefore the crossbar from the device must be set accordingly.

ADC phy Lane

FPGA Rx lane / Logical Lane

0

2

1

0

2

7

3

6

4

5

5

4

6

3

7

1

DAC - crossbar config *** EXAMPLE ***

Due to physical constraints, Tx lanes are reordered as described in the following table:

e.g physical lane 2 from DAC connects to logical lane 7 from the FPGA. Therefore the crossbar from the device must be set accordingly.

DAC phy Lane

FPGA Tx lane / Logical Lane

0

0

1

2

2

7

3

6

4

1

5

5

6

4

7

3

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.