ADRV9364Z7020 HDL Project

Overview

The ADRV9364-Z7020 is built on a portfolio of highly integrated System-On-Module (SOMs) based on the Xilinx Zynq-7000 All Programmable (AP) SoC. Starting with the AD9364, it is schematically & HDL similar to the FMCOMMS4.

The purpose of the ADRV9364-Z7020 RF SOM is to provide an RF platform to software developers, system architects, product developers, etc, who want a single platform operating over a wide tuning range (70 MHz - 6 GHz) that is capable of being used for prototype, evaluation and reference design to help with production volume.

Supported boards

Supported devices

Supported carriers

Block design

The block design is very similar to FMCOMMS4.

Block diagram

The data path and clock domains are depicted in the below diagram.

ADRV9364-Z7020 block diagram

Configuration modes

The AD9361 IP in this HDL project is configured to work in both CMOS and LVDS interfaces; it supports two configuration modes:

  • 2R2T - 2x receive and 2x transmit RF channels

  • 1R1T - 1x receive and 1x transmit RF channel

Both support only the dual port half duplex operating mode. The maximum data rate (for combined I and Q words) is 61.44MSPS in DDR. For more details about these modes, check the AD9361 Reference Manual, Table 48 “Maximum Data Rates and Signal Bandwidths”.

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Zynq

axi_iic_main

0x4160_0000

axi_sysid_0

0x4500_0000

axi_ad9361_adc_dma

0x7C40_0000

axi_ad9361_dac_dma

0x7C42_0000

axi_ad9361

0x7902_0000

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

iic_main

axi_iic_main

0x4160_0000

—

SPI connections

The SPI signals are controlled by a separate AXI based SPI core.

SPI type

SPI manager instance

SPI subordinate

CS

HPS

SPI 0

AD9361

0

GPIOs

The Software GPIO number is calculated as follows:

  • Zynq-7000: if PS7 is used, then offset is 54

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

gpio_clksel

INOUT

51

105

gpio_resetb

INOUT

46

100

gpio_sync

INOUT

45

99

gpio_en_agc

INOUT

44

98

gpio_ctl[3:0]

INOUT

43:40

97:94

gpio_status[7:0]

INOUT

39:32

93:86

Interrupts

Below are the Programmable Logic interrupts used in the project.

Instance name

HDL

Linux Zynq

Actual Zynq

axi_ad9361_adc_dma

13

57

89

axi_ad9361_dac_dma

12

56

88

axi_ad9361

11

55

87

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.

Go to the hdl/projects/adrv9364z7020/$carrier location and run the make command.

Linux/Cygwin/WSL

~$
cd hdl/projects/adrv9364z7020/ccbob_cmos
~/hdl/projects/adrv9364z7020/ccbob_cmos$
make

Directory

Description

ccbob_cmos

ADRV9364Z7020-SOM (CMOS Mode) + ADRV1CRR-BOB

ccbob_lvds

ADRV9364Z7020-SOM (LVDS Mode) + ADRV1CRR-BOB

ccusb_lvds

ADRV9364Z7020-SOM (LVDS Mode) + ADRV1CRR-USB

ccpackrf_lvds

ADRV9361Z7035-SOM (LVDS Mode) + ADRV1CRR-PACKRF*

Legend

  • * removed, last release that supported the project is hdl_2021_r2

Directory/File

Description

common/adrv9364z7020_bd.tcl

ADRV9364Z7020-SOM board design file.

common/ccbob_bd.tcl

carrier, break out board design file.

common/ccusb_bd.tcl

carrier, usb board design file.

Note

FMC & BOB carrier designs include loopback daughtercards for connectivity testing.

Directory/File

Description

common/ adrv9364z7020_constr.xdc

ADRV9364Z7020-SOM base constraints file.

common/ adrv9364z7020_constr_cmos.xdc

ADRV9364Z7020-SOM CMOS mode constraints file.

common/ adrv9364z7020_constr_lvds.xdc

ADRV9364Z7020-SOM LVDS mode constraints file.

common/ccbob_constr.xdc

carrier, break out board constraints file.

common/ccusb_constr.xdc

carrier, usb board constraints file.

Note

FMC & BOB carrier designs include loopback daughtercards for connectivity testing.

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.