CN0363 HDL project

Overview

The EVAL-CN0363-PMDZ is a dual channel colorimeter featuring a modulated light source transmitter, programmable gain transimpedance amplifiers on each channel, and a very low noise, 24-bit sigma delta ADC. The output of the ADC connects via a standard PMOD connector to a FPGA. The FPGA takes the sampled data from the ADC and implements a synchronous detection algorithm. By using modulated light and digital synchronous detection, rather than a constant (dc) source, the system strongly rejects any noise sources at frequencies other than the modulation frequency, providing excellent accuracy.

The dual channel circuit measures the ratio of light absorbed by the liquids in the sample and reference containers at three different wavelengths. This forms the basis of many chemical analysis and environmental monitoring instruments used to measure concentrations and characterize materials through absorption spectroscopy.

The EVAL-CN0363-PMDZ HDL reference design is based on the Analog Devices base reference design for the ZED board. In addition to the base reference design EVAL-CN0363-PMDZ HDL reference design implements function blocks to communicate over a SPI bus with the AD7175-2 Sigma-Delta ADC to configure it and receive the raw ADC data as well a configure the AD5201 digital potentiometer. The data received from the ADC is passed to a processing pipeline which performs a digital synchronous detector and finally write the data to system memory using a DMA. The HDL reference design is also responsible for generating the LED excitation signal. A simplified functional block diagram of the system is given below.

Supported boards

Supported devices

Supported carriers

Block design

Block diagram

The data path and clock domains are depicted in the below diagram:

CN0363_PMDZ block diagram

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Zynq

axi_adc

0x43C0_0000

spi_cn0363_axi_regmap

0x44A0_0000

axi_dma

0x44A3_0000

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

iic_fmc

axi_iic_fmc

0x4162_0000

—

PL

iic_main

axi_iic_main

0x4160_0000

—

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PL

axi_spi_engine

cn0363

0

GPIOs

The Software GPIO number is calculated as follows:

  • Zynq-7000: if PS7 is used, then offset is 54

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

spi_sdi

IN

34

88

gain1_o

OUT

33

87

gain0_o

OUT

32

86

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Zynq

Actual Zynq

axi_dma

13

57

89

spi

12

56

88

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/cn0363/zed
~/hdl/projects/cn0363/zed$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.