PULSAR-ADC HDL project

Overview

Depending on the type of connector it uses, the PulSAR family is divided into the products which have PMOD connectors and FMC connectors.

PulSAR converters which have PMOD boards associated with them are low power ADCs which offer very high performance from 14-bits up to 18-bits with throughputs ranging from 100ksps to 1.3MSPS. The boards are designed to demonstrate the ADC’s performance and to provide an easy digital interface for a variety of system applications. The PulSAR family share the same interface and the same PCB, the differences being found in their performance. A full description of these products are available in their respective data sheets and should be consulted when utilizing the boards.

With PMOD

The ADAQ40xx family is also part of the PulSAR converters with PMOD connector.

This type of boards come with the EVAL-PMD-IB1Z PMOD to field programmable gate array (FPGA) mezzanine card (FMC) interposer board that interfaces with the system demonstration controller board.

The ADAQ4003 is an 18-bit precision data acquisition sub-system SiP design on a laminate that includes the AD4003 ADC with a fully differential driver the ADA4945-1, a reference buffer (the ADA4807-1), a precision resistor iPassive network on a separate die along with discrete capacitors and resistors. The device solves many design challenges for a wide range of applications similar to AD400x, yet it still provides the flexibility. It offers over 75% area savings compared to discrete design and reduces TTM.

With FMC

PulSAR converters which have FMC boards associated with them are AD40xx family.

The AD4003 / AD4007 / AD4011 / AD4020 are low noise, low power, high speed, 18-bit, precision successive approximation register (SAR) analog-to-digital converters (ADCs). The AD4003, AD4007, and AD4011 offer 2 MSPS, 1 MSPS, and 500 kSPS throughputs, respectively. They incorporate ease of use features that reduce signal chain power consumption, reduce signal chain complexity, and enable higher channel density. The high-Z mode, coupled with a long acquisition phase, eliminates the need for a dedicated high power, high speed ADC driver, thus broadening the range of low power precision amplifiers that can drive these ADCs directly while still achieving optimum performance. The input span compression feature enables the ADC driver amplifier and the ADC to operate off common supply rails without the need for a negative supply while preserving the full ADC code range. The low serial peripheral interface (SPI) clock rate requirement reduces the digital input/output power consumption, broadens processor options, and simplifies the task of sending data across digital isolation.

Applications:

  • Battery-powered equipment

  • Data acquisition

  • Instrumentation

  • Medical instruments

  • Process controls

  • Machine automation

Supported boards

PulSAR with PMOD connector:

PulSAR with FMC connector:

Supported devices

PulSAR with PMOD connector:

PulSAR with FMC connector:

Supported carriers

Other required hardware

Note

Only for ADAQ40xx

Block design

Block diagram

The data path and clock domains are depicted in the below diagrams:

PulSAR_ADC_PMDZ

PulSAR_ADC_PMOD block diagram

PulSAR_ADC_FMC

PulSAR_ADC_FMC block diagram

Design configuration

The reference design uses a clock generator for the division of the SPI clock and a PWM generator for the conversion signal. The required parameters can be set in the pulsar_adc_pmdz_bd.tcl file using the following values, where the PULSE_0_PERIOD is computed as Tcyc_min / Tspi_clk:

Part

PULSE_0_PERIOD

AD7942

640

AD7946

320

AD7988-1

1600

AD7685

640

AD7687

640

AD7691

640

AD7686

320

AD7688

320

AD7693

320

AD7988-5

320

AD7980

160

AD7983

120

AD7690

250

AD7982

160

AD7984

120

Configuration modes

The Zedboard-based PulSAR ADC project can be built to use either the FMC connector or the PMOD JA connector.

The FMC_N_PMOD parameter is used to select between them:

  • 0 - for PMOD

  • 1 - for FMC (default)

The PulSAR project supports different configurations required for certain ADCs, like the AD7944.

These modes are selected using the SPI_OP_MODE parameter:

  • 0 - for normal SPI Engine connections (default)

  • 1 - for 3-wire “single” mode where CS drives the SDO line while the CS line is driven by GPIO

  • 2 - SDO is driven by GPIO and the CS line is driven by CS.

Caution

The SPI_OP_MODE parameter must only be used for the FMC variant.

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL(see more at CPU/Memory interconnects addresses).

Instance

Address

spi_pulsar_adc_axi_regmap

0x44A0_0000

axi_pulsar_adc_dma

0x44A3_0000

spi_clkgen

0x44A7_0000

pulsar_adc_trigger_gen

0x44B0_0000

I2C connections

ZedBoard

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

iic_fmc

axi_iic_fmc

0x4162_0000

—

PL

iic_main

axi_iic_main

0x4160_0000

—

CoraZ7S

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

iic_ard

axi_ard_fmc

0x4160_0000

—

Note

Only for AD40xx/ADAQ40xx

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PL

axi_spi_engine

PulSAR_ADC

0

GPIOs

The Software GPIO number is calculated as follows:

  • Zynq-7000: if PS7 is used, then offset is 54

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

pulsar_gpio[0] (PD)*

INOUT

32

86

pulsar_gpio[1] (TURBO)**

INOUT

33

87

pulsar_gpio[2] (SDO - SPI_OP_MODE=2)**

INOUT

34

88

Legend

  • * instantiated only for PulSAR_ADC_PMDZ projects

  • ** instantiated only for FMC_N_PMOD=1 (AD40xx)

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Zynq

Actual Zynq

axi_pulsar_adc_dma

13

57

89

spi_pulsar_adc

12

56

88

iic_fmc/ard

11

55

87

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:.

Linux/Cygwin/WSL

~$
cd hdl/projects/pulsar_adc/zed
~/hdl/projects/pulsar_adc/zed$
make FMC_N_PMOD=1 SPI_OP_MODE=0

Build examples:

Zedboard PMOD support

~$
cd hdl/projects/pulsar_adc/zed
~/hdl/projects/pulsar_adc/zed$
make FMC_N_PMOD=0

Zedboard standard configuration FMC support (default)

~$
cd hdl/projects/pulsar_adc/zed
~/hdl/projects/pulsar_adc/zed$
make FMC_N_PMOD=1 SPI_OP_MODE=0 - builds standard FMC version

Zedboard FMC support for AD7944 4-wire mode (“multi”)

~$
cd hdl/projects/pulsar_adc/zed
~/hdl/projects/pulsar_adc/zed$
make FMC_N_PMOD=1 SPI_OP_MODE=1

Zedboard FMC support for AD7944 chain mode or 3-wire “single”

~$
cd hdl/projects/pulsar_adc/zed
~/hdl/projects/pulsar_adc/zed$
make FMC_N_PMOD=1 SPI_OP_MODE=2

The result of the build, if parameters were used, will be in a folder named by the used configuration. If the following command was run

~$
cd hdl/projects/pulsar_adc/zed
~/hdl/projects/pulsar_adc/zed$
make FMC_N_PMOD=1 SPI_OP_MODE=0

then the folder name will be:

FMC_N_PMOD1_SPI_OP_MODE0

Note

For the CoraZ7S-based projects, the build is done without parameters!

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.