AXI AD9361
The AXI AD9361 IP core can be used to interface the AD9361 device. This documentation only covers the IP core and requires that one must be familiar with the device for a complete and better understanding.
More about the generic framework interfacing ADCs can be read in Generic AXI ADC, and interfacing DACs in Generic AXI DAC.
Features
AXI Lite control/status interface
PRBS monitoring
Hardware and software DC filtering
IQ correction
Internal DDS
Programmable line delays
Receive and transmit loop back
Supports both Altera and AMD Xilinx devices
Files
Name |
Description |
|---|---|
Verilog source for the AXI AD9361. |
|
Verilog source for the ADC Common regmap. |
|
Verilog source for the ADC Channel regmap. |
|
Verilog source for the DAC Common regmap. |
|
Verilog source for the DAC Channel regmap. |
Block Diagram
Functional Description
The axi_ad9361 cores architecture contains:
Interface module in either CMOS Dual Port Full Duplex or LVDS mode for Intel or AMD Xilinx devices.
Receive module, which contains:
ADC channel processing modules, one for each channel
data processing modules ( DC Filter, IQ Correction and Data Format Control)
ADC PN Monitor for interface validation
Transmit module, which contains:
DAC channel processing modules, one for each channel
Different data generators (DDS, pattern, PRBS)
TDD control module for TDD mode, see more information on the HDL support for AD9361 TDD mode wiki page.
AXI control and status modules.
Device (AD9361) Interface Description
The IP supports both LVDS and CMOS Dual Port Full Duplex interfaces (configurable, see parameters section). It avoids all the programmable flavors of the device interface mess. The interface is in fact quite simple, in LVDS mode samples require two active clock edges and in CMOS mode a single edge. The samples are then delineated in-order using the FRAME signal. This is applicable to both DDR and SDR modes. There is a limitation though, the IP core does NOT support swapping of the data ports in CMOS mode. This option is left as a constraint. As an example the PZSDR projects uses SWAP on some boards based on the board layout.
Let’s consider the 2R2T configuration, each frame consists of 4 samples in each direction. In LVDS-DDR mode that is 8 clock edges (4 full clock cycles) identified by a frame pattern of 8’b11110000. The IP interface logic simply collects data on consecutive 8 edges and deframes using the FRAME signal and outputs the samples. The device does the same in the transmit direction. In CMOS mode, the same is done over 4 clock edges.
The interface also provides a single clock tree for the entire core. This clock uses a global buffer that has the minimum skew all across the die. On Altera devices, this is done via the PLL and because the LVDS cores do NOT support a serialization factor of 2, runs at half the interface clock frequency. On AMD Xilinx devices, this is done via the BUFG and the core and interface runs at the same clock frequency.
Altera
The core is tested to work only on Cyclone V Arrow SOC Kit. Since Altera does half-thought board designs that do not favor FMC bank allocations, we are incapable of validating the core on other devices.
AMD Xilinx
Alternative Clocking Methods
Using MMCM 2. Using BUFIO/BUFR
Alternative Use Models
1. Interface Logic Only 2. Disable DSP Functions 3. Removing AXI interface and Processor Control
Internal Interface Description
The main purpose of all (including this) ADI IP cores is to provide a common, well-defined internal interface within the FPGA. This interface consists of the following signals per channel.
ENABLE
The enable signal is strictly for software use and is controlled by the corresponding register bit. The core simply reflects the programmed bit as an output port. In ADI reference projects, this bit is used to activate the channel of interest. It is then used by the PACK/UNPACK cores to route the data based on total number of channels and the selected number of channels. As an example, AXI_AD9361 supports a total of 4 channels 16bits each. This corresponds to a packed channel data width of 64bits. If software enables only two channels the packed 64bits of data is exclusively shared by the enabled 2 channels (each channel gets 32 bits of data).
VALID
The valid signal is sourced by the core to indicate a valid sample on the DATA port. In the receive (ADC) direction this indicates a valid sample and in the transmit (DAC) direction this indicates the current sample is being read by the core. The valid is simply a ‘reflective’ of the ‘sampling rate’. Note that he cores always run at the interface clock. This is to avoid any customized clock handling or transfer within this core. However in many cases interface clock may not be the sampling clock. As an example for AD9361 the interface clock is 244Mhz for a sampling clock of 61MHz. That is each channel’s sampling rate is 61MHz. This translates into the VALID signal being asserted once every 4 clocks. In cores where sampling rate is same as the interface clock, VALID is always asserted and may be safely ignored.
A common interpretation of this is that all channels has the same VALID behavior. This is NOT necessarily true. A majority of use cases may have this as a result of data path equivalency. However, if software decides to enable/disable functions differently among channels, the VALID signals of those channels will NOT be the same.
DATA
The DATA is the raw Analog samples. It follows two simple rules.
The samples are always 16bits, regardless of the ADC/DAC data width. That is the source or destination is intended to handle samples as 16bits. In the transmit direction, if the DAC data width is less than 16bits, the most significant bits are used. In the receive direction, if the ADC data width is less than 16bits, the most significant bits are sign extended. This allows the same source or destination portable across different ADC/DAC data widths. In other words, if the source is generating a 16bits tone the signal appears the same across a 12bit, 14bit or 16bit DAC with only the corresponding amplitude change. The source can thus be independent of the number of bits supported by DAC. In the receive direction, the samples are sign extended. Thus the destination always receives a 16bit sample with different amplitude levels corresponding to the number of bits supported by the ADC. This may seem to break the symmetry rule, but in most DSP functions the samples are rounded up towards the MSB as only precision is allowed to lost or gained at the expense of the LSB bits. The MSB bits retains all the physical nature of the signal.
The DATA is received and transmitted with most significant sample “newest” regardless of the channel width. In other words the most significant sample is the “newest” sample. If the total channel width is 64bits, it carries 4 samples (16bits) per clock. If we were to name these samples as S3 (bits 63 down to 48), S2 (bits 47 down to 32), S1 (bits 31 down to 16) and S0 (bits 15 down to 0), the following is true. In the transmit direction, S0 is sent first and S3 is sent last to the DAC. The analog samples are S0, S1, S2 and S3 across time with S0 being the oldest and S3 being the newest sample. In the receive direction, S0 carries the oldest sample received and S3 carries the newest sample from the ADC.
Configuration Parameters
Name |
Description |
|---|---|
ID |
Core ID should be unique for each IP in the system |
FPGA_TECHNOLOGY |
Used to select between devices |
MODE_1R1T |
Used to select between 2RX2TX (0) and 1RX1TX (1) mode. |
TDD_DISABLE |
Setting this parameter the TDD control will not be implemented in the core. |
CMOS_OR_LVDS_N |
Defines the physical interface type, set 1 for CMOS and 0 for LVDS |
ADC_DATAPATH_DISABLE |
If set, the data path processing logic is not generated in the RX path, and the raw data is pushed directly to the DMA interface. |
ADC_USERPORTS_DISABLE |
Disable the User Control ports in receive path. |
ADC_DATAFORMAT_DISABLE |
Disable the Data Format control module. |
ADC_DCFILTER_DISABLE |
Disable the DC Filter module. |
ADC_IQCORRECTION_DISABLE |
Disable the IQ Correction module in receive path. |
DAC_DATAPATH_DISABLE |
If set, the data path processing logic is not generated in the TX path, and the raw data is pushed directly to the physical interface. |
DAC_IODELAY_ENABLE |
Set IO_DELAY control in transmit path. |
DAC_DDS_DISABLE |
Disable the DDS modules in transmit path. |
DAC_USERPORTS_DISABLE |
Disable the User Control ports in transmit path. |
DAC_IQCORRECTION_DISABLE |
Disable the IQ Correction module in transmit path. |
IO_DELAY_GROUP |
The delay group name which is set for the delay controller |
Interface
Name |
Description |
|---|---|
rx_clk_in_p |
LVDS input clock |
rx_clk_in_n |
LVDS input clock |
rx_frame_in_p |
LVDS input frame signal |
rx_frame_in_n |
LVDS input frame signal |
rx_data_in_p |
LVDS input data lines |
rx_data_in_n |
LVDS input data lines |
rx_clk_in |
CMOS input clock |
rx_frame_in |
CMOS input frame signal |
rx_data_in |
CMOS input data lines |
tx_clk_out_p |
LVDS output clock |
tx_clk_out_n |
LVDS output clock |
tx_frame_out_p |
LVDS output frame signal |
tx_frame_out_n |
LVDS output frame signal |
tx_data_out_p |
LVDS output data lines |
tx_data_out_n |
LVDS output data lines |
tx_clk_out |
CMOS output clock |
tx_frame_out |
CMOS output frame signal |
tx_data_out |
CMOS output data lines |
enable |
ENSM control signal, see User Guide for more information |
txnrx |
ENSM control signal, see User Guide for more information |
tdd_sync |
SYNC input for frame synchronization in TDD mode |
tdd_sync_cntr |
SYNC output for frame synchronization in TDD mode |
delay_clk |
Delay clock input for IO_DELAY control, 200 MHz (7 series) or 300 MHz (Ultrascale) |
dac_sync_in |
Synchronization signal of the transmit path for slave devices (ID>0) |
dac_sync_out |
Synchronization signal of the transmit path for master device (ID==0) |
l_clk |
This clock should be used for further data processing |
clk |
Must be driven by |
rst |
Core reset signal |
adc_enable_q* |
If set, the channel is enabled (one for each channel) |
adc_enable_i* |
If set, the channel is enabled (one for each channel) |
adc_valid_q* |
Indicates valid data at the current channel (one for each channel) |
adc_valid_i* |
Indicates valid data at the current channel (one for each channel) |
adc_data_q* |
Received data output (one for each channel) |
adc_data_i* |
Received data output (one for each channel) |
adc_dovf |
Data overflow, must be connected to the DMA |
adc_r1_mode |
If set, core is functioning in single channel mode (one I/Q pair) |
dac_enable_q* |
If set, the channel is enabled (one for each channel) |
dac_enable_i* |
If set, the channel is enabled (one for each channel) |
dac_valid_q* |
Indicates valid data request at the current channel (one for each channel) |
dac_valid_i* |
Indicates valid data request at the current channel (one for each channel) |
dac_data_q* |
Transmitted data output (one for each channel) |
dac_data_i* |
Transmitted data output (one for each channel) |
dac_dunf |
Data underflow, must be connected to the DMA |
dac_r1_mode |
If set, core is functioning in single channel mode (one I/Q pair) |
up_enable |
GPI control of the ENABLE line in TDD mode, when HDL TDD control is DISABLED |
up_txnrx |
GPI control of the TXNRX line in TDD mode, when HDL TDD control is DISABLED |
up_dac_gpio_in |
GPI ports connected to the AXI memory map for custom use |
up_dac_gpio_out |
GPI ports connected to the AXI memory map for custom use |
up_adc_gpio_in |
GPI ports connected to the AXI memory map for custom use |
up_adc_gpio_out |
GPO ports connected to the AXI memory map for custom use |
s_axi |
Standard AXI Slave Memory Map interface |
Register Map
The register map of the core contains instances of several generic register maps like ADC common, ADC channel, DAC common, DAC channel etc. The following table presents the base addresses of each instance, after that can be found the detailed description of each generic register map.
The absolute address of a register should be calculated by adding the instance base address to the registers relative address. For a more detailed explanation, see ADC register access and DAC register access.
HDL reg |
Software reg |
Name |
Description |
|---|---|---|---|
0x0000 |
0x0000 |
BASE |
See the Base table for more details. |
0x0000 |
0x0000 |
RX COMMON |
See the ADC Common table for more details. |
0x0000 |
0x0000 |
RX CHANNELS |
See the ADC Channel table for more details. |
0x1000 |
0x4000 |
TX COMMON |
See the DAC Common table for more details. |
0x1000 |
0x4000 |
TX CHANNELS |
See the DAC Channel table for more details. |
0x2000 |
0x8000 |
TDD CONTROL |
See the Transceiver TDD Control table for more details. |
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x0 |
0x0 |
VERSION |
Version and Scratch Registers |
|||
[31:0] |
VERSION |
RO |
0x00000000 |
Version number. Unique to all cores. |
||
0x1 |
0x4 |
ID |
Version and Scratch Registers |
|||
[31:0] |
ID |
RO |
0x00000000 |
Instance identifier number. |
||
0x2 |
0x8 |
SCRATCH |
Version and Scratch Registers |
|||
[31:0] |
SCRATCH |
RW |
0x00000000 |
Scratch register. |
||
0x3 |
0xc |
CONFIG |
Version and Scratch Registers |
|||
[0] |
IQCORRECTION_DISABLE |
RO |
0x0 |
If set, indicates that the IQ Correction module was not implemented. (as a result of a configuration of the IP instance) |
||
[1] |
DCFILTER_DISABLE |
RO |
0x0 |
If set, indicates that the DC Filter module was not implemented. (as a result of a configuration of the IP instance) |
||
[2] |
DATAFORMAT_DISABLE |
RO |
0x0 |
If set, indicates that the Data Format module was not implemented. (as a result of a configuration of the IP instance) |
||
[3] |
USERPORTS_DISABLE |
RO |
0x0 |
If set, indicates that the logic related to the User Data Format (e.g. decimation) was not implemented. (as a result of a configuration of the IP instance) |
||
[4] |
MODE_1R1T |
RO |
0x0 |
If set, indicates that the core was implemented in 1 channel mode. (e.g. refer to AD9361 data sheet) |
||
[5] |
DELAY_CONTROL_DISABLE |
RO |
0x0 |
If set, indicates that the delay control is disabled for this IP. (as a result of a configuration of the IP instance) |
||
[6] |
DDS_DISABLE |
RO |
0x0 |
If set, indicates that the DDS is disabled for this IP. (as a result of a configuration of the IP instance) |
||
[7] |
CMOS_OR_LVDS_N |
RO |
0x0 |
CMOS or LVDS mode is used for the interface. (as a result of a configuration of the IP instance) |
||
[8] |
PPS_RECEIVER_ENABLE |
RO |
0x0 |
If set, indicates the PPS receiver is enabled. (as a result of a configuration of the IP instance) |
||
[9] |
SCALECORRECTION_ONLY |
RO |
0x0 |
If set, indicates that the IQ Correction module implements only scale correction. IQ correction must be enabled. (as a result of a configuration of the IP instance) |
||
[12] |
EXT_SYNC |
RO |
0x0 |
If set the transport layer cores (ADC/DAC) have implemented the support for external synchronization signal. |
||
[13] |
RD_RAW_DATA |
RO |
0x0 |
If set, the ADC has the capability to read raw data in register CHAN_RAW_DATA from adc_channel. |
||
0x4 |
0x10 |
PPS_IRQ_MASK |
PPS Interrupt mask |
|||
[0] |
PPS_IRQ_MASK |
RW |
0x1 |
Mask bit for the 1PPS receiver interrupt |
||
0x7 |
0x1c |
FPGA_INFO |
FPGA device information library/scripts/adi_intel_device_info_enc.tcl (Intel encoded values) library/scripts/adi_xilinx_device_info_enc.tcl (Xilinx encoded values) |
|||
[31:24] |
FPGA_TECHNOLOGY |
RO |
0x00 |
Encoded value describing the technology/generation of the FPGA device (arria 10/7series) |
||
[23:16] |
FPGA_FAMILY |
RO |
0x00 |
Encoded value describing the family variant of the FPGA device(e.g., SX, GX, GT or zynq, kintex, virtex) |
||
[15:8] |
SPEED_GRADE |
RO |
0x00 |
Encoded value describing the FPGA’s speed-grade |
||
[7:0] |
DEV_PACKAGE |
RO |
0x00 |
Encoded value describing the device package. The package might affect high-speed interfaces |
||
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x10 |
0x40 |
RSTN |
ADC Interface Control & Status |
|||
[2] |
CE_N |
RW |
0x0 |
Clock enable, default is enabled(0x0). An inverse version of the signal is exported out of the module to control clock enables |
||
[1] |
MMCM_RSTN |
RW |
0x0 |
MMCM reset only (required for DRP access). Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. |
||
[0] |
RSTN |
RW |
0x0 |
Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. |
||
0x11 |
0x44 |
CNTRL |
ADC Interface Control & Status |
|||
[16] |
SDR_DDR_N |
RW |
0x0 |
Interface type (1 represents SDR, 0 represents DDR) |
||
[15] |
SYMB_OP |
RW |
0x0 |
Select symbol data format mode (0x1) |
||
[14] |
SYMB_8_16B |
RW |
0x0 |
Select number of bits for symbol format mode (1 represents 8b, 0 represents 16b) |
||
[12:8] |
NUM_LANES |
RW |
0x00 |
Number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane). For AD7768, AD7768-4 and AD777x number of active lanes : 1/2/4/8 where supported. |
||
[3] |
SYNC |
RW |
0x0 |
Initialize synchronization between multiple ADCs |
||
[2] |
R1_MODE |
RW |
0x0 |
Select number of RF channels 1 (0x1) or 2 (0x0). |
||
[1] |
DDR_EDGESEL |
RW |
0x0 |
Select rising edge (0x0) or falling edge (0x1) for the first part of a sample (if applicable) followed by the successive edges for the remaining parts. This only controls how the sample is delineated from the incoming data post DDR registers. |
||
[0] |
PIN_MODE |
RW |
0x0 |
Select interface pin mode to be clock multiplexed (0x1) or pin multiplexed (0x0). In clock multiplexed mode, samples are received on alternative clock edges. In pin multiplexed mode, samples are interleaved or grouped on the pins at the same clock edge. |
||
0x12 |
0x48 |
CNTRL_2 |
ADC Interface Control & Status |
|||
[1] |
EXT_SYNC_ARM |
RW |
0x0 |
Setting this bit will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a ADC, and across multiple instances. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
||
[2] |
EXT_SYNC_DISARM |
RW |
0x0 |
Setting this bit will disarm the trigger mechanism sensitive to an external sync signal. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
||
[8] |
MANUAL_SYNC_REQUEST |
RW |
0x0 |
Setting this bit will issue an external sync event if it is hooked up inside the fabric. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
||
0x13 |
0x4c |
CNTRL_3 |
ADC Interface Control & Status |
|||
[8] |
CRC_EN |
RW |
0x0 |
Setting this bit will enable the CRC generation. |
||
[7:0] |
CUSTOM_CONTROL |
RW |
0x00 |
Select output format decode mode.(for ADAQ8092: bit 0 - enables digital output randomizer decode , bit 1 - enables alternate bit polarity decode). |
||
0x15 |
0x54 |
CLK_FREQ |
ADC Interface Control & Status |
|||
[31:0] |
CLK_FREQ |
RO |
0x00000000 |
Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock. |
||
0x16 |
0x58 |
CLK_RATIO |
ADC Interface Control & Status |
|||
[31:0] |
CLK_RATIO |
RO |
0x00000000 |
Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr). |
||
0x17 |
0x5c |
STATUS |
ADC Interface Control & Status |
|||
[4] |
ADC_CTRL_STATUS |
RO |
0x0 |
If set, indicates that the device’s register data is available on the data bus. |
||
[3] |
PN_ERR |
RO |
0x0 |
If set, indicates pn error in one or more channels. |
||
[2] |
PN_OOS |
RO |
0x0 |
If set, indicates pn oos in one or more channels. |
||
[1] |
OVER_RANGE |
RO |
0x0 |
If set, indicates over range in one or more channels. |
||
[0] |
STATUS |
RO |
0x0 |
Interface status, if set indicates no errors. If not set, there are errors, software may try resetting the cores. |
||
0x18 |
0x60 |
DELAY_CNTRL |
ADC Interface Control & Status( |
|||
[17] |
DELAY_SEL |
RW |
0x0 |
Delay select, a 0x0 to 0x1 transition in this register initiates a delay access controlled by the registers below. |
||
[16] |
DELAY_RWN |
RW |
0x0 |
Delay read (0x1) or write (0x0), the delay is accessed directly (no increment or decrement) with an address corresponding to each pin, and data corresponding to the total delay. |
||
[15:8] |
DELAY_ADDRESS |
RW |
0x00 |
Delay address, the range depends on the interface pins, data pins are usually at the lower range. |
||
[4:0] |
DELAY_WDATA |
RW |
0x00 |
Delay write data, a value of 1 corresponds to (1/200)ns for most devices. |
||
0x19 |
0x64 |
DELAY_STATUS |
ADC Interface Control & Status( |
|||
[9] |
DELAY_LOCKED |
RO |
0x0 |
Indicates delay locked (0x1) state. If this bit is read 0x0, delay control has failed to calibrate the elements. |
||
[8] |
DELAY_STATUS |
RO |
0x0 |
If set, indicates busy status (access pending). The read data may not be valid if this bit is set. |
||
[4:0] |
DELAY_RDATA |
RO |
0x00 |
Delay read data, current delay value in the elements |
||
0x1a |
0x68 |
SYNC_STATUS |
ADC Synchronization Status register |
|||
[0] |
ADC_SYNC |
RO |
0x0 |
ADC synchronization status. Will be set to 1 after the synchronization has been completed or while waiting for the synchronization signal in JESD204 systems. |
||
0x1c |
0x70 |
DRP_CNTRL |
ADC Interface Control & Status |
|||
[28] |
DRP_RWN |
RW |
0x0 |
DRP read (0x1) or write (0x0) select (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
[27:16] |
DRP_ADDRESS |
RW |
0x000 |
DRP address, designs that contain more than one DRP accessible primitives have selects based on the most significant bits (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
[15:0] |
RESERVED |
RO |
0x0000 |
Reserved for backward compatibility. |
||
0x1d |
0x74 |
DRP_STATUS |
ADC Interface Control & Status |
|||
[17] |
DRP_LOCKED |
RO |
0x0 |
If set indicates that the DRP has been locked. |
||
[16] |
DRP_STATUS |
RO |
0x0 |
If set indicates busy (access pending). The read data may not be valid if this bit is set (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
[15:0] |
RESERVED |
RO |
0x0000 |
Reserved for backward compatibility. |
||
0x1e |
0x78 |
DRP_WDATA |
ADC DRP Write Data |
|||
[15:0] |
DRP_WDATA |
RW |
0x0000 |
DRP write data (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
0x1f |
0x7c |
DRP_RDATA |
ADC DRP Read Data |
|||
[15:0] |
DRP_RDATA |
RO |
0x0000 |
DRP read data (does not include GTX lanes). |
||
0x20 |
0x80 |
ADC_CONFIG_WR |
ADC Write Configuration Data |
|||
[31:0] |
ADC_CONFIG_WR |
RW |
0x00000000 |
Custom Write to the available registers. |
||
0x21 |
0x84 |
ADC_CONFIG_RD |
ADC Read Configuration Data |
|||
[31:0] |
ADC_CONFIG_RD |
RO |
0x00000000 |
Custom read of the available registers. |
||
0x22 |
0x88 |
UI_STATUS |
User Interface Status |
|||
[2] |
UI_OVF |
RW1C |
0x0 |
User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
||
[1] |
UI_UNF |
RW1C |
0x0 |
User Interface underflow. If set, indicates an underflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
||
[0] |
UI_RESERVED |
RW1C |
0x0 |
Reserved for backward compatibility. |
||
0x23 |
0x8c |
ADC_CONFIG_CTRL |
ADC RD/WR configuration |
|||
[31:0] |
ADC_CONFIG_CTRL |
RW |
0x00000000 |
Control RD/WR requests to the device’s register map: bit 1 - RD (‘b1) , WR (‘b0), bit 0 - enable WR/RD operation. |
||
0x28 |
0xa0 |
USR_CNTRL_1 |
ADC Interface Control & Status |
|||
[7:0] |
USR_CHANMAX |
RW |
0x00 |
This indicates the maximum number of inputs for the channel data multiplexers. User may add different processing modules post data capture as another input to this common multiplexer. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
0x29 |
0xa4 |
ADC_START_CODE |
ADC Synchronization start word |
|||
[31:0] |
ADC_START_CODE |
RW |
0x00000000 |
This sets the startcode that is used by the ADCs for synchronization NOT-APPLICABLE if START_CODE_DISABLE is set (0x1). |
||
0x2e |
0xb8 |
ADC_GPIO_IN |
ADC GPIO inputs |
|||
[31:0] |
ADC_GPIO_IN |
RO |
0x00000000 |
This reads auxiliary GPI pins of the ADC core |
||
0x2f |
0xbc |
ADC_GPIO_OUT |
ADC GPIO outputs |
|||
[31:0] |
ADC_GPIO_OUT |
RW |
0x00000000 |
This controls auxiliary GPO pins of the ADC core NOT-APPLICABLE if GPIO_DISABLE is set (0x1). |
||
0x30 |
0xc0 |
PPS_COUNTER |
PPS Counter register |
|||
[31:0] |
PPS_COUNTER |
RO |
0x00000000 |
Counts the core clock cycles (can be a device clock or interface clock) between two 1PPS pulse. |
||
0x31 |
0xc4 |
PPS_STATUS |
PPS Status register |
|||
[0] |
PPS_STATUS |
RO |
0x0 |
If this bit is asserted there is no incomming 1PPS signal. Maybe the source is out of sync or it’s not active. |
||
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x100 + 0x10*n |
0x400 + 0x40*n |
CHAN_CNTRLn |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[11] |
ADC_LB_OWR |
RW |
0x0 |
If set, forces ADC_DATA_SEL to 1, enabling data loopback |
||
[10] |
ADC_PN_SEL_OWR |
RW |
0x0 |
If set, forces ADC_PN_SEL to 0x9, device specific pn (e.g. ad9361) If both ADC_PN_TYPE_OWR and ADC_PN_SEL_OWR are set, they are ignored |
||
[9] |
IQCOR_ENB |
RW |
0x0 |
if set, enables IQ correction or scale correction. NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1). |
||
[8] |
DCFILT_ENB |
RW |
0x0 |
if set, enables DC filter (to disable DC offset, set offset value to 0x0). NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1). |
||
[6] |
FORMAT_SIGNEXT |
RW |
0x0 |
if set, enables sign extension (applicable only in 2’s complement mode). The data is always sign extended to the nearest byte boundary. NOT-APPLICABLE if DATAFORMAT_DISABLE is set (0x1). |
||
[5] |
FORMAT_TYPE |
RW |
0x0 |
Select offset binary (0x1) or 2’s complement (0x0) data type. This sets the incoming data type and is required by the post processing modules for any data conversion. NOT-APPLICABLE if DATAFORMAT_DISABLE is set (0x1). |
||
[4] |
FORMAT_ENABLE |
RW |
0x0 |
Enable data format conversion (see register bits above). NOT-APPLICABLE if DATAFORMAT_DISABLE is set (0x1). |
||
[3] |
RESERVED |
RO |
0x0 |
Reserved for backward compatibility. |
||
[2] |
RESERVED |
RO |
0x0 |
Reserved for backward compatibility. |
||
[1] |
ADC_PN_TYPE_OWR |
RW |
0x0 |
If set, forces ADC_PN_SEL to 0x1, modified pn23 If both ADC_PN_TYPE_OWR and ADC_PN_SEL_OWR are set, they are ignored |
||
[0] |
ENABLE |
RW |
0x0 |
If set, enables channel. A 0x0 to 0x1 transition transfers all the control signals to the respective channel processing module. If a channel is part of a complex signal (I/Q), even channel is the master and the odd channel is the slave. Though a single control is used, both must be individually selected. |
||
0x101 + 0x10*n |
0x404 + 0x40*n |
CHAN_STATUSn |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[12] |
CRC_ERR |
RW1C |
0x0 |
CRC errors. If set, indicates CRC error. Software must first clear this bit before initiating a transfer and monitor afterwards. |
||
[11:4] |
STATUS_HEADER |
RO |
0x00 |
The status header sent by the ADC.(compatible with AD7768/AD7768-4/AD777x). |
||
[2] |
PN_ERR |
RW1C |
0x0 |
PN errors. If set, indicates spurious mismatches in sync state. This bit is cleared if OOS is set and is only indicates errors when OOS is cleared. |
||
[1] |
PN_OOS |
RW1C |
0x0 |
PN Out Of Sync. If set, indicates an OOS status. OOS is set, if 64 consecutive patterns mismatch from the expected pattern. It is cleared, when 16 consecutive patterns match the expected pattern. |
||
[0] |
OVER_RANGE |
RW1C |
0x0 |
If set, indicates over range. Note that over range is independent of the data path, it indicates an over range over a data transfer period. Software must first clear this bit before initiating a transfer and monitor afterwards. |
||
0x102 + 0x10*n |
0x408 + 0x40*n |
CHAN_RAW_DATAn |
ADC Raw Data Reading Where n is from 0 to 15. |
|||
[31:0] |
ADC_READ_DATA |
RO |
0x00000000 |
Raw data read from the ADC. |
||
0x104 + 0x10*n |
0x410 + 0x40*n |
CHAN_CNTRLn_1 |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[31:16] |
DCFILT_OFFSET |
RW |
0x0000 |
DC removal (if equipped) offset. This is a 2’s complement number added to the incoming data to remove a known DC offset. NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1). |
||
[15:0] |
DCFILT_COEFF |
RW |
0x0000 |
DC removal filter (if equipped) coefficient. The format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1). |
||
0x105 + 0x10*n |
0x414 + 0x40*n |
CHAN_CNTRLn_2 |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[31:16] |
IQCOR_COEFF_1 |
RW |
0x0000 |
IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the scale value and the format is 1.1.14 (sign, integer and fractional bits). If matrix multiplication is used, this is the channel I coefficient and the format is 1.1.14 (sign, integer and fractional bits). If SCALECORRECTION_ONLY is set, this implements the scale value correction for the current channel with the format 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1). |
||
[15:0] |
IQCOR_COEFF_2 |
RW |
0x0000 |
IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the offset value and the format is 2’s complement. If matrix multiplication is used, this is the channel Q coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1). |
||
0x106 + 0x10*n |
0x418 + 0x40*n |
CHAN_CNTRLn_3 |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[19:16] |
ADC_PN_SEL |
RW |
0x0 |
Selects the PN monitor sequence type (available only if ADC supports it).
|
||
[3:0] |
ADC_DATA_SEL |
RW |
0x0 |
Selects the data source to DMA. 0x0: input data (ADC) 0x1: loopback data (DAC) |
||
0x108 + 0x10*n |
0x420 + 0x40*n |
CHAN_USR_CNTRLn_1 |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[25] |
USR_DATATYPE_BE |
RO |
0x0 |
The user data type format- if set, indicates big endian (default is little endian). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[24] |
USR_DATATYPE_SIGNED |
RO |
0x0 |
The user data type format- if set, indicates signed (2’s complement) data (default is unsigned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[23:16] |
USR_DATATYPE_SHIFT |
RO |
0x00 |
The user data type format- the amount of right shift for actual samples within the total number of bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[15:8] |
USR_DATATYPE_TOTAL_BITS |
RO |
0x00 |
The user data type format- number of total bits used for a sample. The total number of bits must be an integer multiple of 8 (byte aligned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[7:0] |
USR_DATATYPE_BITS |
RO |
0x00 |
The user data type format- number of bits in a sample. This indicates the actual sample data bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
0x109 + 0x10*n |
0x424 + 0x40*n |
CHAN_USR_CNTRLn_2 |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[31:16] |
USR_DECIMATION_M |
RW |
0x0000 |
This holds the user decimation M value of the channel that is currently being selected on the multiplexer above. The total decimation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[15:0] |
USR_DECIMATION_N |
RW |
0x0000 |
This holds the user decimation N value of the channel that is currently being selected on the multiplexer above. The total decimation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
0x10a + 0x10*n |
0x428 + 0x40*n |
CHAN_CNTRLn_4 |
ADC Interface Control & Status Where n is from 0 to 15. |
|||
[31:3] |
RESERVED |
RO |
0x00000000 |
Reserved for backward compatibility. |
||
[2:0] |
SOFTSPAN |
RW |
0x7 |
Softspan configuration register. |
||
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x10 |
0x40 |
RSTN |
DAC Interface Control & Status |
|||
[2] |
CE_N |
RW |
0x0 |
Clock enable, default is enabled(0x0). An inverse version of the signal is exported out of the module to control clock enables |
||
[1] |
MMCM_RSTN |
RW |
0x0 |
MMCM reset only (required for DRP access). Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. |
||
[0] |
RSTN |
RW |
0x0 |
Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core. |
||
0x11 |
0x44 |
CNTRL_1 |
DAC Interface Control & Status |
|||
[0] |
SYNC |
RW |
0x0 |
Setting this bit synchronizes channels within a DAC, and across multiple instances. This bit self clears. |
||
[1] |
EXT_SYNC_ARM |
RW |
0x0 |
Setting this bit will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a DAC, and across multiple instances. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
||
[2] |
EXT_SYNC_DISARM |
RW |
0x0 |
Setting this bit will disarm the trigger mechanism sensitive to an external sync signal. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
||
[8] |
MANUAL_SYNC_REQUEST |
RW |
0x0 |
Setting this bit will issue an external sync event if it is hooked up inside the fabric. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears. |
||
0x12 |
0x48 |
CNTRL_2 |
DAC Interface Control & Status |
|||
[16] |
SDR_DDR_N |
RW |
0x0 |
Interface type (1 represents SDR, 0 represents DDR) |
||
[15] |
SYMB_OP |
RW |
0x0 |
Select data symbol format mode (0x1) |
||
[14] |
SYMB_8_16B |
RW |
0x0 |
Select number of bits for symbol format mode (1 represents 8b, 0 represents 16b) |
||
[12:8] |
NUM_LANES |
RW |
0x00 |
Number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane) |
||
[7] |
PAR_TYPE |
RW |
0x0 |
Select parity even (0x0) or odd (0x1). |
||
[6] |
PAR_ENB |
RW |
0x0 |
Select parity (0x1) or frame (0x0) mode. |
||
[5] |
R1_MODE |
RW |
0x0 |
Select number of RF channels 1 (0x1) or 2 (0x0). |
||
[4] |
DATA_FORMAT |
RW |
0x0 |
Select data format 2’s complement (0x0) or offset binary (0x1). NOT-APPLICABLE if DAC_DP_DISABLE is set (0x1). |
||
[3:0] |
RESERVED |
NA |
0x0 |
Reserved |
||
0x13 |
0x4c |
RATECNTRL |
DAC Interface Control & Status |
|||
[7:0] |
RATE |
RW |
0x00 |
The effective dac rate (the maximum possible rate is dependent on the interface clock). The samples are generated at 1/RATE of the interface clock. |
||
0x14 |
0x50 |
FRAME |
DAC Interface Control & Status |
|||
[0] |
FRAME |
RW |
0x0 |
The use of frame is device specific. Usually setting this bit to 1 generates a FRAME (1 DCI clock period) pulse on the interface. This bit self clears. |
||
0x15 |
0x54 |
STATUS1 |
DAC Interface Control & Status |
|||
[31:0] |
CLK_FREQ |
RO |
0x00000000 |
Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock. |
||
0x16 |
0x58 |
STATUS2 |
DAC Interface Control & Status |
|||
[31:0] |
CLK_RATIO |
RO |
0x00000000 |
Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr). |
||
0x17 |
0x5c |
STATUS3 |
DAC Interface Control & Status |
|||
[0] |
STATUS |
RO |
0x0 |
Interface status, if set indicates no errors. If not set, there are errors, software may try resetting the cores. |
||
0x18 |
0x60 |
DAC_CLKSEL |
DAC Interface Control & Status |
|||
[0] |
DAC_CLKSEL |
RW |
0x0 |
Allows changing of the clock polarity. Note: its default value is CLK_EDGE_SEL |
||
0x1a |
0x68 |
SYNC_STATUS |
DAC Synchronization Status register |
|||
[0] |
DAC_SYNC_STATUS |
RO |
0x0 |
DAC synchronization status. Will be set to 1 while waiting for the external synchronization signal This bit has an effect only the EXT_SYNC synthesis parameter is set. |
||
0x1c |
0x70 |
DRP_CNTRL |
DRP Control & Status |
|||
[28] |
DRP_RWN |
RW |
0x0 |
DRP read (0x1) or write (0x0) select (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
[27:16] |
DRP_ADDRESS |
RW |
0x000 |
DRP address, designs that contain more than one DRP accessible primitives have selects based on the most significant bits (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
[15:0] |
RESERVED |
RO |
0x0000 |
Reserved for backwards compatibility |
||
0x1d |
0x74 |
DRP_STATUS |
DAC Interface Control & Status |
|||
[17] |
DRP_LOCKED |
RO |
0x0 |
If set indicates the MMCM/PLL is locked |
||
[16] |
DRP_STATUS |
RO |
0x0 |
If set indicates busy (access pending). The read data may not be valid if this bit is set (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
[15:0] |
RESERVED |
RO |
0x0000 |
Reserved for backwards compatibility |
||
0x1e |
0x78 |
DRP_WDATA |
DAC Interface Control & Status |
|||
[15:0] |
DRP_WDATA |
RW |
0x0000 |
DRP write data (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
0x1f |
0x7c |
DRP_RDATA |
DAC Interface Control & Status |
|||
[15:0] |
DRP_RDATA |
RO |
0x0000 |
DRP read data (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1). |
||
0x20 |
0x80 |
DAC_CUSTOM_RD |
DAC Read Configuration Data |
|||
[31:0] |
DAC_CUSTOM_RD |
RO |
0x00000000 |
Custom Read of the available registers. |
||
0x21 |
0x84 |
DAC_CUSTOM_WR |
DAC Write Configuration Data |
|||
[31:0] |
DAC_CUSTOM_WR |
RW |
0x00000000 |
Custom Write of the available registers. |
||
0x22 |
0x88 |
UI_STATUS |
User Interface Status |
|||
[4] |
IF_BUSY |
RO |
0x0 |
Interface busy. If set, indicates that the data interface is busy. |
||
[1] |
UI_OVF |
RW1C |
0x0 |
User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
||
[0] |
UI_UNF |
RW1C |
0x0 |
User Interface underflow. If set, indicates an underflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit. |
||
0x23 |
0x8c |
DAC_CUSTOM_CTRL |
DAC Control Configuration Data |
|||
[31:0] |
DAC_CUSTOM_CTRL |
RW |
0x00000000 |
Custom Control of the available registers. |
||
0x28 |
0xa0 |
USR_CNTRL_1 |
DAC User Control & Status |
|||
[7:0] |
USR_CHANMAX |
RW |
0x00 |
This indicates the maximum number of inputs for the channel data multiplexers. User may add different processing modules as inputs to the dac. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
0x2e |
0xb8 |
DAC_GPIO_IN |
DAC GPIO inputs |
|||
[31:0] |
DAC_GPIO_IN |
RO |
0x00000000 |
This reads auxiliary GPI pins of the DAC core |
||
0x2f |
0xbc |
DAC_GPIO_OUT |
DAC GPIO outputs |
|||
[31:0] |
DAC_GPIO_OUT |
RW |
0x00000000 |
This controls auxiliary GPO pins of the DAC core NOT-APPLICABLE if GPIO_DISABLE is set (0x1). |
||
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x100 + 0x10*n |
0x400 + 0x40*n |
CHAN_CNTRLn_1 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[21:16] |
DDS_PHASE_DW |
RO |
0x00 |
The DDS phase data width offers the HDL parameter configuration with the same name. This information is used in conjunction with CHAN_CNTRL_9 and CHAN_CNTRL_10. More info at AD Direct Digital Synthesis. |
||
[15:0] |
DDS_SCALE_1 |
RW |
0x0000 |
The DDS scale for tone 1. Sets the amplitude of the tone. The format is 1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on 16-bits, note that if you do use both channels and set both scale to 0x4000, it is over-range. The final output is (tone_1_fullscale * scale_1) + (tone_2_fullscale * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
0x101 + 0x10*n |
0x404 + 0x40*n |
CHAN_CNTRLn_2 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[31:16] |
DDS_INIT_1 |
RW |
0x0000 |
The DDS phase initialization for tone 1. Sets the initial phase offset of the tone. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
[15:0] |
DDS_INCR_1 |
RW |
0x0000 |
Sets the frequency of the phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{16}) * clkratio / f_{if}\); where f_out is the generated output frequency, and f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase increment for tone 1 is extended in CHAN_CNTRL_9. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
0x102 + 0x10*n |
0x408 + 0x40*n |
CHAN_CNTRLn_3 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[15:0] |
DDS_SCALE_2 |
RW |
0x0000 |
The DDS scale for tone 2. Sets the amplitude of the tone. The format is 1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on 16-bits, note that if you do use both channels and set both scale to 0x4000, it is over-range. The final output is (tone_1_fullscale * scale_1) + (tone_2_fullscale * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
0x103 + 0x10*n |
0x40c + 0x40*n |
CHAN_CNTRLn_4 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[31:16] |
DDS_INIT_2 |
RW |
0x0000 |
The DDS phase initialization for tone 2. Sets the initial phase offset of the tone. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase init for tone 2 is extended in CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
[15:0] |
DDS_INCR_2 |
RW |
0x0000 |
Sets the frequency of the phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{16}) * clkratio / f_{if}\); where f_out is the generated output frequency, and f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase increment for tone 2 is extended in CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
0x104 + 0x10*n |
0x410 + 0x40*n |
CHAN_CNTRLn_5 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[31:16] |
DDS_PATT_2 |
RW |
0x0000 |
The DDS data pattern for this channel. |
||
[15:0] |
DDS_PATT_1 |
RW |
0x0000 |
The DDS data pattern for this channel. |
||
0x105 + 0x10*n |
0x414 + 0x40*n |
CHAN_CNTRLn_6 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[2] |
IQCOR_ENB |
RW |
0x0 |
if set, enables IQ correction. NOT-APPLICABLE if DAC_DP_DISABLE is set (0x1). |
||
[1] |
DAC_LB_OWR |
RW |
0x0 |
If set, forces DAC_DDS_SEL to 0x8, loopback If DAC_LB_OWR and DAC_PN_OWR are both set, they are ignored |
||
[0] |
DAC_PN_OWR |
RW |
0x0 |
IF set, forces DAC_DDS_SEL to 0x09, device specific pnX If DAC_LB_OWR and DAC_PN_OWR are both set, they are ignored |
||
0x106 + 0x10*n |
0x418 + 0x40*n |
CHAN_CNTRLn_7 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[3:0] |
DAC_DDS_SEL |
RW |
0x0 |
Select internal data sources (available only if the DAC supports it).
|
||
0x107 + 0x10*n |
0x41c + 0x40*n |
CHAN_CNTRLn_8 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[31:16] |
IQCOR_COEFF_1 |
RW |
0x0000 |
IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the scale value and the format is 1.1.14 (sign, integer and fractional bits). If matrix multiplication is used, this is the channel I coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1). |
||
[15:0] |
IQCOR_COEFF_2 |
RW |
0x0000 |
IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the offset value and the format is 2’s complement. If matrix multiplication is used, this is the channel Q coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1). |
||
0x108 + 0x10*n |
0x420 + 0x40*n |
USR_CNTRLn_3 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[25] |
USR_DATATYPE_BE |
RW |
0x0 |
The user data type format- if set, indicates big endian (default is little endian). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[24] |
USR_DATATYPE_SIGNED |
RW |
0x0 |
The user data type format- if set, indicates signed (2’s complement) data (default is unsigned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[23:16] |
USR_DATATYPE_SHIFT |
RW |
0x00 |
The user data type format- the amount of right shift for actual samples within the total number of bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[15:8] |
USR_DATATYPE_TOTAL_BITS |
RW |
0x00 |
The user data type format- number of total bits used for a sample. The total number of bits must be an integer multiple of 8 (byte aligned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[7:0] |
USR_DATATYPE_BITS |
RW |
0x00 |
The user data type format- number of bits in a sample. This indicates the actual sample data bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
0x109 + 0x10*n |
0x424 + 0x40*n |
USR_CNTRLn_4 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[31:16] |
USR_INTERPOLATION_M |
RW |
0x0000 |
This holds the user interpolation M value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
[15:0] |
USR_INTERPOLATION_N |
RW |
0x0000 |
This holds the user interpolation N value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1). |
||
0x10a + 0x10*n |
0x428 + 0x40*n |
USR_CNTRLn_5 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[0] |
DAC_IQ_MODE |
RW |
0x0 |
Enable complex mode. In this mode the driven data to the DAC must be a sequence of I and Q sample pairs. |
||
[1] |
DAC_IQ_SWAP |
RW |
0x0 |
Allows IQ swapping in complex mode. Only takes effect if complex mode is enabled. |
||
0x10b + 0x10*n |
0x42c + 0x40*n |
CHAN_CNTRLn_9 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[31:16] |
DDS_INIT_1_EXTENDED |
RW |
0x0000 |
The extended DDS phase initialization for tone 1. Sets the initial phase offset of the tone. The extended init(phase) value should be calculated according to DDS_PHASE_DW value from CHAN_CNTRL_1 NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
[15:0] |
DDS_INCR_1_EXTENDED |
RW |
0x0000 |
Sets the frequency of tone 1’s phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{phaseDW}) * clkratio / f_{if}\); Where f_out is the generated output frequency, DDS_PHASE_DW value can be found in CHAN_CNTRL_1 in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
0x10c + 0x10*n |
0x430 + 0x40*n |
CHAN_CNTRLn_10 |
DAC Channel Control & Status (channel - 0) Where n is from 0 to 15. |
|||
[31:16] |
DDS_INIT_2_EXTENDED |
RW |
0x0000 |
The extended DDS phase initialization for tone 2. Sets the initial phase offset of the tone. The extended init(phase) value should be calculated according to DDS_PHASE_DW value from CHAN_CNTRL_2 NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
[15:0] |
DDS_INCR_2_EXTENDED |
RW |
0x0000 |
Sets the frequency of tone 2’s phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{phaseDW}) * clkratio / f_{if}\); Where f_out is the generated output frequency, DDS_PHASE_DW value can be found in CHAN_CNTRL_2 in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1). |
||
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x10 |
0x40 |
TDD_CONTROL_0 |
TDD Control & Status |
|||
[5] |
TDD_GATED_TX_DMAPATH |
RW |
0x0 |
If this bit is set, the core requests data from the TX DMA, just when the data path is active. Otherwise will requests continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity. |
||
[4] |
TDD_GATED_RX_DMAPATH |
RW |
0x0 |
If this bit is set, the core provides data for the RX DMA, just when the data path is active. Otherwise will provides continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity. |
||
[3] |
TDD_TXONLY |
RW |
0x0 |
If this bit is set- the TDD controller ignores all the TX_* timing registers below and assumes continuous receive operation within a frame. |
||
[2] |
TDD_RXONLY |
RW |
0x0 |
If this bit is set- the TDD controller ignores all the RX_* timing registers below and assumes continuous transmit operation within a frame. |
||
[1] |
TDD_SECONDARY |
RW |
0x0 |
Enable the secondary transmit/receive on the active frame. If this bit is clear - the controller only uses the _1 timing registers below. If this bit is set - the controller uses the _1 and _2 timing registers below. |
||
[0] |
TDD_ENABLE |
RW |
0x0 |
If set, enables the TDD controller- software must set this bit after programming all the registers that controls the tdd timing. Any device settings needs to be done (for example bring the AD9361 to the alert state) prior to to setting this bit. The controller keeps the frame counters in reset if this bit is reset. A 0 to 1 transition in this bit starts the frame counter and tdd mode of operation. |
||
0x11 |
0x44 |
TDD_CONTROL_1 |
TDD Control & Status |
|||
[7:0] |
TDD_BURST_COUNT |
RW |
0x00 |
If set to 0x0 and enabled (TDD_ENABLE is set) - the controller operates in TDD mode as long as the TDD_ENABLE bit is set. If set to a non-zero value, the controller operates for the set number of frames and stops. |
||
0x12 |
0x48 |
TDD_CONTROL_2 |
TDD Control & Status |
|||
[23:0] |
TDD_COUNTER_INIT |
RW |
0x000000 |
The controller sets the frame counter to this value when starting TDD operation. This is the starting offset value for the TDD frame counter. |
||
0x13 |
0x4c |
TDD_FRAME_LENGTH |
TDD Control & Status |
|||
[23:0] |
TDD_FRAME_LENGTH |
RW |
0x000000 |
The frame length is the terminal count for the 10ms counter running at the digital interface clock- as an example for a 245.76MHz clock it is 0x258000. |
||
0x14 |
0x50 |
TDD_SYNC_TERMINAL_TYPE |
TDD Control & Status |
|||
[0] |
TDD_SYNC_TERMINAL_TYPE |
RW |
0x0 |
Set this bit, if the current terminal will generate the syncronization pulse, reset otherwise. |
||
0x18 |
0x60 |
TDD_STATUS |
TDD Control & Status |
|||
[0] |
TDD_RXTX_VCO_OVERLAP |
RO |
0x0 |
This bit is asserted, if exist a time interval when both the TX and RX VCOs are powered up. |
||
[1] |
TDD_RXTX_RF_OVERLAP |
RO |
0x0 |
This bit is asserted, if exist a time interval when both the TX and RX RF datapath are powered up. |
||
0x20 |
0x80 |
TDD_VCO_RX_ON_1 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_RX_ON_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the RX VCO powers up at the first time. The controller enables the receive VCO, when the frame count reaches this value. The VCO may have to be enabled before data can be received. The user needs to make sure, that the RF device is in a state, from where this operation is valid. |
||
0x21 |
0x84 |
TDD_VCO_RX_OFF_1 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_RX_OFF_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the RX VCO powers down at the first time. The controller disables the receive VCO, when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. |
||
0x22 |
0x88 |
TDD_VCO_TX_ON_1 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_TX_ON_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the TX VCO powers up at the first time. The controller enables the transmit VCO, when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. |
||
0x23 |
0x8c |
TDD_VCO_TX_OFF_1 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_TX_OFF_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the TX VCO powers down at the first time. The controller disables the transmit VCO when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. |
||
0x24 |
0x90 |
TDD_RX_ON_1 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_ON_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the RX data path is activated at the first time. The controller enables the receive chain when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. |
||
0x25 |
0x94 |
TDD_RX_OFF_1 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_OFF_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the RX data path is deactivated the first time. The controller disables the receive chain when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid. |
||
0x26 |
0x98 |
TDD_TX_ON_1 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_ON_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the TX data path is activated at the first time. The controller enables the transmit chain, when the frame count reaches this value. This register and the TX_DP_ON register controls the delay between the data path being activated and the time to actually push the transmit data through the transmit chain in the device. |
||
0x27 |
0x9c |
TDD_TX_OFF_1 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_OFF_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the TX data path is deactivated at the first time. The controller disables the transmit chain, when the frame count reaches this value. This register and the TX_DP_OFF register controls the delay between the data path being deactivated and the time to actually stop transmitting data through the transmit chain in the device. |
||
0x28 |
0xa0 |
TDD_RX_DP_ON_1 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_DP_ON_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the controller starts to accept data from the digital interface for receive. |
||
0x29 |
0xa4 |
TDD_RX_DP_OFF_1 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_DP_OFF_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the controller stops to accept data from the digital interface for receive. |
||
0x2a |
0xa8 |
TDD_TX_DP_ON_1 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_DP_ON_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the controller starts to request data from the system memory for transmit. The data rate is controlled by the TDD controller. |
||
0x2b |
0xac |
TDD_TX_DP_OFF_1 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_DP_OFF_1 |
RW |
0x000000 |
Defines the offset (from frame count equal zero), when the controller stop requesting data from the system memory for transmit. |
||
0x30 |
0xc0 |
TDD_VCO_RX_ON_2 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_RX_ON_2 |
RW |
0x000000 |
The secondary pointer for VCO_RX_ON. |
||
0x31 |
0xc4 |
TDD_VCO_RX_OFF_2 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_RX_OFF_2 |
RW |
0x000000 |
The secondary pointer for VCO_RX_OFF. |
||
0x32 |
0xc8 |
TDD_VCO_TX_ON_2 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_TX_ON_2 |
RW |
0x000000 |
The secondary pointer for VCO_TX_ON. |
||
0x33 |
0xcc |
TDD_VCO_TX_OFF_2 |
TDD Control & Status |
|||
[23:0] |
TDD_VCO_TX_OFF_2 |
RW |
0x000000 |
The secondary pointer for VCO_TX_OFF. |
||
0x34 |
0xd0 |
TDD_RX_ON_2 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_ON_2 |
RW |
0x000000 |
The secondary pointer for RX_ON. |
||
0x35 |
0xd4 |
TDD_RX_OFF_2 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_OFF_2 |
RW |
0x000000 |
The secondary pointer for RX_OFF. |
||
0x36 |
0xd8 |
TDD_TX_ON_2 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_ON_2 |
RW |
0x000000 |
The secondary pointer for TX_ON. |
||
0x37 |
0xdc |
TDD_TX_OFF_2 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_OFF_2 |
RW |
0x000000 |
The secondary pointer for TX_OFF. |
||
0x38 |
0xe0 |
TDD_RX_DP_ON_2 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_DP_ON_2 |
RW |
0x000000 |
The secondary pointer for RX_DP_ON. |
||
0x39 |
0xe4 |
TDD_RX_DP_OFF_2 |
TDD Control & Status |
|||
[23:0] |
TDD_RX_DP_OFF_2 |
RW |
0x000000 |
The secondary pointer for RX_DP_OFF. |
||
0x3a |
0xe8 |
TDD_TX_DP_ON_2 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_DP_ON_2 |
RW |
0x000000 |
The secondary pointer for TX_DP_ON. |
||
0x3b |
0xec |
TDD_TX_DP_OFF_2 |
TDD Control & Status |
|||
[23:0] |
TDD_TX_DP_OFF_2 |
RW |
0x000000 |
The secondary pointer for TX_DP_OFF. |
||
Software Support
The software for this IP can be found as part of the FMCOMMS2/3/4/5 reference designs.
Linux device driver at drivers/iio/adc/ad9361.c
Linux device trees for this can be found at ADI Linux repository
Linux documentation on wiki
No-OS device driver at drivers/rf-transceiver/ad9361
No-OS project at projects/ad9361