Asymmetric AXI Stream FIFO
The Asymmetric AXI Stream FIFO core is a simple FIFO (First Input First Output) with AXI streaming interfaces, supporting synchronous and asynchronous operation modes with an asymmetric data width on its salve and master interface. It can be used to mitigate data width differences or transfer an AXI stream to a different clock domain.
Features
Supports Intel/Altera and AMD Xilinx devices
Configurable data width and depth
Asymmetric data width
Supports asynchronous (double clocked) mode
Supports TLAST to indicate packet boundary
Supports TKEEP to indicate valid data bytes
Supports FULL/EMPTY and ALMOST_FULL/ALMOST_EMPTY status signals
Files
Name |
Description |
|---|---|
Verilog source for the peripheral. |
Configuration Parameters
Name |
Description |
|---|---|
M_DATA_WIDTH |
Data width of the Master AXI streaming interface. |
S_DATA_WIDTH |
Data width of the Slave AXI streaming interface. |
ADDRESS_WIDTH |
Defines the depth of the FIFO. |
ASYNC_CLK |
Clocking mode. If set, the FIFO operates on asynchronous mode. |
M_AXIS_REGISTERED |
Add and additional register stage to the AXI stream master interface. |
ALMOST_EMPTY_THRESHOLD |
Defines the offset (in data beats) between the almost empty and empty assertion. |
ALMOST_FULL_THRESHOLD |
Defines the offset (in data beats) between the almost full and full assertion. |
TLAST_EN |
Enable |
TKEEP_EN |
Enable |
REDUCED_FIFO |
Reduce the FIFO size when master and slave data widths are not equal |
Interface
Name |
Description |
|---|---|
s_axis |
Slave AXI stream. |
s_axis_aclk |
Slave AXI stream clock signal |
s_axis_aresetn |
Slave AXI stream reset signal (active low) |
s_axis_room |
Indicates how much space (in data beats) is in the FIFO |
s_axis_almost_full |
If set the FIFO is almost full |
m_axis |
Master AXI stream. |
m_axis_aclk |
Master AXI stream clock signal |
m_axis_aresetn |
Master AXI stream reset signal (active low) |
m_axis_level |
Indicates how much data is in the FIFO |
s_axis_full |
If set the FIFO is full |
m_axis_almost_empty |
If set the FIFO is almost empty |
m_axis_empty |
If set the FIFO is empty |
Detailed Description
The FIFO is based on the util_axis_fifo, using it as its atomic building block.
The configuration of the atomic util_axis_fifo blocks are calculated as follows:
// define which interface has a wider bus
localparam RATIO_TYPE = (S_DATA_WIDTH >= M_DATA_WIDTH) ? 1 : 0;
// bus width ratio
localparam RATIO = (RATIO_TYPE) ? S_DATA_WIDTH/M_DATA_WIDTH : M_DATA_WIDTH/S_DATA_WIDTH;
// atomic parameters
localparam A_WIDTH = (RATIO_TYPE) ? M_DATA_WIDTH : S_DATA_WIDTH;
localparam A_ADDRESS = (REDUCED_FIFO) ? (ADDRESS_WIDTH-$clog2(RATIO)) : ADDRESS_WIDTH;
localparam A_ALMOST_FULL_THRESHOLD = (REDUCED_FIFO) ? ((ALMOST_FULL_THRESHOLD+RATIO-1)/RATIO) : ALMOST_FULL_THRESHOLD;
localparam A_ALMOST_EMPTY_THRESHOLD = (REDUCED_FIFO) ? ((ALMOST_EMPTY_THRESHOLD+RATIO-1)/RATIO) : ALMOST_EMPTY_THRESHOLD;
Status Signal Delays
Important
In case of asynchronous mode, because of the delays introduced by the clock domain crossing logic, the ROOM and LEVEL indicators can not reflect the actual state of the FIFO in real time. Source and destination logic should take this into account when controlling the data stream into and from the FIFO. Carefully adjusting the ALMOST_EMPTY/ALMOST_FULL indicators can provide a save operating margin.
The FIFO has three different status indicator ports on both side, which provides information about the state of the FIFO for both the source and destination logic:
FULL or EMPTY - If these outputs are asserted the FIFO is full or empty. In case of a full FIFO all the write operations are suspended. In case of an empty FIFO all the read operations are suspended.
ALMOST_EMPTY/ALMOST_FULL - It can be used to foresee a potential FULL or EMPTY state, asserting before the EMPTY/FULL before a predefined number of words. The offset between ALMOST_EMPTY and EMPTY, and between ALMOST_FULL and FULL can be set by using the parameters ALMOST_EMPTY_THRESHOLD and ALMOST_FULL_THRESHOLD. The offset values are automatically adjusted according to M_DATA_WIDTH and S_DATA_WIDTH ratio when REDUCED_FIFO is enabled.
S_AXIS_ROOM - Indicate how many word can be written in the FIFO at the current moment, until the FIFO become FULL.
M_AXIS_LEVEL - Indicate how many word can be read from the FIFO at the current moment, until the FIFO become EMPTY.
FIFO Depth Calculation
The FIFO Depth is calculated based on M_DATA_WIDTH, S_DATA_WIDTH, ADDRESS_WIDTH and REDUCED_FIFO parameters:
When M_DATA_WIDTH and S_DATA_WIDTH are equal or REDUCED_FIFO is disabled, the ADDRESS_WIDTH specified is not changed.
When M_DATA_WIDTH and S_DATA_WIDTH are not equal and the REDUCED_FIFO is enabled, the ADDRESS_WIDTH is reduced by log2 ratio of the master and slave data widths.
Software Support
Linux project at drivers/staging/axis-fifo
Linux driver at drivers/staging/axis-fifo/axis-fifo.c