AD57XX_ARDZ HDL project

Overview

This page documents the HDL reference design for the EVAL-AD5780ARDZ, EVAL-AD5781ARDZ and EVAL-AD5791ARDZ evaluation boards.

The EVAL-AD5780ARDZ facilitates fast prototyping of the AD5780 circuit, and can be substituted with either the AD5760 or AD5790, which must be ordered separately. Similarly, the EVAL-AD5781ARDZ and EVAL-AD5791ARDZ come with the AD5781 and AD5791 respectively.

The AD5790, AD5791, AD5760, AD5780 and AD5781 are a family of precision, single-channel voltage output DACs, with resolutions from 16-bits up to 20-bits. They offer guaranteed monotonic operation, and low nonlinearity (down to 0.5 LSB INL and DNL)

The evaluation boards provide an on-board -14 V and +14 V dual power supply. These evaluation boards also utilize external reference boards with an output voltage of +10 V and -10 V. The eval boards are connected to the carrier board through the Arduino Shield connector.

This project has a SPI Engine instance to control and acquire data from the DAC. This instance provides support for sending continuous samples at the maximum sample rate.

Supported boards

Supported devices

Supported carriers

Block design

Block diagram

The data path and clock domains are depicted in the below diagrams:

../../_images/ad57xx_de10nano_hdl.svg

AD5780-ARDZ HDL design block diagram for the DE10-Nano

../../_images/ad57xx_coraz7s_hdl.svg

AD5780-ARDZ HDL design block diagram for the Cora Z7S

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Zynq*/DE10-Nano**

spi_ad57xx_axi_regmap*

0x44A0_0000

ad57xx_tx_dma*

0x44A4_0000

trig_gen*

0x44B0_0000

axi_ad57xx_clkgen*

0x44B1_0000

axi_dmac_0**

0x0003_0000

axi_spi_engine_0**

0x0004_0000

trig_gen**

0x0005_0000

spi_clk_pll_reconfig**

0x0006_0000

Legend

  • * instantiated only for Cora Z7S

  • ** instantiated only for DE10-Nano

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL*

iic_ard

axi_ard_fmc

0x4160_0000

24AA32A

PS**

i2c1

sys_hps_i2c1

—

—

Legend

  • * instantiated only for Cora Z7S

  • ** instantiated only for DE10-Nano

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PL

axi_spi_engine

AD57XX

0

GPIOs

The Software GPIO number is calculated as follows:

  • Cora Z7S: the offset is 54

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

ad57xx_ardz_ldacb

INOUT

34

88

ad57xx_ardz_clrb

INOUT

33

87

ad57xx_ardz_resetb

INOUT

32

86

  • DE10-Nano: the offset is 32

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

DE10-Nano

ad57xx_ardz_ldacb

INOUT

34

2

ad57xx_ardz_clrb

INOUT

33

1

ad57xx_ardz_resetb

INOUT

32

0

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Zynq

Actual Zynq

ad57xx_tx_dma

13

57

89

spi_ad57xx

12

56

88

axi_iic_ard

11

55

87

Instance name

HDL

Linux DE10-Nano

Actual DE10-Nano

axi_spi_engine_0

5

45

77

axi_dmac_0

4

44

76

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/ad57xx_ardz/coraz7s
~/hdl/projects/ad57xx_ardz/coraz7s$
make
~$
cd hdl/projects/ad57xx_ardz/de10nano
~/hdl/projects/ad57xx_ardz/de10nano$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.