M2K HDL Project

Overview

The ADALM2000 (M2K), is built around the XC7Z010 Xilinx Zynq FPGA.

Booting is done from a 32MB QSPI FLASH, connected directly to the PS7 block.

The system memory is 512MB RAM, which is also used for the file system. The DDR interface is a 16 bits interface running at 500 MHz. The frequency was chosen so that a single PLL runs inside of the PS7 block generating all the required PS7 clocks, consuming minimum power.

The FPGA drives 16 GPIOs for the logic analyzer, 2 GPIOs for triggers, a 14 pin interface to the AD9963’s ADC and a 14 pin interface to the AD9963’s DAC. It also has several generic GPIOs, an SPI and an I2C interface for configuring the board.

The control GPIOs and the SPI are driven by the PS7 block in order to minimize the PL resource usage.

The I2C is implemented by an AXI I2C IP because the PS7 I2C has several limitations, which makes it not suitable for this project.

The oscilloscope related logic transfers data from the AD9963 chip with the AD9963 TRX interface goes through the decimation block, the analog triggering block, the history FIFO and streams data to memory using the DMA.

The analog waveform generator transfers data from the memory using two DMAs, then goes through the interpolation block and ends with the AD9963 TX interface, which transfers data to the AD9963 chip. Two DMAs are used in order to have different orders of magnitude for the frequency of the two AWG channels, without needing to transfer a very large number of samples.

The logic analyzer and pattern generator logic are mostly implemented in the same IP to which a history FIFO and DMAs are added.

Supported boards

Supported devices

Block design

Detailed description

The PS7 hardware block is the main processing block of the system, having an ARM processor running at 500MHz. It is running a Linux operating system.

To minimize the power utilization for the design, the PS7 block is the only block generating clocks in the system. The clock configuration is done in such a way that a single PLL is used to derive all the necessary clocks for the ARM processor, the DDR and the peripherals. It generates a 27MHz clock (FCLK0) for the AXI interface and a 55MHz clock for the oscilloscope DMA and one of the two analog waveform generator DMAs.

The PS7 has enabled SPI0, UART1 and USB0 peripherals. The QUAD SPI flash interface is enabled in Single SS 4 bit IO mode.

The DDR interface is a 16 bit interface running at 500MHz.

The HP ports have been assigned in a way to optimize the data throughput through each of the active ports, considering that HP0 and HP1 share the path to memory (same for HP2 and HP3).

BANK 0 and BANK 1 are configured in LVCMOS 1.8V mode.

The AXI_AD9963 IP is implementing the interfacing with the AD9963 chip. It features a dual 12-bit ADC working up to 100MSPS and a dual 12-bit DAC with up to 170MSPS. It also features a DLL, which can provide the clock for both the ADC and the DAC path.

The TRX (ADC) interface is set at 100 MSPS, full duplex mode, double data rate (DDR), two channels. The clock comes from the AD9963 chip. The IO standard is CMOS at 3.3V.

The TX (DAC) interface works at 75 MSPS data rate with interpolation by 2 on the AD9963 chip. The DAC path inside AD9963 chip works at 150MHz, pushing part of the spurs outside the 100MHz bandwidth. Given that the reference clock for AD9963 is 100MHz and DACs maximum sampling rate is 170MSPS, this is the best option available. The 75MHz clock is not available in the FPGA. To reduce the number of PLL used in the FPGA, we are using AD9963 and a BUFR (divide by 2) to generate this clock. When the clock is generated by AD9963, DDR transfer is not available. The TX interface works at 150MHz, SDR. The IO standard is CMOS at 3.3V.

More information at AXI AD9963 documentation.

The AXI_ADC_TRIGGER IP implements triggering for the ADC path and also controls the TRIGGER pins. It works on two clock domains, the ADC clock and the AXI interface clock.

The configuration of the IP is done through the AXI interface.

The data path runs at the ADC clock.

Triggers based on the two trigger digital pins, trigger[0] for ADC A and trigger[1] for ADC B can be selected between high, low, any edge, rise edge, fall edge

Triggers based on the analog data on a channel will be active if data is larger than a limit, smaller than a limit, passing through the limit, passing through high or passing through low. The data format must be 2’s complement.

The output of the core can embed the triggers in the data words, as only 12 bits of the 16-bit word are used for data. These need to be extracted before being forwarded to the DMA. Embedding the trigger with the data allows for additional IPs with unknown pipeline length to be introduced in the path.

More information at AXI ADC Trigger documentation.

The UTIL_VAR_FIFO IP allows M2K to store and display data before the trigger. In the design, it has a length of 8192 samples and can easily be increased. The IP controls an external BRAM. If DEPTH is 0, the FIFO is bypassed. When the DEPTH is changed, the read and write pointers are reset, effectively resetting the FIFO. There is a 2 cycle clock latency, even if it’s bypassed. If valid is not always asserted (decimation is active), the latency is one clock cycle instead of two.

More information at Util VAR FIFO documentation.

The data alignment as event history or alignment between instruments is done via triggers.

The system has two external trigger ports, TI and TO. Both can be used as input or output. By default, TI is input and TO output. The in/out direction is controlled by axi_adc_trigger.

Each instrument can be triggered by an external event or from ADC or LA. The AXI ADC Trigger and AXI Logic Analyzer can generate triggers on well-defined user scenarios.

The instrument trigger of each instance is the same one with the trigger condition set data alignment.

The Util Extract IP will extract the trigger that was embedded in the data stream by the AXI ADC Trigger IP. Not used in the lates design.

More information at Util Extract documentation.

The AD9963 RX interface clock has a set value of 100MHz, so the interface always runs at 100MSPS for each of the two channels. For some applications, 100MSPS are not required and leads to lots of samples transferred to memory, which are redundant. For these cases, the decimation IP is used.

The decimation block allows decimating the input data so that the sampling frequency to be reduced by 10, 100, 1000, 10000, 100000, with filtering. The filtering is implemented by a 6 sections CIC programmable rate filter, which allows decimation by 5/50/500/5000/50000 and a compensation FIR filter (decimation by 2).

At the end of the filter chain, there is an arbitrary decimation block. The arbitrary decimation can be activated independently and it does not implement any type of filtering.

More information at AXI ADC Decimate documentation.

The TX interface is set at 75 MSPS. For some generated signals, this sampling rate is too high and leads to a bad utilization of the memory and the USB bandwidth. In order to avoid that, the interpolation IP can be used.

The interpolation block allows interpolation by 10, 100, 1000, 10000,100000 with filtering. The filtering is implemented using an FIR compensation filter (interpolation by 2) for the CIC and a 6 stage CIC interpolation filter, allowing interpolation by 5/50/500/5000/50000.

At the end of the filter blocks, we have an arbitrary interpolation zero-order hold block which holds the value for a configurable number of samples.

More information at AXI DAC Interpolate documentation.

The AXI Logic Analyzer IP implements both the logic analyzer and the pattern generator, as they share the same pins.

There are 16-channel digital I/O pins running at 100 MSPS. All the pins can be configured either as inputs (logic analyzer) or outputs (pattern generator). The logic analyzer path allows a pre trigger history of 8192 samples per channel.

The pattern generator supports open drain outputs, configurable per pin. Additionally to the 16 data pins, there are two trigger pins, which can be configured as input or output. Because they can be used with either analog or digital instruments, they are controlled by the AXI_ADC_TRIGGER IP.

The logic analyzer path can work at lower than the 100MSPS rate by configuring the down sampling block. The same thing is done for the pattern generator by configuring the up sampling block.

Triggering for the logic analyzer is implemented in this IP. It can generate triggers based on the external trigger signals and the 16-bit input signals. For each of the 18 pins it can detect rise edge, fall edge, any edge, high or low.

To provide data before triggering, a variable length FIFO is used with this IP. The depth of the FIFO is configured through the TRIGGER_OFFSET register. It can be bypassed if TRIGGER_OFFSET is 0. If the FIFO is active, it is filled before being read, not forwarding any data until it is full. The maximum size of the FIFO is 8192 samples. The FIFO is implemented using BRAM blocks configured for minimal power consumption.

More information at AXI Logic Analyzer documentation.

Location

Name

Notes

BANK 35, 3.3V. No pins available

F14

IIC_SCL

Enable pull-up

F13

IIC_SDA

Enable pull-up

E12

AD9963_RESETN

Reset for the AD9963 chip

G15

ADF4360_CS

SPI interface, chip select for ADF4360

E11

AD9963_CSN

SPI interface, chip select for AD9963

E13

SPI_CLK

SPI interface, clock

F12

SPI_SDIO

SPI interface, data

F15

EN_POWER_ANALOG

Power on analog path

BANK 34, 3.3V. No pins available

M12

TRIGGER[0]

Trigger pin 0

N12

TRIGGER[1]

Trigger pin 1

K11

DATA_BD[0]

Data pin 0. SRCC

K12

DATA_BD[1]

Data pin 1

K13

DATA_BD[2]

Data pin 2

L13

DATA_BD[3]

Data pin 3

L14

DATA_BD[4]

Data pin 4

M14

DATA_BD[5]

Data pin 5

L15

DATA_BD[6]

Data pin 6

M15

DATA_BD[7]

Data pin 7

N13

DATA_BD[8]

Data pin 8

P14

DATA_BD[9]

Data pin 9

R12

DATA_BD[10]

Data pin 10

R13

DATA_BD[11]

Data pin 11

P11

DATA_BD[12]

Data pin 12

R11

DATA_BD[13]

Data pin 13

P15

DATA_BD[14]

Data pin 14

R15

DATA_BD[15]

Data pin 15

N11

RX_CLK

AD9963 RX interface clock. MRCC

P13

RX_IQ

AD9963 RX IQ pin

P10

RXD[0]

AD9963 RX data pin 0

R10

RXD[1]

AD9963 RX data pin 1

P8

RXD[2]

AD9963 RX data pin 2

P9

RXD[3]

AD9963 RX data pin 3

N7

RXD[4]

AD9963 RX data pin 4

N8

RXD[5]

AD9963 RX data pin 5

M10

RXD[6]

AD9963 RX data pin 6

M11

RXD[7]

AD9963 RX data pin 7

R7

RXD[8]

AD9963 RX data pin 8

R8

RXD[9]

AD9963 RX data pin 9

M9

RXD[10]

AD9963 RX data pin 10

N9

RXD[11]

AD9963 RX data pin 11

L12

TX_CLK

AD9963 TX interface clock. MRCC

N14

TX_IQ

AD9963 TX IQ pin

H12

TXD[0]

AD9963 TX data pin 0

G11

TXD[1]

AD9963 TX data pin 1

H13

TXD[2]

AD9963 TX data pin 2

G12

TXD[3]

AD9963 TX data pin 3

H14

TXD[4]

AD9963 TX data pin 4

G14

TXD[5]

AD9963 TX data pin 5

K15

TXD[6]

AD9963 TX data pin 6

J15

TXD[7]

AD9963 TX data pin 7

J14

TXD[8]

AD9963 TX data pin 8

J13

TXD[9]

AD9963 TX data pin 9

J11

TXD[10]

AD9963 TX data pin 10

H11

TXD[11]

AD9963 TX data pin 11

BANK 500, 1.8V. 3 Available pins

PS_MIO1

QSPI0_SS

QSPI FLASH

PS_MIO2

QSPI0_IO0

QSPI FLASH

PS_MIO3

QSPI0_IO1

QSPI FLASH

PS_MIO4

QSPI0_IO2

QSPI FLASH

PS_MIO5

QSPI0_IO3

QSPI FLASH

PS_MIO6

QSPI0_SCLK

QSPI FLASH

PS_MIO7

VDD (1.8)

PS_MIO8

VDD (1.8)

PS_MIO12

UART_TX

Debug UART

PS_MIO13

UART_RX

Debug UART

PS_MIO14

USR_BTN

Button

PS_MIO15

USR_LED

LED

PS_MIO9

—

Available

PS_MIO10

—

Available

PS_MIO11

—

Available

BANK 501, 1.8V. 3 Available pins

PS_MIO28

USB0_D4

USB

PS_MIO29

USB0_DIR

USB

PS_MIO30

USB0_STP

USB

PS_MIO31

USB0_NXT

USB

PS_MIO32

USB0_D0

USB

PS_MIO33

USB0_D1

USB

PS_MIO34

USB0_D2

USB

PS_MIO35

USB0_D3

USB

PS_MIO36

USB0_CLK

USB

PS_MIO37

USB0_D5

USB

PS_MIO38

USB0_D6

USB

PS_MIO39

USB0_D7

USB

PS_MIO52

USB_RESET_B

USB

PS_MIO48

—

Available

PS_MIO49

—

Available

PS_MIO53

—

Available

Block diagram

The data path and clock domains are depicted in the below diagram.

M2K block diagram

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Zynq

axi_iic_main

0x4160_0000

logic_analyzer

0x7010_0000

axi_ad9963

0x7020_0000

logic_analyzer_dmac

0x7C40_0000

pattern_generator_dmac

0x7C42_0000

ad9963_adc_dmac

0x7C44_0000

ad9963_dac_dmac_b

0x7C46_0000

ad9963_dac_dmac_a

0x7C48_0000

adc_trigger

0x7C4C_0000

axi_adc_decimate

0x7C50_0000

axi_dac_interpolate

0x7C5A_0000

SPI connections

The SPI signals are controlled by a separate AXI based SPI core.

SPI type

SPI manager instance

SPI subordinate

CS

PS

SPI 0

AD9963

0

GPIOs

The device control and monitor signals are interfaced to a GPIO module.

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

en_power_analog

OUTPUT

1

55

ad9963_resetn

OUTPUT

0

54

Interrupts

Below are the Programmable Logic interrupts used in the project.

Instance name

HDL

Linux Zynq

Actual Zynq

axi_iic_main

14

58

90

logic_analyzer_dmac

13

57

89

pattern_generator_dmac

12

56

88

ad9963_adc_dmac

10

54

86

ad9963_dac_dmac_a

9

53

85

ad9963_dac_dmac_b

8

52

84

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.

Go to the hdl/projects/m2k location and run the make command.

Linux/Cygwin/WSL

~$
cd hdl/projects/m2k
~/hdl/projects/m2k$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Building the M2K firmware

Check out the build section from the README.md: https://github.com/analogdevicesinc/m2k-fw.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.