AD411x-AD717x HDL project

Overview

The AD4111 /AD4112 /AD4114 /AD4115/ AD4116 is a low power, low noise, 24-bit, sigma-delta (Σ-Δ) analog-to-digital converter (ADC), high impedance (≥1 MΩ) bipolar, ±10 V voltage inputs, and 0 mA to 20 mA current inputs. The AD4111 /AD4112 /AD4114 /AD4115 / AD4116 also integrates key analog and digital signal conditioning blocks to configure eight individual setups for each analog input channel in use.

The AD4111 /AD4112 /AD4114 features a maximum output data rate of 31.25 kSPS, AD4115 features a maximum output data rate of 125 kSPS and AD4116 features a maximum output data rate of 62.5 kSPS.

The AD7172-2 /AD7172-4 /AD7173-8 /AD7175-2/ AD7175-8 /AD7176-2 /AD7177-2 is a low noise, low power, multiplexed, Σ-Δ analog-to-digital converter (ADC) for low bandwidth input signals. The AD7172-2 /AD7172-4 /AD7173-8 /AD7175-2 / AD7175-8 /AD7176-2 /AD7177-2 integrates key analog and digital signal conditioning blocks to allow users to configure an individual setup for each analog input channel in use.

The AD7172-2 /AD7172-4 /AD7173-8 features a maximum output data rate of 31.25 kSPS, AD7175-2/ AD7175-8 /AD7176-2 features a maximum output data rate of 250 kSPS and AD7177-2 features a maximum output data rate of 10 kSPS.

The digital filter allows flexible settings, including simultaneous 50 Hz and 60 Hz rejection at a 27.27 SPS output data rate. The user can select different filter settings depending on the requirements of each channel in the application.

This project has a SPI Engine instance to control and acquire data from the AD411x/AD717x precision ADC. This instance provides support for capturing continuous samples at the maximum sample rate.

Supported boards

Supported devices

Supported carriers

Block design

Block diagram

The data path and clock domains are depicted in the below diagram:

AD411x_ad717x block diagram

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

DE10-Nano

axi_dmac_0

0x0002_0000

axi_spi_engine_0

0x0003_0000

trigger_generator

0x0004_0000

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PS**

i2c1

sys_hps_i2c1

—

—

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PL

axi_spi_engine

ad411x_ad717x

0

GPIOs

The Software GPIO number is calculated as follows:

  • DE10-Nano: the offset is 32

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

DE10-Nano

spi_miso

INPUT

34

2

error

INPUT

33

1

sync_error

INPUT

32

0

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux DE10-Nano

Actual DE10-Nano

axi_spi_engine_0

5

45

77

axi_dmac_0

4

44

76

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/ad411x_ad717x/de10nano
~/hdl/projects/ad411x_ad717x/de10nano$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.