AD-QUADMXFE1-EBZ HDL project

Overview

The AD-QUADMXFE1-EBZ reference design is a processor based (e.g. Microblaze) embedded system, which showcases the QUAD-MXFE evaluation board.

The Quad-MxFE System Development Platform contains four MxFE (Mixed-signal Front End) software defined, direct RF sampling transceivers, as well as associated RF front-ends, clocking, and power circuitry. The target application is phased array radars, electronic warfare, and ground-based SATCOM, specifically a 16 transmit/16 receive channel direct sampling phased array at L/S/C band (0.1 GHz to ~5GHz).

  • 16x RF receive (RX) channels (32x digital RX channels), with 16 ADCs going from 1.5 GSPS to 4 GSPS, and 48x Digital Down Converters (DDCs), each including complex Numerically-Controlled Oscillators (NCOs)

  • 16x RF transmit (TX) channels (32x digital TX channels), with 16 DACs going from 3 GSPS to 12 GSPS, and 48x Digital Up Converters (DUCs), each including complex Numerically-Controlled Oscillators (NCOs)

Supported boards

Supported devices

Supported carriers

Block design

The design consists from a receive and a transmit chain.

The receive chain transports the captured samples from ADC to the system memory (DDR). Before transferring the data to DDR the samples are stored in a buffer implemented on block rams from the FPGA fabric (util_adcfifo). The size of the buffer is sized to store up to M x 16k samples per converter if a single channel is selected or 16k samples per converter if all channels are selected.

The transmit chain transports samples from the system memory to the DAC devices. Before streaming out the data to the DAC through the JESD link the samples first are loaded into a buffer (util_dacfifo) which will cyclically stream the samples at the tx_device_clk data rate.

All cores from the receive and transmit chains are programmable through an AXI-Lite interface.

The transmit and receive chains must operate at the same data rates having a common device clock.

Block diagram

The data path and clock domains are depicted in the below diagrams.

Default configuration

The 4 MxFE RX and TX links are connected to a single transceiver block (AMD Xilinx’s JESD204 PHY IP) having 8 RX and 16 TX lanes in total.

The 4 RX links merge into a single receive Link Layer and a single Transport Layer having a compatible configuration as described below.

Similarly to RX, the single transmit Link Layer and Transport Layer handle the 4 TX links.

The number of lanes on RX is reduced to half to keep the same lane rate as the TX link (which has double the number of channels of RX).

  • JESD204C with lane rate 16.5Gbps

  • REF_CLK_RATE=250 MHz

  • RX: L=2, M=8, S=1, NP=16, PLL_SEL=2 (QPLL1)

  • TX: L=4, M=16, S=1, NP=16, PLL_SEL=2 (QPLL1)

AD-QUADMXFE1-EBZ/VCU118 block diagram

Important

This configuration was built with the following parameters, and it is equivalent to running only make:

/hdl/projects/ad_quadmxfe1_ebz/vcu118$
make JESD_MODE=64B66B \
     RX_LANE_RATE=16.5 \
     TX_LANE_RATE=16.5 \
     REF_CLK_RATE=250 \
     RX_JESD_M=8 \
     RX_JESD_L=2 \
     TX_JESD_M=16 \
     TX_JESD_L=4

Block name

IP name

Documentation

Additional info

AXI_DMAC

axi_dmac

AXI DMAC

2 instances, one for RX and one for TX

DATA_OFFLOAD

data_offload

Data Offload

2 instances, one for RX and one for TX

RX JESD LINK

axi_mxfe_rx_jesd

JESD204B/C Link Receive Peripheral

Instantiaded by adi_axi_jesd204_rx_create procedure

RX JESD TPL

rx_mxfe_tpl_core

ADC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_rx_create procedure

TX JESD LINK

axi_mxfe_tx_jesd

JESD204B/C Link Transmit Peripheral

Instantiaded by adi_axi_jesd204_tx_create procedure

TX JESD TPL

tx_mxfe_tpl_core

DAC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_tx_create procedure

UTIL_CPACK

util_cpack2

Channel CPACK Utility

—

UTIL_UPACK

util_upack2

Channel UPACK Utility

—

QUADS 121-122

jesd204_phy_121_122

AMD PG198

AMD Xilinx JESD204 PHY IP

QUADS 125-126

jesd204_phy_125_126

AMD PG198

AMD Xilinx JESD204 PHY IP

Example block design with DAC & ADC {M=8 L=4}

The 4 MxFE RX and TX links are connected to a single transceiver block, having 16x RX and 16x TX lanes in total (4 * L).

The 4 RX links merge into a single receive Link Layer, and a single Transport Layer, having a compatible configuration as detailed below. Similarly, the single transmit Link Layer and Transport Layer handle the four TX links.

  • JESD204B with lane rate 10Gbps

  • RX, TX: L=4, M=8, S=1, NP=16, NUM_LINKS=4

AD-QUADMXFE1-EBZ/VCU118 JESD204B block diagram

Important

This configuration was built using the make command with the following parameters:

/hdl/projects/ad_quadmxfe1_ebz/vcu118$
make JESD_MODE=8B10B \
     RX_JESD_L=4 \
     RX_JESD_M=8 \
     RX_JESD_NP=16 \
     RX_NUM_LINKS=4 \
     TX_JESD_L=4 \
     TX_JESD_M=8 \
     TX_JESD_NP=16 \
     TX_NUM_LINKS=4

Block name

IP name

Documentation

Additional info

AXI_ADXCVR

axi_adxcvr

AXI ADXCVR

2 instances, one for RX and one for TX

AXI_DMAC

axi_dmac

AXI DMAC

2 instances, one for RX and one for TX

DATA_OFFLOAD

data_offload

Data Offload

2 instances, one for RX and one for TX

RX JESD LINK

axi_mxfe_rx_jesd

JESD204B/C Link Receive Peripheral

Instantiaded by adi_axi_jesd204_rx_create procedure

RX JESD TPL

rx_mxfe_tpl_core

ADC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_rx_create procedure

TX JESD LINK

axi_mxfe_tx_jesd

JESD204B/C Link Transmit Peripheral

Instantiaded by adi_axi_jesd204_tx_create procedure

TX JESD TPL

tx_mxfe_tpl_core

DAC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_tx_create procedure

UTIL_ADXCVR

util_adxcvr

UTIL_ADXCVR core for AMD Xilinx devices

Used for both AXI ADXCVR instances

UTIL_CPACK

util_cpack2

Channel CPACK Utility

—

UTIL_UPACK

util_upack2

Channel UPACK Utility

—

Configuration modes

The following are the parameters of this project that can be configured:

  • JESD_MODE: used link layer encoder mode

    • 64B66B - 64b66b link layer defined in JESD204C, uses AMD IP as Physical Layer

    • 8B10B - 8b10b link layer defined in JESD204B, uses ADI IP as Physical Layer

  • RX_LANE_RATE: lane rate of the RX link (MxFE to FPGA)

  • TX_LANE_RATE: lane rate of the TX link (FPGA to MxFE)

  • [RX/TX]_PLL_SEL: used only in 64B66B mode:

    • 0 - CPLL for lane rates 4-12.5 Gbps and integer sub-multiples

    • 1 - QPLL0 for lane rates 19.6-32.75 Gbps and integer sub-multiples (e.g. 9.8-16.375)

    • 2 - QPLL1 for lane rates 16.0-26.0 Gbps and integer sub-multiple (e.g. 8.0-13.0)

    • For more details, see JESD204 PHY v4.0 Product Guide (AMD PG198) and UltraScale Architecture GTY Transceivers User Guide (AMD UG578)

  • REF_CLK_RATE: the rate of the reference clock, used only in 64B66B mode

  • [RX/TX]_JESD_M: number of converters per link

  • [RX/TX]_JESD_L: number of lanes per link

  • [RX/TX]_JESD_S: number of samples per frame

  • [RX/TX]_JESD_NP: number of bits per sample

  • [RX/TX]_NUM_LINKS: number of links

  • RX_KS_PER_CHANNEL: RX number of samples stored in internal buffers in kilosamples per converter (M), for each channel in a block RAM, for a contiguous capture

  • TX_KS_PER_CHANNEL: TX number of samples loaded for each channel in a block RAM for a contiguous cyclic streaming

  • DAC_TPL_XBAR_ENABLE: enable NxN crossbar functionality at the transport layer, where N is the number of channels

Clock scheme

AD-QUADMXFE1-EBZ/VCU118 clock scheme

Limitations

One MxFE has 8 lanes, with maximum lane rate supported in JESD204C = 24.75Gbps.

Maximum data rate for one MxFE per direction = 8 * 24.75Gbps * 64/66 = 192 Gbps = 24 GB/s.

The existing Quad board has half the lanes, so this gives us 12GB/s per MxFE per direction. The bandwidth requirement per direction is = 4 * 12GB/s = 48 GB/s.

By direction, we imply FPGA to DAC path or ADC to FPGA path.

The theoretical throughput of the DDR from the VCU118 is 19.2 GB/s, so far away from the exiting quad MxFE requirements, but an HBM FPGA would solve that.

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Depending on the value of the parameter $ADI_PHY_SEL, some IPs are instantiated and some are not. If JESD204C is chosen, then the JESD physical layer used will be the AMD Xilinx JESD204 PHY (see AMD PG198), otherwise the ADI UTIL_ADXCVR core for AMD Xilinx devices.

Check-out the table below to find out the conditions.

Instance

Depends on parameter

Zynq/Microblaze

axi_mxfe_rx_xcvr

$ADI_PHY_SEL==1

0x44A6_0000

jesd204_phy_121_122

$ADI_PHY_SEL==0

0x44A6_0000

rx_mxfe_tpl_core

0x44A1_0000

axi_mxfe_rx_jesd

0x44A9_0000

axi_mxfe_rx_dma

0x7C42_0000

mxfe_rx_data_offload

0x7C45_0000

axi_mxfe_tx_xcvr

$ADI_PHY_SEL==1

0x44B6_0000

jesd204_phy_125_126

$ADI_PHY_SEL==0

0x44B6_0000

tx_mxfe_tpl_core

0x44B1_0000

axi_mxfe_tx_jesd

0x44B9_0000

axi_mxfe_tx_dma

0x7C43_0000

mxfe_tx_data_offload

0x7C46_0000

SPI connections

The AD9081 SPI interface is a 4-wire SPI by default, however the part can be run in a 3-wire interface if desired. There is a separate SPI bus for each of the AD9081s to allow for parallel operation if desired, but the FPGA currently supports sequential operation.

The HMC7043 and ADF4371 are both wired for 3-wire SPI only. The ADF4371s share a common SPI bus with 4 CS lines. The HMC7043 has a separate dedicated SPI bus as well.

SPI type

SPI manager instance

SPI subordinate

CS

PS

SPI 1

AD9081

3:0

PS

SPI 2

HMC7043

4

PS

SPI 2

ADF4371

3:0

GPIOs

GPIO muxing enables multiple functions of gpio_0 pins, to have either the NCO sync function or to be regular software-controllable GPIOs.

e.g. function selection for gpio[0] line of MxFE(0,1,2,3) done through GPIO[108].

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

mxfe0/1/2/3_gpio0

INOUT

64

118

mxfe0/1/2/3_gpio1

INOUT

65

119

mxfe0/1/2/3_gpio2

INOUT

66

120

mxfe0/1/2/3_gpio3

INOUT

67

121

mxfe0/1/2/3_gpio4

INOUT

68

122

mxfe0/1/2/3_gpio5

INOUT

69

123

mxfe0/1/2/3_gpio6

INOUT

70

124

mxfe0/1/2/3_gpio7

INOUT

71

125

mxfe0/1/2/3_gpio8

INOUT

72

126

mxfe0/1/2/3_gpio9

INOUT

73

127

mxfe0/1/2/3_gpio10

INOUT

74

128

Function selection for the first six GPIO lines is done with the following control GPIOs:

  • MxFE(0,1,2,3)_gpio[0] = GPIO[108] (see here)

GPIO_0_MODE (GPIO[108]) = 0 -> Software-controlled GPIO

GPIO name

Pin direction

Pin data out

MxFE0_gpio[0]

SW controlled

SW controlled

MxFE1_gpio[0]

SW controlled

SW controlled

MxFE2_gpio[0]

SW controlled

SW controlled

MxFE3_gpio[0]

SW controlled

SW controlled

GPIO_0_MODE (GPIO[108]) = 1 -> LMFC based Master-Slave NCO sync

See here.

GPIO name

Pin direction

Pin data out

MxFE0_gpio[0]

OUT

MxFE3_gpio[0]

MxFE1_gpio[0]

OUT

MxFE3_gpio[0]

MxFE2_gpio[0]

OUT

MxFE3_gpio[0]

MxFE3_gpio[0]

IN

—

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux MicroBlaze

Actual MicroBlaze

axi_mxfe_tx_jesd

15

59

91

axi_mxfe_rx_jesd

14

58

90

axi_mxfe_tx_dma

13

57

89

axi_mxfe_rx_dma

12

56

88

axi_gpio_2

8

52

84

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.

Then go to the hdl/projects/ad_quadmxfe1_ebz/vcu118 location and run the make command.

Linux/Cygwin/WSL

Example of running the make command without parameters (using the default configuration):

~$
cd hdl/projects/ad_quadmxfe1_ebz/vcu118
~/hdl/projects/ad_quadmxfe1_ebz/vcu118$
make

Example of running the make command with parameters:

~$
cd hdl/projects/ad_quadmxfe1_ebz/vcu118
~/hdl/projects/ad_quadmxfe1_ebz/vcu118$
make JESD_MODE=8B10B \
     RX_JESD_M=4 \
     RX_JESD_L=2 \
     TX_JESD_M=4 \
     TX_JESD_L=2

Configuration names are encoded with [B/C]_[TX MODE]_[RX MODE] where [B/C]: B for 8B/10B (a.k.a. JESD204B) and C for 64B66B (a.k.a. JESD204C).

If a value is not specified, then the default value applies.

default

B_9_10

B_5_6

C_10_11

C_11_4

C_23_25

C_29_24

C_12_13

C_3_2

JESD_MODE

64B66B

8B10B

8B10B

64B66B

64B66B

64B66B

64B66B

64B66B

64B66B

RX_LANE_RATE

16.5

N/A

N/A

16.5

16.5

24.75

24.75

24.75

16.5

TX_LANE_RATE

16.5

N/A

N/A

16.5

16.5

24.75

24.75

24.75

16.5

RX_PLL_SEL

2

N/A

N/A

1

1

1

TX_PLL_SEL

2

N/A

N/A

1

1

1

REF_CLK_RATE

250

N/A

N/A

250

250

250

250

250

250

RX_JESD_M

8

8

4

4

8

4

8

2

4

RX_JESD_L

2

4

2

4

2

4

4

4

1

RX_JESD_S

1

1

1

1

1

2

1

1

1

RX_JESD_NP

16

12

12

RX_NUM_LINKS

4

TX_JESD_M

16

8

4

4

16

4

8

2

8

TX_JESD_L

4

4

2

4

4

4

4

4

2

TX_JESD_S

1

1

1

1

1

2

1

1

1

TX_JESD_NP

16

12

12

TX_NUM_LINKS

4

RX_KS_PER_CHANNEL

32

64

32

16

16

64

16

TX_KS_PER_CHANNEL

16

16

16

16

16

64

16

DAC_TPL_XBAR_ENABLE

0

The result of the build, if parameters were used, will be in a folder named by the configuration used:

if the following command was run

make JESD_MODE=8B10B RX_JESD_M=4 RX_JESD_L=2 TX_JESD_M=4 TX_JESD_L=2

then the folder name will be:

MODE8B10B_RXM4_RXL2_TXM4_TXL2 because of truncation of some keywords so the name will not exceed the limits of the Operating System (JESD, LANE, etc. are removed) of 260 characters.

A more comprehensive build guide can be found in the Build an HDL project user guide.

Important

Make sure you install the fans/heat sinks before powering on the setup! For more details, read here.

Software considerations

ADC - crossbar config

Due to physical constraints, RX lanes are reordered as described in the following table.

For example, physical lane 2 from ADC connects to logical lane 7 from the FPGA. Therefore the crossbar from the device must be set accordingly.

logical lane

0

1

2

3

4

5

6

7

8

9

10

11

12

13

14

15

physical lane

13

10

11

9

3

15

12

14

2

5

0

4

8

7

6

1

DAC - crossbar config

Due to physical constraints, TX lanes are reordered as described in the following table:

For example, physical lane 2 from DAC connects to logical lane 10 from the FPGA. Therefore the crossbar from the device must be set accordingly.

logical lane

0

1

2

3

4

5

6

7

8

9

10

11

12

13

14

15

physical lane

13

8

9

7

3

15

12

14

6

5

2

4

0

10

1

11

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.