AD9084-EBZ HDL project

Overview

The AD9084-EBZ reference design (also known as Apollo) is a processor based (e.g. Microblaze) embedded system. This reference design works with EVAL-AD9084. The design consists from a receive and a transmit chain.

The receive chain transports the captured samples from ADC to the system memory (DDR). Before transferring the data to DDR, the samples are stored in a buffer implemented on BRAMs from the FPGA fabric (util_adcfifo). The space allocated in the buffer for each channel depends on the number of currently active channels. It goes up to M x 64k samples if a single channel is selected or 64k samples per channel if all channels are selected.

The transmit chain transports samples from the system memory to the DAC devices. Before streaming out the data to the DAC through the JESD link, the samples first are loaded into a buffer (util_dacfifo) which will cyclically stream the samples at the tx_device_clk data rate. The space allocated in the transmit buffer for each channel depends on the number of currently active channels. It goes up to M x 64k samples if a single channel is selected or 64k samples per channel if all channels are selected.

All cores from the receive and transmit chains are programmable through an AXI-Lite interface.

The transmit and receive chains can operate at different data rates having separate rx_device_clk/tx_device_clk and corresponding lane rates but must share the same reference clock.

Supported boards

Supported devices

Supported carriers

Evaluation board

Carrier

FMC slot

Maximum number of lanes

AD9084-EBZ

FM87

FMCB

16 (8 per Apollo side)

VCU118

FMC+

24 (12 per Apollo side)

VCK190

FMC2

8 (4 per Apollo side)

VPK180

FMC+

8 (4 per Apollo side)

Block design

Important

The Apollo chip is split into two sides, each side having up to 12 JESD lanes and 4 converters:

  • Side A

  • Side B

The ASYMMETRIC_A_B_MODE parameter is used to enable the asymmetric A/B mode where each Apollo side has a separate JESD link inside the block design.

If the ASYMMETRIC_A_B_MODE parameter is set to 0, the block design will merge the two sides into a single link.

Given the following JESD204 configuration and assuming that ASYMMETRIC_A_B_MODE = 0:

  • L = 8

  • M = 4

  • S = 1

  • N = NP = 16

  • NUM_LINKS = 2

The resulted design will configure each Apollo side with the following parameters, but will merge the two sides into a single JESD link inside the design:

  • L = 8

  • M = 4

  • S = 1

  • N = NP = 16

If however, NUM_LINKS = 1, the design will configure each side with the following parameters:

  • L = 4

  • M = 2

  • S = 1

  • N = NP = 16

Given the following JESD204 configuration and assuming that ASYMMETRIC_A_B_MODE = 1:

  • L = 8

  • M = 4

  • S = 1

  • N = NP = 16

  • NUM_LINKS is ignored

The resulted design will configure each Apollo side with the following parameters, each having it’s own JESD link inside the design:

  • L = 8

  • M = 4

  • S = 1

  • N = NP = 16

Block diagram

The data path and clock domains are depicted in the below diagrams:

Example block design for ASYMMETRIC_A_B_MODE=1; M=4; L=8; JESD204C

AD9084-FMC JESD204C ASYMMETRIC_A_B_MODE=1 M=4 L=8 NUM_LINKS=2 block diagram

Warning

Build instructions:

The project must be built with the following parameters:

$
make JESD_MODE=64B66B  \
     RX_LANE_RATE=20.625 \
     TX_LANE_RATE=20.625 \
     RX_JESD_M=4       \
     RX_JESD_L=8       \
     RX_JESD_S=1       \
     RX_JESD_NP=16     \
     TX_JESD_M=4       \
     TX_JESD_L=8       \
     TX_JESD_S=1       \
     TX_JESD_NP=16     \
     ASYMMETRIC_A_B_MODE=1 \
     RX_B_LANE_RATE=20.625 \
     TX_B_LANE_RATE=20.625 \
     RX_B_JESD_M=4     \
     RX_B_JESD_L=8     \
     RX_B_JESD_S=1     \
     RX_B_JESD_NP=16   \
     TX_B_JESD_M=4     \
     TX_B_JESD_L=8     \
     TX_B_JESD_S=1     \
     TX_B_JESD_NP=16

The Rx link is operating with the following parameters on each Apollo side:

  • Rx Deframer parameters: L=8, M=4, F=1, S=1, NP=16, N=16 (Mode 47)

  • Sample Rate: 2500 MSPS

  • RX_DEVICE_CLK: 312.5 MHz (Lane Rate/66)

  • REF_CLK: 625 MHz (Lane Rate/33)

  • JESD204C Lane Rate: 20.625 Gbps

  • QPLL1

The Tx link is operating with the following parameters:

  • Tx Framer parameters: L=8, M=4, F=1, S=1, NP=16, N=16 (Mode 47)

  • Sample Rate: 2500 MSPS

  • Dual link: No

  • TX_DEVICE_CLK: 312.5 MHz (Lane Rate/66)

  • REF_CLK: 625 MHz (Lane Rate/33)

  • JESD204C Lane Rate: 20.625 Gbps

  • QPLL1

Configuration modes

The block design supports configuration of parameters and scales.

We have listed a couple of examples at section Building the HDL project and the default modes for each project.

Note

The parameters for Rx or Tx links can be changed from the system_project.tcl file, located in hdl/projects/ad9084_ebz/$CARRIER/system_project.tcl

Important

For JESD204B:

\[Lane Rate = \frac{IQ Sample Rate * M * NP * \frac{10}{8}}{L}\]

For JESD204C:

\[Lane Rate = \frac{IQ Sample Rate * M * NP * \frac{66}{64}}{L}\]

The following are the parameters of this project that can be configured:

  • JESD_MODE: used link layer encoder mode

    • 64B66B - 64b66b link layer defined in JESD204C, uses ADI IP as Physical Layer (except for Versal / Intel)

    • 8B10B - 8b10b link layer defined in JESD204B, uses ADI IP as Physical Layer

  • HSCI_ENABLE: enables the HSCI IP (Xilinx only)

  • ASYMMETRIC_A_B_MODE: enables the asymmetric A/B mode where each Apollo side has a separate JESD link (Xilinx only)

  • RX_LANE_RATE: lane rate of the Rx link (MxFE to FPGA) (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • TX_LANE_RATE: lane rate of the Tx link (FPGA to MxFE) (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • REF_CLK_RATE: the rate of the reference clock (Versal and Intel only)

  • DEVICE_CLK_RATE: the rate of the device clock (Intel only)

  • [RX/TX]_JESD_M: number of converters per link (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • [RX/TX]_JESD_L: number of lanes per link (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • [RX/TX]_JESD_S: number of samples per frame (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • [RX/TX]_JESD_NP: number of bits per sample (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • [RX/TX]_NUM_LINKS: number of links (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • [RX/TX]_KS_PER_CHANNEL: Number of samples stored in internal buffers in kilosamples per converter (M) (A or A&B link if ASYMMETRIC_A_B_MODE = 0)

  • RX_B_LANE_RATE: lane rate of the Rx link (MxFE to FPGA) (B link)

  • TX_B_LANE_RATE: lane rate of the Tx link (FPGA to MxFE) (B link)

  • [RX/TX]_B_JESD_M: number of converters per link (B link)

  • [RX/TX]_B_JESD_L: number of lanes per link (B link)

  • [RX/TX]_B_JESD_S: number of samples per frame (B link)

  • [RX/TX]_B_JESD_NP: number of bits per sample (B link)

  • [RX/TX]_B_NUM_LINKS: number of links (B link)

  • [RX/TX]_B_KS_PER_CHANNEL: Number of samples stored in internal buffers in kilosamples per converter (M) (B link)

Clock scheme

The clock sources depend on the carrier that is used:

VCU118

AD9084-EBZ VCU118 clock scheme

Limitations

Warning

For the parameter selection, the following restrictions apply:

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Depending on the values of parameters $ASYMMETRIC_A_B_MODE, $ADI_PHY_SEL and $HSCI_ENABLE, some IPs are instatiated and some are not.

Check-out the table below to find out the conditions.

Instance

Depends on parameter

Microblaze

ZynqMP

apollo_rx_xcvr

$ADI_PHY_SEL==1

0x44A6_0000

N/A

apollo_rx_jesd

0x44A9_0000

0xA4A9_0000

rx_apollo_tpl_core

0x44A1_0000

0xA4A1_0000

apollo_rx_dma

0x7C42_0000

0xBC42_0000

apollo_rx_data_offload

0x7C45_0000

0xBC45_0000

apollo_rx_b_xcvr

$ADI_PHY_SEL==1 & $ASYMMETRIC_A_B_MODE==1

0x44AA_0000

N/A

apollo_rx_b_jesd

$ASYMMETRIC_A_B_MODE==1

0x44AC_0000

0xA4AC_0000

rx_b_apollo_tpl_core

$ASYMMETRIC_A_B_MODE==1

0x44AB_0000

0xA4AB_0000

apollo_rx_b_dma

$ASYMMETRIC_A_B_MODE==1

0x7C47_0000

0xBC47_0000

apollo_rx_b_data_offload

$ASYMMETRIC_A_B_MODE==1

0x7C4A_0000

0xBC4A_0000

apollo_tx_xcvr

$ADI_PHY_SEL==1

0x44B6_0000

N/A

apollo_tx_jesd

0x44B9_0000

0xA4B9_0000

tx_apollo_tpl_core

0x44B1_0000

0xA4B1_0000

apollo_tx_dma

0x7C43_0000

0xBC43_0000

apollo_tx_data_offload

0x7C44_0000

0xBC44_0000

apollo_tx_b_xcvr

$ADI_PHY_SEL==1 & $ASYMMETRIC_A_B_MODE==1

0x44BA_0000

N/A

apollo_tx_b_jesd

$ASYMMETRIC_A_B_MODE==1

0x44BC_0000

0xA4BC_0000

tx_b_apollo_tpl_core

$ASYMMETRIC_A_B_MODE==1

0x44BB_0000

0xA4BB_0000

apollo_tx_b_dma

$ASYMMETRIC_A_B_MODE==1

0x7C48_0000

0xBC48_0000

apollo_tx_b_data_offload

$ASYMMETRIC_A_B_MODE==1

0x7C49_0000

0xBC44_0000

axi_hsci

$HSCI_ENABLE==1

0x7C50_0000

0xBC50_0000

axi_hsci_clkgen

$HSCI_ENABLE==1

0x44AD_0000

0xA4AD_0000

axi_spi_2

0x44A8_0000

0xA4A8_0000

For the Intel carriers, only a part of the CPU interrupts are specified, as the rest depend on the values of $TX_NUM_OF_LANES (see projects/ad9084_ebz/common/ad9084_ebz_qsys.tcl for more details).

Instance

Intel

apollo_rx_jesd204.link_reconfig

0x000C_0000

apollo_rx_jesd204.link_management

0x000C_4000

apollo_tx_jesd204.link_reconfig

0x000C_8000

apollo_tx_jesd204.link_management

0x000C_C000

apollo_rx_tpl.s_axi

0x000D_2000

apollo_tx_tpl.s_axi

0x000D_4000

apollo_rx_dma.s_axi

0x000D_8000

apollo_tx_dma.s_axi

0x000D_C000

apollo_gpio.s1

0x000E_0000

apollo_spi.spi_control_port

0x000E_A000

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PS

spi0

ADF4382

0

PS

spi0

HMC7044

1

PL

axi_spi_2

AD9084

0

GPIOs

The following table lists the GPIO signals used in this project that are connected to the Apollo evaluation board and are common between all the carriers.

Apollo GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

Software GPIO

(from FPGA view)

Microblaze

ZynqMP

resetb

OUT

62

62

30

trig_b[1:0]

OUT

61:60

61:60

29:28

trig_a[1:0]

OUT

59:58

59:58

27:26

trig_in

IN

53

53

21

aux_gpio

INOUT

48

48

16

gpio[30:15]

INOUT

47:32

47:32

15:0

The following table lists the GPIO signals that are only present in the Versal projects.

They are used from the linux kernel to control the reset sequence of the GTY/GTYP transceivers.

Versal transceivers GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

ZynqMP

tx_reset_datapath

IN

71

39

rx_reset_datapath

IN

70

38

tx_reset_pll_and_datapath

IN

69

37

rx_reset_pll_and_datapath

IN

68

36

gt_reset

IN

67

35

mst_resetdone

OUT

66

34

tx_resetdone

OUT

65

33

rx_resetdone

OUT

64

32

tx_b_reset_datapath

IN

79

47

rx_b_reset_datapath

IN

78

46

tx_b_reset_pll_and_datapath

IN

77

45

rx_b_reset_pll_and_datapath

IN

76

44

gt_b_reset

IN

75

43

mst_b_resetdone

OUT

74

42

tx_b_resetdone

OUT

73

41

rx_b_resetdone

OUT

72

40

The following table lists the GPIOs that are only preset on the Intel carriers.

Intel GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

ZynqMP

tx_fifo_bypass_bypass

IN

63

31

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Microblaze

Linux ZynqMP

axi_apollo_rx_dma

13

13

97

axi_apollo_tx_dma

12

12

96

axi_apollo_rx_jesd

11

11

95

axi_apollo_tx_jesd

10

10

94

axi_spi_2

9

9

93

axi_apollo_rx_b_dma

4

4

88

axi_apollo_tx_b_dma

3

3

87

axi_apollo_rx_b_jesd

2

2

86

axi_apollo_tx_b_jesd

1

1

85

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.

Then go to the projects/ad9084_ebz location and run the make command by typing in you command prompt:

Example for building the project with parameters:

Linux/Cygwin/WSL

~$
cd hdl/projects/ad9084_ebz/vck190
~/hdl/projects/ad9084_ebz/vck190$
make RX_LANE_RATE=2.5 TX_LANE_RATE=2.5     \
     RX_JESD_L=8 RX_JESD_M=4 RX_JESD_S=1   \
     RX_JESD_NP=16 TX_JESD_L=8 TX_JESD_M=4 \
     TX_JESD_S=1 TX_JESD_NP=16

The following dropdowns contain tables with the parameters that can be used to configure this project, depending on the carrier used. Where a cell contains a — (dash) it means that the parameter doesn’t exist for that project (ad9084_ebz/$carrier).

Warning

For the parameter selection, the following restrictions apply:

NP notation is equivalent with N'

Parameter

Default value of the parameters

FM87

VCU118

VCK190

VPK180

JESD_MODE

64B66B

64B66B

64B66B

64B66B

HSCI_ENABLE

-

1

1*

1*

REF_CLK_RATE*

312.5

—

312.5

312.5

DEVICE_CLK_RATE**

312.5

—

—

—

RX_LANE_RATE

20.625

20.625

20.625

20.625

TX_LANE_RATE

20.625

20.625

20.625

20.625

RX_JESD_M

4

4

4

4

RX_JESD_L

8

8

4

4

RX_JESD_S

1

1

1

1

RX_JESD_NP

16

16

16

16

RX_NUM_LINKS

2

1

2

2

TX_JESD_M

4

4

4

4

TX_JESD_L

8

8

4

4

TX_JESD_S

1

1

1

1

TX_JESD_NP

16

16

16

16

TX_NUM_LINKS

2

1

2

2

RX_KS_PER_CHANNEL

16

32

64

64

TX_KS_PER_CHANNEL

16

32

64

64

ASYMMETRIC_A_B_MODE

-

1

0

0

RX_B_LANE_RATE

-

20.625

20.625

20.625

TX_B_LANE_RATE

-

20.625

20.625

20.625

RX_B_JESD_M

-

4

4

4

RX_B_JESD_L

-

8

4

4

RX_B_JESD_S

-

1

1

1

RX_B_JESD_NP

-

16

16

16

TX_B_JESD_M

-

4

4

4

TX_B_JESD_L

-

8

4

4

TX_B_JESD_S

-

1

1

1

TX_B_JESD_NP

-

16

16

16

RX_B_KS_PER_CHANNEL

-

32

64

64

TX_B_KS_PER_CHANNEL

-

32

64

64

ADC_DO_MEM_TYPE

—

—

—

—

DAC_DO_MEM_TYPE

—

—

— | —

Legend

- — this feature is not supported

* — can be disabled

The result of the build, if parameters were used, will be in a folder named by the configuration used:

if the following command was run

make RX_LANE_RATE=2.5 TX_LANE_RATE=2.5 RX_JESD_L=8 RX_JESD_M=4 RX_JESD_S=1 RX_JESD_NP=16 TX_JESD_L=8 TX_JESD_M=4 TX_JESD_S=1 TX_JESD_NP=16

then the folder name will be:

RXRATE2_5_TXRATE2_5_RXL8_RXM4_RXS1_RXNP16_TXL8_TXM4_TXS1_TXNP16 because of truncation of some keywords so the name will not exceed the limits of the Operating System (JESD, LANE, etc. are removed) of 260 characters.

A more comprehensive build guide can be found in the Build an HDL project user guide.

Software considerations

ADC - crossbar config

Due to physical constraints, Rx lanes are reordered as described in the following table.

e.g physical lane 2 from ADC from A side connects to logical lane 1 from the VCU118. Therefore the crossbar from the device must be set accordingly.

ADC A phy Lane

VCU118

VCK190 / VPK180

FM87

0

7

5

11

1

5

1

9

2

1

3

8

3

2

7

10

4

11

N/C

7

5

3

N/C

3

6

8

N/C

1

7

9

N/C

5

8

10

N/C

N/C

9

6

N/C

N/C

10

4

N/C

N/C

11

0

N/C

N/C

ADC B phy Lane

VCU118

VCK190 / VPK180

FM87

0

10

1

11

1

6

7

9

2

4

10

8

3

0

3

5

4

3

N/C

3

5

2

N/C

10

6

5

N/C

7

7

7

N/C

1

8

8

N/C

N/C

9

1

N/C

N/C

10

11

N/C

N/C

11

9

N/C

N/C

DAC - crossbar config

Due to physical constraints, Tx lanes are reordered as described in the following table.

e.g physical lane 2 from DAC from A side connects to logical lane 9 from the VCU118. Therefore the crossbar from the device must be set accordingly.

DAC A phy Lane

VCU118

VCK190 / VPK180

FM87

0

10

11

2

1

8

3

1

2

9

8

5

3

11

9

7

4

5

N/C

9

5

1

N/C

8

6

3

N/C

3

7

7

N/C

11

8

4

N/C

N/C

9

6

N/C

N/C

10

2

N/C

N/C

11

0

N/C

N/C

DAC B phy Lane

VCU118

VCK190 / VPK180

FM87

0

4

3

9

1

6

2

11

2

2

5

1

3

0

7

8

4

1

N/C

7

5

7

N/C

5

6

10

N/C

2

7

3

N/C

3

8

5

N/C

N/C

9

8

N/C

N/C

10

9

N/C

N/C

11

11

N/C

N/C

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.