CN0540 HDL project

Overview

The HDL reference design for the CN0540 provides a high resolution, wide-bandwidth, high dynamic range, Integrated Electronics Piezoelectric (IEPE) compatible interface data acquisition system (DAQ) for interfacing with Integrated Circuit Piezo (ICP)/IEPE piezo vibration sensors. Most solutions which interface with piezo sensors in the market are AC coupled, lacking DC and sub-hertz measurement capability. This reference design is a DC coupled solution in which DC and sub-hertz precision are achieved. By looking at the complete data set from the vibration sensor in the frequency domain (DC - 50 kHz), the type and source of a machine fault can be better predicted using the; position, amplitude and number of harmonics found in the FFT spectrum.

The data acquisition board incorporates a precision 24-bit, 1024kSPS Sigma-delta ADC AD7768-1 and a 16-bit voltage output DAC LTC2606. Used as the ADC driver is a high linearity FDA ADA4945-1 and a 200mA programmable 2-terminal current source LT3092. Analog input protection is provided by the switch ADG5421F.

This project has a SPI Engine instance to control and acquire data from the AD7768-1 24-bit precision ADC. This instance provides support for capturing continuous samples at the maximum sample rate.

Supported boards

Supported devices

Supported carriers

Block design

Block diagram

The data path and clock domains are depicted in the below diagram:

CN0540_ARDZ block diagram

Jumper setup

Jumper/Solder link

Default Position

Description

P10

Inserted

Connects the power source to the circuit and may be removed for testing without a power source

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Zynq*/DE10-Nano**

axi_iic_ard*

0x4160_0000

spi_cn0540_axi_regmap*

0x44A0_0000

axi_cn0540_dma*

0x44A3_0000

xadc_in*

0x44A5_0000

spi_clkgen*

0x44A7_0000

axi_dmac_0**

0x0002_0000

axi_spi_engine_0**

0x0003_0000

Legend

  • * instantiated only for Cora Z7S

  • ** instantiated only for DE10-Nano

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

axi_iic

axi_iic_cn0540

0x4160_0000

LTC2606

PS

i2c1

sys_hps_i2c1

—

—

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PL

axi_spi_engine

cn0540

0

GPIOs

The Software GPIO number is calculated as follows:

  • Cora Z7S: the offset is 54

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

cn0540_shutdown

INOUT

40

94

cn0540_reset_adc

INOUT

39

93

cn0540_csb_aux

INOUT

38

92

cn0540_sw_ff

INOUT

37

91

cn0540_drdy_aux

INOUT

36

90

cn0540_blue_led

INOUT

35

89

cn0540_yellow_led

INOUT

34

88

cn0540_sync_in

INOUT

33

87

cn0540_drdy

INOUT

32

86

  • DE10-Nano: the offset is 32

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

DE10-Nano

ltc2308_cs

OUT

41

9

cn0540_blue_led

OUT

40

8

cn0540_yellow_led

OUT

39

7

cn0540_sw_ff

IN

38

6

cn0540_shutdown

OUT

36

4

cn0540_drdy_aux

OUT

35

3

cn0540_csb_aux

OUT

34

2

cn0540_sync_in

OUT

33

1

cn0540_reset_adc

OUT

32

0

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Zynq

Actual Zynq

axi_cn0540_dma

13

57

89

spi_cn0540

12

56

88

axi_iic_ard

11

55

87

Instance name

HDL

Linux DE10-Nano

Actual DE10-Nano

axi_spi_engine_0

5

45

77

axi_dmac_0

4

44

76

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/cn0540/coraz7s
~/hdl/projects/cn0540/coraz7s$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.