PULSAR-LVDS-ADC HDL project

Overview

The AD7625, AD7626, AD7960, AD7961 devices are parts from ADC LVDS PulSAR family. The AD7625 / AD7626 is a 16-bit, 6 MSPS / 10 MSPS, charge redistribution successive approximation register (SAR) architecture, analog to-digital converter (ADC). SAR architecture allows unmatched performance both in noise (92dB SNR) and in linearity (±1 LSB INL / ±0.45 LSB INL). The AD7626 contains a high speed 16-bit sampling ADC, an internal conversion clock, and an internal buffered reference. On the CNV edge, it samples the voltage difference between IN+ and IN- pins. The voltages on these pins swing in opposite phase between 0 V and REF.

The 4.096V reference voltage, REF, can be generated internally or applied externally. All converted results are available on a single LVDS self-clocked or echoed-clock serial interface reducing external hardware connections. The AD7625 / AD7626 is available in a 32-lead LFCSP (5mm by 5mm) with operation specified from -40°C to +85°C.

The AD7960 / AD7961 is an 18-bit/16-bit, 5 MSPS, charge redistribution successive approximation (SAR), analog-to-digital converter (ADC). The SAR architecture allows unmatched performance both in noise and in linearity. The AD7960 / AD7961 contains a low power, high speed, 18-bit/16-bit sampling ADC, an internal conversion clock, and an internal reference buffer.

On the CNV± edge, the AD7960 / AD7961 samples the voltage difference between the IN+ and IN− pins. The voltages on these pins swing in opposite phase between 0 V and 4.096 V and between 0 V and 5 V. The reference voltage is applied to the part externally. All conversion results are available on a single LVDS self clocked or echoed clock serial interface. The AD7960 is available in a 32-lead LFCSP (QFN) with operation specified from −40°C to +85°C.

Applications:

  • Digital imaging systems

  • High speed data acquisition

  • High dynamic range telecommunications receivers

  • Spectrum analysis

  • Test equipment

Supported boards

Supported devices

Supported carriers

Block design

Block diagram

The data path and clock domains are depicted in the below diagram:

PulSAR LVDS ADC block diagram

Configuration modes

The RESOLUTION_16_18N configuration parameter defines the resolution of the ADC (16 or 18 bits). By default it is set to 0. Depending of the project, some hardware modifications need to be done on the board and/or make command:

In case of the AD7960 project:

~$
make RESOLUTION_16_18N=0

In case of the AD7625/AD7626/AD7961 project:

~$
make RESOLUTION_16_18N=1

Jumper setup AD7625/AD7626

Jumper/Solder link

Default Position

Description

LK2

Inserted

Connects REFIN to the 1.2V external reference.

LK3

Inserted

Connects the 4.096 V output from the ADR4540 after buffer AD8031 solution.

LK6

B

Connects the output of the VCM buffer to the VCM of the amplifier.

LK9

A

Connects to the 7 V supply coming from the ADP7102.

LK10

A

Connects to the −2.5 V coming from the ADP2300.

JP1,JP2

B

Connects CNV+ and CNV− from the FPGA.

JP6

B

Connects 7 V to amplifier +VS.

JP10

B

Connects −2.5 V to amplifier −VS.

JP11,JP12

B

Connect outputs from the ADA4899-1 to the inputs of the ADC.

JP13,JP14

B

Connect outputs from the ADA4899-1 to the inputs of the ADC.

Jumper setup AD7960/AD7961

Jumper/Solder link

Default Position

Description

LK2,LK3

Inserted

Option to use external amplifier supplies + VS and – VS.

LK4

Inserted

Connects to +7 V coming from ADP7102.

LK5

B

Connects to −2.5 V coming from ADP2300.

LK6

B

Connects the output of VCM buffer to VCM of amplifier.

LK7

B

Connects the +5 V output from ADR4550 to REF buffer AD8031.

JP1,JP2

B

Connects analog inputs VIN+ and VIN− to the inputs of the ADC driver. ADA4899-1 or ADA4897-1.

JP3,JP4

B

Connect outputs from ADA4899-1 to inputs of AD7960.

JP5

A

Connect the VCM output from AD7960 to AD8031.

JP7

A

Connects REFIN to 2.048 V external reference.

JP8

B

Connects +7 V to amplifier +VS.

JP9

B

Connects −2.5 V to amplifier −VS.

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Zynq

axi_pulsar_lvds

0x44A0_0000

axi_pulsar_lvds_dma

0x44A3_0000

axi_pwm_gen

0x44A6_0000

reference_clkgen

0x44A8_0000

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

iic_fmc

axi_iic_fmc

0x4162_0000

—

PL

iic_main

axi_iic_main

0x4160_0000

—

GPIOs

The Software GPIO number is calculated as follows:

  • Zynq-7000: if PS7 is used, then offset is 54

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

en3_fmc **

INOUT

35

89

en2_fmc **

INOUT

34

88

en1_fmc

INOUT

33

87

en0_fmc

INOUT

32

86

Legend

  • ** instantiated only for AD7960/AD7961

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Zynq

Actual Zynq

axi_ad7616_dma

13

57

89

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/pulsar_lvds_adc/zed
~/hdl/projects/pulsar_lvds_adc/zed$
make RESOLUTION_16_18N=0

The result of the build, if parameters were used, will be in a folder named by the configuration used:

if the following command was run

make RESOLUTION_16_18N=0

then the folder name will be:

RESOLUTION_16_18N0

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.