AXI ADRV9001

?axi_adrv9001 IP-XACT not found.Generate it and the documentation:(cd library/axi_adrv9001; make)(cd docs; make html)

The AXI ADRV9001 IP Core can be used to interface the ADRV9001 family, meaning:

This documentation only covers the IP core and requires that one must be familiar with the device for a complete and better understanding.

More about the generic framework interfacing ADCs that contains the up_adc_channel and up_adc_common modules can be read in Generic AXI ADC. Regarding the DAC, more information related to its generic framework can be found at Generic AXI DAC.

Features

  • AXI-based configuration

  • Supports both Altera and AMD Xilinx devices

  • LVDS and CMOS synchronous data interface options

  • PRBS monitoring

  • DC filtering

  • IQ correction

  • Programmable line delays (AMD)

  • Receive and transmit loop backs

  • Internal DDS

  • DAC selectable input source: DDS/DMA/ADC/TEST_RAMP

Files

Name

Description

library/axi_adrv9001/adrv9001_aligner4.v

Verilog source for 4-port aligner.

library/axi_adrv9001/adrv9001_aligner8.v

Verilog source for 8-port aligner.

library/axi_adrv9001/adrv9001_pack.v

Verilog source packing two input beats into one.

library/axi_adrv9001/adrv9001_rx_link.v

Verilog source for the RX Link.

library/axi_adrv9001/adrv9001_rx.v

Verilog source for the RX Serdes Interface.

library/axi_adrv9001/adrv9001_tx_link.v

Verilog source for the TX Link.

library/axi_adrv9001/adrv9001_tx.v

Verilog source for the TX Serdes Interface.

library/axi_adrv9001/axi_adrv9001_core.v

Verilog source for the AXI ADRV9001 core.

library/axi_adrv9001/axi_adrv9001_if.v

Verilog source for the ADRV9001 interface module.

library/axi_adrv9001/axi_adrv9001_rx_channel.v

Verilog source for the ADRV9001 RX channel.

library/axi_adrv9001/axi_adrv9001_rx.v

Verilog source for the AXI ADRV9001 RX Interface.

library/axi_adrv9001/axi_adrv9001_tdd.v

Verilog source for the Transceiver TDD Control.

library/axi_adrv9001/axi_adrv9001_tx_channel.v

Verilog source for the ADRV9001 TX channel.

library/axi_adrv9001/axi_adrv9001_tx.v

Verilog source for the AXI ADRV9001 TX Interface.

library/axi_adrv9001/axi_adrv9001.v

Verilog source for the AXI ADRV9001.

library/axi_adrv9001/axi_adrv9001_ip.tcl

TCL script to generate the Vivado IP-integrator project.

Block diagram

AXI ADRV9001 block diagram

Functional Description

The axi_adrv9001 core’s architecture contains:

Physical Interface

The following operation modes are supported by the physical layer (PHY). CMOS (CSSI) and LVDS (LSSI) selection is done through a synthesis parameter. Other parameters (column B, G, H) can be modified at run time, preferably while the core is in reset.

A

B

C

D

E

F

G

H

CSSI 1-lane

1

32

80

80

2.5

SDR

8

CSSI 1-lane

1

32

160

80

5

DDR

4

CSSI 1-lane [1]

1

16

80

80

—

SDR

4

CSSI 1-lane [1]

1

16

160

80

—

DDR

2

CSSI 1-lane [2]

1

8

80

80

—

SDR

2

CSSI 1-lane [2]

1

8

160

80

—

DDR

1

CSSI 4-lane

4

8

80

80

10

SDR

2

CSSI 4-lane

4

8

160

80

20

DDR

1

LSSI 1-lane

1

32

983.04

491.52

30.72

DDR

4

LSSI 2-lane

2

16

983.04

491.52

61.44

DDR

2

Columns description:

  • A - SSI Modes

  • B - Data Lanes Per Channel

  • C - Serialization factor Per data lane

  • D - Max data lane rate (MHz)

  • E - Max Clock rate (MHz)

  • F - Max Sample Rate for I/Q (MHz)

  • G - Data Type

  • H - User Interface Clock to Sample Clock ratio (aka DDS Rate) for Xilinx devices

The following equations apply:

\[MaxDataLaneRate = \frac{MaxSampleRateForIQ*16*2}{DataLanesPerChannel}\]
\[MaxClockRate = \frac{MaxDataLaneRate} {1+(DataType = DDR)}\]
\[UserInterfaceClock = \frac{MaxClockRate} {InternalDivider}\]
\[UserInterfaceClock = \frac{MaxSampleRateForIQ*32}{DataLanesPerChannel*(1+(DataType = DDR))*InternalDivider}\]
\[DDS rate = \frac{32} {DataLanesPerChannel*(1+(DataType = DDR))*InternalDivider}\]

Where:

  • MaxDataLaneRate - number of bits transferred in a second per active lane

  • MaxClockRate - the source-synchronous interface clock frequency

  • UserInterfaceClock - the frequency of the clock the user interface logic is connected

  • InternalDivider - the division factor with which the source-synchronous interface clock is divided, to get the user interface clock. This is implementation-specific. Xilinx CMOS and LVDS = 4; Intel CMOS = 1

Since the UserInterfaceClock (column H) is an integer multiple of the MaxSampleRateForIQ, the interface towards the user logic has a valid qualifier which is not active on every clock cycle.

Requirements

  • Rx1 clock and Rx2 clock should be length matched

  • Clock and data in SSI interface must be length matched

Xilinx Physical interface

RX Component mode

For Rx interfaces, the source-synchronous associated clock is used to sample the input data. Software configuration is required, which is described in Configure ADC common interface section. Input delays of the FPGA or output delays of the ADRV9001 can be tuned by software for optimized sampling.

../../_images/rxcomponentmodephy.svg

TX Using dedicated clock

For Tx interfaces, the clock received from the transceiver is used to drive the output data. Software configuration is required for clock rate selection, which is described in Configure DAC common interface section. Input delays of the ADRV9001 can be tuned by software for optimized sampling.

../../_images/txcomponentmodephy.svg

Configure DAC common interface

Register 0x0048 REG_CNTRL_2

  • [12:8] - NUM_LANES (new) - number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane)

  • [14] - SYMB_8_16B (new) - select number of bits for symbol format mode (1 represents 8b, 0 represents 16b)

  • [15] - SYMB_OP (new) - select symbol data format mode

  • [16] - SDR_DDR_N (new) - interface type (1 represents SDR, 0 represents DDR)

Register 0x04c REG_RATECNTRL

  • [7:0] RATE - must be set according to column H of the table

Configure ADC common interface

Register 0x0044 REG_CNTRL

  • [12:8] - NUM_LANES (new) - number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane)

  • [14] - SYMB_8_16B (new) - select number of bits for symbol format mode (1 represents 8b, 0 represents 16b)

  • [15] - SYMB_OP (new) - select symbol data format mode

  • [16] - SDR_DDR_N (new) - interface type ( 1 represents SDR, 0 represents DDR)

Configuration Parameters

Name

Description

ID

Core ID should be unique for each IP in the system

CMOS_LVDS_N

Defines the physical interface type, set 1 for CMOS and 0 for LVDS

TDD_DISABLE

By setting this parameter, the TDD control will not be implemented in the core

DDS_DISABLE

If resource utilization is a concern, by setting this parameter you can remove the dual tone DDS logic from the Tx channels. This will reduce resource utilization significantly, but will lose the ability to generate a test tone

INDEPENDENT_1R1T_SUPPORT

0 - Rx2 (adc_2_*) and Tx2 (dac_2_*) data channels will be disabled; RX2 TPL, TX2 TPL cores are disabled. 1 - Allows independent control of Rx2/Tx2 PHY either from Rx12/Tx12 TPL or Rx2/Tx2 TPL blocks;

COMMON_2R2T_SUPPORT

0 - puts the Rx12/Tx12 TPL in R1_MODE, having access only to Rx1/Tx1 PHYs; 1 - Allows Rx12/Tx12 TPL to operate in 2R 2T mode having control over Rx2/Tx2 PHY

DISABLE_RX1_SSI

Setting this parameter disables RX1 interface, PHY Link and TPL

DISABLE_RX2_SSI

Setting this parameter disables RX2 interface, PHY Link and TPL

DISABLE_TX1_SSI

Setting this parameter disables TX1 interface, PHY Link and TPL

DISABLE_TX2_SSI

Setting this parameter disables TX2 interface, PHY Link and TPL

RX_USE_BUFG

Used in case of Xilinx 7 series devices; If set, will insert a global clock buffer on the Rx clock path. Useful if user logic does not fit in a clock region

TX_USE_BUFG

Used in case of Xilinx 7 series devices; If set, will insert a global clock buffer on the Tx clock path. Useful if user logic does not fit in a clock region

USE_RX_CLK_FOR_TX1

Select the clock to drive the TX1 SSI interface 0 = TX1 dedicated clock 1 = RX1 SSI clock 2 = RX2 SSI clock

USE_RX_CLK_FOR_TX2

Select the clock to drive the TX2 SSI interface 0 = TX2 dedicated clock 1 = RX1 SSI clock 2 = RX2 SSI clock

EXT_SYNC

DAC channel sync 1 = external or 0 = internal

IO_DELAY_GROUP

The delay group name which is set for the delay controller

FPGA_TECHNOLOGY

Auto populated by IPI

FPGA_FAMILY

Auto populated by IPI

SPEED_GRADE

Auto populated by IPI

DEV_PACKAGE

Auto populated by IPI

Interface

Note

There are two ADC interfaces, composed of enable, valid, data and underflow signals. For simplicity, we will look only at the data part:

  • * - adc_1_data_i0/adc_1_data_i1

  • * - adc_2_data_i

Name

Description

rx1_dclk_in_n_NC

rx1 CMOS - NC or LVDS - input clock N

rx1_dclk_in_p_dclk_in

rx1 CMOS or LVDS - input clock P

rx1_idata_in_n_idata0

rx1 CMOS - I data 0 or LVDS - I data N

rx1_idata_in_p_idata1

rx1 CMOS - I data 1 or LVDS - I data P

rx1_qdata_in_n_qdata2

rx1 CMOS - Q data 2 or LVDS - Q data N

rx1_qdata_in_p_qdata3

rx1 CMOS - Q data 3 or LVDS - Q data P

rx1_strobe_in_n_NC

rx1 CMOS - NC or LVDS - input strobe N

rx1_strobe_in_p_strobe_in

rx1 CMOS - strobe or LVDS - input strobe P

rx2_dclk_in_n_NC

rx2 CMOS - NC or LVDS - input clock N

rx2_dclk_in_p_dclk_in

rx2 CMOS or LVDS - input clock P

rx2_idata_in_n_idata0

rx2 CMOS - I data 0 or LVDS - I data N

rx2_idata_in_p_idata1

rx2 CMOS - I data 1 or LVDS - I data P

rx2_qdata_in_n_qdata2

rx2 CMOS - Q data 2 or LVDS - Q data N

rx2_qdata_in_p_qdata3

rx2 CMOS - Q data 3 or LVDS - Q data P

rx2_strobe_in_n_NC

rx2 CMOS - NC or LVDS - input strobe N

rx2_strobe_in_p_strobe_in

rx2 CMOS - strobe or LVDS - input strobe P

tx1_dclk_in_n_NC

tx1 CMOS - NC or LVDS - input clock N

tx1_dclk_in_p_dclk_in

tx1 CMOS or LVDS - input clock P

tx1_dclk_out_n_NC

tx1 CMOS - NC or LVDS - output clock N

tx1_dclk_out_p_dclk_out

tx1 CMOS or LVDS - output clock P

tx1_idata_out_n_idata0

tx1 CMOS - I data 0 or LVDS - I data N

tx1_idata_out_p_idata1

tx1 CMOS - I data 1 or LVDS - I data P

tx1_qdata_out_n_qdata2

tx1 CMOS - Q data 2 or LVDS - Q data N

tx1_qdata_out_p_qdata3

tx1 CMOS - Q data 3 or LVDS - Q data P

tx1_strobe_out_n_NC

tx1 CMOS - NC or LVDS - output strobe N

tx1_strobe_out_p_strobe_out

tx1 CMOS - strobe or LVDS - output strobe P

tx2_dclk_in_n_NC

tx2 CMOS - NC or LVDS - input clock N

tx2_dclk_in_p_dclk_in

tx2 CMOS or LVDS - input clock P

tx2_dclk_out_n_NC

tx2 CMOS - NC or LVDS - output clock N

tx2_dclk_out_p_dclk_out

tx2 CMOS or LVDS - output clock P

tx2_idata_out_n_idata0

tx2 CMOS - I data 0 or LVDS - I data N

tx2_idata_out_p_idata1

tx2 CMOS - I data 1 or LVDS - I data P

tx2_qdata_out_n_qdata2

tx2 CMOS - Q data 2 or LVDS - Q data N

tx2_qdata_out_p_qdata3

tx2 CMOS - Q data 3 or LVDS - Q data P

tx2_strobe_out_n_NC

tx2 CMOS - NC or LVDS - output strobe N

tx2_strobe_out_p_strobe_out

tx2 CMOS - strobe or LVDS - output strobe P

adc_1_rst

Channel reset signal

adc_1_enable_i*

If set, the channel 0 or 1, I component is enabled

adc_1_valid_i*

Indicates valid data at the channel 0 or 1, I component

adc_1_data_i*

Received data output for channel 0 or 1, I component

adc_1_enable_q*

If set, the channel 0 or 1, Q component is enabled

adc_1_valid_q*

Indicates valid data at the channel 0 or 1, Q component

adc_1_data_q*

Received data output for channel 0 or 1, Q component

adc_1_dovf

Data overflow, signal comming from pack

adc_2_rst

Channel reset signal

adc_2_enable_i*

If set, the channel 1, I/Q component is enabled - used only if r1_mode is disabled

adc_2_valid_i*

Indicates valid data at the channel 1, I/Q component - used only if r1_mode is disabled

adc_2_data_i*

Received data output for channel 1, Q component - used only if r1_mode is disabled

adc_2_enable_q*

If set, the channel 1, I/Q component is enabled - used only if r1_mode is disabled

adc_2_valid_q*

Indicates valid data at the channel 1, I/Q component - used only if r1_mode is disabled

adc_2_data_q*

Received data output for channel 1, Q component - used only if r1_mode is disabled

adc_2_dovf

Data overflow, signal comming from pack

dac_1_rst

Channel reset signal

dac_1_enable_i*

If set, the channel 0, I component is enabled

dac_1_valid_i*

Signals the DAC channel 0, I component, is ready to receive data

dac_1_data_i*

Data input for channel 0, I component

dac_1_enable_q*

If set, the channel 0, Q component is enabled

dac_1_valid_q*

Signals the DAC channel 0, Q component, is ready to receive data

dac_1_data_q*

Data input for channel 0, Q component

dac_1_dunf

Data underflow, signal comming from upack

dac_2_rst

Channel reset signal

dac_2_enable_i*

If set, the channel 1, I/Q component is enabled - used only if r1_mode is disabled

dac_2_valid_i*

Signals the DAC channel 1, I/Q component - is ready to receive data - used only if r1_mode is disabled

dac_2_data_i*

Data input for channel 1, I/Q component - used only if r1_mode is disabled

dac_2_enable_q*

If set, the channel 1, I/Q component is enabled - used only if r1_mode is disabled

dac_2_valid_q*

Signals the DAC channel 1, I/Q component - is ready to receive data - used only if r1_mode is disabled

dac_2_data_q*

Data input for channel 1, I/Q component - used only if r1_mode is disabled

dac_2_dunf

Data underflow, signal comming from upack

gpio_rx1_enable_in

input gpio rx1 enable

gpio_rx2_enable_in

input gpio rx2 enable

gpio_tx1_enable_in

input gpio tx1 enable

gpio_tx2_enable_in

input gpio tx2 enable

rx1_enable

out gpio rx1 enable pin

rx2_enable

out gpio rx2 enable pin

tx1_enable

out gpio tx1 enable pin

tx2_enable

out gpio tx2 enable pin

tdd_sync

SYNC input for frame synchronization in TDD mode

tdd_sync_cntr

SYNC output for frame synchronization in TDD mode

delay_clk

Delay clock input for IO_DELAY control, 200 MHz (7 series) or 300 MHz (Ultrascale)

dac_sync_in

Synchronization signal of the transmit path for slave devices (ID>0)

s_axi

Standard AXI Slave Memory Map interface

Register Map

The register map of the core contains instances of several generic register maps like ADC common, ADC channel, DAC common, DAC channel etc. The following table presents the base addresses of each instance, after that can be found the detailed description of each generic register map.

The absolute address of a register should be calculated by adding the instance base address to the registers relative address. For a more detailed explanation, see ADC register access and DAC register access.

Register Map base addresses for axi_adrv9001

HDL reg

Software reg

Name

Description

0x0000

0x0000

RX1 COMMON

See the ADC Common table for more details

0x0000

0x0000

RX1 CHANNELS

See the ADC Channel table for more details

0x0200

0x0800

RX1 DELAY CONTROL

See the IO Delay Control table for more details

0x0400

0x1000

RX2 COMMON

See the ADC Common table for more details

0x0400

0x1000

RX2 CHANNELS

See the ADC Channel table for more details

0x0600

0x1800

RX2 DELAY CONTROL

See the IO Delay Control table for more details

0x0800

0x2000

TX1 COMMON

See the DAC Common table for more details

0x0800

0x2000

TX1 CHANNELS

See the DAC Channel table for more details

0x1000

0x4000

TX2 COMMON

See the DAC Common table for more details

0x1000

0x4000

TX2 CHANNELS

See the DAC Channel table for more details

0x1200

0x4800

TDD1 CONTROL

See the Transceiver TDD1 Control table for more details

0x1300

0x4C00

TDD2 CONTROL

See the Transceiver TDD2 Control table for more details

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 0x0 VERSION

Version and Scratch Registers

[31:0] VERSION RO 0x00000000

Version number. Unique to all cores.

0x1 0x4 ID

Version and Scratch Registers

[31:0] ID RO 0x00000000

Instance identifier number.

0x2 0x8 SCRATCH

Version and Scratch Registers

[31:0] SCRATCH RW 0x00000000

Scratch register.

0x3 0xc CONFIG

Version and Scratch Registers

[0] IQCORRECTION_DISABLE RO 0x0

If set, indicates that the IQ Correction module was not implemented. (as a result of a configuration of the IP instance)

[1] DCFILTER_DISABLE RO 0x0

If set, indicates that the DC Filter module was not implemented. (as a result of a configuration of the IP instance)

[2] DATAFORMAT_DISABLE RO 0x0

If set, indicates that the Data Format module was not implemented. (as a result of a configuration of the IP instance)

[3] USERPORTS_DISABLE RO 0x0

If set, indicates that the logic related to the User Data Format (e.g. decimation) was not implemented. (as a result of a configuration of the IP instance)

[5] DELAY_CONTROL_DISABLE RO 0x0

If set, indicates that the delay control is disabled for this IP. (as a result of a configuration of the IP instance)

[6] DDS_DISABLE RO 0x0

If set, indicates that the DDS is disabled for this IP. (as a result of a configuration of the IP instance)

[7] CMOS_OR_LVDS_N RO 0x0

CMOS or LVDS mode is used for the interface. (as a result of a configuration of the IP instance)

[8] PPS_RECEIVER_ENABLE RO 0x0

If set, indicates the PPS receiver is enabled. (as a result of a configuration of the IP instance)

[10] USE_RX_CLK_FOR_TX RO 0x1
Indicates that the RXn channel SSI clock is used for TXn SSI clock.
  • 0 = TX0

  • 1 = TX1

[12] EXT_SYNC RO 0x0

If set the transport layer cores (ADC/DAC) have implemented the support for external synchronization signal.

[14] SELECTABLE_CLK RO 0x1

If set indicates that axi_adrv9001 Rx to Tx selectable clock option is available.

0x7 0x1c FPGA_INFO

FPGA device information library/scripts/adi_intel_device_info_enc.tcl (Intel encoded values) library/scripts/adi_xilinx_device_info_enc.tcl (Xilinx encoded values)

[31:24] FPGA_TECHNOLOGY RO 0x00

Encoded value describing the technology/generation of the FPGA device (arria 10/7series)

[23:16] FPGA_FAMILY RO 0x00

Encoded value describing the family variant of the FPGA device(e.g., SX, GX, GT or zynq, kintex, virtex)

[15:8] SPEED_GRADE RO 0x00

Encoded value describing the FPGA’s speed-grade

[7:0] DEV_PACKAGE RO 0x00

Encoded value describing the device package. The package might affect high-speed interfaces

0x10 0x40 RSTN

ADC Interface Control & Status

[0] RSTN RW 0x0

Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core.

0x11 0x44 CNTRL

ADC Interface Control & Status

[16] SDR_DDR_N RW 0x0

Interface type (1 represents SDR, 0 represents DDR)

[15] SYMB_OP RW 0x0

Select symbol data format mode (0x1)

[14] SYMB_8_16B RW 0x0

Select number of bits for symbol format mode (1 represents 8b, 0 represents 16b)

[12:8] NUM_LANES RW 0x00

Number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane). For AD7768, AD7768-4 and AD777x number of active lanes : 1/2/4/8 where supported.

[3] SYNC RW 0x0

Initialize synchronization between multiple ADCs

[2] R1_MODE RW 0x0

Select number of RF channels 1 (0x1) or 2 (0x0).

[1] DDR_EDGESEL RW 0x0

Select rising edge (0x0) or falling edge (0x1) for the first part of a sample (if applicable) followed by the successive edges for the remaining parts. This only controls how the sample is delineated from the incoming data post DDR registers.

[0] PIN_MODE RW 0x0

Select interface pin mode to be clock multiplexed (0x1) or pin multiplexed (0x0). In clock multiplexed mode, samples are received on alternative clock edges. In pin multiplexed mode, samples are interleaved or grouped on the pins at the same clock edge.

0x12 0x48 CNTRL_2

ADC Interface Control & Status

[1] EXT_SYNC_ARM RW 0x0

Setting this bit will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a ADC, and across multiple instances. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

[2] EXT_SYNC_DISARM RW 0x0

Setting this bit will disarm the trigger mechanism sensitive to an external sync signal. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

[8] MANUAL_SYNC_REQUEST RW 0x0

Setting this bit will issue an external sync event if it is hooked up inside the fabric. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

0x15 0x54 CLK_FREQ

ADC Interface Control & Status

[31:0] CLK_FREQ RO 0x00000000

Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock.

0x16 0x58 CLK_RATIO

ADC Interface Control & Status

[31:0] CLK_RATIO RO 0x00000000

Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr).

0x17 0x5c STATUS

ADC Interface Control & Status

[3] PN_ERR RO 0x0

If set, indicates pn error in one or more channels.

[2] PN_OOS RO 0x0

If set, indicates pn oos in one or more channels.

[0] STATUS RO 0x0

Interface status, if set indicates no errors. If not set, there are errors, software may try resetting the cores.

0x22 0x88 UI_STATUS

User Interface Status

[2] UI_OVF RW1C 0x0

User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit.

0x28 0xa0 USR_CNTRL_1

ADC Interface Control & Status

[7:0] USR_CHANMAX RW 0x00

This indicates the maximum number of inputs for the channel data multiplexers. User may add different processing modules post data capture as another input to this common multiplexer. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x100 + 0x10*n 0x400 + 0x40*n CHAN_CNTRLn

ADC Interface Control & Status Where n is from 0 to 15.

[11] ADC_LB_OWR RW 0x0

If set, forces ADC_DATA_SEL to 1, enabling data loopback

[10] ADC_PN_SEL_OWR RW 0x0

If set, forces ADC_PN_SEL to 0x9, device specific pn (e.g. ad9361) If both ADC_PN_TYPE_OWR and ADC_PN_SEL_OWR are set, they are ignored

[9] IQCOR_ENB RW 0x0

if set, enables IQ correction or scale correction. NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1).

[8] DCFILT_ENB RW 0x0

if set, enables DC filter (to disable DC offset, set offset value to 0x0). NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1).

[6] FORMAT_SIGNEXT RW 0x0

if set, enables sign extension (applicable only in 2’s complement mode). The data is always sign extended to the nearest byte boundary. NOT-APPLICABLE if DATAFORMAT_DISABLE is set (0x1).

[5] FORMAT_TYPE RW 0x0

Select offset binary (0x1) or 2’s complement (0x0) data type. This sets the incoming data type and is required by the post processing modules for any data conversion. NOT-APPLICABLE if DATAFORMAT_DISABLE is set (0x1).

[4] FORMAT_ENABLE RW 0x0

Enable data format conversion (see register bits above). NOT-APPLICABLE if DATAFORMAT_DISABLE is set (0x1).

[3] RESERVED RO 0x0

Reserved for backward compatibility.

[3] RESERVED RO 0x0

Reserved for backward compatibility.

[1] ADC_PN_TYPE_OWR RW 0x0

If set, forces ADC_PN_SEL to 0x1, modified pn23 If both ADC_PN_TYPE_OWR and ADC_PN_SEL_OWR are set, they are ignored

[0] ENABLE RW 0x0

If set, enables channel. A 0x0 to 0x1 transition transfers all the control signals to the respective channel processing module. If a channel is part of a complex signal (I/Q), even channel is the master and the odd channel is the slave. Though a single control is used, both must be individually selected.

0x101 + 0x10*n 0x404 + 0x40*n CHAN_STATUSn

ADC Interface Control & Status Where n is from 0 to 15.

[12] CRC_ERR RW1C 0x0

CRC errors. If set, indicates CRC error. Software must first clear this bit before initiating a transfer and monitor afterwards.

[11:4] STATUS_HEADER RO 0x00

The status header sent by the ADC.(compatible with AD7768/AD7768-4/AD777x).

[2] PN_ERR RW1C 0x0

PN errors. If set, indicates spurious mismatches in sync state. This bit is cleared if OOS is set and is only indicates errors when OOS is cleared.

[1] PN_OOS RW1C 0x0

PN Out Of Sync. If set, indicates an OOS status. OOS is set, if 64 consecutive patterns mismatch from the expected pattern. It is cleared, when 16 consecutive patterns match the expected pattern.

[0] OVER_RANGE RW1C 0x0

If set, indicates over range. Note that over range is independent of the data path, it indicates an over range over a data transfer period. Software must first clear this bit before initiating a transfer and monitor afterwards.

0x102 + 0x10*n 0x408 + 0x40*n CHAN_RAW_DATAn

ADC Raw Data Reading Where n is from 0 to 15.

[31:0] ADC_READ_DATA RO 0x00000000

Raw data read from the ADC.

0x104 + 0x10*n 0x410 + 0x40*n CHAN_CNTRLn_1

ADC Interface Control & Status Where n is from 0 to 15.

[31:16] DCFILT_OFFSET RW 0x0000

DC removal (if equipped) offset. This is a 2’s complement number added to the incoming data to remove a known DC offset. NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1).

[15:0] DCFILT_COEFF RW 0x0000

DC removal filter (if equipped) coefficient. The format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if DCFILTER_DISABLE is set (0x1).

0x105 + 0x10*n 0x414 + 0x40*n CHAN_CNTRLn_2

ADC Interface Control & Status Where n is from 0 to 15.

[31:16] IQCOR_COEFF_1 RW 0x0000

IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the scale value and the format is 1.1.14 (sign, integer and fractional bits). If matrix multiplication is used, this is the channel I coefficient and the format is 1.1.14 (sign, integer and fractional bits). If SCALECORRECTION_ONLY is set, this implements the scale value correction for the current channel with the format 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1).

[15:0] IQCOR_COEFF_2 RW 0x0000

IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the offset value and the format is 2’s complement. If matrix multiplication is used, this is the channel Q coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1).

0x106 + 0x10*n 0x418 + 0x40*n CHAN_CNTRLn_3

ADC Interface Control & Status Where n is from 0 to 15.

[19:16] ADC_PN_SEL RW 0x0

Selects the PN monitor sequence type (available only if ADC supports it).

  • 0x0: pn9a (device specific, modified pn9)

  • 0x1: pn23a (device specific, modified pn23)

  • 0x4: pn7 (standard O.150)

  • 0x5: pn15 (standard O.150)

  • 0x6: pn23 (standard O.150)

  • 0x7: pn31 (standard O.150)

  • 0x9: pnX (device specific, e.g. ad9361)

  • 0x0A: Nibble ramp (Device specific e.g. adrv9001)

  • 0x0B: 16 bit ramp (Device specific e.g. adrv9001)

[3:0] ADC_DATA_SEL RW 0x0

Selects the data source to DMA. 0x0: input data (ADC) 0x1: loopback data (DAC)

0x108 + 0x10*n 0x420 + 0x40*n CHAN_USR_CNTRLn_1

ADC Interface Control & Status Where n is from 0 to 15.

[25] USR_DATATYPE_BE RO 0x0

The user data type format- if set, indicates big endian (default is little endian). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[24] USR_DATATYPE_SIGNED RO 0x0

The user data type format- if set, indicates signed (2’s complement) data (default is unsigned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[23:16] USR_DATATYPE_SHIFT RO 0x00

The user data type format- the amount of right shift for actual samples within the total number of bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[15:8] USR_DATATYPE_TOTAL_BITS RO 0x00

The user data type format- number of total bits used for a sample. The total number of bits must be an integer multiple of 8 (byte aligned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[7:0] USR_DATATYPE_BITS RO 0x00

The user data type format- number of bits in a sample. This indicates the actual sample data bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

0x109 + 0x10*n 0x424 + 0x40*n CHAN_USR_CNTRLn_2

ADC Interface Control & Status Where n is from 0 to 15.

[31:16] USR_DECIMATION_M RW 0x0000

This holds the user decimation M value of the channel that is currently being selected on the multiplexer above. The total decimation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[15:0] USR_DECIMATION_N RW 0x0000

This holds the user decimation N value of the channel that is currently being selected on the multiplexer above. The total decimation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 + 0x1*n 0x0 + 0x4*n DELAY_CONTROL_n

Delay Control & Status Where n is from 0 to 15.

[4:0] DELAY_CONTROL_IO_n RW 0x00

Tap value for input/output delay primitive of the n’th interface line. If the delay controller is not locked (indicate issues with delay_clk), the read-back value of this register will be 0xFFFFFFFF. Otherwise will be the last set up value.

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 0x0 VERSION

Version and Scratch Registers

[31:0] VERSION RO 0x00000000

Version number. Unique to all cores.

0x1 0x4 ID

Version and Scratch Registers

[31:0] ID RO 0x00000000

Instance identifier number.

0x2 0x8 SCRATCH

Version and Scratch Registers

[31:0] SCRATCH RW 0x00000000

Scratch register.

0x3 0xc CONFIG

Version and Scratch Registers

[0] IQCORRECTION_DISABLE RO 0x0

If set, indicates that the IQ Correction module was not implemented. (as a result of a configuration of the IP instance)

[1] DCFILTER_DISABLE RO 0x0

If set, indicates that the DC Filter module was not implemented. (as a result of a configuration of the IP instance)

[2] DATAFORMAT_DISABLE RO 0x0

If set, indicates that the Data Format module was not implemented. (as a result of a configuration of the IP instance)

[3] USERPORTS_DISABLE RO 0x0

If set, indicates that the logic related to the User Data Format (e.g. decimation) was not implemented. (as a result of a configuration of the IP instance)

[5] DELAY_CONTROL_DISABLE RO 0x0

If set, indicates that the delay control is disabled for this IP. (as a result of a configuration of the IP instance)

[6] DDS_DISABLE RO 0x0

If set, indicates that the DDS is disabled for this IP. (as a result of a configuration of the IP instance)

[7] CMOS_OR_LVDS_N RO 0x0

CMOS or LVDS mode is used for the interface. (as a result of a configuration of the IP instance)

[8] PPS_RECEIVER_ENABLE RO 0x0

If set, indicates the PPS receiver is enabled. (as a result of a configuration of the IP instance)

[10] USE_RX1_CLK_FOR_TX RO 0x1

If set indicates that the RX1 channel SSI clock is used for TXn ch SSI clock.

[11] USE_RX2_CLK_FOR_TX RO 0x1

If set indicates that the RX2 channel SSI clock is used for TXn ch SSI clock.

[12] EXT_SYNC RO 0x0

If set the transport layer cores (ADC/DAC) have implemented the support for external synchronization signal.

[14] SELECTABLE_CLK RO 0x1

If set indicates that axi_adrv9001 Rx to Tx selectable clock option is available.

0x7 0x1c FPGA_INFO

FPGA device information library/scripts/adi_intel_device_info_enc.tcl (Intel encoded values) library/scripts/adi_xilinx_device_info_enc.tcl (Xilinx encoded values)

[31:24] FPGA_TECHNOLOGY RO 0x00

Encoded value describing the technology/generation of the FPGA device (arria 10/7series)

[23:16] FPGA_FAMILY RO 0x00

Encoded value describing the family variant of the FPGA device(e.g., SX, GX, GT or zynq, kintex, virtex)

[15:8] SPEED_GRADE RO 0x00

Encoded value describing the FPGA’s speed-grade

[7:0] DEV_PACKAGE RO 0x00

Encoded value describing the device package. The package might affect high-speed interfaces

0x10 0x40 RSTN

DAC Interface Control & Status

[0] RSTN RW 0x0

Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core.

0x11 0x44 CNTRL_1

DAC Interface Control & Status

[0] SYNC RW 0x0

Setting this bit synchronizes channels within a DAC, and across multiple instances. This bit self clears.

[1] EXT_SYNC_ARM RW 0x0

Setting this bit will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a DAC, and across multiple instances. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

[2] EXT_SYNC_DISARM RW 0x0

Setting this bit will disarm the trigger mechanism sensitive to an external sync signal. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

[8] MANUAL_SYNC_REQUEST RW 0x0

Setting this bit will issue an external sync event if it is hooked up inside the fabric. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

0x12 0x48 CNTRL_2

DAC Interface Control & Status

[16] SDR_DDR_N RW 0x0

Interface type (1 represents SDR, 0 represents DDR)

[15] SYMB_OP RW 0x0

Select data symbol format mode (0x1)

[14] SYMB_8_16B RW 0x0

Select number of bits for symbol format mode (1 represents 8b, 0 represents 16b)

[12:8] NUM_LANES RW 0x00

Number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane)

[5] R1_MODE RW 0x0

Select number of RF channels 1 (0x1) or 2 (0x0).

[4] DATA_FORMAT RW 0x0

Select data format 2’s complement (0x0) or offset binary (0x1). NOT-APPLICABLE if DAC_DP_DISABLE is set (0x1).

[3:0] RESERVED NA 0x0

Reserved

0x13 0x4c RATECNTRL

DAC Interface Control & Status

[7:0] RATE RW 0x00

The effective dac rate (the maximum possible rate is dependent on the interface clock). The samples are generated at 1/RATE of the interface clock.

0x15 0x54 STATUS1

DAC Interface Control & Status

[31:0] CLK_FREQ RO 0x00000000

Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock.

0x16 0x58 STATUS2

DAC Interface Control & Status

[31:0] CLK_RATIO RO 0x00000000

Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr).

0x18 0x60 DAC_CLKSEL

DAC Interface Control & Status

[0] DAC_CLKSEL RW 0x0

Allows changing of the clock polarity. Note: its default value is CLK_EDGE_SEL

0x1a 0x68 SYNC_STATUS

DAC Synchronization Status register

[0] DAC_SYNC_STATUS RO 0x0

DAC synchronization status. Will be set to 1 while waiting for the external synchronization signal This bit has an effect only the EXT_SYNC synthesis parameter is set.

0x22 0x88 UI_STATUS

User Interface Status

[1] UI_OVF RW1C 0x0

User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit.

0x28 0xa0 USR_CNTRL_1

DAC User Control & Status

[7:0] USR_CHANMAX RW 0x00

This indicates the maximum number of inputs for the channel data multiplexers. User may add different processing modules as inputs to the dac. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x100 + 0x10*n 0x400 + 0x40*n CHAN_CNTRLn_1

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[21:16] DDS_PHASE_DW RO 0x00

The DDS phase data width offers the HDL parameter configuration with the same name. This information is used in conjunction with CHAN_CNTRL_9 and CHAN_CNTRL_10. More info at AD Direct Digital Synthesis.

[15:0] DDS_SCALE_1 RW 0x0000

The DDS scale for tone 1. Sets the amplitude of the tone. The format is 1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on 16-bits, note that if you do use both channels and set both scale to 0x4000, it is over-range. The final output is (tone_1_fullscale * scale_1) + (tone_2_fullscale * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x101 + 0x10*n 0x404 + 0x40*n CHAN_CNTRLn_2

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_1 RW 0x0000

The DDS phase initialization for tone 1. Sets the initial phase offset of the tone. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_1 RW 0x0000

Sets the frequency of the phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{16}) * clkratio / f_{if}\); where f_out is the generated output frequency, and f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase increment for tone 1 is extended in CHAN_CNTRL_9. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x102 + 0x10*n 0x408 + 0x40*n CHAN_CNTRLn_3

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[15:0] DDS_SCALE_2 RW 0x0000

The DDS scale for tone 2. Sets the amplitude of the tone. The format is 1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on 16-bits, note that if you do use both channels and set both scale to 0x4000, it is over-range. The final output is (tone_1_fullscale * scale_1) + (tone_2_fullscale * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x103 + 0x10*n 0x40c + 0x40*n CHAN_CNTRLn_4

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_2 RW 0x0000

The DDS phase initialization for tone 2. Sets the initial phase offset of the tone. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase init for tone 2 is extended in CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_2 RW 0x0000

Sets the frequency of the phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{16}) * clkratio / f_{if}\); where f_out is the generated output frequency, and f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase increment for tone 2 is extended in CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x104 + 0x10*n 0x410 + 0x40*n CHAN_CNTRLn_5

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_PATT_2 RW 0x0000

The DDS data pattern for this channel.

[15:0] DDS_PATT_1 RW 0x0000

The DDS data pattern for this channel.

0x105 + 0x10*n 0x414 + 0x40*n CHAN_CNTRLn_6

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[2] IQCOR_ENB RW 0x0

if set, enables IQ correction. NOT-APPLICABLE if DAC_DP_DISABLE is set (0x1).

[1] DAC_LB_OWR RW 0x0

If set, forces DAC_DDS_SEL to 0x8, loopback If DAC_LB_OWR and DAC_PN_OWR are both set, they are ignored

[0] DAC_PN_OWR RW 0x0

IF set, forces DAC_DDS_SEL to 0x09, device specific pnX If DAC_LB_OWR and DAC_PN_OWR are both set, they are ignored

0x106 + 0x10*n 0x418 + 0x40*n CHAN_CNTRLn_7

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[3:0] DAC_DDS_SEL RW 0x0

Select internal data sources (available only if the DAC supports it).

  • 0x00: internal tone (DDS)

  • 0x01: pattern (SED)

  • 0x02: input data (DMA)

  • 0x03: 0x00

  • 0x04: inverted pn7

  • 0x05: inverted pn15

  • 0x06: pn7 (standard O.150)

  • 0x07: pn15 (standard O.150)

  • 0x08: loopback data (ADC)

  • 0x09: pnX (Device specific e.g. ad9361)

  • 0x0A: Nibble ramp (Device specific e.g. adrv9001)

  • 0x0B: 16 bit ramp (Device specific e.g. adrv9001)

0x107 + 0x10*n 0x41c + 0x40*n CHAN_CNTRLn_8

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] IQCOR_COEFF_1 RW 0x0000

IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the scale value and the format is 1.1.14 (sign, integer and fractional bits). If matrix multiplication is used, this is the channel I coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1).

[15:0] IQCOR_COEFF_2 RW 0x0000

IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the offset value and the format is 2’s complement. If matrix multiplication is used, this is the channel Q coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1).

0x108 + 0x10*n 0x420 + 0x40*n USR_CNTRLn_3

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[25] USR_DATATYPE_BE RW 0x0

The user data type format- if set, indicates big endian (default is little endian). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[24] USR_DATATYPE_SIGNED RW 0x0

The user data type format- if set, indicates signed (2’s complement) data (default is unsigned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[23:16] USR_DATATYPE_SHIFT RW 0x00

The user data type format- the amount of right shift for actual samples within the total number of bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[15:8] USR_DATATYPE_TOTAL_BITS RW 0x00

The user data type format- number of total bits used for a sample. The total number of bits must be an integer multiple of 8 (byte aligned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[7:0] USR_DATATYPE_BITS RW 0x00

The user data type format- number of bits in a sample. This indicates the actual sample data bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

0x109 + 0x10*n 0x424 + 0x40*n USR_CNTRLn_4

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] USR_INTERPOLATION_M RW 0x0000

This holds the user interpolation M value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[15:0] USR_INTERPOLATION_N RW 0x0000

This holds the user interpolation N value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

0x10a + 0x10*n 0x428 + 0x40*n USR_CNTRLn_5

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[0] DAC_IQ_MODE RW 0x0

Enable complex mode. In this mode the driven data to the DAC must be a sequence of I and Q sample pairs.

[1] DAC_IQ_SWAP RW 0x0

Allows IQ swapping in complex mode. Only takes effect if complex mode is enabled.

0x10b + 0x10*n 0x42c + 0x40*n CHAN_CNTRLn_9

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_1_EXTENDED RW 0x0000

The extended DDS phase initialization for tone 1. Sets the initial phase offset of the tone. The extended init(phase) value should be calculated according to DDS_PHASE_DW value from CHAN_CNTRL_1 NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_1_EXTENDED RW 0x0000

Sets the frequency of tone 1’s phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{phaseDW}) * clkratio / f_{if}\); Where f_out is the generated output frequency, DDS_PHASE_DW value can be found in CHAN_CNTRL_1 in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x10c + 0x10*n 0x430 + 0x40*n CHAN_CNTRLn_10

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_2_EXTENDED RW 0x0000

The extended DDS phase initialization for tone 2. Sets the initial phase offset of the tone. The extended init(phase) value should be calculated according to DDS_PHASE_DW value from CHAN_CNTRL_2 NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_2_EXTENDED RW 0x0000

Sets the frequency of tone 2’s phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{phaseDW}) * clkratio / f_{if}\); Where f_out is the generated output frequency, DDS_PHASE_DW value can be found in CHAN_CNTRL_2 in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x10 0x40 TDD_CONTROL_0

TDD Control & Status

[5] TDD_GATED_TX_DMAPATH RW 0x0

If this bit is set, the core requests data from the TX DMA, just when the data path is active. Otherwise will requests continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity.

[4] TDD_GATED_RX_DMAPATH RW 0x0

If this bit is set, the core provides data for the RX DMA, just when the data path is active. Otherwise will provides continuously on the adjusted rate. The purpose of this feature is to facilitate debug. This bit must be SET to preserve data integrity.

[3] TDD_TXONLY RW 0x0

If this bit is set- the TDD controller ignores all the TX_* timing registers below and assumes continuous receive operation within a frame.

[2] TDD_RXONLY RW 0x0

If this bit is set- the TDD controller ignores all the RX_* timing registers below and assumes continuous transmit operation within a frame.

[1] TDD_SECONDARY RW 0x0

Enable the secondary transmit/receive on the active frame. If this bit is clear - the controller only uses the _1 timing registers below. If this bit is set - the controller uses the _1 and _2 timing registers below.

[0] TDD_ENABLE RW 0x0

If set, enables the TDD controller- software must set this bit after programming all the registers that controls the tdd timing. Any device settings needs to be done (for example bring the AD9361 to the alert state) prior to to setting this bit. The controller keeps the frame counters in reset if this bit is reset. A 0 to 1 transition in this bit starts the frame counter and tdd mode of operation.

0x11 0x44 TDD_CONTROL_1

TDD Control & Status

[7:0] TDD_BURST_COUNT RW 0x00

If set to 0x0 and enabled (TDD_ENABLE is set) - the controller operates in TDD mode as long as the TDD_ENABLE bit is set. If set to a non-zero value, the controller operates for the set number of frames and stops.

0x12 0x48 TDD_CONTROL_2

TDD Control & Status

[23:0] TDD_COUNTER_INIT RW 0x000000

The controller sets the frame counter to this value when starting TDD operation. This is the starting offset value for the TDD frame counter.

0x13 0x4c TDD_FRAME_LENGTH

TDD Control & Status

[23:0] TDD_FRAME_LENGTH RW 0x000000

The frame length is the terminal count for the 10ms counter running at the digital interface clock- as an example for a 245.76MHz clock it is 0x258000.

0x14 0x50 TDD_SYNC_TERMINAL_TYPE

TDD Control & Status

[0] TDD_SYNC_TERMINAL_TYPE RW 0x0

Set this bit, if the current terminal will generate the syncronization pulse, reset otherwise.

0x18 0x60 TDD_STATUS

TDD Control & Status

[0] TDD_RXTX_VCO_OVERLAP RO 0x0

This bit is asserted, if exist a time interval when both the TX and RX VCOs are powered up.

[1] TDD_RXTX_RF_OVERLAP RO 0x0

This bit is asserted, if exist a time interval when both the TX and RX RF datapath are powered up.

0x20 0x80 TDD_VCO_RX_ON_1

TDD Control & Status

[23:0] TDD_VCO_RX_ON_1 RW 0x000000

Defines the offset (from frame count equal zero), when the RX VCO powers up at the first time. The controller enables the receive VCO, when the frame count reaches this value. The VCO may have to be enabled before data can be received. The user needs to make sure, that the RF device is in a state, from where this operation is valid.

0x21 0x84 TDD_VCO_RX_OFF_1

TDD Control & Status

[23:0] TDD_VCO_RX_OFF_1 RW 0x000000

Defines the offset (from frame count equal zero), when the RX VCO powers down at the first time. The controller disables the receive VCO, when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid.

0x22 0x88 TDD_VCO_TX_ON_1

TDD Control & Status

[23:0] TDD_VCO_TX_ON_1 RW 0x000000

Defines the offset (from frame count equal zero), when the TX VCO powers up at the first time. The controller enables the transmit VCO, when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid.

0x23 0x8c TDD_VCO_TX_OFF_1

TDD Control & Status

[23:0] TDD_VCO_TX_OFF_1 RW 0x000000

Defines the offset (from frame count equal zero), when the TX VCO powers down at the first time. The controller disables the transmit VCO when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid.

0x24 0x90 TDD_RX_ON_1

TDD Control & Status

[23:0] TDD_RX_ON_1 RW 0x000000

Defines the offset (from frame count equal zero), when the RX data path is activated at the first time. The controller enables the receive chain when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid.

0x25 0x94 TDD_RX_OFF_1

TDD Control & Status

[23:0] TDD_RX_OFF_1 RW 0x000000

Defines the offset (from frame count equal zero), when the RX data path is deactivated the first time. The controller disables the receive chain when the frame count reaches this value. The user needs to make sure, that the RF device is in a state, from where this operation is valid.

0x26 0x98 TDD_TX_ON_1

TDD Control & Status

[23:0] TDD_TX_ON_1 RW 0x000000

Defines the offset (from frame count equal zero), when the TX data path is activated at the first time. The controller enables the transmit chain, when the frame count reaches this value. This register and the TX_DP_ON register controls the delay between the data path being activated and the time to actually push the transmit data through the transmit chain in the device.

0x27 0x9c TDD_TX_OFF_1

TDD Control & Status

[23:0] TDD_TX_OFF_1 RW 0x000000

Defines the offset (from frame count equal zero), when the TX data path is deactivated at the first time. The controller disables the transmit chain, when the frame count reaches this value. This register and the TX_DP_OFF register controls the delay between the data path being deactivated and the time to actually stop transmitting data through the transmit chain in the device.

0x28 0xa0 TDD_RX_DP_ON_1

TDD Control & Status

[23:0] TDD_RX_DP_ON_1 RW 0x000000

Defines the offset (from frame count equal zero), when the controller starts to accept data from the digital interface for receive.

0x29 0xa4 TDD_RX_DP_OFF_1

TDD Control & Status

[23:0] TDD_RX_DP_OFF_1 RW 0x000000

Defines the offset (from frame count equal zero), when the controller stops to accept data from the digital interface for receive.

0x2a 0xa8 TDD_TX_DP_ON_1

TDD Control & Status

[23:0] TDD_TX_DP_ON_1 RW 0x000000

Defines the offset (from frame count equal zero), when the controller starts to request data from the system memory for transmit. The data rate is controlled by the TDD controller.

0x2b 0xac TDD_TX_DP_OFF_1

TDD Control & Status

[23:0] TDD_TX_DP_OFF_1 RW 0x000000

Defines the offset (from frame count equal zero), when the controller stop requesting data from the system memory for transmit.

0x30 0xc0 TDD_VCO_RX_ON_2

TDD Control & Status

[23:0] TDD_VCO_RX_ON_2 RW 0x000000

The secondary pointer for VCO_RX_ON.

0x31 0xc4 TDD_VCO_RX_OFF_2

TDD Control & Status

[23:0] TDD_VCO_RX_OFF_2 RW 0x000000

The secondary pointer for VCO_RX_OFF.

0x32 0xc8 TDD_VCO_TX_ON_2

TDD Control & Status

[23:0] TDD_VCO_TX_ON_2 RW 0x000000

The secondary pointer for VCO_TX_ON.

0x33 0xcc TDD_VCO_TX_OFF_2

TDD Control & Status

[23:0] TDD_VCO_TX_OFF_2 RW 0x000000

The secondary pointer for VCO_TX_OFF.

0x34 0xd0 TDD_RX_ON_2

TDD Control & Status

[23:0] TDD_RX_ON_2 RW 0x000000

The secondary pointer for RX_ON.

0x35 0xd4 TDD_RX_OFF_2

TDD Control & Status

[23:0] TDD_RX_OFF_2 RW 0x000000

The secondary pointer for RX_OFF.

0x36 0xd8 TDD_TX_ON_2

TDD Control & Status

[23:0] TDD_TX_ON_2 RW 0x000000

The secondary pointer for TX_ON.

0x37 0xdc TDD_TX_OFF_2

TDD Control & Status

[23:0] TDD_TX_OFF_2 RW 0x000000

The secondary pointer for TX_OFF.

0x38 0xe0 TDD_RX_DP_ON_2

TDD Control & Status

[23:0] TDD_RX_DP_ON_2 RW 0x000000

The secondary pointer for RX_DP_ON.

0x39 0xe4 TDD_RX_DP_OFF_2

TDD Control & Status

[23:0] TDD_RX_DP_OFF_2 RW 0x000000

The secondary pointer for RX_DP_OFF.

0x3a 0xe8 TDD_TX_DP_ON_2

TDD Control & Status

[23:0] TDD_TX_DP_ON_2 RW 0x000000

The secondary pointer for TX_DP_ON.

0x3b 0xec TDD_TX_DP_OFF_2

TDD Control & Status

[23:0] TDD_TX_DP_OFF_2 RW 0x000000

The secondary pointer for TX_DP_OFF.

References