Channel UPACK Utility

?util_upack2 IP-XACT not found.Generate it and the documentation:(cd library/util_pack/util_upack2; make)(cd docs; make html)

The channel UPACK utility core is meant to allow one or more channels to be enabled by software without any padding. This allows full usage of the DMA bandwidth without any overhead. This core normally works with an DAC and DMA modules. The DAC interface is channel based (one interface per each DAC channel) and consists of enable, valid and data signals. The DMA interface is a single FIFO interface consisting of valid and data signals. The enable signals are usually controlled by software. The core simply unpacks the DMA data into the individual channels as defined by the enables.

Features

  • Supports Altera and AMD Xilinx devices

  • Supports up to 64 channels

  • Supports configurable channel data width

Files

Name

Description

library/util_pack/util_upack2/util_upack2.v

Verilog source for the peripheral.

Configuration Parameters

Name

Description

Interface

Name

Description

s_axis

FIFO interface to the source.

fifo_rd_en

Assert to indicate that the DAC core is ready to consume DAC data.

fifo_rd_valid

Indicates that the enabled DAC channels data are valid.

enable_*

Indicates the status of the channel, if asserted the channel is active.

fifo_rd_data_*

DAC data bus to the DAC core (sink).

Detailed Description

The core “collects” samples from the DMA interface (or any other source) and passes it to the DAC on every valid request from the DAC. This is best explained through some examples. Let’s consider a 4 channel DAC with a channel data width of 32 bits. That is, the DAC requires two 16-bit samples be present at its input for all channels when the valid is asserted. The DMA interface in this case is an interleaved 8 samples (128 bits) stream. This is because irrespective of the DAC channel data width, the software always sees data as “samples interleaved”. The same data set may drive a DAC core with a channel width of 128 bits or 16 bits.

This data unpacking now needs to factor in the valid and the number of samples that are to be read from the DMA. It is quite simple: a valid at the DAC interface translates into a data required count based on the number of enables. So if three channels are enabled the requirement is 6 samples, so the core initiates a read from the DMA three out of four clock cycles.

../../_images/upack_4channel.svg

Four channel enabled (4’b1111)

../../_images/upack_3channel.svg

Three channel enabled (4’b1110)

../../_images/upack_2channel.svg

Two channel enabled (4’b1100)

References