Generic AXI DAC

This page presents a generic framework, which is used to design and develop an AXI based IP core for interfacing a Digital to Analog Converter (DAC) device with a high speed serial (JESD204B) or source synchronous parallel interface (LVDS/CMOS). This is a generic framework, there can be minor differences on each and every IP, the user should study this wiki page along with the IP’s wiki page.

The main role of this page to ease the understanding of each DAC IP, and to provide a base knowledge which can be used to develop new IPs for currently unsupported devices.

Important

Any kind of feedback regarding the DAC IP architecture or the following document is highly appreciated and can be addressed through the EngineerZone community forum.

Files

Name

Description

library/common/up_dac_common.v

Verilog source for the DAC Common regmap.

library/common/up_dac_channel.v

Verilog source for the DAC Channel regmap.

Architecture

The main function of an AXI DAC IP is to handle all the low level signalling, which is defined by the device’s digital data interface, and to forward the received data from the DMA or any other data source to the device. Beside this functionality there are a few processing modules inside the data path of the core, which can be used for signal conditioning. All these processing modules are optional, the are enabled or disabled by setting the appropriate parameters. The following block diagram presents a generic AXI DAC IP cores data path.

AXI DAC Datapath

Transmit PHY

The most important part of the core is the Transmit PHY module. This module contains all the IO primitive instantiations and all the control logic required to transmit data to the device.

Note

All the PHY modules follows the same naming convention: axi_<device_name>_if.v (e.g. axi_ad9467_if.v)

In some cases, when the IP supports multiple interface type, the name of the PHY module look like: axi_<device_name>_<interface_type>_if.v (e.g. axi_ad9361_lvds_if.v)

Currently the Transmit PHY supports two different transmit interface:

All these interfaces are supported on both Altera (Intel) and Xilinx devices.

This module is perfect choice for those, who wants a HDL logic for the device interface, with a minimal resource footprint.

DAC Channel

  • Data source multiplexer

  • IQ correction module

DAC Core

The DAC core is the top file of the IP core, the naming convention of this file is: axi_<device_name>.v. Here are instantiated all the internal module discussed above, and a wrapper module (up_axi), which converts the AXI interface into a more simplistic addressable, memory mapped interface, so called Microprocessor Interface or uP interface. This interface is used to interconnect the different memory mapped module pieces.

Interface

A generic AXI DAC core have at least three different interfaces:

  • The physical data interface (LVDS or CMOS) or the JESD204B data interface from the link layer.

  • Read FIFO interface for the transmit or source module (e.g. DMA).

  • AXI Slave Memory Mapped interface for register map access.

LVDS or CMOS TX interface

Pin

Type

Description

tx_clk_in_[p|n]

clock input

clock input (device’s DCO)

tx_clk_out_[p|n]

clock output

clock output (device’s DCI)

tx_data_out_[p|n]

output[resolution-1:0]

parallel data output (note that multiple parallel data buses can exist)

JESD TX interface

Pin

Type

Description

tx_clk

clock input

core clock or device clock (must be (line clock)/40)

tx_data

output[DW-1:0]

data input; DW=32*MAX_LANE_NO

Read FIFO interface

Pin

Type

Description

dac_clk

clock output

Interface’s clock signal

dac_enable_0

output

Enable signal for the first channel, asserted if channel is active

dac_valid_0

output

Data valid signal for the first channel, to validate data on the bus

dac_data_0

input[DW-1:0]

Data signal for the first channel

dac_enable_x

output

Enable signal for the channel x, asserted if channel is active

dac_valid_x

output

Data valid signal for the channel x, to validate data on the bus

dac_data_x

input[DW-1:0]

Data signal for the channel x

dac_dunf

input

Data underflow signal from the receiver or sink module (e.g DMA)

AXI Memory Map Slave

Pin

Type

Description

s_axi_*

Standard AXI Slave Memory Map interface for register map access

Register Map

The following block diagram presents the different register maps physical location in the core. These register maps are generic and can be found in each AXI DAC core.

AXI DAC Register Map

The base and DAC common register map is implemented in the same verilog file. It contains registers which controls and monitors the overall core, like:

  • Reset bits

  • Attributes of the transmit interface module

  • DRP (Dynamic Reconfiguration Port) access for different IO resources (Clock Management Units, PLLs, Gigabit Transceivers etc.)

  • Status registers (PN Monitor status, frequency of the interface clock)

Note

The DAC Common register map is implemented in the library/common/up_dac_common.v verilog file. To find the instantiation of this module search for up_dac_common inside the IP’s directory.

The DAC Channel register map controls and monitors channel specific attributes. Each channel of the core has an individual channel register map. It contains all the registers, which are necessary to control and monitor the processing modules of the data path. For detailed description of the available processing modules see DAC Channel section.

Note

The DAC Channel register map is implemented in the library/common/up_dac_channel.v verilog file. To find the instantiation of this module search for up_dac_channel inside the IP’s directory.

Register access

The DAC IP supports 16 channels, numbered from 0 to 15. Usually, the base registers start at offset 0x0 and the common (global) registers start at address 0x10. Each channel has its own register block, starting from address 0x100 (for channel 0). Each subsequent channel is spaced by 0x10 (HDL register address) or 0x40 (Software addressing).

..note:

There are cases in which the offset is different from ``0x0``. Please refer to
the register map table of the specific IP for more details.

Let’s say the DAC IP base address is 0x44A0_0000. Here is how the channel offset is computed:

\[\begin{split}\text{HDL}_{reg} = 0x100 + (n \times 0x10) \\\end{split}\]
\[\text{Software}_{addr} = IP_BaseAddr + (\text{HDL}_{reg} << 2) = 0x44A0\_0000 + 0x400 + (n \times 0x40)\]

This means the first register’s address ( ``CHAN_CNTRL_0``) is:

  • For channel 0:

    • 0x0100 (HDL register)=> 0x44A0_0400 (Software addressing)

  • For channel 3:

    • 0x0130 (HDL register) => 0x44A0_04C0 (Software addressing)

  • For channel 15:

    • 0x01F0 (HDL register) => 0x44A0_07C0 (Software addressing)

If you want to access the ``CHAN_CNTRL_3`` register, its address is:

  • For channel 0:

    • 0x0106 (HDL register) => 0x44A0_0418 (Software addressing)

  • For channel 5:

    • 0x0156 (HDL register) => 0x44A0_0558 (Software addressing)

In general, the address for the CHAN_CNTRL_3 register of channel *n* can be calculated as:

\[\begin{split}\text{HDL}_{reg} = 0x100 + (n \times 0x10) + 0x06 \\\end{split}\]
\[\text{Software}_{addr} = IP_base_addr + 0x400 + (n \times 0x40) + 0x18\]

The software addresses for all channels can be found in the table below:

Name

Address range

Base

0x000 to 0x0BC

Common

0x040 to 0x0C4

Channel 0

0x400 to 0x430

Channel 1

0x440 to 0x470

Channel 2

0x480 to 0x4B0

Channel 3

0x4C0 to 0x4F0

…

…

Channel 15

0x7C0 to 0x7F0

Typical Register Map base addresses

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 0x0 VERSION

Version and Scratch Registers

[31:0] VERSION RO 0x00000000

Version number. Unique to all cores.

0x1 0x4 ID

Version and Scratch Registers

[31:0] ID RO 0x00000000

Instance identifier number.

0x2 0x8 SCRATCH

Version and Scratch Registers

[31:0] SCRATCH RW 0x00000000

Scratch register.

0x3 0xc CONFIG

Version and Scratch Registers

[0] IQCORRECTION_DISABLE RO 0x0

If set, indicates that the IQ Correction module was not implemented. (as a result of a configuration of the IP instance)

[1] DCFILTER_DISABLE RO 0x0

If set, indicates that the DC Filter module was not implemented. (as a result of a configuration of the IP instance)

[2] DATAFORMAT_DISABLE RO 0x0

If set, indicates that the Data Format module was not implemented. (as a result of a configuration of the IP instance)

[3] USERPORTS_DISABLE RO 0x0

If set, indicates that the logic related to the User Data Format (e.g. decimation) was not implemented. (as a result of a configuration of the IP instance)

[4] MODE_1R1T RO 0x0

If set, indicates that the core was implemented in 1 channel mode. (e.g. refer to AD9361 data sheet)

[5] DELAY_CONTROL_DISABLE RO 0x0

If set, indicates that the delay control is disabled for this IP. (as a result of a configuration of the IP instance)

[6] DDS_DISABLE RO 0x0

If set, indicates that the DDS is disabled for this IP. (as a result of a configuration of the IP instance)

[7] CMOS_OR_LVDS_N RO 0x0

CMOS or LVDS mode is used for the interface. (as a result of a configuration of the IP instance)

[8] PPS_RECEIVER_ENABLE RO 0x0

If set, indicates the PPS receiver is enabled. (as a result of a configuration of the IP instance)

[9] SCALECORRECTION_ONLY RO 0x0

If set, indicates that the IQ Correction module implements only scale correction. IQ correction must be enabled. (as a result of a configuration of the IP instance)

[12] EXT_SYNC RO 0x0

If set the transport layer cores (ADC/DAC) have implemented the support for external synchronization signal.

[13] RD_RAW_DATA RO 0x0

If set, the ADC has the capability to read raw data in register CHAN_RAW_DATA from adc_channel.

0x4 0x10 PPS_IRQ_MASK

PPS Interrupt mask

[0] PPS_IRQ_MASK RW 0x1

Mask bit for the 1PPS receiver interrupt

0x7 0x1c FPGA_INFO

FPGA device information library/scripts/adi_intel_device_info_enc.tcl (Intel encoded values) library/scripts/adi_xilinx_device_info_enc.tcl (Xilinx encoded values)

[31:24] FPGA_TECHNOLOGY RO 0x00

Encoded value describing the technology/generation of the FPGA device (arria 10/7series)

[23:16] FPGA_FAMILY RO 0x00

Encoded value describing the family variant of the FPGA device(e.g., SX, GX, GT or zynq, kintex, virtex)

[15:8] SPEED_GRADE RO 0x00

Encoded value describing the FPGA’s speed-grade

[7:0] DEV_PACKAGE RO 0x00

Encoded value describing the device package. The package might affect high-speed interfaces

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x10 0x40 RSTN

DAC Interface Control & Status

[2] CE_N RW 0x0

Clock enable, default is enabled(0x0). An inverse version of the signal is exported out of the module to control clock enables

[1] MMCM_RSTN RW 0x0

MMCM reset only (required for DRP access). Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core.

[0] RSTN RW 0x0

Reset, default is IN-RESET (0x0), software must write 0x1 to bring up the core.

0x11 0x44 CNTRL_1

DAC Interface Control & Status

[0] SYNC RW 0x0

Setting this bit synchronizes channels within a DAC, and across multiple instances. This bit self clears.

[1] EXT_SYNC_ARM RW 0x0

Setting this bit will arm the trigger mechanism sensitive to an external sync signal. Once the external sync signal goes high it synchronizes channels within a DAC, and across multiple instances. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

[2] EXT_SYNC_DISARM RW 0x0

Setting this bit will disarm the trigger mechanism sensitive to an external sync signal. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

[8] MANUAL_SYNC_REQUEST RW 0x0

Setting this bit will issue an external sync event if it is hooked up inside the fabric. This bit has an effect only the EXT_SYNC synthesis parameter is set. This bit self clears.

0x12 0x48 CNTRL_2

DAC Interface Control & Status

[16] SDR_DDR_N RW 0x0

Interface type (1 represents SDR, 0 represents DDR)

[15] SYMB_OP RW 0x0

Select data symbol format mode (0x1)

[14] SYMB_8_16B RW 0x0

Select number of bits for symbol format mode (1 represents 8b, 0 represents 16b)

[12:8] NUM_LANES RW 0x00

Number of active lanes (1 : CSSI 1-lane, LSSI 1-lane, 2 : LSSI 2-lane, 4 : CSSI 4-lane)

[7] PAR_TYPE RW 0x0

Select parity even (0x0) or odd (0x1).

[6] PAR_ENB RW 0x0

Select parity (0x1) or frame (0x0) mode.

[5] R1_MODE RW 0x0

Select number of RF channels 1 (0x1) or 2 (0x0).

[4] DATA_FORMAT RW 0x0

Select data format 2’s complement (0x0) or offset binary (0x1). NOT-APPLICABLE if DAC_DP_DISABLE is set (0x1).

[3:0] RESERVED NA 0x0

Reserved

0x13 0x4c RATECNTRL

DAC Interface Control & Status

[7:0] RATE RW 0x00

The effective dac rate (the maximum possible rate is dependent on the interface clock). The samples are generated at 1/RATE of the interface clock.

0x14 0x50 FRAME

DAC Interface Control & Status

[0] FRAME RW 0x0

The use of frame is device specific. Usually setting this bit to 1 generates a FRAME (1 DCI clock period) pulse on the interface. This bit self clears.

0x15 0x54 STATUS1

DAC Interface Control & Status

[31:0] CLK_FREQ RO 0x00000000

Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock.

0x16 0x58 STATUS2

DAC Interface Control & Status

[31:0] CLK_RATIO RO 0x00000000

Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr).

0x17 0x5c STATUS3

DAC Interface Control & Status

[0] STATUS RO 0x0

Interface status, if set indicates no errors. If not set, there are errors, software may try resetting the cores.

0x18 0x60 DAC_CLKSEL

DAC Interface Control & Status

[0] DAC_CLKSEL RW 0x0

Allows changing of the clock polarity. Note: its default value is CLK_EDGE_SEL

0x1a 0x68 SYNC_STATUS

DAC Synchronization Status register

[0] DAC_SYNC_STATUS RO 0x0

DAC synchronization status. Will be set to 1 while waiting for the external synchronization signal This bit has an effect only the EXT_SYNC synthesis parameter is set.

0x1c 0x70 DRP_CNTRL

DRP Control & Status

[28] DRP_RWN RW 0x0

DRP read (0x1) or write (0x0) select (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1).

[27:16] DRP_ADDRESS RW 0x000

DRP address, designs that contain more than one DRP accessible primitives have selects based on the most significant bits (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1).

[15:0] RESERVED RO 0x0000

Reserved for backwards compatibility

0x1d 0x74 DRP_STATUS

DAC Interface Control & Status

[17] DRP_LOCKED RO 0x0

If set indicates the MMCM/PLL is locked

[16] DRP_STATUS RO 0x0

If set indicates busy (access pending). The read data may not be valid if this bit is set (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1).

[15:0] RESERVED RO 0x0000

Reserved for backwards compatibility

0x1e 0x78 DRP_WDATA

DAC Interface Control & Status

[15:0] DRP_WDATA RW 0x0000

DRP write data (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1).

0x1f 0x7c DRP_RDATA

DAC Interface Control & Status

[15:0] DRP_RDATA RO 0x0000

DRP read data (does not include GTX lanes). NOT-APPLICABLE if DRP_DISABLE is set (0x1).

0x20 0x80 DAC_CUSTOM_RD

DAC Read Configuration Data

[31:0] DAC_CUSTOM_RD RO 0x00000000

Custom Read of the available registers.

0x21 0x84 DAC_CUSTOM_WR

DAC Write Configuration Data

[31:0] DAC_CUSTOM_WR RW 0x00000000

Custom Write of the available registers.

0x22 0x88 UI_STATUS

User Interface Status

[4] IF_BUSY RO 0x0

Interface busy. If set, indicates that the data interface is busy.

[1] UI_OVF RW1C 0x0

User Interface overflow. If set, indicates an overflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit.

[0] UI_UNF RW1C 0x0

User Interface underflow. If set, indicates an underflow occurred during data transfer at the user interface (FIFO interface). Software must write a 0x1 to clear this register bit.

0x23 0x8c DAC_CUSTOM_CTRL

DAC Control Configuration Data

[31:0] DAC_CUSTOM_CTRL RW 0x00000000

Custom Control of the available registers.

0x28 0xa0 USR_CNTRL_1

DAC User Control & Status

[7:0] USR_CHANMAX RW 0x00

This indicates the maximum number of inputs for the channel data multiplexers. User may add different processing modules as inputs to the dac. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

0x2e 0xb8 DAC_GPIO_IN

DAC GPIO inputs

[31:0] DAC_GPIO_IN RO 0x00000000

This reads auxiliary GPI pins of the DAC core

0x2f 0xbc DAC_GPIO_OUT

DAC GPIO outputs

[31:0] DAC_GPIO_OUT RW 0x00000000

This controls auxiliary GPO pins of the DAC core NOT-APPLICABLE if GPIO_DISABLE is set (0x1).

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x80 0x200 TPL_CNTRL

JESD, TPL Control

[3:0] PROFILE_SEL RW

Selects one of the available deframer/framers from the transport layer. Valid only if PROFILE_NUM > 1.

0x81 0x204 TPL_STATUS

JESD, TPL Status

[3:0] PROFILE_NUM RO

Number of supported framer/deframer profiles.

0x90 + 0x2*n 0x240 + 0x8*n TPL_DESCRIPTORn_1

JESD, TPL descriptor for profile n Where n is from 0 to 2.

[31:24] JESD_F RO

Octets per Frame per Lane.

[23:16] JESD_S RO

Samples per Converter per Frame.

[15:8] JESD_L RO

Lane Count.

[7:0] JESD_M RO

Converter Count.

0x91 + 0x2*n 0x244 + 0x8*n TPL_DESCRIPTORn_2

JESD, TPL descriptor for profile n Where n is from 0 to 2.

[7:0] JESD_N RO

Converter Resolution.

[15:8] JESD_NP RO

Total Number of Bits per Sample.

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x100 + 0x10*n 0x400 + 0x40*n CHAN_CNTRLn_1

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[21:16] DDS_PHASE_DW RO 0x00

The DDS phase data width offers the HDL parameter configuration with the same name. This information is used in conjunction with CHAN_CNTRL_9 and CHAN_CNTRL_10. More info at AD Direct Digital Synthesis.

[15:0] DDS_SCALE_1 RW 0x0000

The DDS scale for tone 1. Sets the amplitude of the tone. The format is 1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on 16-bits, note that if you do use both channels and set both scale to 0x4000, it is over-range. The final output is (tone_1_fullscale * scale_1) + (tone_2_fullscale * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x101 + 0x10*n 0x404 + 0x40*n CHAN_CNTRLn_2

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_1 RW 0x0000

The DDS phase initialization for tone 1. Sets the initial phase offset of the tone. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_1 RW 0x0000

Sets the frequency of the phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{16}) * clkratio / f_{if}\); where f_out is the generated output frequency, and f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase increment for tone 1 is extended in CHAN_CNTRL_9. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x102 + 0x10*n 0x408 + 0x40*n CHAN_CNTRLn_3

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[15:0] DDS_SCALE_2 RW 0x0000

The DDS scale for tone 2. Sets the amplitude of the tone. The format is 1.1.14 fixed point (signed, integer, fractional). The DDS in general runs on 16-bits, note that if you do use both channels and set both scale to 0x4000, it is over-range. The final output is (tone_1_fullscale * scale_1) + (tone_2_fullscale * scale_2). NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x103 + 0x10*n 0x40c + 0x40*n CHAN_CNTRLn_4

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_2 RW 0x0000

The DDS phase initialization for tone 2. Sets the initial phase offset of the tone. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase init for tone 2 is extended in CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_2 RW 0x0000

Sets the frequency of the phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{16}) * clkratio / f_{if}\); where f_out is the generated output frequency, and f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. If DDS_PHASE_DW is greater than 16(from CHAN_CNTRL_1), the phase increment for tone 2 is extended in CHAN_CNTRL_10. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x104 + 0x10*n 0x410 + 0x40*n CHAN_CNTRLn_5

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_PATT_2 RW 0x0000

The DDS data pattern for this channel.

[15:0] DDS_PATT_1 RW 0x0000

The DDS data pattern for this channel.

0x105 + 0x10*n 0x414 + 0x40*n CHAN_CNTRLn_6

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[2] IQCOR_ENB RW 0x0

if set, enables IQ correction. NOT-APPLICABLE if DAC_DP_DISABLE is set (0x1).

[1] DAC_LB_OWR RW 0x0

If set, forces DAC_DDS_SEL to 0x8, loopback If DAC_LB_OWR and DAC_PN_OWR are both set, they are ignored

[0] DAC_PN_OWR RW 0x0

IF set, forces DAC_DDS_SEL to 0x09, device specific pnX If DAC_LB_OWR and DAC_PN_OWR are both set, they are ignored

0x106 + 0x10*n 0x418 + 0x40*n CHAN_CNTRLn_7

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[3:0] DAC_DDS_SEL RW 0x0

Select internal data sources (available only if the DAC supports it).

  • 0x00: internal tone (DDS)

  • 0x01: pattern (SED)

  • 0x02: input data (DMA)

  • 0x03: 0x00

  • 0x04: inverted pn7

  • 0x05: inverted pn15

  • 0x06: pn7 (standard O.150)

  • 0x07: pn15 (standard O.150)

  • 0x08: loopback data (ADC)

  • 0x09: pnX (Device specific e.g. ad9361)

  • 0x0A: Nibble ramp (Device specific e.g. adrv9001)

  • 0x0B: 16 bit ramp (Device specific e.g. adrv9001)

0x107 + 0x10*n 0x41c + 0x40*n CHAN_CNTRLn_8

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] IQCOR_COEFF_1 RW 0x0000

IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the scale value and the format is 1.1.14 (sign, integer and fractional bits). If matrix multiplication is used, this is the channel I coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1).

[15:0] IQCOR_COEFF_2 RW 0x0000

IQ correction (if equipped) coefficient. If scale & offset is implemented, this is the offset value and the format is 2’s complement. If matrix multiplication is used, this is the channel Q coefficient and the format is 1.1.14 (sign, integer and fractional bits). NOT-APPLICABLE if IQCORRECTION_DISABLE is set (0x1).

0x108 + 0x10*n 0x420 + 0x40*n USR_CNTRLn_3

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[25] USR_DATATYPE_BE RW 0x0

The user data type format- if set, indicates big endian (default is little endian). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[24] USR_DATATYPE_SIGNED RW 0x0

The user data type format- if set, indicates signed (2’s complement) data (default is unsigned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[23:16] USR_DATATYPE_SHIFT RW 0x00

The user data type format- the amount of right shift for actual samples within the total number of bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[15:8] USR_DATATYPE_TOTAL_BITS RW 0x00

The user data type format- number of total bits used for a sample. The total number of bits must be an integer multiple of 8 (byte aligned). NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[7:0] USR_DATATYPE_BITS RW 0x00

The user data type format- number of bits in a sample. This indicates the actual sample data bits. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

0x109 + 0x10*n 0x424 + 0x40*n USR_CNTRLn_4

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] USR_INTERPOLATION_M RW 0x0000

This holds the user interpolation M value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

[15:0] USR_INTERPOLATION_N RW 0x0000

This holds the user interpolation N value of the channel that is currently being selected on the multiplexer above. The total interpolation factor is of the form M/N. NOT-APPLICABLE if USERPORTS_DISABLE is set (0x1).

0x10a + 0x10*n 0x428 + 0x40*n USR_CNTRLn_5

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[0] DAC_IQ_MODE RW 0x0

Enable complex mode. In this mode the driven data to the DAC must be a sequence of I and Q sample pairs.

[1] DAC_IQ_SWAP RW 0x0

Allows IQ swapping in complex mode. Only takes effect if complex mode is enabled.

0x10b + 0x10*n 0x42c + 0x40*n CHAN_CNTRLn_9

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_1_EXTENDED RW 0x0000

The extended DDS phase initialization for tone 1. Sets the initial phase offset of the tone. The extended init(phase) value should be calculated according to DDS_PHASE_DW value from CHAN_CNTRL_1 NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_1_EXTENDED RW 0x0000

Sets the frequency of tone 1’s phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{phaseDW}) * clkratio / f_{if}\); Where f_out is the generated output frequency, DDS_PHASE_DW value can be found in CHAN_CNTRL_1 in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

0x10c + 0x10*n 0x430 + 0x40*n CHAN_CNTRLn_10

DAC Channel Control & Status (channel - 0) Where n is from 0 to 15.

[31:16] DDS_INIT_2_EXTENDED RW 0x0000

The extended DDS phase initialization for tone 2. Sets the initial phase offset of the tone. The extended init(phase) value should be calculated according to DDS_PHASE_DW value from CHAN_CNTRL_2 NOT-APPLICABLE if DDS_DISABLE is set (0x1).

[15:0] DDS_INCR_2_EXTENDED RW 0x0000

Sets the frequency of tone 2’s phase accumulator. Its value can be calculated by \(INCR = (f_{out} * 2^{phaseDW}) * clkratio / f_{if}\); Where f_out is the generated output frequency, DDS_PHASE_DW value can be found in CHAN_CNTRL_2 in case DDS_PHASE_DW is not 16, f_if is the frequency of the digital interface, and clock_ratio is the ratio between the sampling clock and the interface clock. NOT-APPLICABLE if DDS_DISABLE is set (0x1).

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 + 0x1*n 0x0 + 0x4*n DELAY_CONTROL_n

Delay Control & Status Where n is from 0 to 15.

[4:0] DELAY_CONTROL_IO_n RW 0x00

Tap value for input/output delay primitive of the n’th interface line. If the delay controller is not locked (indicate issues with delay_clk), the read-back value of this register will be 0xFFFFFFFF. Otherwise will be the last set up value.

References