AXI ADXCVR
The AXI ADXCVR utility IP core is used to control and configure the highspeed transceivers. There are separate AXI ADXCVR cores for Intel and AMD Xilinx designs, due to the small differences between the AMD Xilinx’s and Intel’s transceivers architecture. For the AMD Xilinx architecture, the transceivers are instantiated in UTIL_ADXCVR.
Features
Supports Intel and AMD Xilinx devices.
Software can access the core’s registers through an AXI4 Lite Memory Mapped interface.
Link reset and monitor for Intel and AMD Xilinx.
Reconfiguration interface control with broadcast capability for AMD Xilinx.
Access to the Statistical eye scan interface of the PHY (AMD Xilinx).
Supports up to 16 transceiver lanes per link (AMD Xilinx).
Intel Devices
For Intel devices, the ADI JESD204 IP is using the AXI ADXCVR core, which can be accessed by the link_management interface. It provides a global reset signal for the JESD204B framework. Resets the XCVR reset controller IP, the link PLL reset controller, the PHY itself, and also the link layer of the stack. Besides the reset generation, monitors the PLLs and the PHY state.
Parameters
Name |
Description |
|---|---|
ID |
Instance identification number, if more than one instance is used. |
NUM_OF_LANES |
The number of lanes (primitives) used in this link. |
XCVR_TYPE |
Refers to the transceiver speed grade 0-9. |
FPGA_TECHNOLOGY |
Encoded value describing the technology/generation of the FPGA device (e.g. Cyclone V, Arria 10, Stratix 10). |
FPGA_FAMILY |
Encoded value describing the family variant of the FPGA device (e.g. SX, GX, GT). |
SPEED_GRADE |
Encoded value describing the FPGA’s speed-grade. |
DEV_PACKAGE |
Encoded value describing the device package. The package might affect high-speed interfaces. |
FPGA_VOLTAGE |
Contains the value(0-5000 mV) at wich the FPGA device supplied. |
TX_OR_RX_N |
If set (0x1), configures the link in transmit mode, otherwise receive. |
Interfaces
Name |
Description |
|---|---|
s_axi_aclk |
System clock. (in general 100 MHz) |
s_axi_aresetn |
System reset. |
s_axi |
Subordinate AXI4 Lite Memory Mapped interface |
up_ch_* |
Connect logical port |
Register Map
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x0 |
0x0 |
VERSION |
Version Register |
|||
[31:0] |
VERSION |
RO |
Version number. |
|||
0x1 |
0x4 |
ID |
Instance Identification Register |
|||
[31:0] |
ID |
RO |
Instance identifier number. |
|||
0x2 |
0x8 |
SCRATCH |
Scratch (GP R/W) Register |
|||
[31:0] |
SCRATCH |
RW |
Scratch register. |
|||
0x4 |
0x10 |
RESETN |
Reset Control Register |
|||
[0] |
RESETN |
RW |
If clear, link is held in reset, set this bit to 0x1 to activate link. Note that the reference clock must be active before setting this bit. |
|||
0x5 |
0x14 |
STATUS |
Status Reporting Register |
|||
[0] |
STATUS |
RO |
After setting the RESETN bit above, wait for this bit to set. If set, indicates successful link activation. |
|||
0x6 |
0x18 |
STATUS_32 |
Status Reporting Register |
|||
[31:NUM_OF_LANES+1] |
RESERVED |
RO |
0 |
|||
[NUM_OF_LANES] |
UP_PLL_LOCKED |
RO |
After setting the RESETN bit above, wait for this bit be to set. |
|||
[NUM_OF_LANES-1:0] |
CHANNEL_N_READY |
RO |
After setting the RESETN bit above, wait for this registers to be set. |
|||
0x7 |
0x1c |
FPGA_INFO |
FPGA device information Intel Encoded Values |
|||
[31:24] |
FPGA_TECHNOLOGY |
RO |
Encoded value describing the technology/generation of the FPGA device (e.g., cyclone V, arria 10, stratix 10) |
|||
[23:16] |
FPGA_FAMILY |
RO |
Encoded value describing the family variant of the FPGA device(e.g., SX, GX, GT or zynq, kintex, virtex) |
|||
[15:8] |
SPEED_GRADE |
RO |
Encoded value describing the FPGA’s speed-grade |
|||
[7:0] |
DEV_PACKAGE |
RO |
Encoded value describing the device package. The package might affect high-speed interfaces |
|||
0x9 |
0x24 |
GENERIC_INFO |
Physical layer info |
|||
[31:28] |
RESERVED |
RO |
0 |
|||
[27:24] |
XCVR_TYPE |
RO |
Refers to the transceiver speed grade 0-9. |
|||
[23:12] |
RESERVED |
RO |
0 |
|||
[11:9] |
RESERVED |
RO |
0 |
|||
[8] |
TX_OR_RX_N |
RO |
Transceiver type (transmit or receive) |
|||
[7:0] |
NUM_OF_LANES |
RO |
Physical layer number of lanes. |
|||
0x50 |
0x140 |
FPGA_VOLTAGE |
FPGA device voltage information |
|||
[15:0] |
FPGA_VOLTAGE |
RO |
The voltage of the FPGA device in mv |
|||
Software Guidelines
When the board powers up, both ATX and fPLL’s must have a stable reference clock in order to lock automatically. If this requirement can not be respected by the system (e.g. the reference clocks are generated by a device that requires software configuration, through an interface implemented in FPGA), the software needs to reconfigure both PLLs, and just after that resets the transceivers.
AMD Xilinx Devices
In AMD Xilinx Devices, the core configures itself to be interfaced with the GT variant supported by the UTIL_ADXCVR core. All the transceiver primitives are configured and programmed identically.
Parameters
Name |
Description |
|---|---|
ID |
Instance identification number, if more than one instance is used |
NUM_OF_LANES |
The number of lanes (primitives) used in this link |
XCVR_TYPE |
Define the current GT type, GTXE2(2), GTHE3(5), GTHE4(7) |
FPGA_TECHNOLOGY |
Encoded value describing the technology/generation of the FPGA device (7series/ultrascale) |
FPGA_FAMILY |
Encoded value describing the family variant of the FPGA device(e.g., zynq, kintex, virtex) |
SPEED_GRADE |
Encoded value describing the FPGA’s speed-grade |
DEV_PACKAGE |
Encoded value describing the device package. The package might affect high-speed interfaces |
FPGA_VOLTAGE |
Contains the value(0-5000 mV) at wich the FPGA device supplied |
TX_OR_RX_N |
If set (0x1), configures the link in transmit mode, otherwise receive |
QPLL_ENABLE |
If set (0x1), configures the link to use QPLL on QUAD basis. If multiple links are sharing the same transceiver, only one of them may enable the QPLL. |
LPM_OR_DFE_N |
Chosing between LPM or DFE of modes for the RX Equalizer |
RATE |
Defines the initial values for Transceiver Control Register (CONTROL 0x0008) |
TX_DIFFCTRL |
Driver Swing Control(TX Configurable Driver) |
TX_POSTCURSOR |
Transmitter post-cursor TX pre-emphasis control |
TX_PRECURSOR |
Transmitter pre-cursor TX pre-emphasis control |
SYS_CLK_SEL |
Selects the PLL reference clock source to drive the RXOUTCLK Table 1 |
OUT_CLK_SEL |
select the transceiver reference clock as the source of TXOUTCLK Table 2 |
Interfaces
Name |
Description |
|---|
Register Map
Address |
Reg Name |
|||||
|---|---|---|---|---|---|---|
HDL |
DWORD |
BITS |
Field Name |
Type |
Default Value |
Description |
0x0 |
0x0 |
VERSION |
Version Register |
|||
[31:0] |
VERSION |
RO |
Version number. |
|||
0x1 |
0x4 |
ID |
Instance Identification Register |
|||
[31:0] |
ID |
RO |
Instance identifier number. |
|||
0x2 |
0x8 |
SCRATCH |
Scratch (GP R/W) Register |
|||
[31:0] |
SCRATCH |
RW |
Scratch register. |
|||
0x4 |
0x10 |
RESETN |
Reset Control Register |
|||
[1] |
BUFSTATUS_RST |
RW |
Initially this flag is held in reset with value 0x1, in order for a user to see the RX BUFSTATUS, this flag needs to be set to 0x0. |
|||
[0] |
RESETN |
RW |
If clear, link is held in reset, set this bit to 0x1 to activate link. Note that the reference clock and DRP clock must be active before setting this bit. |
|||
0x5 |
0x14 |
STATUS |
Status Reporting Register |
|||
[6:5] |
BUFSTATUS |
RO |
BUFSTATUS provides status for either the RX buffer or the TX buffer. If BUFSTATUS is referring to the TX buffer, once BUFSTATUS is set High it remains High until RESETN is activated. Else if BUFSTATUS is referring to the RX buffer, once BUFSTSTATUS is High it can be cleared using BUFSTATUS_RST. If BUFTATUS[6] is 0x1 the internal FIFO overflows and when the BUFSTATUS[5] is 0x1 the internal FIFO underflows. Available from version 17.5.a. For more information consult the transceiver user guide(search for RXBUFSTATUS/TXBUFSTATUS). |
|||
[4] |
PLL_LOCK_N |
RO |
After setting the RESETN bit above, this bit must clear. If does not clears, indicates the CPLL/QPLL did not locked. Available from version 17.4.a |
|||
[0] |
STATUS |
RO |
After setting the RESETN bit above, wait for this bit to set. If set, indicates successful link activation. |
|||
0x7 |
0x1c |
FPGA_INFO |
FPGA device information Xilinx encoded values |
|||
[31:24] |
FPGA_TECHNOLOGY |
RO |
Encoded value describing the technology/generation of the FPGA device (e.g, 7series, ultrascale) |
|||
[23:16] |
FPGA_FAMILY |
RO |
Encoded value describing the family variant of the FPGA device(e.g., zynq, kintex, virtex) |
|||
[15:8] |
SPEED_GRADE |
RO |
Encoded value describing the FPGA’s speed-grade |
|||
[7:0] |
DEV_PACKAGE |
RO |
Encoded value describing the device package. The package might affect high-speed interfaces |
|||
0x8 |
0x20 |
CONTROL |
Transceiver Control Register |
|||
[12] |
LPM_DFE_N |
RW |
Transceiver primitive control, refer Xilinx documentation. |
|||
[10:8] |
RATE |
RW |
Transceiver primitive control, refer Xilinx documentation. |
|||
[5:4] |
SYSCLK_SEL |
RW |
For GTX drives directly the (RX/TX)SYSCLKSEL pin of the transceiver refer to Xilinx documentation. For GTH/GTY drives directly the (RX/TX)PLLCLKSEL pin of the transceiver and indirectly the (RX/TX)SYSCLKSEL pin of the transceiver see Table 1. |
|||
[2:0] |
OUTCLK_SEL |
RW |
Transceiver primitive control Table 2, refer Xilinx documentation. |
|||
0x9 |
0x24 |
GENERIC_INFO |
Physical layer info |
|||
[20] |
QPLL_ENABLE |
RO |
Using QPLL. |
|||
[19:16] |
XCVR_TYPE |
RO |
||||
[13:12] |
LINK_MODE |
RO |
Link layer mode : 01 - 8B10B decoder (aka 204B) 10 - 64B66B decoder (aka 204C); Available from version 17.3.a |
|||
[8] |
TX_OR_RX_N |
RO |
Transceiver type (transmit or receive) |
|||
[7:0] |
NUM_OF_LANES |
RO |
Physical layer number of lanes. |
|||
0x10 |
0x40 |
CM_SEL |
Transceiver Access Register |
|||
[7:0] |
CM_SEL |
RW |
Transceiver common-DRP sel, set to 0xff for broadcast. |
|||
0x11 |
0x44 |
CM_CONTROL |
Transceiver Access Register |
|||
[28] |
CM_WR |
RW |
Transceiver common-DRP sel, set to 0x1 for write, 0x0 for read. |
|||
[27:16] |
CM_ADDR |
RW |
Transceiver common-DRP read/write address. |
|||
[15:0] |
CM_WDATA |
RW |
Transceiver common-DRP write data. |
|||
0x12 |
0x48 |
CM_STATUS |
Transceiver Access Register |
|||
[16] |
CM_BUSY |
RO |
Transceiver common-DRP access busy (0x1) or idle (0x0). |
|||
[15:0] |
CM_RDATA |
RW |
Transceiver common-DRP read data. |
|||
0x18 |
0x60 |
CH_SEL |
Transceiver Access Register |
|||
[7:0] |
CH_SEL |
RW |
Transceiver channel-DRP sel, set to 0xff for broadcast. |
|||
0x19 |
0x64 |
CH_CONTROL |
Transceiver Access Register |
|||
[28] |
CH_WR |
RW |
Transceiver channel-DRP sel, set to 0x1 for write, 0x0 for read. |
|||
[27:16] |
CH_ADDR |
RW |
Transceiver channel-DRP read/write address. |
|||
[15:0] |
CH_WDATA |
RW |
Transceiver channel-DRP write data. |
|||
0x1a |
0x68 |
CH_STATUS |
Transceiver Access Register |
|||
[16] |
CH_BUSY |
RO |
Transceiver channel-DRP access busy (0x1) or idle (0x0). |
|||
[15:0] |
CH_RDATA |
RW |
Transceiver channel-DRP read data. |
|||
0x20 |
0x80 |
ES_SEL |
Transceiver Access Register |
|||
[7:0] |
ES_SEL |
RW |
Transceiver eye-scan-DRP sel, set to 0xff for broadcast. |
|||
0x28 |
0xa0 |
ES_REQ |
Transceiver eye-scan Request Register |
|||
[0] |
ES_REQ |
RW |
Transceiver eye-scan request, set this bit to initiate an eye-scan, this bit auto-clears when scan is complete. |
|||
0x29 |
0xa4 |
ES_CONTROL_1 |
Transceiver eye-scan Control Register |
|||
[4:0] |
ES_PRESCALE |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
0x2a |
0xa8 |
ES_CONTROL_2 |
Transceiver eye-scan Control Register |
|||
[25:24] |
ES_VOFFSET_RANGE |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
[23:16] |
ES_VOFFSET_STEP |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
[15:8] |
ES_VOFFSET_MAX |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
[7:0] |
ES_VOFFSET_MIN |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
0x2b |
0xac |
ES_CONTROL_3 |
Transceiver eye-scan Control Register |
|||
[27:16] |
ES_HOFFSET_MAX |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
[11:0] |
ES_HOFFSET_MIN |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
0x2c |
0xb0 |
ES_CONTROL_4 |
Transceiver eye-scan Control Register |
|||
[11:0] |
ES_HOFFSET_STEP |
RW |
Transceiver eye-scan control, refer Xilinx documentation. |
|||
0x2d |
0xb4 |
ES_CONTROL_5 |
Transceiver eye-scan Control Register |
|||
[31:0] |
ES_STARTADDR |
RW |
Transceiver eye-scan control, DMA start address (ES data is written to this memory address). |
|||
0x2e |
0xb8 |
ES_STATUS |
Transceiver eye-scan Status Register |
|||
[0] |
ES_STATUS |
RO |
If set, indicates an error in ES DMA. |
|||
0x2f |
0xbc |
ES_RESET |
Transceiver eye-scan reset control register |
|||
[n] |
ES_RESETn |
RW |
Controls the EYESCANRESET pin of the GTH/GTY transceivers for lane n. Where n is from 0 to 31. |
|||
0x30 |
0xc0 |
TX_DIFFCTRL |
Transceiver primitive control, refer Xilinx documentation. |
|||
[31:0] |
TX_DIFFCTRL |
RW |
TX driver swing control. |
|||
0x31 |
0xc4 |
TX_POSTCURSOR |
Transceiver primitive control, refer Xilinx documentation. |
|||
[31:0] |
TX_POSTCURSOR |
RW |
Transmiter post-cursor TX pre-emphasis control. |
|||
0x32 |
0xc8 |
TX_PRECURSOR |
Transceiver primitive control, refer Xilinx documentation. |
|||
[31:0] |
TX_PRECURSOR |
RW |
Transmiter pre-cursor TX pre-emphasis control. |
|||
0x50 |
0x140 |
FPGA_VOLTAGE |
FPGA device voltage information |
|||
[15:0] |
FPGA_VOLTAGE |
RO |
The voltage of the FPGA device in mv |
|||
0x60 |
0x180 |
PRBS_CNTRL |
Transceiver PRBS control |
|||
[16] |
PRBSFORCEERR |
RW |
Valid for TX. If set, a single error is forced in the PRBS transmitter for every clock cycle. Can be used to test the PRBS checkers on the other side of the link. |
|||
[8] |
PRBSCNTRESET |
RW |
Valid for RX. Resets the PRBS error counter from the transceiver. Does not self clears. Value of error counter must be accessed via DRP. |
|||
[3:0] |
PRBSSEL |
RW |
PRBS checker or generator test pattern control. All zeros will put the PRBS in bypass mode. For TX non-zero values will stop the normal dataflow from link layer and will inject a pattern instead. See transceiver guide for specific values. |
|||
0x61 |
0x184 |
PRBS_STATUS |
RX Transceiver PRBS status |
|||
[8] |
PRBSERR |
RO |
This sticky status output indicates that PRBS errors have occurred. Value of error counter must be accessed via DRP. |
|||
[0] |
PRBSLOCKED |
RO |
Ignore this bit for GTX transceivers. For others: Indicates that the RX PRBS checker has been error free for 15 XCLK cycles after reset. Once asserted High, it does not deassert until reset of the RX pattern checker via PRBSCNTRESET |
|||
Software Guidelines
The system must have active DRP and reference clocks before any software access. The software is expected to write necessary control parameters to LPM_DFE_N, RATE, SYSCLK_SEL, OUTCLK_SEL register bits and then set RESETN bit to 0x1. After that, monitor the STATUS bit to be set. There are no other requirements for initialization.
The DRP access is identical for common and channel interfaces. The SEL bits may be set to a specific transceiver lane or 0xff to broadcast. A write to the CONTROL register (bits WR, ADDR, WDATA) initiates DRP access in hardware. A read to this register has no effect. In order to write to the transceiver, set WR to 0x1 with the address. In order to read from the transceiver, set WR to 0x0 with the address. As soon as this register is written, the BUSY signal is set and is cleared only after the access is complete. The broadcast read is a logical OR of all the channels. After an access is started, do NOT interrupt the core for any reason (including setting RESETN to 0x0), allow the access to finish itself. Though the core itself is immune to a software abort, the transceiver may fail on further accesses and may require a system-wide reset.
The eye-scan feature also allows a SEL option and a broadcast has the effect of a combined mask. That is, the error counter will be zero ONLY if all the transceiver error counters are zero. To start eye-scan, set ES_REQ to 0x1 and wait for the same bit to self-clear. If eye-scan needs to be stopped, set the ES_REQ bit to 0x0.
Table 1
SYSCLK_SEL |
00 |
01 |
10 |
11 |
|---|---|---|---|---|
GTXE2 |
CPLL |
RESERVED |
RESERVED |
QPLL |
GTHE3 |
CPLL |
RESERVED |
QPLL1 |
QPLL0 |
GTHE4 |
CPLL |
RESERVED |
QPLL1 |
QPLL0 |
GTYE4 |
CPLL |
RESERVED |
QPLL1 |
QPLL0 |
Table 2
OUTCLK_SEL |
001 |
010 |
011 |
100 |
101 |
All other combinations |
|---|---|---|---|---|---|---|
GTXE2 |
OUTCLKPCS |
OUTCLKPMA |
REFCLK |
REFCLK/2 |
RESERVED |
RESERVED |
GTHE3 |
OUTCLKPCS |
OUTCLKPMA |
REFCLK |
REFCLK/2 |
PROGDIVCLK |
RESERVED |
GTHE4 |
OUTCLKPCS |
OUTCLKPMA |
REFCLK |
REFCLK/2 |
PROGDIVCLK |
RESERVED |
GTYE4 |
OUTCLKPCS |
OUTCLKPMA |
REFCLK |
REFCLK/2 |
PROGDIVCLK |
RESERVED |
The REFCLK selected by OUTCLK_SEL depends on the SYSCLK_SEL, it may be CPLL, QPLL0 or QPLL1 refclk.
Physical layer PRBS testing
The PRBS_CNTRL and PRBS_STATUS registers expose controls of internal PRBS generators and checkers allowing the testing the multi-gigabit serial link at the physical layer without the need of the link layer bringup.
TX link procedure
Configure the reference clock and device clocks for under test lane rate. Bring XCVR out from reset.
In the PRBS_CNTRL registers set PRBSSEL to a non-zero value. See the transceiver guides for exact values, different transceiver families may have different encoding for the same pattern.
On the receiving side of the link, set the checker for the same pattern and reset the error counters.
No error should be recorded on the receiver side.
Set the PRBSFORCEERR bit in the PRBS_CNTRL register to force the error injection into the stream of bits.
The error should be detected and recorded on the receiver side.
RX link procedure
Configure the reference clock and device clocks for under test lane rate. Bring XCVR out from reset.
On the transmit side of the link, set a test pattern that is available in the receiving transceiver. Consult the transceiver documentation for details.
In the PRBS_CNTRL registers set PRBSSEL to the corresponding pattern. Reset the error counters with PRBSCNTRESET.
Check PRBS_STATUS fields for results. If the check is successful for non-GTX transceivers the PRBSLOCKED bit must appear as set and PRBSERR must stay low. For GTX transceivers the PRBSLOCKED bit can be ignored and checking the PRBSERR alone is sufficient. If PRBSERR is set, check with DRP accesses the internal error counter to get the number of errors received. See the transceiver guide for details.
Software Support
No-OS project at drivers/axi_core/jesd204
No-OS device driver at drivers/axi_core/jesd204/axi_adxcvr.c
No-OS device driver documentation on wiki
Linux project at linux/drivers/iio/jesd204
Linux device driver at drivers/iio/jesd204/axi_adxcvr.c
Linux device driver documentation on wiki
References
HDL Intel IP core at library/intel/axi_adxcvr
HDL Xilinx IP core at library/xilinx/axi_adxcvr
Ultrascale Architecture GTH Transceivers User Guide - AMD Xilinx