AXI ADC Decimate

?axi_adc_decimate IP-XACT not found.Generate it and the documentation:(cd library/axi_adc_decimate; make)(cd docs; make html)

The AXI ADC Decimate IP core allows decimating the input data by 10/100/1000/10000/100000, with filtering and arbitrary decimation by dropping samples.

More about the generic framework interfacing ADCs can be read here at Generic AXI ADC.

Important

The axi_adc_decimate was designed to interface with 12-bit converters. Even though the input data bus width is 16, it will not work with anything higher than 12-bit sign extended (to 16-bit) data.

Features

  • AXI Lite control/status interface

  • Allows decimation by 10/100/1000/10000/100000 with filtering

  • Allows arbitrary decimation by dropping samples

  • Filtering is implemented by a 6-section CIC programmable rate filter and a compensation FIR filter.

Files

Name

Description

library/axi_adc_decimate/axi_adc_decimate.v

Verilog source for the peripheral.

Block Diagram

AXI ADC Decimate block diagram

Configuration Parameters

Name

Description

CORRECTION_DISABLE

Disable scale correction of the CIC output

Interface

Name

Description

adc_clk

Clock input

adc_rst

Reset, synchronous on the adc_clk clock domain

adc_data_a

Analog data for channel A

adc_data_b

Analog data for channel B

adc_valid_a

Data valid signal for channel A

adc_valid_b

Data valid signal for channel B

adc_dec_data_a

Decimated data for channel A

adc_dec_data_b

Decimated data for channel B

adc_dec_valid_a

Data valid for channel A

adc_dec_valid_b

Data valid for channel B

adc_data_rate

Data rate (decimation ratio)

adc_oversampling_en

Data oversampling enabled

s_axi

Standard AXI Slave Memory Map interface

Detailed Description

For some applications, the maximum sampling rate is not required and leads to lots of samples transferred to memory. To avoid it, the decimation IP can be used.

The decimation block allows decimating the input data so that the sampling frequency can be reduced by 10, 100, 1000, 10000, 100000, with filtering.

The filtering is implemented by a 6-section CIC programmable rate filter which allows decimation by 5/50/500/5000/50000 and a compensation FIR filter (decimation by 2).

At the end of the filter chain, there is an arbitrary decimation block. The arbitrary decimation can be activated independently and it does not implement any type of filtering.

Register Map

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 0x0 VERSION

Version of the peripheral. Follows semantic versioning. Current version 1.0.0.

[31:16] VERSION_MAJOR RO 0x0001

[15:8] VERSION_MINOR RO 0x00

[7:0] VERSION_PATCH RO 0x00

0x1 0x4 SCRATCH

[31:0] SCRATCH RW 0x00000000

Scratch register useful for debug.

0x10 0x40 DECIMATION_RATIO

Control Arbitrary Decimation Ratio.

[31:0] DECIMATION_RATIO RW 0x00000000

Set the arbitrary decimation ratio at the end of the decimation chain. Simply drop samples.

0x11 0x44 DECIMATION_STAGE_ENABLE

Control Filtered Decimation.

[2:0] FILTERED_DECIMATION_RATIO RW 0x0

Enables the filtered decimation: 0: No filtered decimation 1: Decimation by 10. Result should be corrected by a 1.05 factor 2: Decimation by 100. Result should be corrected by a 1.1 factor 3: Decimation by 1000. Result should be corrected by a 1.15 factor 6: Decimation by 10000. Result should be corrected by a 1.2 factor 7: Decimation by 100000. Result should be corrected by a 1.26 factor default: No filtered decimation

0x12 0x48 CONFIG

Configuration Register

[1] CORRECTION_ENABLE_B RW 0x0

If set to 1, correction is enabled on channel B. The decimated data will be multiplied with the value from the CORRECTION_COEFFICIENT_B register.

[0] CORRECTION_ENABLE_A RW 0x0

If set to 1, correction is enabled on channel A. The decimated data will be multiplied with the value from the CORRECTION_COEFFICIENT_A register.

0x13 0x4c CORRECTION_COEFFICIENT_A

Correction Coefficient A

[15:0] CORRECTION_COEFFICIENT RW 0x0000

Scale correction (if equipped) coefficient for channel A. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification.

0x14 0x50 CORRECTION_COEFFICIENT_B

Correction Coefficient B

[15:0] CORRECTION_COEFFICIENT RW 0x0000

Scale correction (if equipped) coefficient for channel B. The format is 1.1.14 (sign, integer and fractional bits). Allows for correction of the CIC filter amplification.

Access Type

Name

Description

RO

Read-only

Reads will return the current register value. Writes have no effect.

RW

Read-write

Reads will return the current register value. Writes will change the current register value.

References