AXI TDD

?axi_tdd IP-XACT not found.Generate it and the documentation:(cd library/axi_tdd; make)(cd docs; make html)

The AXI Time-Division Duplexing Controller IP core is a pulse wave generator capable of addressing RF applications which require Time Division Duplexing, as well as controlling other modules of general applications through its dedicated 32 channel outputs.

The reason of creating the generic TDD controller was to reduce the naming confusion around the existing repurposed TDD core built for AD9361, as well as expanding its number of output channels for systems which require more than six controlling signals.

Note

TDD (Time-Division Duplex) mode allows the user to control the time period of the receive and transmit bursts.

Features

  • Up to 32 independent output channels

  • Start/stop time values per channel

  • Enable and polarity bit values per channel

  • 32 bit-max internal reference counter

  • Initial startup delay before wave generation

  • Configurable frame length and number of frames per burst

  • 3 sources of synchronization: external, internal and software generated

Files

Name

Description

library/axi_tdd/axi_tdd.sv

Top module.

library/axi_tdd/axi_tdd_pkg.sv

SystemVerilog Package.

library/axi_tdd/axi_tdd_regmap.sv

Register Map with CDC synchronizers.

library/axi_tdd/axi_tdd_counter.sv

Internal counters and FSM logic.

library/axi_tdd/axi_tdd_channel.sv

Channel waveform generator.

library/axi_tdd/axi_tdd_sync_gen.sv

Synchronization pulse generator.

library/axi_tdd/axi_tdd_ip.tcl

TCL script to generate the Vivado IP-integrator project.

library/axi_tdd/axi_tdd_hw.tcl

TCL script to generate the Quartus IP-integrator project.

Configuration Parameters

Name

Description

ID

Instance identification number

CHANNEL_COUNT

Number of channels

DEFAULT_POLARITY

Initial channel polarity

REGISTER_WIDTH

Internal counter and register width

BURST_COUNT_WIDTH

Burst counter width

SYNC_INTERNAL

Enable support for internal sync signal

SYNC_EXTERNAL

Enable support for external sync signal

SYNC_EXTERNAL_CDC

Enable synchronization of external sync signal

SYNC_COUNT_WIDTH

Sync generator counter width

Interface

Name

Description

s_axi_aclk

System clock.

s_axi_aresetn

System reset, synchronous active low reset.

s_axi

AXI-Lite bus slave, memory mapped AXI-Lite bus that provides access to module’s register map.

clk

Core clock.

resetn

Core reset, synchronous active low reset.

sync_in

External synchronization input signal.

sync_out

Module synchronization output signal.

tdd_channel

Channels output.

Theory of Operation

The central idea of the TDD controller is “frame”-based operation, i.e. all the timing defined for the individual channels is relative to the beginning of a frame. The FRAME_LENGTH value controls the length of a single frame, while the BURST_COUNT value controls how many frames should be played after enabling the device (a value of 0 means the frames will be repeated indefinitely). Before the start of a burst, an optional startup delay is inserted, defined by the STARTUP_DELAY value in clock cycles.

../../_images/diagram.svg

This diagram illustrates how different channels can be enabled at different times relative to the beginning of a frame.

Note

While the above graphic shows all channels being enabled in a stacked manner, they are completely independent of each other.

Detailed Description

In order to begin its operation, the peripheral must be enabled. This is done by setting the ENABLE bit. Next, the peripheral waits to receive a synchronization signal. There are 3 possible sync sources, which can be independently activated through their corresponding enabling bits: SYNC_INT, SYNC_EXT and SYNC_SOFT can all be active at the same time.

The external synchronization capability allows the alignment of frames between multiple devices in different locations, for example using a GPSDO 1 PPS output. The internal sync signal is generated based on a dedicated counter, when its value matches the one defined in SYNC_PERIOD_LOW / SYNC_PERIOD_HIGH. The software generated sync pulse is triggered at an arbitrary point in time when writing a ‘1’ value in SYNC_SOFT.

The next diagram shows the peripheral’s FSM, which transitions between 4 states: IDLE, ARMED, WAITING and RUNNING.

../../_images/fsm.svg

In case a synchronization signal is received while the TDD core is running, the signal can reset the internal counter to zero by setting SYNC_RST to ‘1’. This can alter the counter value in both WAITING or RUNNING states.

The generic TDD controller can have up to 32 output channels, each of them having its unique values when the channel is set/reset under CHX_ON / CHX_OFF. They are continuously compared to the internal counter’s value while the core is RUNNING.

Every bit in CHANNEL_ENABLE / CHANNEL_POLARITY corresponds to a specific channel. The bit position is correlated to the channel index, so the LSB will always be associated with CH0 and the MSB with CH31.

The following registers will not be updated unless the peripheral is disabled:

  • BURST_COUNT

  • STARTUP_DELAY

  • FRAME_LENGTH

  • CHANNEL_POLARITY

  • SYNC_PERIOD_LOW

  • SYNC_PERIOD_HIGH

  • CHX_ON

  • CHX_OFF

The user must configure them before enabling the peripheral. Any subsequent write while the peripheral is enabled will be ignored.

An exception to this rule is CHANNEL_ENABLE, which allows enabling / disabling independent channels on-the-fly. The new value will come into effect when in ARMED state or at the end of a frame. CONTROL can also be modified on-the-fly with immediate effect (after going through the synchronization stage).

STATUS can be used for debugging purposes, reflecting the current peripheral state.

By adapting the synthesis parameters to the application requirements, the module is highly flexible and can substantially reduce resource utilization.

Register Map

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x0 0x0 VERSION

Version of the peripheral. Follows semantic versioning. Current version 2.00.62.

[31:16] VERSION_MAJOR RO 0x0002

[15:8] VERSION_MINOR RO 0x00

[7:0] VERSION_PATCH RO 0x62

0x1 0x4 PERIPHERAL_ID

[31:0] PERIPHERAL_ID RO ID

Value of the ID configuration parameter.

0x2 0x8 SCRATCH

[31:0] SCRATCH RW 0x00000000

Scratch register useful for debug.

0x3 0xc IDENTIFICATION

[31:0] IDENTIFICATION RO 0x5444444e

Peripheral identification (‘T’, ‘D’, ‘D’, ‘N’).

0x4 0x10 INTERFACE_DESCRIPTION

[30:24] SYNC_COUNT_WIDTH RO SYNC_​COUNT_​WIDTH

Width of internal synchronization counter.

[21:16] BURST_COUNT_WIDTH RO BURST_​COUNT_​WIDTH

Width of burst counter.

[13:8] REGISTER_WIDTH RO REGISTER_​WIDTH

Width of internal reference counter and timing registers.

[7] SYNC_EXTERNAL_CDC RO SYNC_​EXTERNAL_​CDC

Enable CDC for external synchronization pulse.

[6] SYNC_EXTERNAL RO SYNC_​EXTERNAL

Enable external synchronization support.

[5] SYNC_INTERNAL RO SYNC_​INTERNAL

Enable internal synchronization support.

[4:0] CHANNEL_COUNT_EXTRA RO CHANNEL_​COUNT_​EXTRA

Number of channels starting from CH1, excluding CH0. CHANNEL_COUNT_EXTRA = CHANNEL_COUNT-1

0x5 0x14 DEFAULT_POLARITY

[31:0] DEFAULT_POLARITY RO DEFAULT_​POLARITY

Default polarity per every channel - LSB corresponds to CH0, MSB to CH31.

0x10 0x40 CONTROL

TDD Control

[4] SYNC_SOFT RW1C 0x0

Trigger the TDD core through a register write.

[3] SYNC_EXT RW 0x0

Enable external sync trigger. This bit is implemented if SYNC_EXTERNAL is set.

[2] SYNC_INT RW 0x0

Enable internal sync trigger. This bit is implemented if SYNC_INTERNAL is set.

[1] SYNC_RST RW 0x0

Reset the internal counter while running when receiving a sync event.

[0] ENABLE RW 0x0

Module enable.

0x11 0x44 CHANNEL_ENABLE

TDD Channel Enable

[31:0] CHANNEL_ENABLE RW 0x00000000

Enable bits per channel - LSB corresponds to CH0, MSB to CH31.

0x12 0x48 CHANNEL_POLARITY

TDD Channel Polarity

[31:0] CHANNEL_POLARITY RW 0x00000000

Polarity bits per channel - LSB corresponds to CH0, MSB to CH31.

0x13 0x4c BURST_COUNT

TDD Number of frames per burst

[31:0] BURST_COUNT RW 0x00000000

If set to 0 and enabled - the controller operates in TDD mode as long as the ENABLE bit is set. If set to a non-zero value, the controller operates for the set number of frames and then stops.

0x14 0x50 STARTUP_DELAY

TDD Transmission startup delay

[31:0] STARTUP_DELAY RW 0x00000000

The initial delay value before the beginning of the first frame; defined in clock cycles-1.

0x15 0x54 FRAME_LENGTH

TDD Frame length

[31:0] FRAME_LENGTH RW 0x00000000

The length of the transmission frame; defined in clock cycles-1.

0x16 0x58 SYNC_PERIOD_LOW

TDD Sync counter

[31:0] SYNC_PERIOD_LOW RW 0x00000000

The LSB slice of the internal sync pulse period defined in clock cycles-1. This register is implemented if SYNC_COUNT_WIDTH>0.

0x17 0x5c SYNC_PERIOD_HIGH

TDD Sync counter

[31:0] SYNC_PERIOD_HIGH RW 0x00000000

The MSB slice of the internal sync pulse period defined in clock cycles-1. This register is implemented if SYNC_COUNT_WIDTH>32.

0x18 0x60 STATUS

Peripheral Status

[1:0] STATE RO 0x0

The current state of the peripheral FSM; used for debugging purposes.

0x20 + 0x2*n 0x80 + 0x8*n CHn_ON

Channel Set Where n is from 0 to 31.

[31:0] CHn_ON RW 0x00000000

The offset (from frame count equal zero), when CHn is set.

0x21 + 0x2*n 0x84 + 0x8*n CHn_OFF

Channel Reset Where n is from 0 to 31.

[31:0] CHn_OFF RW 0x00000000

The offset (from frame count equal zero), when CHn is reset.

Access Type

Name

Description

RO

Read-only

Reads will return the current register value. Writes have no effect.

RW

Read-write

Reads will return the current register value. Writes will change the current register value.

RW1C

Read,write-1-to-clear

Reads will return the current register value. Writing the register will clear those bits of the register which were set to 1 in the value written. Bits are set by hardware.

References