MAX96724 HDL project

Overview

The MAX96724 deserializer converts four GMSL™2/1 inputs to 1, 2, or 4 MIPI D-PHY or C-PHY outputs. The device allows simultaneous transmit bidirectional transmissions over 50Ω coax or 100Ω STP cables that meet the GMSL channel specification.

Up to four remotely located sensors can be supported using industry-standard coax or STP interconnects. Each GMSL2 serial link operates at a fixed rate of 3 Gbps or 6 Gbps in the forward direction and 187.5Mbps in the reverse direction. The MAX96724/F/R supports both aggregation and replication of video data, enabling streams from multiple remotely located sensors to be combined and routed to one or more of the available CSI-2 outputs.

The MAX96724 DPHY Evaluation Kit (EV Kit) provides a proven design and reliable platform to evaluate the MAX96724 device using standard FAKRA coaxial cables.

Supported boards

Supported devices

Supported carriers

Block design

The data path designed in this reference design is as follows:

  • the virtual channel inputs of one CSI-2 output port of the deserializer are captured using Xilinx’s MIPI CSI-2 Rx Subsystem IP

  • data is written into memory by using a Xilinx video-related DMA implementation Video Framebuffer Write

  • the control of the camera modules is realized through I2C using Xilinx’s AXI IIC logic

Block diagram

The data path (through the deserializer) and the writing in memory are illustrated in the block diagram.

MAX96724 EVKIT HDL-related block diagram

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Address

mipi_csi2_rx_subsyst_0

0x84A0_0000

axi_iic_mipi

0x84A2_0000

v_frmbuf_wr_0

0x84A4_0000

v_frmbuf_wr_1

0x84A6_0000

v_frmbuf_wr_2

0x84A8_0000

v_frmbuf_wr_3

0x84AA_0000

axi_sysid_0

0x8500_0000

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

iic_fmc

axi_iic_mipi

0x84A2_0000

—

GPIOs

The Software GPIO number is calculated as follows:

  • ZynqMP: if PS8 EMIOs are used, then offset is 78

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

ZynqMP

fan_en_b

OUT

0

78

csirxss_rstn

OUT

1

79

ap_rstn_frmbuf_0

OUT

2

80

ap_rstn_frmbuf_1

OUT

3

81

ap_rstn_frmbuf_2

OUT

4

82

ap_rstn_frmbuf_3

OUT

5

83

rpi_en

OUT

6

84

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux ZynqMP

Actual ZynqMP

csirxss_irq

13

109

141

iic2intc_irpt

12

108

140

v_frmbuf_wr0/interrupt

11

107

139

v_frmbuf_wr1/interrupt

10

106

138

v_frmbuf_wr2/interrupt

9

105

137

v_frmbuf_wr3/interrupt

8

104

136

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source, you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/max96724/kv260
~/hdl/projects/max96724/kv260$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.