AXI HDMI RX

?axi_hdmi_rx IP-XACT not found.Generate it and the documentation:(cd library/axi_hdmi_rx; make)(cd docs; make html)

The AXI HDMI RX IP core can be used to interface the ADV7611 device using an FPGA.

Features

  • AXI based configuration

  • Supports multiple resolution (max 1080p)

  • Supports embedded sync video reception (16bit data)

  • YCbCr or RGB color space output

  • Supported on FMC-IMAGEON Xilinx Reference Design

Files

Name

Description

library/axi_hdmi_rx/axi_hdmi_rx.v

Verilog source for the peripheral.

Block Diagram

AXI HDMI RX block diagram

Configuration Parameters

Name

Description

ID

Core ID should be unique for each axi_hdmi_rx IP in the system.

IO_INTERFACE

Type of the IO interface. 0 - Allow sampling of data on falling edge of the HDMI clock. others - always sample the input data on rising edge.

Interfaces

Name

Description

hdmi_rx_clk

Pixel clock.

hdmi_rx_data

HDMI data.

s_axi

DMA AXIS interface (vdma).

hdmi_clk

Output clock.

hdmi_dma_sof

Start of frame.

hdmi_dma_de

Data enable.

hdmi_dma_data

HDMI DMA data.

hdmi_dma_ovf

Data overflow signal.

hdmi_dma_unf

Data underflow signal.

Detailed description

The top module (axi_hdmi_rx), instantiates:

  • axi_hdmi_rx_core module

  • the HDMI RX register map

  • the AXI handling interface

In axi_hdmi_rx_core module the video information is manipulated by passing through several processing blocks (see Block Diagram):

  • Embedded Sync module acquires the video information and splits it into video data and synchronization signals.

  • Chroma supersampling block, super samples the video information to obtain a 24 bit video information, has no impact on the video quality.

  • CSC (Color Space Conversion) –converts the video information from YCbCr color space to RGB color space. If YCbCr is the desired output color space the CSC block can be bypassed by setting to 1 the value of CSC_BYPASS in CNTRL register.

  • Sync monitoring - monitors the recovered hsync and vsync against the programmed expected resolution. Asserts out of sync and resolutions mismatch indicators in the TPM_STATUS2 register.

Register Map

Address

Reg Name

HDL

DWORD

BITS

Field Name

Type

Default Value

Description

0x10 0x40 RSTN_RX

HDMI Interface Control & Status

[0] RSTN RW 0x0

Reset, a common reset is used for all the interface modules, The default is reset (0x0), software must write 0x1 to bring up the core.

0x11 0x44 CNTRL

HDMI Interface Control & Status

[3] EDGE_SEL RW 0x0

If set (0x1), incoming data is registered on the falling edge of the clock first. The default uses rising edge.

[2] BGR RW 0x0

If set (0x1), output BGR. The default is RGB.

[1] PACKED RW 0x0

If set (0x1) pack 24bit RGB data on 32bit dwords. The default pads the MSB to zeros.

[0] CSC_BYPASS RW 0x0

If set (0x1) bypasses color space conversion (if equipped).

0x15 0x54 CLK_FREQ_RX

HDMI Interface Control & Status

[31:0] CLK_FREQ RO 0x00000000

Interface clock frequency. This is relative to the processor clock and in many cases is 100MHz. The number is represented as unsigned 16.16 format. Assuming a 100MHz processor clock the minimum is 1.523kHz and maximum is 6.554THz. The actual interface clock is CLK_FREQ * CLK_RATIO (see below). Note that the actual sampling clock may not be the same as the interface clock- software must consider device specific implementation parameters to calculate the final sampling clock.

0x16 0x58 CLK_RATIO_RX

HDMI Interface Control & Status

[31:0] CLK_RATIO RO 0x00000000

Interface clock ratio - as a factor actual received clock. This is implementation specific and depends on any serial to parallel conversion and interface type (ddr/sdr/qdr).

0x18 0x60 VDMA_STATUS_RX

HDMI Interface Control & Status

[1] VDMA_OVF RW1C 0x0

If set, indicates vdma overflow.

[0] VDMA_UNF RW1C 0x0

If set, indicates vdma underflow.

0x19 0x64 TPM_STATUS1

HDMI Interface Control & Status

[1] HDMI_TPM_OOS RW1C 0x0

If set, indicates TPM OOS at the HDMI interface.

0x20 0x80 TPM_STATUS2

HDMI Interface Control & Status

[3] VS_OOS RW1C 0x0

If set, indicates VSYNC OOS - the core is unabled to detect/track VSYNC. Consecutive frames have different number of lines.

[2] HS_OOS RW1C 0x0

If set, indicates HSYNC OOS - the core is unabled to detect/track HSYNC. Consecutive lines have different lengths.

[1] VS_MISMATCH RW1C 0x0

If set, indicates received (detected) & programmed VSYNC (number of lines) mismatch. Incoming frames are stable but not the expected resolution.

[0] HS_MISMATCH RW1C 0x0

If set, indicates received (detected) & programmed HSYNC (number of pixels) mismatch. Incoming frames are stable but not the expected resolution.

0x100 0x400 HVCOUNTS1

HDMI Interface Control & Status

[31:16] VS_COUNT RW 0x0000

This is the expected active horizontal pixel lines (active resolution length). e.g. 1080 (1080p)

[15:0] HS_COUNT RW 0x0000

This is the expected horizontal pixel count (no. of pixel clocks per line). e.g. 1920 (1080p)

0x101 0x404 HVCOUNTS2

HDMI Interface Control & Status

[31:16] VS_COUNT RO 0x0000

This is the detected horizontal active pixel lines (active resolution length). This field is valid only if VS_OOS is zero.

[15:0] HS_COUNT RO 0x0000

This is the detected horizontal pixel count (no. of pixel clocks per line). This field is valid only if HS_OOS is zero.

Access Type

Name

Description

RW

Read-write

Reads will return the current register value. Writes will change the current register value.

RO

Read-only

Reads will return the current register value. Writes have no effect.

RW1C

Read,write-1-to-clear

Reads will return the current register value. Writing the register will clear those bits of the register which were set to 1 in the value written. Bits are set by hardware.

Design considerations

Additional IPs needed:

The AXI DMAC is used to get the video information from the core into memory. The audio path is separated from the video path, for audio axi_spdif_tx core is needed to receive the audio information from the ADV7611 device and transmit it to the memory. The whole system needs to be controlled by a processor (ARM or a softcore) that can program the registers.

Software support

The core can be controlled by no-Os or Linux

References