DC2677A HDL project

Overview

Demonstration circuit 2677A (DC2677A) is a reference design for robust industrial data acquisition applications for the LTC2358-18. The LTC2358-18 is capable of high voltage measurements with a large input common range; however, the DC2677A implements input protection that allows up to 400V of continuous input protection. Combined with gas discharge tubes, which provide protection from surges, the DC2677A is capable of surviving extreme abuse.

This reference design includes the LTC2358-18 SAR ADC, ADA4522-2 dual zero-drift operational amplifier, and an LT6658 dual-output, high current reference for sensor excitation.

The digital interface is an HSMC (high-speed mezzanine connector), which is compatible with Altera Cyclone V SoCkit and other Altera FPGA evaluation boards that support 3.3V CMOS I/O.

Applications:

  • Programmable Logic Controllers

  • Industrial Process Control

  • Power Line Monitoring

  • Test and Measurement

Supported boards

Supported devices

Supported carriers

  • C5SoC (Cyclone V SoC) HSMC

Block design

Block diagram

The data path and clock domains are depicted in the below diagram:

DC2677A block diagram

Jumper setup

Jumper/Solder link

Position

Description

J15

Short Pin 2-3

CLKSEL0 - Default for clock connection on HPS

J16

Short Pin 2-3

CLKSEL1 - Default for clock connection on HPS

J17

Short Pin 1-2

BOOTSEL0 - Needed for SD card boot

J19

Short Pin 2-3

BOOTSEL1 - Needed for SD card boot

J18

Short Pin 1-2

BOOTSEL2 - Needed for SD card boot

JP2

Short Pin 7-8

HSMC Voltage level setting. Set to 3.3V

SW6[4:0]

10010

MSEL - Sets configuration scheme to default ASx4 mode. (1 = OFF, 0 = ON).

Hardware setup

Signal

DC2677A Testpoint

Cyclone V SoCKit HSMC LTC2358/LTC2357/LTC2353

sdo[0]

SDO0

lvds_rxn1/lvds_rxn2/lvds_rxp3

sdo[1]

—

lvds_rxp2/lvds_rxp3/lvds_rxn4

sdo[2]

—

lvds_rxn2/lvds_rxn4

sdo[3]

—

lvds_rxp3/lvds_rxp5

sdo[4]

—

lvds_rxn4

sdo[5]

—

lvds_rxp5

sdo[6]

—

lvds_rxn5

sdo[7]

SDO7

lvds_rxp6

sdi

SDI

lvds_rxn6

scki

—

lvds_rxn3

scko

—

lvds_rxp4

lvds_cmos_n

LVDS/CMOS

lvds_rxp1

cnv

CNV

lvds_rxp0

busy

BUSY

lvds_rxp7

cs_n

CSL

lvds_rxn7

pd

PD

lvds_rxn0

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Cyclone V

axi_ltc235x

0xff320000

adc_pwm_gen

0xff340000

axi_adc_dma

0xff300000

GPIOs

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Cyclone V

cs_n

OUT

1

1

pd

OUT

0

0

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Cyclone V

Actual Cyclone V

video_dmac

4

44

76

axi_adc_dma

2

42

74

sys_spi

1

41

73

sys_gpio_bd

0

40

72

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/dc2677a/c5soc
~/hdl/projects/dc2677a/c5soc$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.