HDL Architecture

Every HDL design of a reference project can be divided into:

  1. Base design for the carrier board (projects/common/$CARRIER) — description of what the carrier contains

    • an embedded processor - soft or hard;

    • all the peripheral IPs (that are necessary to run a Linux distribution on the system);

    • these designs are specific to each carrier, making them carrier dependent;

    • it describes part of the system_wrapper module;

    • located in projects/common; one for each carrier;

    • here we do most of the PS configuration, add SPI, I2C and GPIOs;

    • in some cases, we have scripts to instantiate the PL DDR as ADC offload memory or DAC offload memory.

  2. Base design for the evaluation board (projects/$EVAL_BOARD/common) — description of what the evaluation contains

    • instantiates all the necessary IPs to control the evaluation board and to capture or send data;

    • the data paths defined in this block design are common across multiple carrier platforms, making them carrier independent;

    • it describes part of the system_wrapper module;

    • located at hdl/projects/$EVAL_BOARD/common (*_bd.tcl for AMD Xilinx FPGAs, and *_qsys.tcl for Intel FPGAs).

  3. Specific design for the system (projects/$EVAL_BOARD/$CARRIER)

    • we source the carrier board configuration (#1), then the evaluation board configuration (#2) and then we do some specific parameter modification, if required.

How they’re instantiated

In case of a project, inside the system_bd.tcl file we have to source the base design of the carrier first (#1), then the base design of the evaluation board (#2).

Example

Take FMCOMMS2 with ZedBoard; the system_bd.tcl file will have the following designs sourced to be used:

source $ad_hdl_dir/projects/common/zed/zed_system_bd.tcl
source ../common/fmcomms2_bd.tcl

Typical project diagram

../_images/base_platform.svg

Base Design

The base design contains all the I/O peripherals, memory interfaces and processing components, which are necessary for a fully functional Linux system. The majority of these components are Intel and AMD Xilinx IP cores.

Usually, they contain:

  • Microprocessor

  • Memory interface controller

  • Peripheral interfaces

Microprocessor

In our designs, we use only three types:

Intel

AMD Xilinx

Lattice

SoC

FPGA

SoC

FPGA

ACAP

FPGA

HPS

NIOS II

PS7 PS8

MicroBlaze

Versal

riscv-rx

Worth mentioning in case of SoCs, the Hard Processor System (HPS) or Processing System 7/8 (PS7/8) do not contain just the dual-core ARM® Cortex® - A9 MPCore™ processor, they also have other integrated peripherals and memory interfaces. For more information please visit the manufacturer’s website, listed in the table above.

Memory interface controller

In almost all cases, the carrier board is not made and designed by Analog Devices, so the external memory solution of the system is given.

Meaning, we cannot support, modify or alter this important part of the system. In several cases we even have system limitations because of it (e.g. the memory interface is not fast enough to handle the required data throughput).

In the following two links, one can find the landing page of the available memory solutions for Intel and AMD:

Peripheral interfaces

These interfaces are used to control external peripherals located on the prototyping board or the FMC I/O board.

In HDL, these ports are named slightly different than how they’re in the documentations. Thus, to make it easier for beginners, here you have the naming of the ports depending on the microprocessor used.

CPU/Memory interconnects addresses

The memory addresses that will be used by software are based on the HDL addresses of the IP register map, to which an offset is added, depending on the architecture of the used FPGA (see also ad_cpu_interconnect procedure; architecture is specified by sys_zynq variable, for AMD FPGAs).

Zynq-7000 and 7 Series

Because this was the original target, this is the reference address used, the common one, to which depending on the architecture, you add an offset to get to the address space for the peripherals (as they differ from one to the other).

Zynq UltraScale+ MP

If the address is between 0x4000_0000 - 0x4FFF_FFFF then the AXI peripherics will be placed in 0x8000_0000 - 0x8FFF_FFFF range by adding 0x4000_0000 to the address.

If the address is between 0x7000_0000 - 0x7FFF_FFFF then the AXI peripherics will be placed in 0x9000_0000 - 0x9FFF_FFFF range by adding 0x2000_0000 to the address.

Versal

If the address is between 0x4400_0000 - 0x4FFF_FFFF then the AXI peripherics will be placed in 0xA400_0000 - 0xAFFF_FFFF range by adding 0x6000_0000 to the address.

If the address is between 0x7000_0000 - 0x7FFF_FFFF then the AXI peripherics will be placed in 0xB000_0000 - 0xBFFF_FFFF range by adding 0x4000_0000 to the address.

Intel

Applying to DE10-Nano, C5SoC.

The address usually (but not always) starts from 0x0002_0000, or the first available block of a bigger size. In Quartus block design you should be able to determine it.

SPI

In general, the base design of the carrier (#1) has two Serial Peripheral Interfaces (SPIs), which are used as a control interface for FMC/HSMC devices. These SPI interfaces are controlled by the integrated SPI controller of the Hard Processor System (HPS) or Processing System 7/8 (PS7/8) or an Intel or AMD SPI controller core.

I2C/I2S/SPDIF

A couple of carriers require these standard interfaces for different purposes (e.g. a configuration interface for an audio peripheral device). These peripherals do not necessarily have vital roles in the reference design – it’s more like a generic goal to support all the provided peripherals of the carrier board.

HDMI

There is HDMI support for all carriers which are using the ADV7511 as HDMI transmitter. The HDMI transmitter core can be found here (axi_hdmi_tx).

GPIOs

The general rule of thumb is to define 64 GPIO pins for the design:

  • bits [31: 0] always belong to the carrier board;

  • bits [63:32] will be assigned to switches, buttons and/or LEDs, which can be found on the FMC board;

  • bits [95:64] will be used when the FPGA type is Zynq UltraScale+ MPSoC.

When some of these GPIOs are not used, the input pins should have the output pins driven to them, so that Vivado will not complain about inputs not being assigned to.

Depending on the processor type, add these values to the GPIO number from the HDL project to obtain the final number used in software:

  • PS7 EMIO offset = 54

  • PS8 EMIO offset = 78

  • MicroBlaze offset = no offset

  • Versal offset = -32

Connectivity

  • Ethernet

  • USB OTG

These interface designs are borrowed from the golden reference design of the board.

Interrupts

When developing the Linux software parts for an HDL project, the interrupts number to the PS have a different number in the software side.

Not a rule, but in our designs we preffer to use firstly the interrupts from 15 and to go down to 0. Be careful when assigning one, because it might be used in the base design of the carrier!

Always check which are used (in /projects/common/$carrier/$carrier_system_bd.tcl)

Interrupts table

HDL

Linux Zynq

Actual Zynq

Linux ZynqMP

Actual ZynqMP

S10SoC

Linux Cyclone V

Actual Cyclone V

15

59

91

111

143

32

55

87

14

58

90

110

142

31

54

86

13

57

89

109

141

30

53

85

12

56

88

108

140

29

52

84

11

55

87

107

139

28

51

83

10

54

86

106

138

27

50

82

9

53

85

105

137

26

49

81

8

52

84

104

136

25

48

80

7

36

68

96

128

24

47

79

6

35

67

95

127

23

46

78

5

34

66

94

126

22

45

77

4

33

65

93

125

21

44

76

3

32

64

92

124

20

43

75

2

31

63

91

123

19

42

74

1

30

62

90

122

18

41

73

0

29

61

89

121

17

40

72

HDL

riscv-rx no-OS

15

15

14

14

13

13

12

12

11

11

10

10

9

9

8

8

7

7

6

6

5

5

4

4

3

3

2

2

1

1

0

0

Board design and capabilities

AMD platforms

The board files of these carriers can be found here.

Board name

Boots from

FMC connector 1

FMC connector 2

VADJ FMC connector

Family

AC701 **

JTAG

HPC (2 GTP @ 6.6 Gbps)

—

3.3V/*2.5V/1.8V

Artix-7

Cora Z7S

SD card

—

—

—

Zynq-7000

KCU105

JTAG

HPC (8 GTH @ 16.3 Gbps)

LPC (1 GTH @ 16.3 Gbps)

*1.8V/1.5V/1.2V

Kintex UltraScale

Microzed **

JTAG

—

—

—

Zynq-7000

VC709 **

JTAG

HPC (10 GTH @ 13.1 Gbps)

—

*1.8V

Virtex-7

VCK190

SD card

FMC+ (12 GTY @ 28.21 Gbps)

FMC+ (12 GTY @ 28.21 Gbps)

*1.5V/1.2V

Versal AI Core

VCU118

JTAG

FMC+ (24 GTY @ 28.21 Gbps)

LPC

*1.8V/1.5V/1.2V

Virtex UltraScale+

VMK180

SD card

FMC+ (12 GTY @ 28.21 Gbps)

FMC+ (12 GTY @ 28.21 Gbps)

*1.5V/1.2V

Versal Prime Series

VPK180

SD card

FMC+ (8 GTYP @ 32.75 Gbps)

—

*1.5V/1.2V

Versal Premium

ZC702

SD card

LPC

LPC

3.3V/*2.5V/1.8V

Zynq-7000

ZCU102

SD card

HPC (8 GTH @ 16.3 Gbps)

HPC (8 GTH @ 16.3 Gbps)

*1.8V/1.5V/1.2V

Zynq UltraScale+ MP SoC

ZedBoard

SD card

LPC

—

3.3V/2.5V/*1.8V

Zynq-7000

LFCPNX-EVN

JTAG | SPI flash

HPC

—

—

CertusPro-NX

Note

The column with the VADJ value applies to the FMC connectors when they exist. If both of them exist, then it is the same for both of them. If there is only one FMC connector, then it applies to only one. If both are missing, then a — (dash) will appear.

Note

** = not supported anymore, but projects with these carriers can be found in older releases

Note

(* bold) = default VADJ FMC1 & FMC2 columns -> depending on the power supply of the device connected to the FMC, the custom VADJ will have the value supported by both the carrier and the device(s)

Discontinued AMD platforms

Projects with these carriers can still be found on our repository, as well as their board files.

Board name

Boots from

FMC connector 1

FMC connector 2

VADJ FMC connector

Family

KC705

JTAG

HPC (4 GTX @ 10.3125 Gbps)

LPC (1 GTX @ 10.3125 Gbps)

3.3V/*2.5V/1.8V

Kintex-7

VC707

JTAG

HPC (8 GTX @ 12.5 Gbps)

HPC (8 GTX @ 12.5 Gbps)

*1.8V/1.5V/1.2V

Virtex-7

VCU128

JTAG

FMC+ (24 GTY @ 28.21 Gbps)

—

*1.8V/1.5V/1.2V

Virtex UltraScale+ HBM

ZC706

SD card

HPC (8 GTX @ 10.3125 Gbps)

LPC (1 GTX @ 10.3125 Gbps)

3.3V/*2.5V/1.8V

Zynq-7000

Intel platforms

Board name

Connector 1

Connector 2

A10GX ** (Arria 10 GX)

FMC LPC ()

FMC HPC (8 x 17.4 Gbps)

A10SoC (Arria 10 SoC)

FMC HPC (8)

FMC LPC (8)

S10SoC (Stratix 10 SoC)

FMC+ (24 @ 28.3 Gbps)

FMC+ (24 @ 28.3 Gbps)

C5SoC (Cyclone V SoC)

HSMC

—

DE10-Nano

Arduino shield

—

FM87 (Agilex 7 I-Series)

FMC+ (16 @ 32 Gbps)

FMC+ (16 @ 32 Gbps)

Note

** = not supported anymore, but projects with these carriers can be found in older releases

VADJ values

Board name

FMC connector 1

FMC connector 2

A10GX

*1.8V/1.5V/1.35V/1.2V

*1.8V/1.5V/1.35V/1.2V

A10SoC

*1.8V/1.5V/1.35V/1.25V/1.2V/1.1V

*1.8V/1.5V/1.35V/1.2V/1.1V

S10SoC

*3.3V/1.8V/1.2V

*3.3V/1.8V/1.2V

FM87

*1.2V

*1.2V

Note

(* bold) = default VADJ FMC1 & FMC2 columns -> depending on the power supply of the device connected to the FMC, the custom VADJ will have the value supported by both the carrier and the device(s)

File structure of a project

Tip

In /projects/common/$carrier_name/ you can find templates for the system_top.v, Makefile, etc. to help you when creating a new project.

Project files for AMD boards

A project for an AMD FPGA board should contain the following files:

  • Makefile — auto-generated file; contains all the IP dependencies needed for the project to be built

  • system_project.tcl — script that creates the actual Vivado project and runs the synthesis/implementation of the design

  • system_bd.tcl — sources the base design of the carrier first, then the base design of the evaluation board, and afterwards it contains all the IP instances and connections that must be added on top of the sourced files, to complete the design of the project (these are specific to the combination of this carrier and board)

  • system_constr.xdc — constraints file of the design; it’s the connection between the physical pins of the FPGA and the HDL code that describes the behavior; here you define the FMC I/O pins, board-specific clock signals, timing constraints, etc. The constraints specific to the carrier are imported in the system_project.tcl file

  • system_top.v — contains everything about the HDL part of the project; it instantiates the system_wrapper module, I/O buffers, I/ODDRs, modules that transform signals from LVDS to single-ended, etc. The I/O ports of this Verilog module will be connected to actual I/O pads of the FPGA.

    • system_wrapper — is a tool-generated file and can be found at <project_name>.srcs/sources_1/bd/system/hdl/system_wrapper.v

      • the I/O ports of this module are declared in either system_bd.tcl or in the base design of the evaluation board (#2) file

      • this can be visualized in Vivado at the Block Design section

      • the base design, board design and system_bd.tcl describe this module, making the connections between the instantiated IPs

Project files for Intel boards

A project for an Intel FPGA board should contain the following files:

  • Makefile — auto-generated file; contains all the IP dependencies needed for the project to be built

  • system_project.tcl — script that creates the actual Quartus project and runs the synthesis/implementation of the design. It also contains the I/O definitions for the interfaces between the board and the FPGA

  • system_qsys.tcl — also called platform designer; sources the base design of the carrier first, then the base design of the evaluation board, and afterwards it contains all the IP instances and connections that must be added on top of the sourced files, to complete the design of the project (these are specific to the combination of this carrier and board)

  • system_constr.sdc — contains clock definitions and other path constraints

  • system_top.v — contains everything about the HDL part of the project; it instantiates the system_bd module, I/O buffers, specific SPI modules, modules that transform signals from LVDS to single-ended, etc. The I/O ports of this Verilog module will be connected to actual I/O pads of the FPGA

Examples

Some carriers have a different name for these files, for example A10SoC has constraints file for both PL side and PS side:

  • a10soc_plddr4_assign.tcl — constraints file for the PL

  • a10soc_system_assign.tcl — constraints file for the PS

Project files for Lattice boards

A project for a Lattice FPGA board should contain the following files:

  • Makefile — auto-generated file; contains all the IP dependencies needed for the project to be built

  • system_project_pb.tcl — used to build the Propel Builder project (block design); linked in project-lattice.mk, run by propelbld (Windows), propelbldwrap (Linux);

  • system_project.tcl — used to build the Radiant project; Linked in project-lattice.mk, run by pnmainc (Windows), radiantc (Linux);

  • system_pb.tcl — linker script for the projects, sourced in adi_project_pb procedure that is called in system_project_pb.tcl and it is defined in adi_project_lattice_pb.tcl; sources the base design of the carrier first, then the base design of the evaluation board, and afterwards it contains all the IP instances and connections that must be added on top of the sourced files, to complete the design of the project (these are specific to the combination of this carrier and board)

  • system_constr.sdc — contains clock definitions and other path constraints

  • system_constr.pdc — contains clock definitions and other path constraints + physical constraints

  • system_top.v — contains everything about the HDL part of the project; it instantiates the <project_name>.v system_wrapper module, I/O buffers, I/ODDRs, modules that transform signals from LVDS to single-ended, etc. The I/O ports of this Verilog module will be connected to actual I/O pads of the FPGA