DAQ3 HDL Project

Overview

The DAQ3 reference design showcases the EVAL-FMCDAQ3-EBZ evaluation board, which is comprised of the AD9680 dual, 14-bit, 1.25 GSPS, JESD204B (subclass 1) ADC, the AD9152 dual, 16-bit, 2.5 GSPS, JESD204B (subclass 1) DAC, and the AD9528 JESD204B/C clock generator, and some power management components. It is clocked by an internally generated carrier platform via the FMC connector, comprising a completely self contained data acquisition and signal synthesis prototyping platform.

Supported boards

Supported devices

Supported carriers

Evaluation board

Carrier

FMC slot

EVAL-FMCDAQ3-EBZ

KCU105

FMC HPC

VCU118

FMC+

ZCU102

FMC HPC0

ZC706

FMC HPC

Block design

The difference between the KCU105/VCU118/ZC706 designs and the ZCU102 one, is the use of DATA_OFFLOAD: in the Zynq UltraScale-based designs, it is not used due to HP ports’ superior bandwidth.

Block diagram

KCU105/VCU118/ZC706

The data path and clock domains are depicted in the below diagram:

EVAL-FMCDAQ3-EBZ block diagram

This configuration was built using the make command with the following parameters:

/hdl/projects/daq3/zc706$
make RX_JESD_M=2 \
     RX_JESD_L=4 \
     RX_JESD_S=1 \
     TX_JESD_M=2 \
     TX_JESD_L=4 \
     TX_JESD_S=1

Block name

IP name

Documentation

Additional info

AXI_ADXCVR

axi_adxcvr

AXI ADXCVR

2 instances, one for RX and one for TX

AXI_DMAC

axi_dmac

AXI DMAC

2 instances, one for RX and one for TX

DATA_OFFLOAD

data_offload

Data Offload

2 instances, one for RX and one for TX

RX JESD LINK

axi_mxfe_rx_jesd

JESD204B/C Link Receive Peripheral

Instantiaded by adi_axi_jesd204_rx_create procedure

RX JESD TPL

axi_ad9680_tpl_core

ADC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_rx_create procedure

TX JESD LINK

axi_mxfe_tx_jesd

JESD204B/C Link Transmit Peripheral

Instantiaded by adi_axi_jesd204_tx_create procedure

TX JESD TPL

axi_ad9152_tpl_core

DAC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_tx_create procedure

UTIL_ADXCVR

util_daq3_xcvr

UTIL_ADXCVR core for AMD Xilinx devices

Used for both AXI ADXCVR instances

UTIL_CPACK

axi_ad9680_cpack

Channel CPACK Utility

—

UTIL_UPACK

axi_ad9152_upack

Channel UPACK Utility

—

ZCU102

The data path and clock domains are depicted in the below diagram.

EVAL-FMCDAQ3-EBZ/ZCU102 block diagram

This configuration was built using the make command with the following parameters:

/hdl/projects/daq3/zcu102$
make RX_JESD_M=2 \
     RX_JESD_L=4 \
     RX_JESD_S=1 \
     TX_JESD_M=2 \
     TX_JESD_L=4 \
     TX_JESD_S=1

Block name

IP name

Documentation

Additional info

AXI_ADXCVR

axi_adxcvr

AXI ADXCVR

2 instances, one for RX and one for TX

AXI_DMAC

axi_dmac

AXI DMAC

2 instances, one for RX and one for TX

RX JESD LINK

axi_mxfe_rx_jesd

JESD204B/C Link Receive Peripheral

Instantiaded by adi_axi_jesd204_rx_create procedure

RX JESD TPL

axi_ad9680_tpl_core

ADC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_rx_create procedure

TX JESD LINK

axi_mxfe_tx_jesd

JESD204B/C Link Transmit Peripheral

Instantiaded by adi_axi_jesd204_tx_create procedure

TX JESD TPL

axi_ad9152_tpl_core

DAC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_tx_create procedure

UTIL_ADXCVR

util_daq3_xcvr

UTIL_ADXCVR core for AMD Xilinx devices

Used for both AXI ADXCVR instances

UTIL_CPACK

axi_ad9680_cpack

Channel CPACK Utility

—

UTIL_UPACK

axi_ad9152_upack

Channel UPACK Utility

—

Clock scheme

  • Internal clock sources for both the ADC and the DAC, coming from AD9528 clock-generator chip (device clocks and reference clocks)

  • External trigger coming from J1 SMA connector

Configuration modes

The design has one JESD204B receive chain and one transmit chain, each with 4 lanes.

Each chain consists of a transport layer represented by a JESD TPL module, a link layer represented by a JESD LINK module, and a physical layer shared among chains, represented by an XCVR module.

The HDL project in its current state, has the link operating in subclass 1.

  • Rx/Tx device clock - 308.25 MHz

  • Reference clock - 616.5 MHz

  • JESD204B Rx/Tx lane rate - 12.33 Gbps

The following are the parameters of this project that can be configured:

  • [RX/TX]_JESD_M: number of converters per link

  • [RX/TX]_JESD_L: number of lanes per link

  • [RX/TX]_JESD_S: number of samples per frame

Detailed description

The digital interface consists of 4 transmit and 4 receive lanes running at 12.33 Gbps (default).

The devices’ interfaces are shared by the same set of transceivers, followed by the individual JESD204B and ADC/DAC pcores. The transceivers then interface to the cores at 128 bits at 308.25MHz. The cores are programmable through an AXI-lite interface.

The data path consists of independent DMA interfaces for the transmit and receive paths. The data is sent or received based on the configuration (programmable) from separate transmit and receive chains.

The DAC data may be sourced from an internal data generator (DDS, pattern or PRBS) or from the external DDR via DMA. The internal DDS phase and frequency are programmable.

The ADC data is sent to the DDR via DMA. The core also supports PN monitoring at the sample level. This is different from the JESD204B-specific PN sequence (though they both claim to be from the same equation).

The device control and monitor signals are interfaced to a GPIO module. The SPI signals are controlled by a separate AXI based SPI core.

  • JESD204B in subclass 1 with lane rate 12.33 Gbps

  • Rx, Tx: L=2, M=4, S=1, NP=16

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

Zynq/Microblaze

ZynqMP

axi_ad9152_tpl_core

0x44A0_4000

0x84A0_4000

axi_ad9152_xcvr

0x44A6_0000

0x84A6_0000

axi_ad9152_jesd

0x44A9_0000

0x84A9_0000

axi_ad9152_dma

0x7C42_0000

0x9C42_0000

ad9152_data_offload

0x7C43_0000

—

axi_ad9680_tpl_core

0x44A1_0000

0x84A1_0000

axi_ad9680_xcvr

0x44A5_0000

0x84A5_0000

axi_ad9680_jesd

0x44AA_0000

0x84AA_0000

axi_ad9680_dma

0x7C40_0000

0x9C40_0000

ad9680_data_offload

0x7C41_0000

—

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PS

SPI 0

AD9528

0

PS

SPI 0

AD9152

1

PS

SPI 0

AD9680

2

GPIOs

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

Software GPIO

(from FPGA view)

Zynq-7000

Zynq MP

adc_pd

INOUT

38

92

116

dac_txen

INOUT

37

91

115

adc_fdb

INOUT

36

90

114

adc_fda

INOUT

35

89

113

dac_irq

INOUT

34

88

112

clkd_status

INOUT

32

86

110

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL PS

HDL MB

Linux Zynq

Actual Zynq

Linux ZynqMP

Actual ZynqMP

axi_ad9680_dma

13

12

57

89

109

141

axi_ad9152_dma

12

13

56

88

108

140

axi_ad9680_jesd

11

14

55

87

107

139

axi_ad9152_jesd

10

15

54

86

106

138

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.

Then go to the hdl/projects/daq3/$carrier location and run the make command.

Linux/Cygwin/WSL

Example of running the make command without parameters (using the default configuration):

~$
cd hdl/projects/daq3/zcu102
~/hdl/projects/daq3/zcu102$
make

Example of running the make command with parameters:

~$
cd hdl/projects/daq3/zcu102
~/hdl/projects/daq3/zcu102$
make RX_JESD_M=4 RX_JESD_L=2 TX_JESD_M=4 TX_JESD_L=2

The result of the build, if parameters were used, will be in a folder named by the configuration used: RXM4_RXL2_TXM4_TXL2.

A more comprehensive build guide can be found in the Build an HDL project user guide.

Software considerations

ADC - crossbar config

RX lanes are not reordered, they are the same as the physical lanes.

DAC - crossbar config

Due to physical constraints, TX lanes are reordered as described in the following table:

For example, physical lane 2 from DAC connects to logical lane 1 from the FPGA. Therefore the crossbar from the device must be set accordingly.

logical lane

0

1

2

3

physical lane

0

2

3

1

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.