AXI Stream FIFO

?util_axis_fifo IP-XACT not found.Generate it and the documentation:(cd library/util_axis_fifo; make)(cd docs; make html)

The AXI Stream FIFO core is a simple FIFO (First Input First Output) with AXI streaming interfaces, supporting synchronous and asynchronous operation modes. It can be used to mitigate data rate differences or transfer an AXI stream to a different clock domain.

Features

  • Supports Intel/Altera and AMD Xilinx devices

  • Configurable data width and depth

  • Supports asynchronous (double clocked) mode

  • Supports TLAST to indicate packet boundary

  • Supports FULL/EMPTY and ALMOST_FULL/ALMOST_EMPTY status signals

  • Supports zero-deep implementation

Files

Name

Description

library/util_axis_fifo/util_axis_fifo.v

Verilog source for the peripheral.

Configuration Parameters

Name

Description

DATA_WIDTH

Data width of AXI streaming interface.

ADDRESS_WIDTH

Width of the address, defines the depth of the FIFO.

ASYNC_CLK

Clocking mode. If set, the FIFO operates on asynchronous mode.

M_AXIS_REGISTERED

Add and additional register stage to the AXI stream master interface.

ALMOST_EMPTY_THRESHOLD

Defines the offset (in data beats) between the almost empty and empty assertion.

ALMOST_FULL_THRESHOLD

Defines the offset (in data beats) between the almost full and full assertion.

TLAST_EN

Enable TLAST logical port on the AXI streaming interface.

TKEEP_EN

Enable TKEEP logical port on the AXI streaming interface.

Interface

Name

Description

s_axis

Slave AXI stream.

s_axis_aclk

Slave AXI stream clock signal

s_axis_aresetn

Slave AXI stream reset signal (active low)

s_axis_room

Indicates how much space (in data beats) is in the FIFO

s_axis_almost_full

If set, the FIFO is almost full

m_axis

Master AXI stream.

m_axis_aclk

Master AXI stream clock signal

m_axis_aresetn

Master AXI stream reset signal (active low)

m_axis_level

Indicates how much data is in the FIFO

s_axis_full

If set, the FIFO is full

m_axis_almost_empty

If set, the FIFO is almost empty

m_axis_empty

If set, the FIFO is empty

Detailed Description

The util_axis_fifo is a generic First Input First Output module, that can be used to control clock and data rate differences or to do data buffering on a AXI4 stream based data path. FIFO’s write interface is an AXI4 slave streaming interface, and the FIFO’s read interface is an AXI4 master streaming interface. The depth of the FIFO is defined by the equation, which is a function of the ADDRESS_WIDTH and DATA_WIDTH parameters:

FIFO depth in bytes = DATA_WIDTH/8 * 2 ^ ADDRESS_WIDTH

The FIFO has three different status indicator ports on both side, which provides information about the state of the FIFO for both the source and destination logic:

  • FULL or EMPTY - If these outputs are asserted, the FIFO is full or empty. In case of a full FIFO, all the write operations are suspended. In case of an empty FIFO, all the read operations are suspended.

  • ALMOST_EMPTY/ALMOST_FULL - It can be used to foresee a potential FULL or EMPTY state, asserting before the EMPTY/FULL before a predefined number of words. The offset between ALMOST_EMPTY and EMPTY, and between ALMOST_FULL and FULL can be set by using the parameters ALMOST_EMPTY_THRESHOLD and ALMOST_FULL_THRESHOLD.

  • S_AXIS_ROOM - Indicate how many words can be written in the FIFO at the current moment, until the FIFO becomes FULL.

  • M_AXIS_LEVEL - Indicate how many words can be read from the FIFO at the current moment, until the FIFO becomes EMPTY.

Important

In case of asynchronous mode, because of the delays introduced by the clock domain crossing logic, the ROOM and LEVEL indicators can not reflect the actual state of the FIFO in real time. Source and destination logic should take this into account when controlling the data stream into and from the FIFO. Carefully adjusting the ALMOST_EMPTY/ALMOST_FULL indicators can provide a safe operating margin.

References