Util Extract

?util_extract IP-XACT not found.Generate it and the documentation:(cd library/util_extract; make)(cd docs; make html)

The Util Extract core allows the extraction of the trigger signal and restoration of the data signal that was embedded in the data stream by the AXI ADC Trigger.

Files

Name

Description

library/util_extract/util_extract.v

Verilog source for the peripheral.

Configuration Parameters

Name

Description

NUM_OF_CHANNELS

Number of channels

DATA_WIDTH

Data width. It assumes the trigger is in bit (n*16)-1, with n being the channel number

Interface

Name

Description

clk

Clock input. Should be synchronous to the input and the output data

data_in

Input data from the FIFO. Will replace each trigger bit with the sign extended version of the data. It should be data from the output of the variable fifo

data_in_trigger

Data from which the trigger is extracted. It should be data from the input of the variable fifo

data_valid

Valid for the input data

data_out

Data without the embedded trigger

valid_out

Valid for the output data

trigger_out

Trigger output. Is an logic OR of the triggers from all the channels that are captured simulaneously

References