AD916x-FMC HDL project

Overview

The AD9161 /AD9162 /AD9163 /AD9164 is a high performance, 16-bit (AD9164, AD9163, AD9162)/11-bit (AD9161) resolution digital-to-analog converter (DAC) that supports data rates to 6 GSPS.

The DAC core is based on a quad-switch architecture coupled with a 2x interpolator filter that enables an effective DAC update rate of up to 12 GSPS in some modes. The high dynamic range and bandwidth makes this DAC ideally suited for the most demanding high speed radio frequency (RF) DAC applications.

The data interface is programmable in terms of lane speed and number of lanes (up to 8 JESD204 Interface Framework serializer/deserializer SERDES lanes) to enable application flexibility. A serial peripheral interface (SPI) configures the DACs and monitors the status of all registers.

Supported boards

Supported devices

Supported carriers

Block design

Block diagram

The data path and clock domains are depicted in the below diagram:

AD916x block diagram

Block name

IP name

Documentation

Additional info

AXI_ADXCVR

axi_adxcvr

AXI ADXCVR

—

AXI_DMAC

axi_dmac

AXI DMAC

—

DATA_OFFLOAD

data_offload

Data Offload

—

TX JESD LINK

axi_ad916x_jesd

JESD204B/C Link Transmit Peripheral

Instantiaded by adi_axi_jesd204_tx_create procedure

TX JESD TPL

axi_ad916x_core

DAC JESD204B/C Transport Peripheral

Instantiated by adi_tpl_jesd204_tx_create procedure

UTIL_ADXCVR for AMD

library/xilinx/util_adxcvr

UTIL_ADXCVR core for AMD Xilinx devices

—

UTIL_UPACK

util_upack2

Channel UPACK Utility

—

Configuration modes

The configuration parameters that can be set along with the make command are:

  • ADI_DAC_DEVICE: specifies the DAC device

    • AD9161 (default)

    • AD9162

    • AD9163

    • AD9164

  • ADI_DAC_MODE: specifies the JESD operation mode

    • 08 (default)

    • can vary from 01 to 08 depending on the selected device (ADI_DAC_DEVICE)

  • ADI_LANE_RATE: specifies the lane rate

    • 12.5 GHz(default)

    • 4.16 GHz

If the desired configuration is not listed between the supported modes, the user can configure the parameters manually, trough make (according to the datasheet of each chip, Table “JESD204B Parameters for Interpolation Rate and Number of Lanes”):

  • M: number of converters per link (set by the ADI_DAC_MODE (default))

  • L: number of lanes per link (set by the ADI_DAC_MODE (default))

  • S: number of samples per frame (set by the ADI_DAC_MODE (default))

  • F: number of octets per frame (set by the ADI_DAC_MODE (default))

  • HD: high-density (set by the ADI_DAC_MODE (default))

  • N: converter resolution (set by the ADI_DAC_MODE (default))

  • NP: number of bits per sample (set by the ADI_DAC_MODE (default))

Clock scheme

The EVAL-AD916x can be tested using the on-board clock generator or using and external clock source. The jumper positions are described below:

Jumper/Solder link

Position

Description

J61

Mounted

Use the onboard clk. generator

J61

Unmounted

Use external clk. source

For example, building the project for AD9163 in MODE 2 (2 lanes with 12.5 GHz lane rate) (see projects/ad916x_fmc/common/config.tcl for more details) requires an external clock source and jumper J61 removed.

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

ZynqMP

dac_jesd204_transport

0x84A0_4000

dac_jesd204_xcvr

0x84A6_0000

dac_jesd204_link

0x84A9_0000

dac_dma

0x9C42_0000

dac_data_offload

0x9C43_0000

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PS

SPI 0

AD9508

1

PS

SPI 0

ADF4355

1

PS

SPI 0

AD916x

1

GPIOs

The Software GPIO number is calculated as follows:

  • ZCU102: the offset is 78 (PS8)

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

ZCU102

fmc_hmc849vctrl

INOUT

23

100

fmc_txen_0

INOUT

22

99

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux ZynqMP

Actual ZynqMP

dac_dma

10

106

138

dac_jesd204_link

12

108

140

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository, and then build the project as follows:

Linux/Cygwin/WSL

~$
cd hdl/projects/ad916x_fmc/zcu102
~/hdl/projects/ad916x_fmc/zcu102$
make

AD916x supports various modes for JESD. By default, when running the above command, it will build the project for AD9162 in Mode 8, which has the following JESD parameters: L=8, M=2, S=2, F=1, N=16, NP=16 at a lane rate of 12.5 GHz. Other configurations (or for other devices), can be specified by using the ADI_LANE_RATE, ADI_DAC_DEVICE, ADI_DAC_MODE parameters:

~$
cd hdl/projects/ad916x_fmc/zcu102
~/hdl/projects/ad916x_fmc/zcu102$
make ADI_LANE_RATE=12.5 ADI_DAC_DEVICE=AD9163 ADI_DAC_MODE=02

You can also overwrite some JESD parameters if there is a need for a custom mode. The following commands should be run (check the datasheet of each chip, Table “JESD204B Parameters for Interpolation Rate and Number of Lanes” for more context):

~$
cd hdl/projects/ad916x_fmc/zcu102
~/hdl/projects/ad916x_fmc/zcu102$
make ADI_DAC_DEVICE=AD9164 ADI_LANE_RATE=12.5 M=1 L=8 S=4 NP=16

or:

~$
cd hdl/projects/ad916x_fmc/zcu102
~/hdl/projects/ad916x_fmc/zcu102$
make ADI_DAC_DEVICE=AD9164 ADI_LANE_RATE=12.5 ADI_DAC_MODE=08 M=1 S=4

For other supported modes, check projects/ad916x_fmc/common/config.tcl.

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.