ADA4355-FMC HDL project

Overview

The ADA4355/ ADA4356 is a complete, high performance, current input µModule. For space savings, the ADA4355/ ADA4356 includes all the required active and passive components to realize a complete current to bits data acquisition solution, supporting a small form factor, optical modules as well as multichannel systems.

The high speed transimpedance amplifier (TIA) supports short optical pulses: 10 ns for the ADA4355 and 20 ns for the ADA4356, enabling high spatial resolution in Time of Flight (ToF) measurements. Both devices provide three TIA gain (TZ) settings to maximize dynamic range. An internal, selectable, analog low-pass filter (LPF) can limit the devices bandwidth with a corner frequency of 100 MHz to minimize broadband noise while also serving as an antialiasing filter for the 125 MSPS ADC.

The 14-bit ADC converts the amplified voltage signal at a rate of up to 125 MSPS and outputs the digitized signals through two serial, low voltage differential signaling (LVDS) data lanes, operating at rates of up to 1 Gbps per lane. The data clock output (DCO) operates at frequencies of up to 500 MHz and supports double data rate (DDR) operation.

Supported boards

Supported devices

Supported carriers

Evaluation board

Carrier

FMC slot

EVAL-ADA4355

ZedBoard

FMC

Block design

Warning

The VADJ for the Zedboard must be set to 2.5V.

Block diagram

The data path and clock domains are depicted in the below diagram:

ADA4355_FMC/ZedBoard block diagram

Configuration modes

The BUFMRCE_EN configuration parameter defines the supported board used which is differentiated by how the frame clock signals are distributed. For ADA4355 the XDC constraints are not optimized for ISERDES, as the frame clock signals are located in a different I/O bank from the other related signals. To address this, a BUFMRCE buffer is used to distribute the frame clock to all ISERDES instances.

By default it is set to 0. Depending on the part, some hardware modifications need to be done on the board and/or make command:

In case of the ADA4356:

~$
make BUFMRCE_EN=0

In case of the ADA4355:

~$
make BUFMRCE_EN=1

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at HDL Architecture).

Instance

Zynq/Microblaze

axi_ada4355_adc

0x44A0_0000

axi_ada4355_dma

0x44A3_0000

I2C connections

I2C type

I2C manager instance

Alias

Address

I2C subordinate

PL

iic_fmc

axi_iic_fmc

0x4162_0000

—

PL

iic_main

axi_iic_main

0x4160_0000

—

GPIOs

The Software GPIO number is calculated as follows:

  • Zynq-7000: if PS7 is used, then offset is 54

GPIO signal

Direction

HDL GPIO EMIO

Software GPIO

(from FPGA view)

Zynq-7000

apd_supp_en **

INOUT

42

96

trig_fmc_out **

OUT

41

95

trig_fmc_in **

IN

40

94

freq_sel1 **

INOUT

39

93

gain_sel3 **

INOUT

38

92

gpio_test **

INOUT

37

91

gpio_1p8va_en *

IN

37

91

gain_sel2 **

INOUT

36

90

gain_sel2 *

IN

36

90

gpio_vld_en **

INOUT

35

89

gpio_1p8vd_en *

INOUT

35

89

freq_sel0 **

INOUT

34

88

fsel *

INOUT

34

88

gain_sel1

INOUT

33

87

gain_sel0

INOUT

32

86

Legend

  • * instantiated only for BUFMRCE_EN=1 (ADA4355)

  • ** instantiated only for BUFMRCE_EN=0 (ADA4356)

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Linux Zynq

Actual Zynq

axi_ada4355_dma

13

57

89

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

PS

SPI 0

ADA4355

0

PS

SPI 1

AD5142

1

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributes the bit/elf files of these projects as part of the ADI Kuiper Linux. If you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository.

Linux/Cygwin/WSL

Example for building with the default configuration (BUFMRCE_EN=0):

~$
cd hdl/projects/ada4355_fmc/zed
~/hdl/projects/ada4355_fmc/zed$
make

Example for building with parameters:

~/hdl/projects/ada4355_fmc/zed$
make BUFMRCE_EN=1

The result of the build, if parameters were used, will be in a folder named by the configuration used.

If the following command was run

make BUFMRCE_EN=1

then the folder name will be: BUFMRCEEN1.

Check Configuration modes for more details.

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.