AD-FMCLIDAR1-EBZ HDL project (OBSOLETE)

Warning

The support for AD-FMCLIDAR1-EBZ HDL project has been discontinued, the latest release branch where it can be found is hdl_2019_r1. This page is left for legacy purposes only.

Overview

The AD-FMCLIDAR1-EBZ is a prototyping platform for LiDAR applications that can be used on FPGA development boards enabled with FMC HPC connector and JESD204B support capability. It offers developers a working-out-of-box platform that can be used for developing software and algorithms for a broad range of applications.

The full system hardware includes Data Acquisition(DAQ) Board, Laser Transmitter Board, and the AFE Receiver Board.

Supported boards

Supported carriers

Important

The Arria10SOC carrier requires a hardware rework to function correctly. The rework connects FMC_A header pins directly to the FPGA so that they can be accessed by the fabric.

Changes required:

  • REMOVE: R575, R576, R621, R633, R612, R613

  • POPULATE: R574, R577, R620, R632, R610, R611

Block design

Block diagram

The main scope of the HDL design is to provide all the required digital interfaces for the data acquisition board of the prototyping system.

The following block diagram presents the simplified system architecture:

AD-FMCLIDAR1-EBZ block diagram

AXI Laser Driver IP

The axi_laser_driver IP is responsible to generate a narrow pulse for the laser driver circuit, to control the TIA channel selection on the analog front end (AFE) board, and to synchronize the data acquisition to the generated pulses.

More information about the IP can be found at AXI Laser Driver.

Control interfaces

Name

Type

Details

adc_fd*

GPIO

Monitors the AD9094 Fast detect output lines

adc_pwdn

GPIO

Controls the AD9094 Power-Down input line

spi_adc_*

4-wire SPI

AD9094 configuration interface

spi_vco_*

3-wire SPI

ADF436-7 configuration interface

spi_clkgen_*

4-wire SPI

AD9528 configuration interface

laser_driver_pn

LVDS output

It controls the laser driver circuit, it is generated by the axi_laser_driver IP instance

laser_gpio[13:0]

GPIO

Unused GPIO line on the lase board

tia_chsel[7:0]

CMOS output

TIA channel selection lines, it is controlled by the axi_laser_driver instance

afe_dac_sdasclloadclr_n

I2C/GPIO

AD5627 configuration interface

rx_ref_clk_pn

LVDS

JESD204B reference clock for the high-speed gigabit transceivers; runs at 250MHz

rx_device_clk_pn

LVDS

JESD204B device clock for the transport layer and additional data processing; runs at 250MHz

rx_data_pn[3:0]

CML

JESD204B high-speed serial lanes; runs at 10Gbps

rx_sync_pn[1:0]

LVDS

JESD204B SYNC signals for interface synchronization

rx_sysref_pn

LVDS

JESD204B SYSREF signal for deterministic latency

JESD204B interface

The JESD204B interface runs in Subclass 1 mode to ensure the deterministic latency of the link. The following tables are summarizing the JESD204B important configuration parameter and attributes.

Parameter name

Abbreviation

Value

Number of lanes

L

4

Number of converter

M

4

Converter resolution

NP

8

Total number of Bits per Sample

NP

8

Samples per frame

S

1

Octets per frame

F

1

Frames per Multiframe

K

32

Number of control bits

CS

0

Rates and Clocks

Value

Sample rate

1 GSPS

Lane rate

10 Gbps

GT reference clock

250 MHz

Device clock

250 MHz

CPU/Memory interconnects addresses

The addresses are dependent on the architecture of the FPGA, having an offset added to the base address from HDL (see more at CPU/Memory interconnects addresses).

Instance

ZCU102

ZC706

afe_dac_iic

0x7c800000

—

axi_ad9694_xcvr

0x44A50000

0x44A50000

ad9694_tpl_core

0x44A10000

0x44A10000

ad9694_jesd

0x44AA0000

0x44AA0000

ad9694_dma

0x7c400000

0x7c400000

axi_spi_vco

0x7c500000

0x7c500000

axi_spi_afe_adc

0x7c600000

0x7c600000

axi_laser_driver_0

0x7c700000

0x7c700000

Instance

A10SoC

sys_spi_clockgen

0x00000060

sys_spi_vco

0x00000080

sys_spi_afe_adc

0x000000A0

ad9694_jesd204.link_reconfig

0x00040000

ad9694_jesd204.link_management

0x00044000

ad9694_jesd204.link_pll_reconfig

0x00045000

ad9694_jesd204.phy_reconfig_0

0x00048000

ad9694_jesd204.phy_reconfig_1

0x00049000

ad9694_jesd204.phy_reconfig_2

0x0004a000

ad9694_jesd204.phy_reconfig_3

0x0004b000

axi_ad9694_dma

0x0004c000

axi_ad9694

0x00050000

axi_laser_driver_0

0x00060000

avl_laser_gpio

0x00070000

SPI connections

SPI type

SPI manager instance

SPI subordinate

CS

ZC706/ZCU102

A10SoC

ZC706/ZCU102

A10SoC

PS

PL

SPI 0

—

AD9094

0

PS

PL

SPI 1

SYS_SPI/AXI_SPI

AD9528

0

PL

PL

AXI_QUAD_SPI

SYS_SPI/AXI_SPI

ADF4360-7

0

PL

—

AXI_QUAD_SPI

SYS_SPI/AXI_SPI

AD5627

0

GPIOs

GPIO signal

Direction (from FPGA view)

HDL GPIO EMIO

Software GPIO Zynq MP

Software GPIO Zynq

Software GPIO Arria 10

Xilinx

Intel

laser_gpio[13:0]

INOUT

51-38

—

129-116

105-92

—

afe_adc_convst

OUTPUT

37

37

115

91

5

afe_dac_load

OUTPUT

36

36

114

90

4

afe_dac_clr_n

OUTPUT

35

35

113

89

3

adc_pdwn

INOUT

34

34

112

88

2

adc_fdb

INOUT

33

33

111

87

1

adc_fda

INOUT

32

32

110

86

0

Interrupts

Below are the Programmable Logic interrupts used in this project.

Instance name

HDL

Microblaze

Linux ZynqMP

Actual ZynqMP

ad9694_jesd

11

14

109

141

afe_dac_iic

12

14

109

141

ad9694_dma

13

12

107

139

axi_spi_vco

10

15

110

142

axi_spi_afe_adc

9

8

103

135

axi_laser_driver_0

8

7

102

134

Instance name

HDL

A10SoC

sys_spi_clockgen

8

27

sys_spi_vco

9

28

sys_spi_afe_adc

10

29

ad9694_jesd204

11

30

axi_ad9694_dma

12

31

axi_laser_driver_0

13

32

avl_laser_gpio.irq

14

33

Known issues

If the Lidar board do not power up.

Problem: The Lidar boards do not power up because the PG_C2M pull-up resistor value on the carrier (Arria 10) is too high.

Solution: On Arria 10 - place a 4k7 ohms resistor in parallel with R5517.

Note:

The PG_C2M can no longer be software controlled. As soon as there is an auxiliary 3V3 on the carrier, the Lidar platform receives the power up command. This problem only affects Lidar Rev B.

Building the HDL project

The design is built upon ADI’s generic HDL reference design framework. ADI distributed the bit/elf files of this project as part of the ADI Kuiper Linux until the 2019_R1 release. The prebuilt files can be found in the previous link. Afterwards, it was discontinued.

But, if you want to build the sources, ADI makes them available on the HDL repository. To get the source you must clone the HDL repository and checkout the last release branch where this project still exists, hdl_2019_r1.

Then go to the hdl/projects/ad_fmclidar1_ebz/$zc706 location and run the make command. You can also go to the other folder for different carriers.

/hdl$
git checkout hdl_2019_r1
/hdl$
cd projects/ad_fmclidar1_ebz/zc706
/hdl/projects/ad_fmclidar1_ebz/zc706$
make

A more comprehensive build guide can be found in the Build an HDL project user guide.

Resources

Parts

Laser Board

DAQ Board

AFE Board

More information

Support

Analog Devices, Inc. will provide limited online support for anyone using the reference design with ADI components via the EngineerZone FPGA reference designs forum.

For questions regarding the ADI Linux device drivers, device trees, etc. from our Linux GitHub repository, the team will offer support on the EngineerZone Linux software drivers forum.

For questions concerning the ADI No-OS drivers, from our No-OS GitHub repository, the team will offer support on the EngineerZone microcontroller No-OS drivers forum.

It should be noted, that the older the tools’ versions and release branches are, the lower the chances to receive support from ADI engineers.