ADS-B Airplane Tracking Tutorial (Obsolete)

Warning

This model is considered deprecated. See updated model here: HW/SW Co-Design Implementation of ADS-B Receiver Using Analog Devices AD9361/AD9364.

Overview

Due to the complexity of the SDR systems nowadays, there is a significant gap between the concept of a SDR system and the realization of that working design. Bridging this gap typically involves teams of engineers with a variety of different skill sets (RF, DSP, FPGA, software, system integration and etc.), and in many cases projects get de-railed early in the development stage because of difficulty in coordinating the efforts of these varied design entities.

In this tutorial, we will present how model based design provides a collaborative solution for SDR, which allows developers of different backgrounds (RF, DSP, FPGA, software, system integration and etc.) to work together in a single environment, and quickly build and prototype SDR systems while establishing and maintaining a deployable path to production. As a real-world and interesting example of the process, we will actually build a wireless SDR platform that receives and decodes Automatic Dependent Surveillance-Broadcast (ADS-B) signals to allow us to detect and report the position, altitude, and velocity of the commercial aircraft flying in our vicinity.

The signal processing requirements of ADS-B are quite trivial, and most would agree that this type of development methodology is overkill for something of this scope. However, the focus of this tutorial is the model based design flow, not the algorithmic complexity of what is actually being implemented. Rather than show a complex signal processing example at the same time as introducing modern development methodology, we will focus on the development tools used, and showcase things, while still using a real world example.

From simulation to production, the following tasks will be performed in this tutorial:

  1. Design of signal processing algorithms used to decode ADS-B messages

  2. Simulation of the RF transceiver receiving ADS-B signals

  3. Generation of C and HDL code

  4. Verification of the HDL code with recorded and live data on the target transceiver and FPGA

Software and Hardware Requirements

Software Requirements

MATLAB is the simulation tool used in this tutorial. Your MATLAB version should be 2016a or later, and your license needs to include the following components:

Besides, the following items are required in prototype and production stages:

Hardware Requirements

From Simulation to Production Workflow

The following sections will follow the workflow shown in the figure below:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_flow.png

Figure 1 From simulation to production workflow

  1. The first step of component evaluation is to understand if the AD9361 will meet your requirements (the component evaluation stage). Since the AD9361 can tune to 1090MHz (the broadcast frequency for ADS-B), and receive a 2MHz bandwidth signal (the channel bandwidth of ADS-B), the AD9361 is suitable.

  2. The next step of behavioral simulation is to model and simulate the SDR system in Simulink. At this stage the communication algorithm is partitioned into blocks that will be implemented in software and blocks that will be implemented into the programmable logic or embedded software.

  3. After verified in pure simulation environment, this model can be run with “Radio I/O”, where we are capturing signals off the air, and ensuring that our model works with real world impairments.

  4. Once the partitioning and the simulation are complete, in the prototype stage, the SDR model is converted into C code and HDL using Embedded Coder and HDL Coder. A Zynq-based prototyping system is used to verify the performance of the communication algorithm and to help further tune the SDR model before moving to the actual production stage.

  5. Finally, in the production stage the automatically generated C code and HDL are integrated into the complex production system framework. This workflow ensures that once the communication algorithm reaches the production stage it is fully verified and tested and provides a lot of confidence in the system’s robustness.

  6. In each step of this process, we need to test the models with a pre-defined test suite, to make sure we get consistent results throughout the process.

Component Evaluation

Wireless signals that can be detected and decoded are everywhere, and they are easily accessible with today’s Software Defined Radio (SDR) hardware like the Analog Devices AD9361 integrated RF agile transceivers. The Automatic Dependent Surveillance Broadcast (ADS-B) transmissions from commercial aircraft provide a readily available wireless signal that can be used to demonstrate the Zynq and AD9361 rapid prototyping flow. Commercial aircraft use ADS-B transmitters to report their position, velocity, altitude and aircraft ID to air traffic controllers. The flight data format is defined in the International Civil Aviation Organization’s (ICAO) Mode S Extended Squitter specification. ADS-B is being introduced throughout the world to modernize air traffic control and collision avoidance systems. It has already been adopted in Europe and is being gradually introduced in the United States.

The Mode S Extended Squitter standard provides details of the RF transmission format and encoded data fields. The transponder transmission has the following properties:

  • Transmit Frequency: 1090 MHz

  • Modulation: Pulse Position Modulation (PPM)

  • Data Rate: 1 Mbit/s

  • Message Length: 56 usec or 112 usec

  • 24-bit CRC checksum

The tuning frequency and bandwidth are well within the capabilities of the AD9361 RF transceiver, such as the PicoZed SDR board.

The Mode S waveform is fairly simple, as shown below, but there are still several challenges involved in receiving and decoding the transmitted messages.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_fig1.png

Figure 2 Mode S waveform

  • The receive environment typically contains very short messages interspersed with long idle periods. The signals being received can be very weak when the transmitting aircraft is a long distance from the receiver. Legacy waveforms are also transmitted at 1090 MHz. The receiver needs to use the preamble to identify both high and low amplitude Mode S transmissions in a congested frequency band.

  • Bits have one of two possible patterns within the 1 usec bit interval. A logical 1 is ON for the first 1/2 usec and OFF for the second 1/2 usec. A logical 0 is OFF for the first 1/2 usec and ON for the second 1/2 usec. Since the bit decisions are made based on time-based patterns, the receiver needs to use the preamble to accurately find the IQ sample where the message bits start.

  • The Mode S message is composed of 88 information bits and 24 checksum bits. The receiver needs to be able to clear registers, make bit decisions, compute the checksum and read the checksum registers at the correct times. Timing control is required for the receiver to function properly.

  • For an embedded design, the decoding process has to work on a sample by sample basis. Storing large amounts of data for batch processing is not a realistic receiver design for an embedded system.

The combination of a powerful RF front end like the AD9361 and a technical computing language like MATLAB greatly simplifies the problems associated with detecting and decoding these transmissions. Functions for the math and signal processing libraries can be used to identify the sync pattern, calculate the noise floor, make bit decisions and calculate the checksum. The conditional and execution control functions in MATLAB simplify the control logic. Accessing test data is easy, both from binary or text files or streamed directly into MATLAB using the AD9361 SDR platforms.

Behavioral Simulation

Transmit Model

In order to verify the receiver model works properly, especially the detect and decoding algorithm, we construct a transmit model from some known ADS-B message as a test suite.

The transmit model adsbTxGen.m can be found on the Analog Devices GitHub repository:

The input to this function is the known ADS-B message you would like to transmit, and the output is the baseband ADS-B waveform that the receiver can handle. In the MATLAB command window, run the following line:

txData = adsbTxGen('8D86D5E058135037C0A9112B72B7');

It will generate the waveform for the message ‘8D86D5E058135037C0A9112B72B7’. The waveform is saved in the variable txData. You can either leave this variable in the workspace if you will try out the receiver model right away, or save it in a mat file for future reference.

Receive Model

The receiver model ModeS_Simulink_Decode.mdl and its associated files can be found on the Analog Devices GitHub repository:

The model itself is quite straightforward. It takes the pre-recorded ADS-B data, saved in data_Yb.mat as input, and then decode the message. The subsystem of decoding algorithm is shown in the figure below:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_fig9.png

Figure 3 ADS-B decoding algorithm subsystem

The first step in the decoding is to calculate the noise floor and the correlation to the preamble. Digital filter blocks are used for these calculations. The TimingControl is implemented using Stateflow, which is a state machine tool that is used to generate the timing, reset and control signals for the rest of the decoding algorithm. Stateflow is very useful for models where you want to separate the control logic from the data flow. Once the timing and triggers are activated the block named Bit Process takes the input IQ samples and calculates the data bits, and the CRC_Check block computes the checksum. The message parsing takes place in a MATLAB script named DecodeBits.m driven by this Simulink model.

After you run the model, the figure below from the MATLAB command window shows the two messages that were successfully decoded from the one million sample data set. The hex characters that make up the 88-bit message and 24-bit checksum are displayed, and the results of the decoding process show the aircraft ID, message type, and aircraft velocity, altitude, and position.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_fig8.png

Figure 4 Decoded ADS-B messages

In order to verify the detect and decoding algorithm works properly, double click on the Signal From Workspace block, and use the synthetic data txData we just created as the signal source:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_txdata.png

Figure 5 Signal From Workspace configuration

Click play button to run the model. In the command window, you will see the following results:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_txresult.png

Figure 6 Verification results

Since we select the cyclic repetition mode for txData, the decoded result will repeat until the simulation ends. As you can see, the decoded result matches what we have transmitted, so it verifies the receiver model, including the detect and decoding algorithm, works properly.

Radio I/O

After implementing any signal processing algorithm in MATLAB or Simulink, the next natural step is to verify the algorithm’s functionality using real data acquired from the actual SDR hardware system that it is going to run on. In the previous step, the verification of the algorithm is done using different sets of input data captured from the system. This helps validate the algorithm’s functionality, but does not guarantee that the algorithm will perform as expected in environmental conditions other than the ones used to make the data captures, or what the behavior and performance will be for different settings of the analog frontend and digital blocks of the SDR system. In order to verify all of these aspects, it is very beneficial if the algorithm can be run online, receiving live data as input, and tuning the settings of the SDR system for optimal performance.

In this section, we will describe and showcase how to use IIO System Object to capture signals with the target transceiver, but still do the signal processing on the host in MATLAB and Simulink to decode the messages, as shown below:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_sys_obj.png

Figure 7 IIO System Object architecture

The algorithm will be designed with the ultimate goal of deploying the solution onto a Zynq SoC platform, such as PicoZed SDR board. Readers who are interested in following along with the radio I/O models can find the files on the Analog Devices GitHub repository:

To better understand these models, an introduction to IIO System Object provided by ADI can be found here.

MATLAB

To validate the MATLAB ADS-B decoding algorithm operation with real time data acquired from the PicoZed SDR platform, a MATLAB script ad9361_ModeS.m has been developed to perform the following operations:

  1. Calculate the earth zone according to user input

  2. Create and configure the IIO System object

  3. Configure the PicoZed analog frontend and digital blocks through the IIO System object

  4. Receive data frames from the SDR platform using the IIO System object

  5. Detect and decode the ADS-B data

  6. Display the decoded ADS-B information

After an IIO System object is constructed, it must be configured with the IP address of the SDR system, the target device name and input/output channels sizes and numbers. The following piece of code presents an example on how to create and configure the MATLAB IIO System object.

% System Object Configuration
s = iio_sys_obj_matlab; % MATLAB libiio Constructor
s.ip_address = ip;
s.dev_name = 'ad9361';
s.in_ch_no = 4;
s.out_ch_no = 4;
s.in_ch_size = n;
s.out_ch_size = n;

The IIO System object is then used to set the attributes of AD9361, and to receive the ADS-B signals.

% Set the attributes of AD9361
if strcmp(source,'pre-captured')
    input_content{s.getInChannel('RX_LO_FREQ')} = 6e9;
elseif strcmp(source,'live')
    input_content{s.getInChannel('RX_LO_FREQ')} = 1.09e9;
else
    error('Please select a data source: pre-captured or live.');
end
input_content{s.getInChannel('RX_SAMPLING_FREQ')} = 2.5e6;
input_content{s.getInChannel('RX_RF_BANDWIDTH')} = 10e6;
input_content{s.getInChannel('RX1_GAIN_MODE')} = 'fast_attack';
input_content{s.getInChannel('RX1_GAIN')} = 0;
input_content{s.getInChannel('RX2_GAIN_MODE')} = 'fast_attack';
input_content{s.getInChannel('RX2_GAIN')} = 0;
input_content{s.getInChannel('TX_LO_FREQ')} = 6e9;
input_content{s.getInChannel('TX_SAMPLING_FREQ')} = 2.5e6;
input_content{s.getInChannel('TX_RF_BANDWIDTH')} = 10e6;

The attributes of AD9361 is set up based upon the following considerations:

Sampling rate is quite straightforward with the AD9361 based platforms. Transmit date rate normally equals Rx date rate, and ultimately depends on the baseband algorithm. In this example, since the decoding algorithm is designed to work with the sampling rate of 2.5 MSPS, the date rate of AD9361 is set accordingly. By doing this, the received samples can be applied directly to the decoding algorithm, without any additional decimation or interpolation operations.

The RF bandwidth control sets the AD9361’s Rx analog baseband low pass filters’ bandwidth to provide anti-aliasing and out-of-band signal rejection. In order to correctly demodulate the received signals, the system must maximize signal-to-noise ratio (SNR). In order to do this, RF bandwidth needs to be set as narrow as possible while meeting flatness and out-of-band rejection specification to minimize in band noise and spurious signal levels. Therefore, setting the RF bandwidth at an optimal value is critical to receive desired in-band signals and reject out-of-band signals. By observing the spectrum of received signals, we find 10 MHz is a proper value for the RF bandwidth.

Besides setting up the analog filters of AD9361 via RF bandwidth attribute, we can also improve the decoding performance by enabling the digital FIR filters on AD9361 via the IIO System object. According to the spectrum characteristics of the ADS-B signal, we design an FIR filter with data rate of 2.5 MSPS, pass band frequency of 3.25 MHz and stop band frequency of 4 MHz. In this way, we can further focus on the bandwidth of interest.

s.writeFirData('adsb.ftr');

adsb.ftr is a file containing the coefficients of an FIR filter designed using the Analog Devices AD9361 Filter Design Wizard. This tool provides not only a general purpose low pass filter designer, but also magnitude and phase equalization for other stages in the signal path.

The versatile and highly configurable AD9361 transceiver has several gain control modes that enable its use in a variety of applications. The Gain Mode parameter of the IIO System object selects one of the available modes: manual, slow_attack, hybrid and fast_attack. In the case of ADS-B, the fast attack gain mode provides the best results due to the bursty nature of these signals. In addition, fast attack mode is required for this waveform since there is preamble, the AGC needs to react fast enough so that the first bit is captured.

In the end, depending on how you set up the TX_LO_FREQ and RX_LO_FREQ, there are two ways of using this model: using pre-captured data (RF loopback) and using live data off the air.

Pre-captured Data

In this case, we are transmitting and receiving some pre-captured ADS-B signals using PicoZed. These signals are saved in a variable called newModeS.

input_content{1} = (2^13).*newModeS./sqrt(2);
input_content{2} = (2^13).*newModeS./sqrt(2);
input_content{3} = (2^13).*newModeS./sqrt(2);
input_content{4} = (2^13).*newModeS./sqrt(2);

The requirement for this case is to make TX_LO_FREQ = RX_LO_FREQ, and it can be any LO frequency value that PicoZed supports. Due to the nature of pre-captured data, there is plenty of ADS-B valid data in there, so it is a good way to verify whether the hardware setup is appropriate.

Live Data

In this case, we are receiving the real-time ADS-B signals over the air, instead of the signals transmitted by PicoZed. According to ADS-B specification, it is transmitted at the center frequency of 1090 MHz, so the requirements for this case is:

  • RX_LO_FREQ = 1090 MHz, TX_LO_FREQ far away from 1090 MHz in order to avoid interference

  • Use a proper antenna on the Rx side, which is capable of covering the 1090 MHz band. Using a poorly tuned or poorly made antenna will result in a lack of range for your air radar.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_setup.jpg

Figure 8 Test setup with PicoZed SDR board and antenna

With everything set up properly, in order to run the MATLAB model, simply use the following command:

[rssi1,rssi2]=ad9361_ModeS('ip','data source',channel);

where ip is the IP address of the SDR board, and data source specifies the data source of the received signal. Currently, this model supports data sources of ‘pre-captured’ and ‘live’. channel specifies whether signals are received using Channel 1 or Channel 2 of the PicoZed.

For example, the following command receives the pre-captured data on Channel 2:

[rssi1,rssi2]=ad9361_ModeS('192.168.10.2','pre-captured',2);

At the end of the simulation, you will get the RSSI values on both channels in your command window, as well as the result tables shown below:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_table.png

Figure 9 ADS-B result table

This result table shows the information of aircrafts appearing during the simulation. With a proper antenna, this model is able to capture and decode the aircraft signals in an 80 miles range with PicoZed. Since there are two types of Mode S messages (56 usec or 112 usec), some messages contain more information than the other.

When trying out this model with the real-world ADS-B signals, the signal strength is very important for successful decoding, so make sure to put the antenna in a good line of sight location with the aircraft. The received signal strength can be seen by looking at the RSSI values on both channels. For example, if receiving the signals on channel 2, the RSSI of channel 2 should be significantly higher than that of channel 1. You can tell whether there is any useful data by looking at the spectrum analyzer.

Prototype and Production

In this section, we will show how to take the algorithm developed in behavioral simulation, verified in pure simulation and radio I/O, and use HDL Coder and Embedded Coder from MathWorks to generate code and deploy it in the production hardware. It enables rapid design iteration cycles and helps to detect and correct design and specification errors early.

Intermediate Model

The following guide outlines recommended practices for creating a design that can be implemented in hardware efficiently, and for optimizing the generated HDL for your targeted device.

According to the guidelines presented in the reference guide, the intermediate model ModeS_FixPt_Pipelined_ADI.slx and its associated files can be found on the Analog Devices GitHub repository:

In this model, we converted the data type from floating point to fixed point, and we added some pipeline registers as the first step for setting this model up for HDL code generation. It uses the same data set as the behavioral model, so you will get the same decoded messages.

Following this, there are two workflows to follow, one is HW/SW Co-Design provided by MathWorks, and the other is the MathWorks HDL Workflow Advisor flow using the HDL Workflow Advisor Board Support Package provided by ADI. It is recommended to use the HW/SW Co-Design whenever the hardware platform of interest is supported by this workflow.

MathWorks HW/SW Co-Design

Hardware-Software Co-Design is a standard workflow provided by MathWorks Communications System Toolbox Support Package for Xilinx Zynq-Based Radio. Using this workflow, you can prototype an algorithm in Simulink and then deploy it on the ARM processor and FPGA fabric of the Zynq hardware. The hardware-software co-design workflow includes FPGA targeting, HDL IP core generation, and the generation of a software interface model for execution on the ARM processor. To get started, see Hardware-Software Co-Design for Zynq SDR Applications.

The HW/SW Co-Design Implementation of ADS-B Transmitter/Receiver Using Analog Devices AD9361/AD9364 is a shipped example in MATLAB from R2016b. In this example, the stateflow block is removed and replaced with a MATLAB state machine, which means users without a stateflow license can use the model.

Since MathWorks example comes with detailed documentation, we are not going to elaborate here. However, just a reminder - do not forget to set up SDK tools:

Tip

SDK Tools Set Up

  1. Within MATLAB, use Add-Ons > Get Hardware Support Packages to download Embedded Coder Support Package for Xilinx Zynq-7000 Platform.

  2. Follow the installer instructions for installing the support package software.

  3. You must then setup the SDK tools using the setup wizard. This will run automatically following installation. On the first pane, select Configure the Xilinx Design Tools. Click Next.

  4. On the next pane, provide a valid path to the Xilinx SDK development tools. The default install path fills in automatically. Update the path if you installed the SDK in a nondefault location.

  5. To complete the configuration, click Next.

If you already have the Embedded Coder Support Package for Xilinx Zynq-7000 Platform installed, you can start the setup wizard manually. On the MATLAB Home tab, in the Environment section of the Toolstrip, click Add-Ons > Manage Add-Ons. Locate Embedded Coder Support Package for Xilinx Zynq-7000 Platform and click Setup. Then follow the steps above.

Steps to Follow
  1. In MATLAB 2016b, run the following two lines in command window:

    >> hdlsetuptoolpath('ToolName','Xilinx Vivado','ToolPath','PATH_TO_YOUR_VIVADO.BAT_FOR_2015_4');
    >> setupzynqradioipcoregen
    
  2. Open zynqRadioHWSWADSBAD9361AD9364SL.slx.

  3. Right click HDL_ADSB subsystem and launch HDL workflow advisor from there. Please note if you install both MathWorks HW/SW Co-Design and ADI Board Support Package, there might be some issues in Step 4.2 of HDL Workflow Advisor when using the HW/SW Co-Design flow. The solution is to uninstall the ADI Board Support Package.

  4. Go through all the steps in HDL workflow advisor. In the end, program the Zynq hardware.

  5. Open the software interface model, run simulation in external mode and deploy to hardware.

Tip

In HDL workflow advisor Step 4.4, you can download the completed bitstream to the target and restart the board. You can also download the bitstream at the command line:

devzynq = zynq();
% The following address should match the board address
devzynq.IPAddress = '192.168.3.2';
% Path to the generated bitstream
devzynq.programFPGA(...
   'hdl_prj\vivado_ip_prj\vivado_prj.runs\impl_1\system_wrapper.bit')

This bitstream is not persistent across power cycles. If you want the generated FPGA image to load each time you turn on the board, call the downloadImage method:

radio = sdrdev('PicoZed SDR');
downloadImage(radio,'FPGAImage',...
   'hdl_prj\vivado_ip_prj\vivado_prj.runs\impl_1\system_wrapper.bit');

This call renames the generated system_wrapper.bit file to system.bin and downloads the file over an Ethernet connection to the radio hardware.

Tip

  • This example also works for receiving signals off the air, just comment out the transmitter block and adjust the receiver centre frequency.

  • For accurate position calculations, you will need to edit lines 8 and 9 of the position calculation script to give your current location.

>> edit zynqRadioHWSWADSBPositionCalcSingle

Target an ADS-B Airplane Tracker Using HW/SW Co-Design Workflow is also available on the Ettus E310 SDR platform.

ADI Board Support Package for the HDL Workflow Advisor

The ADI Board Support Package (BSP) for the HDL Workflow Advisor, based upon the MathWorks Board and Reference Design Registration System, is a collection of board definitions and reference designs that provide to the MathWorks HDL Workflow Advisor, which is capable of:

  • Generate IP blocks compatible with Analog Devices HDL reference designs for various Analog Devices platforms,

  • Automatically insert the generated IPs into the Analog Devices Vivado HDL reference designs.

A general introduction to the ADI Board Support Package can be found here. In this section, we will go through the steps to apply board support package towards ADS-B model.

Step 1: Download and install BSP

The board support package can be found at Analog Devices GitHub:

To install the Analog Devices BSP, set the MATLAB current folder to the /vendor/AnalogDevices folder found in the location where the BSP was downloaded and run

>> AnalogDevices.install

in the MATLAB command window. After the installation process is complete, run ver in the MATLAB command window to list all the installed packages. If the installation was successful, the HDL Coder BSP Tools and HDL Coder BSP: Analog Devices Inc should appear in the list, as shown below:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_install.png

Figure 13 ADI BSP installation

Tip

To uninstall the Analog Devices BSP, run this in the MATLAB command window:

>> AnalogDevices.uninstall

Step 2: Setup Xilinx tools

Xilinx Vivado 2015.2.1 is required in this process.

In MATLAB, run the following line in command window:

>> hdlsetuptoolpath('ToolName','Xilinx Vivado','ToolPath','PATH_TO_YOUR_VIVADO.BAT_FOR_2015_2_1');

Step 3: Download and open model

The ADS-B hardware targeting model can be found at Analog Devices GitHub:

Open model ModeS_ADI_Codegen.slx in MATLAB.

Step 4: Go through HDL Workflow Advisor

Right click on Detector subsystem, choose HDL Code from the menu, and click on HDL Workflow Advisor to launch this tool, as shown below:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_hdlwa.png

Figure 14 HDL Workflow Advisor

In step 1.1, select IP Core Generation for Target Workflow:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_step1.1.png

Figure 15 Step 1.1 - Set Target Device and Synthesis Tool

In step 1.2, set target interface as below, where all the signals we want to observe are set as AXI4-Lite:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_external.png

Figure 16 Target reference design selection

In step 3.1.2, set reset asserted level to Active-high:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_step3.1.png

Figure 17 Step 3.1.2 - Reset configuration

Then, run each task including Step 4.2. In the end of Step 4.2, you will see a software interface model generated. The external mode runs in this model, which will be introduced later.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_step4.2gm.png

Figure 18 Step 4.2 - Generated model

In Step 4.3, select Custom for Tcl file for synthesis build, and use adi_build.tcl from \ADSB\hdl_prj\vivado_ip_prj\projects\scripts\ folder:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_step4.3.png

Figure 19 Step 4.3 - Custom Tcl file for synthesis build

Tip

adi_build.tcl is a generic file used to automate the build process for BOOT.BIN. You can use it in other ADI BSP projects.

For the other steps not mentioned above, use default settings from HDL Workflow Advisor.

After Step 4.3 finishes running, you will find the newly generated BOOT.BIN inside \ADSB\hdl_prj\vivado_ip_prj\boot\ folder:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_bootbin.png

Figure 20 Boot file generation

Step 5: Copy and paste the generated BOOT.BIN onto SD card

Use the latest image from ADI. Replace the BOOT.BIN on SD card with the newly generated BOOT.BIN from HDL Workflow Advisor.

Step 6: Use MATLAB Coder to generate C code

Open DecodeBits_ADI.prj from your ADSB model folder and fill in the settings as following:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_prj.png

Figure 21 MATLAB Coder project

Then click the “Generate” button, and the code generation process will run automatically. In the end, you will find a new folder called codegen in your current MATLAB directory, which includes the files generated from MATLAB Coder.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_codegen.png

Figure 22 Codegen folder contents

Step 7: Interface the C code with the data from FPGA

The generated C code contains the implementation of the ADS-B data decoding algorithm, but does not contain the functions needed to configure the radio and acquire the data from the ADS-B IP. The easiest way to achieve these two tasks is to use the libiio support for the AD9361 and create an application which uses the libiio functions to configure the radio and read the data from the ADS-B IP through the DMA and afterwards call the auto-generated ADS-B decoding C code. This application is provided together with the ADS-B model. It is called adsb_decode.c and can be found in the linux_app folder from your ADSB model folder, together with the auto-generated C code provided there for reference. The next step is to copy the auto-generated C code along with adsb_decode.c and the Makefile found in the linux_app folder to your SD card and build the application under Linux by running the make all command in the location where the files were copied. The resulting binary file is called adsb_decode and can be ran to verify the system’s functionality. This file is also provided for reference in the linux_app folder.

To transfer the files to your Linux system. You can use tools such as WinSCP:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_winscp.png

Figure 23 Deploying files to target using WinSCP

Tip

If you want to run the adsb_decode binary file provided in the linux_app folder you must change the access permission of adsb_decode after you have had it transferred to your Linux system. You can do it by using the chmod command in a terminal:

chmod +x adsb_decode

Step 8: Observe the results

Use pre-captured data to verify

Before we use adsb_decode to decode real world ADS-B signals, we can verify this file, the new BOOT.BIN, as well as the hardware settings using some pre-captured data and the ADI IIO Oscilloscope.

In IIO scope, set the Receive Chain and Transmit Chain according to the specifications of ADS-B signals. Then, use DAC Buffer Output for DDS Mode. In the end, select file data_noise.mat, which includes the pre-captured data and click Load. You will see the message saying “Waveform loaded successfully” if your file has been applied to the DAC channels you selected.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_oscverify.png

Figure 24 IIO Oscilloscope verification

On Linux side, open a terminal and run the following command:

sudo ./adsb_decode 42.36 -71.06

You will see the following results almost immediately after you execute the command:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_oscverify_results.png

Figure 25 Pre-captured data verification results

Tip

Use Ctrl + c to end the program.

Observe live data

As soon as everything is verified by pre-captured data, we can move on to the live data. Connect the antenna to RX1A of the PicoZed. On Linux side, open a terminal and run the following command:

sudo ./adsb_decode lat lon

Note: lat and lon are latitude and longitude of your current location.

Wait a few seconds to a few minutes, depending on your local air traffic, and you will observe the decoded ADSB messages in the terminal, such as following:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_result.png

Figure 26 Live data results

Tip

For the actual field test, compare the ADS-B information decoded by the system with the data provided by airplane live tracking websites (such as flightradar24.com), and see whether the decoding algorithm displays the correct aircraft ID, altitude, speed, and latitude/longitude coordinates.

Use External Mode

With external mode, you can log signals and tune parameters while the model is running on the target hardware in real-time. When you change parameter values from within Simulink, the modified parameter values are communicated to the target hardware immediately.

The Analog Devices BSP also allows external mode for the supported Analog Devices boards. This enables the Simulink models used for IP core generation to be run in external mode and talk to the target hardware running the Analog Devices Linux distribution.

Before you run external mode, first set up the environment variable 'ADI_ZYNQ_SDR_IPADDRESS' to the IP address of your board. For example, run the following line in the MATLAB command window:

>> setenv('ADI_ZYNQ_SDR_IPADDRESS', '192.168.3.2');

Open the software interface model generated in Step 4.2 of the HDL Workflow Advisor, as shown below:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_softwareinterfacemdl.png

Figure 27 Software interface model

Before running the external mode, make sure that the “Hardware Implementation” options are set as below. Select Analog Devices Zynq SDR for Hardware board, and click Apply.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_after.png

Figure 28 Hardware Implementation configuration

Go to “Code Generation” options, select Debug for Build Configuration, and click Apply:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_buildconfig.png

Figure 29 Build configuration for external mode

Now you can open the software interface model and run it in external mode. Select External from the menu, and click Play button.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_playbutton.png

Figure 30 Starting external mode simulation

You will see a new terminal open up and show the results on hardware:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_externalresult.png

Figure 31 External mode terminal results

Besides, you can open each scope in the interface model and see how the signals behave on hardware. The following is a capture of the Correlators scope:

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/adsb_tutorial_extresult.png

Figure 32 External mode decoded ADS-B messages

Reference

“Four Quick Steps to Production: Using Model-Based Design for Software-Defined Radio” Article Series

  1. Di Pu, Andrei Cozma, and Tom Hill. “Part 1 - the Analog Devices/Xilinx SDR Rapid Prototyping Platform: Its Capabilities, Benefits, and Tools”. Analog Dialogue, Volume 49, Number 3.

  2. Mike Donovan, Andrei Cozma, and Di Pu. “Part 2 - Mode-S Detection and Decoding Using MATLAB and Simulink”. Analog Dialogue, Volume 49, Number 4.

  3. Di Pu, and Andrei Cozma. “Part 3 - Mode-S Signals Decoding Algorithm Validation using Hardware in the Loop”. Analog Dialogue, Volume 49, Number 4.

  4. Mike Donovan, Andrei Cozma, and Di Pu. “Part 4 - Rapid Prototyping using the Zynq SDR Kit and Simulink Code Generation Workflow”. Analog Dialogue, Volume 49, Number 4.

Support

If you have any questions about PicoZed / AD9361 or ADI BSP workflow, please ask on the EngineerZone.

If you have any questions about ADS-B receiver algorithm or HW/SW Co-Design workflow, please contact MathWorks. MathWorks Support