Troubleshooting Guide

Reference for resolving common issues with the X-Band Phased Array Development Platform. Use the section headings below to navigate to the relevant issue category.

Power and Boot Issues

Symptom

Possible Cause

Solution

No power LEDs

Power supply not connected

Verify all power connections and switch positions

Board gets hot quickly

Short circuit

Power off immediately, check for shorts with multimeter

ZCU102 won’t boot

SD card not inserted

Verify SD card fully seated in J1001

ZCU102 won’t boot

Wrong boot mode

Check SW6 settings: ON-OFF-OFF-OFF

Intermittent boot

Loose FMC connection

Reseat AD9081-FMCA-EBZ board

No Ethernet link

Cable not connected

Check cable, verify link LED on RJ45

Board doesn’t power on or powers off

Insufficient PSU current

Use a 12V 6A+ supply; 8A+ when FMC cards are installed

VADJ and AD9081 Power Issues

Two issues commonly prevent 1.8V VADJ from powering the AD9081-FMCA-EBZ:

  1. ADXUD1AEBZ FMC EEPROM — Non-compliant EEPROM prevents VADJ from enabling during boot.

    • Program the FMC EEPROM (see EEPROM Programming), then perform a full power cycle of the FPGA.

  2. AD9081 LTM4616 enable pin voltage — The run-control threshold is 1.7 V. If R1M voltage falls below this, VADJ will not enable.

    • Replace R1M (2.2 kΩ) with a 220 Ω 0402 resistor to raise the enable pin voltage above 1.7 V.

Symptom

Possible Cause

Solution

1.8V VADJ missing after EEPROM programming

Incomplete power cycle

Full power cycle: disconnect AC, wait 10 s, reconnect

VADJ not enabling

LTM4616 enable voltage too low

Replace R1M (2.2 kΩ → 220 Ω 0402)

Wrong voltage on VADJ

Wrong EEPROM programmed

Verify I2C path: /sys/bus/i2c/devices/15-0050/eeprom

VADJ intermittent

FMC connector issue

Reseat FMC connector; inspect pins for damage

EEPROM Programming Issues

Symptom

Possible Cause

Solution

find /sys -name eeprom returns no results

FMC not fully seated

Reseat FMC connector and reboot

EEPROM I2C device missing

ZCU102 not booted

Confirm boot completed; run i2cdetect -y 15 to rescan

fru-dump returns error

FRU binary not found

Verify: ls /usr/local/src/fru_tools/masterfiles/AD-FMCOMMS2-EBZ-FRU.bin

Permission denied during write

Not logged in as root

Log in as root user

Write fails to I2C device

Wrong I2C bus number

Verify correct bus number with i2cdetect

Readback shows incorrect data

Programming incomplete

Reprogram EEPROM; check file integrity with md5sum

EEPROM data doesn’t persist

No power cycle after programming

Always perform a full power cycle after EEPROM changes

Write-protect error

Hardware write-protect enabled

Check for and disable hardware write-protect jumpers

Firmware Verification (MD5 Checksums)

If you suspect corrupted or mismatched boot files, you can verify integrity by comparing MD5 checksums on the ZCU102:

md5sum /boot/Image
md5sum /boot/BOOT.BIN
md5sum /boot/system.dtb

Compare the output against the checksums of the files you originally copied to the SD card (run md5sum on your host machine against the source files). If they don’t match, the file was corrupted during copy or the SD card has errors — reflash and recopy.

Note

Checksums will NOT match between different firmware builds or software versions. This check is only useful to confirm that the files on the SD card are identical to what you intended to copy — not to verify a specific “correct” version.

SD Card and Boot Media Issues

Symptom

Possible Cause

Solution

ZCU102 doesn’t boot

SD card not fully inserted

Verify SD card fully seated in slot J1001

“No SD card” errors

Wrong boot mode

Check SW6: ON-OFF-OFF-OFF

Card not recognized

Incompatible SD card

Use SanDisk or Samsung; try a different card

Intermittent boot failures

Corrupted SD card

Reformat and reflash using BalenaEtcher

Boot hangs at U-Boot

Missing or misnamed boot files

Verify BOOT.BIN, Image, and system.dtb are in SD card root (case-sensitive)

Linux boots but fewer than 40 IIO devices

Wrong device tree

Copy matching system.dtb for your clocking config; full power cycle

VADJ not present after boot

EEPROM not programmed

See EEPROM Programming

“Flash Failed” in BalenaEtcher

Expected behavior

This is normal — verification always fails for Kuiper Linux images; proceed

File copy errors on ADI PCs

Windows auto-encryption

Use network drive mapping; never copy directly through Windows Explorer to SD card

ZCU102 Configuration Issues

Symptom

Possible Cause

Solution

No boot activity or UART output

Wrong boot mode

Verify SW6: ON-OFF-OFF-OFF

USB keyboard or mouse not detected

Wrong USB jumper configuration

Check J7, J109, J110, J112, J113 are on the correct pin pairs

Terminal connected but shows no output

Wrong COM port or settings

Use 115200 baud, 8N1, no flow control; verify CP210x driver installed

Ethernet link doesn’t come up or no IP

Cable or DHCP issue

Try a different cable; configure static IP if DHCP is unavailable

Network not reachable from PC

Subnet mismatch

Ensure PC and ZCU102 are on the same subnet (e.g., 192.168.0.x)

Boot Log Errors (Expected)

Symptom

Cause

Action

Failed to read/write scratchpad errors during boot

ADAR1000 SPI accessed before Stingray power sequencing completes

None — this is expected. The kernel driver probes the ADAR1000s before the power-up script has finished enabling all rails. The devices initialize correctly once the sequencing script runs.

Communication and Network Issues

Symptom

Possible Cause

Solution

Cannot ping ZCU102

Wrong IP address

Check actual IP via serial console: ip addr show; update URI in main.py

iio_info shows no devices

FPGA not configured

Verify FPGA bitstream loaded; check DS2 LED

iio_info “Connection refused”

IIO network daemon not running

Check boot log; verify IIO daemon is active

ADAR1000 not detected

SPI daisy-chain not connected

Verify all SPI connections on hardware

USB-UART not working

Driver not installed

Install Silicon Labs CP210x drivers; check Device Manager

IIO attribute access fails

Wrong device path or driver

Run iio_attr -d to list all IIO devices and verify path

RF Connection Issues

Symptom

Possible Cause

Solution

Poor RF performance

Loose SMA connectors

Hand-tight plus 1/4 turn on all RF cables

Phase errors between channels

Unmatched cable lengths

Use matched-length cable sets for all signal paths

High insertion loss

Damaged connectors

Inspect center pins; replace any damaged cables

No LO distribution

MMCX not fully seated

Re-seat all MMCX connections (push until click)

Poor impedance matching

Wrong cable type

Verify 50 Ω cables rated for >10 GHz (X-Band)

Control interfaces not responding

Loose PMOD or FMC connection

Verify all PMOD and FMC connections are fully seated

TDD Timing Issues

Symptom

Possible Cause

Solution

No transitions seen on TR probe point

TDD not enabled or driver not loaded

Run iio_attr -c axi-core-tdd enable; check lsmod | grep tdd

IIO TDD device not found

Kuiper release too old

TDD support requires Kuiper 2026.1.0 or newer; verify with cat /etc/kuiper-release and reflash if needed (see SD Card Configuration)

IIO TDD device not found

Bitstream doesn’t include TDD core

Confirm FPGA bitstream and device tree include the TDD core

Measured timing doesn’t match configuration

Wrong units or unstable clock

Verify system clock frequency; check µs vs. clock-cycle unit settings

TX leakage visible during RX window

Guard time too short

Increase guard time between TX and RX windows

ADC saturates at TX-to-RX transition

Insufficient guard time

Increase guard time; verify TR switch transitions with oscilloscope

JESD204B errors during TX/RX switching

Clock-domain crossing or sync issue

Increase guard times; verify MxFE sample clock alignment with TDD timing

TDD configuration changes have no effect

Parameters only take effect after disable/enable cycle

Disable TDD → update parameters → re-enable

Warning

Always verify TDD timing with an oscilloscope before enabling high-power TX modes. Insufficient guard time can expose the LNA to transmit energy and cause hardware damage.

pyRadar Software Issues

Installation

Issue

Solution

pip not recognized

Add Python to PATH and restart terminal

Package installation fails

Use python -m pip install <package>

Genalyzer install error

Requires Python 3.10.0 — not compatible with 3.11+

Permission denied

Run terminal as administrator (Windows)

Hardware Connection

Symptom

Possible Cause

Solution

Cannot ping ZCU102

Wrong IP address

Check serial console; update uri in main.py

iio_info shows no devices

FPGA not configured

Verify FPGA bitstream loaded; check boot log

Device connection timeout

Network subnet mismatch

Confirm PC and ZCU102 are on the same subnet

Python Environment

Symptom

Possible Cause

Solution

ModuleNotFoundError: adi

Dependencies not installed

Run pip install -r requirements.txt

Genalyzer import fails

Wrong Python version

Verify IDE is using Python 3.10.0 interpreter

Package version conflicts

Multiple Python installations

Use python -m pip to target the 3.10.0 environment explicitly

Import errors after install

Wrong interpreter selected

Verify IDE Python interpreter path

Hardware Initialization

Symptom

Possible Cause

Solution

AD9081 not detected

IIO device not loaded

Run iio_info; reload FPGA if needed

ADAR1000 connection timeout

SPI daisy-chain issue

Verify all SPI connections on hardware

XUD1A initialization fails

Wrong device path

Check device paths in hardware setup configuration

Calibration fails at startup

Corrupted previous config

Delete rx_cal_data.csv and re-run calibration

Calibration

Symptom

Possible Cause

Solution

Phase errors after calibration

Reference element disabled

Verify reference element is enabled; check channel mapping

Amplitude imbalance persists

Incorrect gain settings

Re-run calibration; check ADAR1000 gain settings

Calibration file not found

Wrong working directory

Verify rx_cal_data.csv is in the pyRadar/ directory

High residual errors

RF connection issue

Inspect all SMA/MMCX connections for damage or looseness

Calibration timeout

Hardware not responding

Check all hardware connections; verify device initialization

Radar Pilot Runtime

Symptom

Possible Cause

Solution

No plot window appears

Missing PyQt5 backend

Run pip install PyQt5

Data capture returns zeros

Wrong channel mapping

Verify ADC channel configuration in tx_rx_cal.py

Pilot crashes immediately

Uncaught exception

Run with debug output; check error messages

Keyboard controls don’t work

keyboard library permissions

Run script with administrator privileges

Plot updates very slow

RX buffer size too large

Reduce RX buffer size in hardware setup

Range calculation incorrect

Wrong FMCW parameters

Verify chirp bandwidth and sample rate settings

Performance

Symptom

Possible Cause

Solution

Low frame rate in live plots

CPU overloaded

Close other applications; reduce plot complexity

Memory usage grows over time

Buffer accumulation in loop

Ensure proper buffer cleanup; check for array accumulation

Network latency high

Slow Ethernet connection

Use gigabit Ethernet; verify cable quality

FFT processing slow

Large buffer sizes

Optimize buffer size for your application

Beam steering lag

Slow SPI communication

Minimize SPI I/O operations per processing frame

Additional Support