Quickstart

The Quick Start Guides provide a simple step by step instruction on how to do an initial system setup for the EVAL-AD-FMCOMMS2 / EVAL-AD-FMCOMMS3-EBZ / EVAL-AD-FMCOMMS4-EBZ boards on various FPGA development boards. They will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported carriers

The AD-FMCOMMS2/3/4-EBZ is, by definition a “FPGA mezzanine card” (FMC), that means it needs a carrier to plug into. The carriers we support are:

Board

FMCOMMS2/3/4

KC705 *

FMC LPC

KCU105

FMC LPC

VC707 *

FMC1 HPC

ZC702

FMC1 LPC

ZC706

FMC LPC

ZCU102

FMC HPC0

ZedBoard

FMC LPC

Note

Support for boards marked with an asterisk (*) was discontinued after the hdl_2023_r2 release.

Supported environments

The supported OS are:

Board

HDL

Linux Software

No-OS Software

KC705 *

Yes

Yes

Yes

KCU105

Yes

Yes

Yes

VC707 *

Yes

Yes

Yes

ZC702

Yes

Yes

Yes

ZC706

Yes

Yes

Yes

ZCU102

Yes

Yes

Yes

ZedBoard

Yes

Yes

Yes

Note

Support for boards marked with an asterisk (*) was discontinued after the hdl_2023_r2 release, including in the no-OS repository.

Hardware setup

On most carriers, the AD-FMCOMMS2/3/4-EBZ board connects to the LPC connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.

ZC702 + FMCOMMS2

Early versions of the ZC702 carriers need to work around AR# 51438, PG signal does not assert by default errata.

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/fmcomms2_zc702_linux.jpeg

Go to the setup guide.

ZC706 + FMCOMMS2

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/fmcomms2_zc706_linux.jpeg

Go to the setup guide.

ZED + FMCOMMS2

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/fmcomms2_zed_linux.jpeg

Go to the setup guide.

ZCU102 + FMCOMMS2

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/fmcomms2_zcu102_linux.jpeg

Go to the setup guide.

KCU105 + FMCOMMS2

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/fmcomms2/images/fmcomms2_kcu105_linux.jpeg

Go to the setup guide.