Quick start guides

The Quick start guides provide simple step by step instructions on how to do an initial system setup for the EVAL-AD9081 / EVAL-AD9082 boards on various FPGA development boards. In these guides, we will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported carriers

The EVAL-AD9081 / EVAL-AD9082, is, by definition a “FPGA mezzanine card” (FMC); that means it needs a carrier to plug into.

Note

EVAL-AD9988 can be an alternative to AD9081-FMCA-EBZ and EVAL-AD9986 can be an alternative to AD9082-FMCA-EBZ.

Both AD9081 and AD9988 have MxFE Quad, 16-bit, 12 GSPS RF DAC & Quad, 12-bit, 4 GSPS RF ADC,

The same goes for AD9082 and AD9986, both have MxFE Quad, 16-bit, 12 GSPS RF DAC & Dual, 12-bit, 6 GSPS RF ADC.

The carriers we support are:

FPGA board

EVAL-AD9081

EVAL-AD9082

Arria 10 SoC

FMCA

N/A

Agilex 7 SoC (FM87)

FMCA

N/A

VCK190

FMCP1 (J51)

FMCP1 (J51)

VPK180

FMCP1

FMCP1

VCU118

FMC+

FMC+

ZC706

FMC HPC

FMC HPC

ZCU102

FMC HPC0

FMC HPC0

Supported Environments

The supported OS are:

FPGA board

HDL

Linux software

No-OS software

Arria 10 SoC

Yes

Yes

No

Agilex 7 SoC (FM87)

Yes

Yes

No

VCK190

Yes

Yes

Yes

VPK180

Yes

Yes

Yes

VCU118

Yes

Yes

Yes

ZC706

Yes

Yes

Yes

ZCU102

Yes

Yes

Yes

Hardware setup

On most carriers, the EVAL-AD9081 / EVAL-AD9082 boards connect to the HPC1 connector (unless otherwise noted). The carrier setup requires power, UART (115200), Ethernet (Linux), HDMI (if available) and/or JTAG (no-OS) connections. A few typical setups are shown below.

ZCU102 + EVAL-AD9081

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/eval-ad9081/images/ad9081_zcu102_setup.png

Figure 1 ZCU102 + EVAL-AD9081 setup

VCK190 + EVAL-AD9081

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/eval-ad9081/images/ad9081_vck190_setup.jpg

Figure 2 VCK190 + EVAL-AD9081 setup