User guide
This user guide describes how to set up the ADAR3000/3001-EVALZ evaluation board for the ADAR3000 and ADAR3001, and how it connects to an FPGA carrier. The ADAR3000 and ADAR3001 data sheets provide additional information and should be consulted when using the evaluation board.
Evaluation board hardware
The ADAR3000/3001-EVALZ carries the beamformer, with its RF inputs RFIN1 to RFIN4 and RF outputs RFOUT1 to RFOUT4 on 2.92 mm connectors, as single-ended 50 Ω coplanar waveguides. It is controlled through the 120-pin SDP connector P5. On the bench it is usually driven by an SDP-S controller board and the ACE software; in this reference design an SDP-I-FMC interposer adapts P5 to the FMC connector of the FPGA carrier instead.
Power supply
The evaluation board is supplied from two bench supplies, applied to the test loops on the board:
The expected draw applies after power up and a soft reset, when the amplifiers are enabled with their default bias setting of 3. With the amplifiers disabled, the 1.2 V draw drops to about 1 mA.
The data sheet gives absolute maximum ratings of 1.32 V on V1P2 and 1.98 V on V1P8, so set the over-voltage protection of the supplies below those values.
Hardware configuration
Set the jumpers as follows for control from an FPGA carrier:
Other headers expose signals for monitoring:
Control interface
All control signals reach the device through the SDP connector P5. The logic
level on the SDP side is VIO, which the controller supplies on P5: 3.3 V from
an SDP-S, and the FMC VADJ rail through the SDP-I-FMC interposer. Two
level translators shift VIO to the device’s 1.8 V:
U1 carries the SPI: chip select, clock, MOSI and MISO.
U3 carries the control pins:
RESET_N(RSTB),UPDATE,RESETandMUTE.
Ahead of U1, the 2:1 mux U5 selects the SPI source. With its select input, SDP GPIO3, low it passes the SDP hardware SPI; with it high it passes bit-banged SPI on SDP GPIO0 to GPIO2.
On the ZCU102, the SPI comes from the ZynqMP PS SPI0 controller routed through EMIO, and the control pins from EMIO GPIOs:
The no-OS driver drives the mux select low during initialization. The complete HDL interface is documented in the ADAR3000 HDL project.
FMC VADJ
Through the interposer, VIO is the carrier’s FMC VADJ rail, which must be
at 1.8 V. VADJ also supplies the FPGA I/O banks behind the FMC
connector; at 0 V no pin on that connector can drive, and the SDP side of the
level translators is unpowered.
On the ZCU102, VADJ is not fixed. At power up the board’s system
controller reads the IPMI FRU EEPROM of the card in the FMC slot, per the
VITA 57.1 standard, and sets VADJ from the DC Load record it finds. If no
valid record is present it leaves VADJ at 0 V. With this setup the card in
the FMC slot is the SDP-I-FMC interposer, and it ships with a blank EEPROM.
The symptom is easy to misread: the FPGA configures, the application runs, SPI
initialization succeeds, and every register read returns 0xFF because MISO
floats. The 1.8 V supply of the evaluation board may also draw far more than
expected, around 47 mA instead of 7 mA, as the control lines drive into the
unpowered FPGA I/O bank. If the no-OS example reports a scratchpad mismatch,
check VADJ before suspecting the software or the wiring.
To set VADJ to 1.8 V, either:
program the interposer’s FRU EEPROM with a record requesting 1.8 V, which persists across power cycles. See FMC EEPROM Programming.
or override
VADJwith the ZCU102 system controller user interface, as described in the ZCU102 Evaluation Board User Guide (UG1182). The override does not persist and has to be repeated after every power cycle.
Schematic, PCB Layout, Bill of Materials
The board is the ADAR3000/3001-EVALZ, schematic 02-059137 revision C. Contact Analog Devices for its design files.