Build Zynq Linux kernel and devicetree
Using a script
We provide a script that does automates the build for Zynq using the Linaro toolchain.
The script takes up to 3 parameters, but if left blank, it uses defaults:
<local_kernel_dir> - default is linux-adi if left blank ; use this, if you want to use an already cloned kernel repo
<devicetree_file> - which device tree should be exported/copied from the build. Default is
zynq-zc702-adv7511-ad9361-fmcomms2-3.dtbfor Zynq<path_to_other_toolchain> - in case you have your own preferred toolchain (other than Linaro’s or Xilinx’s) you can use override it with this 3rd param
The script will:
Clone the ADI kernel tree
Download the Linaro GCC toolchain (if no other is specified)
Build the ADI kernel tree
Export/copy the Image file and device tree file out of the kernel build folder
Running the script in one line, with defaults:
~$
wget https://raw.githubusercontent.com/analogdevicesinc/wiki-scripts/main/linux/build_zynq_kernel_image.sh && \
chmod +x build_zynq_kernel_image.sh && \
./build_zynq_kernel_image.sh
Building with Petalinux
Please see here: Build with Petalinux.
On the development host
Make sure you have u-boot-tools installed, to have the mkimage utility
available. You can install it via your distro’s package manager.
Then
~$
git clone https://github.com/analogdevicesinc/linux.git \
--no-single-branch --depth=10 \
-- linux
or do a git pull in a existing cloned repository.
The depth and no-single-branch options are included to speed up the
cloning by fetching only near the head of each branch/release, you may remove
them to fetch all history, but bear in mind it will go from around 800MB to
around 3.4GB and growing.
Checkout the Release branch
Tip
Use the latest release, if not required otherwise!
The release branches have the format <Year>_R[1|2], starting from 2014_R2.
~$
git checkout origin/2026_R1 -b 2026_R1
Branch 2026_R1 set up to track remote branch 2026_R1 from origin.
Switched to a new branch '2026_R1'
Setup cross compile environment variables
There are a few toolchains that can be used. The AMD Xilinx toolchain is recommended, but the Linaro toolchain can also be used.
Other toolchains/compilers for ARM may work as well, but the ones described here have been tested and found to work.
Using the AMD Xilinx toolchain
Release names and Branches |
Required Vivado/Vitis versions |
|---|---|
2014_R2 |
Vivado 2014.2 |
2015_R2 |
Vivado 2015.2 |
2016_R1 |
Vivado 2015.4.2 |
2016_R2 |
Vivado 2016.2 |
2017_R1 |
Vivado 2016.4 |
2018_R1 |
Vivado 2017.4 |
2018_R2 |
Vivado 2018.2 |
2019_R1 |
Vivado 2018.3 |
2019_R2 |
Vivado 2019.1 |
2021_R1 |
Vivado 2021.1 |
2021_R2 |
Vivado 2021.2 |
2022_R2 |
Vivado 2022.2 |
2023_R2 |
Vivado 2023.2 |
2026_R1 |
Vivado 2026.1 |
~$
source $PATH_TO_XILINX/Vitis/$VITIS_VERSION/settings64.sh
~$
which which arm-linux-gnueabihf-gcc
$PATH_TO_XILINX/Vitis/$VITIS_VERSION/gnu/aarch32/lin/gcc-arm-linux-gnueabi/bin/arm-linux-gnueabihf-gcc
Important
Find the path to the AMD Xilinx installation folder, and then use it to replace this string: $PATH_TO_XILINX that is written above. Same goes for the $VITIS_VERSION, where you choose the Vitis version.
~$
export ARCH=arm
~$
export CROSS_COMPILE="arm-linux-gnueabihf-"
Using the Arm GNU Toolchain
Alternatively, the Arm GNU Toolchain can be used to compile the kernel.
Download the arm-none-linux-gnueabihf tarball for your host from the
Arm GNU Toolchain downloads
page. Always use the latest release just in case.
Extract the downloaded tarball and set the environment variables:
~$
export ARCH=arm
~$
export CROSS_COMPILE=$(pwd)/<extracted-toolchain-dir>/bin/arm-none-linux-gnueabihf-
Configure the kernel
Inside the repository, generate the configuration file before building the kernel tree. The command shown below is generic and is not project specific. As long as the board is a ZYNQ FPGA, use the configuration below.
~$
make zynq_xcomm_adv7511_defconfig
#
# configuration written to .config
#
Build the kernel
Build the kernel via ‘make’. This is the same for all AMD Xilinx ZYNQ FPGAs.
~$
make -j5 UIMAGE_LOADADDR=0x8000 uImage
scripts/kconfig/conf --silentoldconfig Kconfig
CHK include/config/kernel.release
CHK include/generated/uapi/linux/version.h
UPD include/config/kernel.release
CHK include/generated/utsrelease.h
[ -- snip --]
AS arch/arm/boot/compressed/bswapsdi2.o
AS arch/arm/boot/compressed/piggy.gzip.o
LD arch/arm/boot/compressed/vmlinux
OBJCOPY arch/arm/boot/zImage
Kernel: arch/arm/boot/zImage is ready
UIMAGE arch/arm/boot/uImage
Image Name: Linux-3.17.0-126697-g611e217-dir
Created: Fri Nov 28 10:20:40 2014
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3195872 Bytes = 3120.97 kB = 3.05 MB
Load Address: 00008000
Entry Point: 00008000
Build the devicetree FCMOMMS2/3/4/5
Build the one that fits your FPGA carrier and FMC card
device tree |
board |
chip |
|---|---|---|
zynq-adrv9361-z7035-bob |
||
zynq-adrv9361-z7035-bob-cmos |
||
zynq-adrv9361-z7035-packrf |
||
zynq-adrv9361-z7035-fmc |
||
zynq-adrv9361-z7035-fmc-rfcard-tdd |
||
zynq-adrv9364-z7020-bob |
||
zynq-adrv9364-z7020-bob-cmos |
||
zynq-adrv9364-z7020-packrf |
||
zynq-coraz7s |
||
zynq-mini-itx-adv7511 |
ADV7511 (on-board)
|
|
zynq-mini-itx-adv7511-ad9361-fmcomms2-3 |
||
zynq-mini-itx-adv7511-ad9364-fmcomms4 |
ADV7511 (on-board) and the
AD-FMCOMMS4-EBZ board
|
|
zynq-zc702-adv7511 |
ADV7511 (on-board)
|
|
zynq-zc702-adv7511-ad9361-fmcomms2-3 |
||
zynq-zc702-adv7511-ad9361-fmcomms5 |
ADV7511 (on-board) and the
|
|
zynq-zc702-adv7511-ad9364-fmcomms4 |
ADV7511 (on-board) and the
AD-FMCOMMS4-EBZ board
|
|
zynq-zc706-adv7511 |
ADV7511 (on-board)
|
|
zynq-zc706-adv7511-ad6676-fmc |
ADV7511 (on-board) and the
EVAL-AD6676 board
|
|
zynq-zc706-adv7511-ad9265-fmc-125ebz |
ADV7511 (on-board) and the
EVAL-AD9265 board
|
|
zynq-zc706-adv7511-ad9361-fmcomms2-3 |
||
zynq-zc706-adv7511-ad9361-fmcomms5 |
ADV7511 (on-board) and the
AD-FMCOMMS5-EBZ board
|
|
zynq-zc706-adv7511-ad9361-fmcomms5-ext-lo-adf5355 |
ADV7511 (on-board) and the
AD-FMCOMMS5-EBZ board
|
|
zynq-zc706-adv7511-ad9364-fmcomms4 |
ADV7511 (on-board) and the
AD-FMCOMMS4-EBZ board
|
|
zynq-zc706-adv7511-ad9434-fmc-500ebz |
ADV7511 (on-board) and the
EVAL-AD9434-FMC board
|
|
zynq-zc706-adv7511-ad9625-fmcadc2 |
ADV7511 (on-board) and the
AD-FMCADC2-EBZ board
|
|
zynq-zc706-adv7511-ad9739a-fmc |
ADV7511 (on-board) and the
|
|
zynq-zc706-adv7511-adrv9371 |
ADV7511 (on-board) and the
Block Diagram board
|
|
zynq-zc706-adv7511-adrv9375 |
ADV7511 (on-board) and the
Block Diagram board
|
|
zynq-zc706-adv7511-fmcadc4 |
ADV7511 (on-board) and the
AD-FMCADC4-EBZ board
|
|
zynq-zc706-adv7511-fmcdaq2 |
ADV7511 (on-board) and the
AD-FMCDAQ2-EBZ Hardware board
|
|
zynq-zc706-adv7511-fmcdaq3 |
ADV7511 (on-board) and the
AD-FMCDAQ3-EBZ board
|
|
zynq-zc706-adv7511-fmcjesdadc1 |
ADV7511 (on-board) and the
AD-FMCJESDADC1-EBZ board
|
|
zynq-zc706-imageon |
FMC-IMAGEON
|
|
zynq-zed-adv7511 |
ADV7511 (on-board) |
|
zynq-zed-adv7511-ad9361-fmcomms2-3 |
||
zynq-zed-adv7511-ad9364-fmcomms4 |
ADV7511 (on-board) and the
AD-FMCOMMS4-EBZ board
|
|
zynq-zed-adv7511-ad9467-fmc-250ebz |
ADV7511 (on-board) and the
EVAL-AD9467-FMC-250EBZ board
|
|
zynq-zed-adv7511-cn0363 |
ADV7511 (on-board) and the
EVAL-CN0363-PMDZ board
|
|
zynq-zed-imageon |
FMC-IMAGEON
|
Building the device tree uses ‘make’ by turning the .dts file to a .dtb. The command is simply ‘make’ plus the device tree name with a .dtb file extension.
~$
make zynq-zc702-adv7511-ad9361.dtb
DTC arch/arm/boot/dts/zynq-zc702-adv7511-ad9361.dtb
Copy the generated files to your SD Card
The output files for building the kernel and device tree are uImage and <device_tree_name>.dtb. Refer to the code below to find their respective output directories. Take note that the device tree file needs to be renamed to devicetree.dtb. See ADI Kuiper Linux for more information in configuring the SD card with Kuiper.
~$
cp arch/arm/boot/uImage /media/BOOT/uImage
~$
cp arch/arm/boot/dts/zynq-zc702-adv7511-ad9361.dtb /media/BOOT/devicetree.dtb
On the target platform (devicetrees)
To modify devicetrees on the target platform:
Make sure the boot partition is mounted. On new images, this can be done by right-clicking the boot icon on the desktop and selecting the “Mount Volume” option. The partition will then be mounted at /media/analog/boot.
Convert the compiled devicetree related to the target back into an editable format.
~$
cd /media/analog/boot/zynq-zc702-adv7511
/media/analog/boot/zynq-zc702-adv7511$
dtc -I dtb -O dts -o devicetree.dts devicetree.dtb
Modify the devicetree.dts file as required.
Recompile the devicetree file. Note that this will overwrite the original dtb file, copy or rename the original file if you want to keep it before running this step.
~$
cd /media/analog/boot/zynq-zc702-adv7511
/media/analog/boot/zynq-zc702-adv7511$
dtc -I dts -O dtb -o devicetree.dtb devicetree.dts