Quickstart

The Quick start guides provide simple step by step instructions on how to do an initial system setup for the AD-FMCDAQ2-EBZ boards on various FPGA development boards. In these guides, we will discuss how to program the bitstream, run a no-OS program or boot a Linux distribution.

Supported carriers

The AD-FMCDAQ2-EBZ is an FMC (FPGA Mezzanine Card), meaning it requires a compatible carrier board. The officially supported carriers are listed below, as documented in the ADI Quick Start Guides.

The carriers we support are listed below, as well as the FMC port where to connect the evaluation board:

FPGA board

EVAL-AD-FMCDAQ2-EBZ

Arria 10 SoC

FMC HPC1

KCU105

FMC HPC

ZC706

FMC HPC

ZCU102

FMC0 HPC0

Supported Environments

The supported OS are:

FPGA board

HDL

Linux software

No-OS software

Arria 10 SoC

Yes

Yes

—

KCU105

Yes

Yes

Yes

ZC706

Yes

Yes

Yes

ZCU102

Yes

Yes

Yes

Hardware Setup

On most carriers, the AD-FMCDAQ2-EBZ board connects to the HPC connector (unless otherwise noted). The carrier setup requires power, UART (115200), ethernet (for Linux), HDMI (if available) and/or JTAG (for no‑OS). A few typical setups are shown below.

A10SOC + AD-FMCDAQ2-EBZ

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/ad-fmcdaq2-ebz/images/ad-fmcdaq2-ebz_a10soc_setup.jpg

KCU105 + AD-FMCDAQ2-EBZ

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/ad-fmcdaq2-ebz/images/ad-fmcdaq2-ebz_kcu105_setup.jpg

ZC706 + AD-FMCDAQ2-EBZ

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/ad-fmcdaq2-ebz/images/ad-fmcdaq2-ebz_zc706_linux.jpg

ZCU102 + AD-FMCDAQ2-EBZ

https://media.githubusercontent.com/media/analogdevicesinc/system-level/main/docs/solutions/reference-designs/ad-fmcdaq2-ebz/images/ad-fmcdaq2-ebz_zcu102_setup_linux.png