Time Division Duplexing (TDD)

The X-Band platform implements Time Division Duplexing (TDD) through a TDD IP Core (axi-core-tdd) that provides hardware integration and firmware control for precise transmit/receive switching in radar applications.

Important

Software requirement: the TDD engine requires ADI Kuiper Linux 2026.1.0 or newer, the first public release that supports axi-core-tdd. On earlier public releases the TDD IIO device does not appear and TX/RX switching cannot be configured. Download the ARM 64-bit Full image from the Kuiper Downloads page, then follow SD Card Configuration.

TDD Components:

  • Hardware Layer: Interposer board with GPIO signal routing and distribution

  • Firmware Layer: TDD core implemented in ZCU102 FPGA programmable logic

  • Software Layer: Linux IIO drivers and Python API for configuration

  • Signal Layer: 6 synchronized control channels distributed to all boards

Key Features:

  • 6-channel programmable frame-based timing structure

  • Precise control of TX/RX windows with microsecond resolution

  • Simultaneous coordination of AD9081, ADXUD1AEBZ, and ADAR1000 boards

  • Flexible sync triggering (soft command or external GPIO)

  • Flexible configuration for various radar modes (pulse, FMCW, etc.)

System Architecture

Hardware Components

The TDD Functional Package integrates the following hardware elements:

ZCU102 Zynq UltraScale+ MPSoC

  • Contains TDD core in programmable logic

  • Generates 6 GPIO control signals (TDD_CH0 to TDD_CH5)

  • Outputs signals via PMOD connector J55 on the Interposer

  • Runs embedded Linux with IIO framework for TDD configuration

  • Provides real-time timing control with FPGA precision

Interposer Board

  • Central hub for TDD signal distribution

  • Routes signals from ZCU102 to multiple destination boards

  • Provides signal buffering and level conversion as needed

  • Includes labeled signal lines: IMU_GPIO0, IMU_GPIO1, IMU_GPIO2

AD9081 MxFE (Mixed-Signal Front End)

  • Receives TX_EN and RX_EN control signals from TDD package

  • Controls transmit and receive data path enables

  • Synchronizes with JESD204B high-speed data interface

  • Provides DAC output during TX and ADC input during RX

ADXUD1AEBZ Up/Down Converter

  • Receives TR switch control signal

  • Switches between transmit and receive IF paths

  • Provides frequency conversion (X-band ↔ IF)

  • Maintains high TX/RX isolation during switching

ADAR1000 Beamformer Array

  • Receives TR switch control signal

  • Controls RF path switching via integrated T/R switches

  • Manages PA (Power Amplifier) and LNA (Low Noise Amplifier) bias

  • Provides fast switching times (sub-microsecond)

GPIO Signal Connections

TDD Channel Summary

The TDD core exposes 6 channels, each mapped to a specific hardware signal:

Channel

Signal Name

Function

Destination

CHAN[0]

TX_OFFLOAD_SYNC

TX sync trigger

AD9081 TX offload

CHAN[1]

RX_OFFLOAD_SYNC

RX capture window

AD9081 RX offload

CHAN[2]

TDD_ENABLE

Master GPO enable

All boards

CHAN[3]

RX_MXFE_EN

MxFE RX path enable

AD9081 RX path

CHAN[4]

TX_MXFE_EN

MxFE TX path + XUD1A sync

AD9081 TX path + Interposer Pin 13

CHAN[5]

TX_STINGRAY_ENABLE

Stingray TX/RX switching

ADAR1000 TR pin

ZCU102 GPIO Mapping

Signal Descriptions

CHAN[0] — TX_OFFLOAD_SYNC

  • Function: Sync start trigger for the TX offload engine

  • Trigger Modes: Soft sync command (software-initiated) or external GPIO trigger

  • Destination: AD9081 TX offload (TDD.CHAN[0])

CHAN[1] — RX_OFFLOAD_SYNC

  • Function: Defines the RX data capture window

  • Parameters: Controlled by on_ms (start), off_ms (end), startup delay, and RX buffer size

  • Startup Delay: Configurable delay from sync trigger before the RX window opens

  • Destination: AD9081 RX offload (TDD.CHAN[1])

CHAN[2] — TDD_ENABLE

  • Function: Master GPO enable bit for the TDD engine

  • Behavior: When set, TDD waveform generation and control logic become active. Must share timing with TX_MXFE_EN (CHAN[4]) and TX_STINGRAY_ENABLE (CHAN[5])

  • Important: Keep this high during all TDD operation. When configuring TDD properties, set high and leave high

  • Default State: Starts low — no data can be received until this is enabled

CHAN[3] — RX_MXFE_EN

  • Function: Intended to enable the RX path of the MxFE during the receive window defined by the TDD schedule

  • Current Status: Not actively used based on testing — does not produce functional output in current firmware

CHAN[4] — TX_MXFE_EN

  • Function: GPIO that controls the TX/RX state of the XUD1A up/down converter board. High = TX enabled, Low = RX enabled

  • Dual Role: Also controls XUD1A sync timing through Pin 13 of the Interposer board

  • Behavior: When high, the TX buffer plays out. When it goes low, any remaining TX buffer content is truncated

  • use_tx_mxfe_en flag:

    • use_tx_mxfe_en = 0: CHAN[4] stays high for the full frame_length_ms duration

    • use_tx_mxfe_en = 1: CHAN[4] pulses high only for tx_time, then returns low — enabling multiple TX bursts per frame

CHAN[5] — TX_STINGRAY_ENABLE

  • Function: GPO output to the Stingray board that enables the TX path on the ADAR1000

  • Behavior: When low and polarity = 0, RX is enabled on the Stingray

  • Timing: Should match CHAN[4] timing (same timing as TX_MXFE_EN for synchronized TX/RX switching)

  • Note: This channel can also be repurposed as a general programmable GPO

Physical Connections

FPGA Pin → FMC → Interposer Mapping

Signal

FPGA Pin

FMC Connector

Interposer Pin

MxFE TX EN

AG3

D11

P3-13

MxFE RX EN

AH3

D12

P3-14

External Sync

AE2

D14

P3-15

ZCU102 PMOD J55 Connector

  • Type: 2×6 pin header (12 pins total, 0.1” pitch)

  • Location: On ZCU102 carrier board

  • Signals Used: Pins 13, 14, 15 (CHAN[0]–[2]), Pin 7 (Ground)

  • Voltage Levels: 3.3V CMOS compatible

  • Cable: Connects to interposer board via ribbon cable

Interposer Board Distribution

  • Input: Receives signals from ZCU102 PMOD J55

  • Buffering: Provides signal conditioning and drive capability

  • Output Routes:

    • IMU_GPIO0 → AD9081 TX offload sync (CHAN[0])

    • IMU_GPIO1 → AD9081 RX offload sync (CHAN[1])

    • IMU_GPIO2 → Master TDD enable (CHAN[2])

    • Pin 13 → XUD1A sync (driven by CHAN[4])

  • Common Ground: Maintains consistent reference across all boards

RX Buffer Operation

Continuous Listening

An important characteristic of the X-Band system is that the RX buffer (ADC) is always listening and continuously sampling the RF environment:

  • Always Active: The ADC hardware continuously converts received RF signals to digital samples

  • No Timing Required: The receiver does not need to be timed to “catch” returning TX echoes as the TX and RX buffers begin in sync.

  • Continuous Sampling: ADC samples are generated continuously, regardless of TDD state

  • Data Capture Window: The RX_EN signal (TDD_CH1) only controls which samples are captured and processed

RX_EN Function Clarification

The RX_EN signal does NOT control when the hardware listens. Instead, it controls:

  1. Data Capture Gating: Which ADC samples are saved/buffered for processing

  2. JESD204B Streaming: When data is actively streamed to the processor

  3. Processing Window: Which samples are passed to signal processing algorithms

  4. Memory Management: Prevents buffer overflow by limiting captured data

Practical Implications

For Pulsed Radar (Continuous TX, Buffered Capture):

  • TDD generates TX pulses infinitely (frames repeat continuously)

  • ADC continuously runs and samples all frames

  • RX buffer size determines how many pulses are captured

  • Example: Frame length = 1 ms, buffer size = 100 ms → captures 100 TX pulses

  • After buffer fills, processing analyzes the captured pulses for coherent integration

  • RX_EN can be HIGH continuously to capture all data, or windowed per frame

For FMCW Radar:

  • TDD frames repeat continuously (continuous chirping)

  • ADC continuously samples the mixed TX/RX signal

  • RX_EN typically stays HIGH continuously

  • Frame length typically matches chirp duration

  • Buffer size determines how many chirps are captured for processing

Buffer Size and Frame Relationship:

  • TDD frames transmit infinitely once enabled

  • RX buffer acts as a “snapshot” capturing N frames worth of data

  • Number of pulses captured = (Buffer Size) / (Frame Length)

  • Once buffer is full, data is processed and buffer can be restarted

  • This allows continuous radar operation with periodic signal processing

Advantages:

  • Simplifies timing constraints

  • Reduces risk of missing target returns due to timing errors

  • Allows flexibility in defining capture windows

TDD Frame Structure

Frame-Based Operation

The TDD core operates using a frame-based timing model. Each frame represents one TX cycle (pulse) and repeats infinitely.

How TDD and RX Buffer Interact:

  • TDD Operation: Once enabled, TDD frames repeat continuously, generating TX pulses indefinitely

  • RX Buffer Capture: The RX buffer size is set to be a multiple of the frame length

  • Pulse Count: Number of captured pulses = (RX Buffer Size) / (Frame Length)

  • Example: If frame length = 1 ms and RX buffer = 100 ms, you capture 100 TX pulses

TDD Frame Structure and Buffer Capture

Understanding the Frame Structure Diagram

The diagram above illustrates the key concepts of TDD frame-based operation.

Operation:

  • Continuous Operation: Once TDD is enabled, frames repeat indefinitely (Frame 1, Frame 2, Frame 3… Frame N)

  • Each Frame Identical: Every frame has the same structure with one TX pulse and one RX capture window

  • Buffer Determines Capture: The RX buffer spans multiple frames, capturing data from N consecutive frames

  • Pulse Count: The number of TX pulses captured equals Buffer Size ÷ Frame Length

Note

Key Insight: The TDD system repeats frames continuously once TDD_ENABLE (CHAN[2]) is asserted. You control how many pulses are captured by setting the RX buffer size. If your frame is 1 ms, TX pulse is 0.5 ms, and you want 100 pulses, set your RX buffer to 100 ms.

Timing Parameters

The TDD frame structure is defined by programmable timing parameters:

Frame Length

  • Definition: Total duration of one complete TDD cycle

  • Typical Range: 1 µs to several milliseconds

  • Units: Can be specified in time units or clock cycles

  • Considerations: Must accommodate TX pulse, guard times, and RX window

Channel ON/OFF Times

  • Definition: Start and stop times for each TDD channel within the frame

  • Resolution: Sub-microsecond precision

  • Configuration: Each channel (CH0, CH1, CH2) independently programmable

  • Reference: All times relative to frame start (t=0)

RX Buffer Size

  • TDD Behavior: TDD frames repeat infinitely once enabled (continuous TX pulsing)

  • Capture Control: The RX buffer size determines how many pulses are captured

  • Calculation: Number of Captured Pulses = (RX Buffer Size) / (Frame Length)

  • Example: Frame length = 1 ms, RX buffer = 128 ms → captures 128 TX pulses

Secondary Times

  • Definition: Optional additional ON periods within the same frame

  • Usage: Enables multi-pulse modes or complex waveform generation

  • Configuration: Secondary ON/OFF times can be set for each channel

Example Timing Configuration

For a simple pulsed radar with 10 µs TX pulse per frame:

Frame Length: 20 µs

TDD_CH0 (TX Enable):
  - ON time:  0 µs
  - OFF time: 10 µs
  - Duration: 10 µs TX pulse (repeats every frame)

TDD_CH1 (RX Enable):
  - ON time:  0 µs
  - OFF time: 20 µs
  - Duration: 20 µs capture window per frame

TDD_CH2 (TR Switch):
  - ON time:  0 µs (TX mode)
  - OFF time: 10 µs
  - Switches to RX ahead of data enables

RX Buffer Size: 100 µs
Result: TDD pulses for 10 µs every 20 µs period
        RX buffer captures 5 TX pulses (100 µs / 20 µs per frame)
        After buffer fills, you have 5 pulses for coherent processing

TDD Configuration Methods

Software Interface

The TDD core is controlled through the Linux IIO (Industrial I/O) framework:

IIO Device

  • Device Name: axi-core-tdd

  • Type: IIO trigger device

  • Driver: Analog Devices TDD core driver

  • Location: /sys/bus/iio/devices/iio:deviceX/

Configuration Attributes

  • Frame Length: Sets total frame duration

  • Channel ON/OFF Times: Configures timing for each of the 3 channels

  • Enable: Starts/stops TDD operation

  • Secondary Timing: Optional additional pulse periods

ADAR1000 Beamformer Switching

TR Switch Control (CHAN[5] → TX_STINGRAY_ENABLE → TR Pin)

  • Function: Controls integrated T/R switches in each ADAR1000

  • TX Mode (HIGH):

    • RF switches route signal to PA (Power Amplifier) path

    • PA bias enabled for transmit amplification

    • LNA (Low Noise Amplifier) disabled/protected

  • RX Mode (LOW, polarity=0):

    • RF switches route signal to LNA path

    • LNA bias enabled for low-noise amplification

    • PA disabled to save power and reduce noise

  • Switching Time: Sub-microsecond transition

  • Isolation: High TX/RX isolation protects receiver

ADXUD1AEBZ Up/Down Converter Switching

TX/RX Control (CHAN[4] → TX_MXFE_EN → Interposer Pin 13)

  • Function: Switches IF signal paths between TX and RX on the XUD1A

  • TX Mode (HIGH):

    • IF input from MxFE DAC routed to upconverter

    • Upconverter generates X-band TX signal

    • RX path disabled/isolated

  • RX Mode (LOW):

    • X-band RX signal routed to downconverter

    • Downconverter generates IF output to MxFE ADC

    • TX path disabled/isolated

  • Isolation: Maintains high TX/RX isolation for dynamic range

Monitoring and Verification

Signal Probe Points

Two key TDD signals are accessible for oscilloscope verification:

Signal

Board

Probe Location

TX_MXFE_EN (CHAN[4])

Interposer

P3-13

TX_STINGRAY_ENABLE (CHAN[5])

Stingray

TR pin

Oscilloscope Verification

Recommended Measurements

  1. TX_MXFE_EN: Probe P3-13 on the Interposer to verify XUD1A TX/RX switching timing

  2. TX_STINGRAY_ENABLE: Probe the TR pin on the Stingray to verify ADAR1000 TX/RX switching

  3. Guard Times: Measure actual delays between transitions

  4. Frame Period: Verify frame repetition rate

  5. Rise/Fall Times: Check signal quality and edge rates

Performance Considerations

Timing Resolution and Accuracy

Clock-Based Timing

  • Reference: All TDD timing derived from FPGA system clock

  • Typical Clock: 250 MHz system clock

  • Resolution: 4 ns per clock cycle

  • Accuracy: Depends on clock stability and jitter

  • Drift: Minimal drift with quality clock source

Configuration Units

  • Time Units: Microseconds (µs) or milliseconds (ms) for user interface

  • Internal Units: Clock cycles for FPGA implementation

  • Precision: Sub-microsecond precision available

Switching Performance

System Settling Times

  • RF Switches: ADAR1000 switches in < 1 µs

  • IF Switches: ADXUD1A converter switching < 2 µs

  • Amplifier Bias: PA/LNA bias settling 5-20 µs

  • Total TX→RX: Recommend 20-50 µs guard time minimum

  • Total RX→TX: Recommend 10-30 µs guard time minimum

Isolation Performance

  • TX/RX Isolation: Critical for receiver dynamic range

  • Switch Isolation: ADAR1000 provides >40 dB typical

  • Converter Isolation: ADXUD1A provides >35 dB typical

  • System Isolation: Combined isolation typically >30 dB

  • Leakage Impact: Insufficient isolation degrades sensitivity

Radar Performance Implications

Minimum Range

  • Limitation: TX-to-RX guard time sets minimum detectable range

  • Calculation: Min Range = (Guard Time × Speed of Light) / 2

  • Example: 30 µs guard time → ~4.5 km minimum range

  • Mitigation: Reduce guard time if system allows faster settling

Maximum PRF (Pulse Repetition Frequency)

  • Limitation: Frame length sets maximum PRF

  • Calculation: Max PRF = 1 / Frame Length

  • Example: 1 ms frame → 1 kHz PRF

  • Consideration: Must include TX pulse + guard + RX window + margin

Duty Cycle

  • Definition: Fraction of time spent transmitting

  • Calculation: Duty Cycle = TX Duration / Frame Length

  • Example: 100 µs TX / 1 ms frame = 10% duty cycle

  • Impact: Affects average transmit power and thermal management

Range-Doppler Ambiguity

  • Unambiguous Range: c / (2 × PRF)

  • Unambiguous Velocity: λ / (4 × Frame Length)

  • Trade-off: Frame length affects both range and velocity ambiguity

  • Resolution: Choice depends on application requirements