Unboxing and Initial Setup
This section provides step-by-step instructions for unboxing, assembling, and performing initial setup of the X-Band Phased Array Development Platform.
Quick Start Guide
For complete setup of your X-Band platform, follow these guides in order:
Hardware Assembly - Assemble all boards and make connections
ZCU102 Configuration - Configure boot mode, USB, and network settings
SD Card Configuration - Format, flash, and prepare the boot media
EEPROM Programming - Program the FMC EEPROM for proper VADJ power
Tip
First Time Setup: Follow the guides above in sequence. Each step builds on the previous one.
What’s Included
The X-Band Phased Array Development Platform includes:
In the Box:
1x AD9081-FMCA-EBZ - AD9081 MxFE Evaluation Board
1x ADXUD1AEBZ - X/C Band Up/Down Converter
1x ADAR1000EVAL1Z - X/Ku-Band Analog Beamforming Board (Stingray)
Power adapters for ADXUD1AEBZ and ADAR1000EVAL1Z (12V)
Interconnect cables and adapters
Documentation and quick start guides
Required (Not Included):
Xilinx ZCU102 Evaluation Board - Required for FPGA processing
Host computer for development and control
Additional RF test equipment (signal generators, spectrum analyzers, etc.)
Power Requirements
ADAR1000EVAL1Z (Stingray)
12V DC power adapter
On-board power regulation provides all required voltages
ADXUD1AEBZ
12V DC power adapter
On-board power regulation provides all required voltages
AD9081-FMCA-EBZ
Powered via FMC connector from ZCU102 board
No external power required
ZCU102 must provide adequate power via FMC
Configuration Overview
The X-Band platform requires several configuration steps before first use. Each topic has a dedicated guide:
SD Card Setup
Prepare the SD card with ADI Kuiper Linux operating system. The X-Band platform requires release 2026.1.0 or newer (ARM 64-bit Full), available from the Kuiper Downloads page — it is the first public release that supports the TDD engine.
Steps Include:
Format SD card properly
Flash Kuiper Linux image
Copy boot files (BOOT.BIN, Image, system.dtb)
Verify boot operation
📖 See: SD Card Configuration
ZCU102 Hardware Configuration
Configure switches and jumpers on the ZCU102 board for proper operation.
Key Settings:
Boot mode switches (SW6) for SD card boot
USB host mode jumpers for peripherals
UART connection for console access
Network configuration for remote access
📖 See: ZCU102 Configuration
EEPROM Programming
Program the FMC EEPROM on the ADXUD1AEBZ interposer board.
Required For:
Proper 1.8V VADJ power to AD9081
FMC board identification
System initialization
📖 See: EEPROM Programming
Configuration Quick Reference
Essential Settings Summary
Component |
Configuration |
Guide |
|---|---|---|
ZCU102 Boot Mode |
SW6: ON-OFF-OFF-OFF |
|
USB Host Mode |
J7, J109-113 configured |
|
SD Card |
Kuiper Linux 2026.1.0+ (ARM 64-bit Full) + boot files |
|
FMC EEPROM |
Programmed for VADJ |
|
UART Console |
115200 baud, 8N1 |
Initial Power-On
Power-On Sequence:
First: Power on ADAR1000EVAL1Z (12V adapter)
Second: Power on ADXUD1AEBZ (12V adapter)
Third: Power on ZCU102 (which powers AD9081-FMCA-EBZ)
Fourth: Boot ZCU102 with reference design
Verification Steps:
Check that all power LEDs are illuminated
Verify ZCU102 boots properly with FPGA design loaded
Test basic communication with each board
Run initial system verification tests
Safety Considerations
Warning
Always power down all equipment before making connections
Use proper ESD protection when handling boards
Verify power supply voltages before connecting
Do not exceed maximum RF input levels
Caution
The X-Band platform operates at high frequencies
Ensure proper RF shielding and safety practices
Be aware of local regulations for X-Band emissions
Note
For additional setup support, please refer to the individual evaluation board quick start guides linked in the Resources section.