EEPROM Programming

This guide covers programming the FMC EEPROM on the ADXUD1AEBZ interposer board, which is required for proper system operation.

Overview

The ADXUD1AEBZ interposer board contains an FMC (FPGA Mezzanine Card) EEPROM that stores critical configuration information. This EEPROM is not factory programmed and must be programmed before the system can operate correctly.

Why EEPROM Programming is Required

The FMC EEPROM contains:

  • Board identification information

  • VADJ voltage requirements (1.8V for AD9081)

  • Power-on sequence parameters

  • FMC connector configuration

Important

Without proper EEPROM programming, the ZCU102 will not provide 1.8V VADJ power to the AD9081-FMCA-EBZ board, preventing it from powering on correctly.

Prerequisites

Before programming the EEPROM, ensure:

  1. System is assembled with all boards connected:

    • ZCU102 powered and booted

    • AD9081-FMCA-EBZ connected via FMC

    • ADXUD1AEBZ interposer installed

  2. Network or UART connection to ZCU102

  3. Root access to the Linux system

  4. FRU tools installed — included in the Kuiper Linux Full edition (the Basic edition does not ship them; see SD Card Configuration)

EEPROM Programming Procedure

Step 1: Access the System

Connect to your ZCU102 via:

Option A: UART Console

  • Baud rate: 115200, 8N1

  • Connect USB cable to J83 on ZCU102

Option B: SSH

ssh root@<zcu102_ip_address>

Default credentials:

  • Username: root

  • Password: analog

Step 2: Locate EEPROM Devices

First, verify the EEPROM device is detected:

root@analog:~# find /sys -name eeprom

Expected output should include:

/sys/bus/i2c/devices/15-0050/eeprom
/sys/bus/i2c/devices/15-0051/eeprom

Note

The exact I2C bus number (e.g., 15-0050) may vary depending on your system configuration. Use the address that corresponds to the ADXUD1AEBZ FMC connector.

Step 3: Program the FMC EEPROM

Program the EEPROM with the FMC FRU (Field Replaceable Unit) data:

root@analog:~# fru-dump -i /usr/local/src/fru_tools/masterfiles/AD-FMCOMMS2-EBZ-FRU.bin -o /sys/bus/i2c/devices/15-0050/eeprom

Note

Why AD-FMCOMMS2-EBZ FRU? While the ADXUD1AEBZ interposer is a different board, we use the AD-FMCOMMS2-EBZ FRU binary because it encodes the critical 1.8V VADJ voltage requirement needed by the AD9081-FMCA-EBZ. The board product name will show as “AD-FMCOMMS2-EBZ” in the readback output—this is intentional and correct.

Command breakdown:

  • fru-dump: FRU programming utility

  • -i: Input FRU binary file

  • -o: Output target (EEPROM device)

Expected output:

Writing FRU data to /sys/bus/i2c/devices/15-0050/eeprom...
Success: 256 bytes written

Warning

Verify the I2C device path (e.g., 15-0050) matches your system. Using the wrong path may program the incorrect EEPROM or fail entirely.

Step 4: Verify EEPROM Programming

Read back the programmed EEPROM to verify:

root@analog:~# fru-dump -i /sys/bus/i2c/devices/15-0050/eeprom -b

Expected output should display:

Board Manufacturer: Analog Devices
Board Product Name: AD-FMCOMMS2-EBZ
Board Serial Number: <serial>
Board Part Number: <part_number>
FRU File ID: AD-FMCOMMS2-EBZ

Tip

If the readback shows valid FRU data matching the expected board information, programming was successful.

Step 5: Power Cycle the System

After programming, a complete power cycle is required:

root@analog:~# poweroff

After shutdown:

  1. Disconnect all power from the system

  2. Wait 10 seconds for complete discharge

  3. Reconnect power and boot the system

  4. Verify 1.8V VADJ is present (see verification section below)

Important

A reboot is not sufficient - you must perform a complete power cycle (power off, wait, power on) for the VADJ changes to take effect.

Verification

Check VADJ Power Rail

After power cycling, verify 1.8V VADJ is present:

Option A: Measure with Multimeter

  • Locate VADJ test point on AD9081-FMCA-EBZ

  • Measure voltage: should read 1.8V ± 0.1V

Option B: Check IIO Devices

root@analog:~# iio_attr -d

If VADJ is correct, you should see the AD9081 device (typically axi-ad9081-rx-hpc).

Option C: Check System Logs

root@analog:~# dmesg | grep -i vadj

Look for messages indicating 1.8V VADJ configuration.

Verify FMC Detection

Check that the FMC board is properly detected:

root@analog:~# cat /sys/bus/i2c/devices/15-0050/eeprom | hexdump -C | head -20

The output should show valid FRU data (not all 0x00 or 0xFF).

Additional Resources