Skip to content

Workspace Tasks

This section outlines the core tasks users can perform within the Workspace to manage projects and models effectively. Whether you're starting a new project or continuing to work on an existing one, the workspace provides tools to streamline your workflow.

Adding new items

To begin adding content to the Workspace, click the New button. This opens options for creating a new project or uploading a model.

Adding New Items

Note

This Empty State view is only shown on first use of the application.

If the Workspace already contains projects and models, use the Upload Project and Upload Model buttons located in the upper‑right corner of the application window.

Upload Project Button

Upload Model Button

Adding a new project

The Create Project feature allows users to initialize a new workspace for model development and evaluation.

Adding New Project

To start a project from scratch:

  1. Within the Workspace, click on the New Project button to begin. This action will open the Create Project window.
  2. Enter the desired Project Name in the input field.
  3. Select the appropriate Task and Task Type from the dropdown list.
  4. Choose a Model Source using one of the following options:


Option 1: Select a Model from the Library

Select from Library

  1. Choose Select from Library.
  2. The center pane will display available models organized into three categories:

    a. ADI Model Zoo – Curated models provided by ADI.

    b. My Models – Models previously uploaded by the user. By default, this section is empty if you haven't uploaded any custom models.

    c. All – Combined view of ADI and user-uploaded models.

  3. Browse the list and select a model to use in your project.


Option 2: Upload Your Own Model

Upload Own Model

  1. Choose Upload a Model.
  2. Enter the Model Name in the input field.
  3. Upload the model file:

    a. Drag and drop the file into the designated area, or

    b. Click Browse to select the file manually.

  4. After you upload the model, the system automatically detects the framework used and displays it.

  5. Review all entered information to ensure accuracy. Click the Import Project to save your project to the Workspace.

Additional Controls

  • Cancel button

    Clicking the Cancel button redirects the user back to the Workspace without creating the project.

  • Close button

    Clicking the Close (X) icon in the top-right corner closes the window without creating a project.


Uploading a project

The Upload Project feature allows users to upload a previously created and exported project.

After you create a project, the Export Project option becomes available. The exported project file can later be uploaded using the Upload Project option.

To import a project from a local computer:

  1. Click Upload Project to import an existing project from your computer.
  2. Enter a descriptive Project Name for the project.

    Project Name

  3. Drag and drop the project file into the designated area or click Browse to select the file manually.

    Upload Window

    File Requirements

    • Supported format: ZIP and TAR.GZ
    • Maximum file size: 100 MB

    After selecting a file, a progress bar will indicate upload status. During and after upload, the following buttons are available for managing the selected file:

    • Cancel Upload: Stops file upload midway and discards the selected file.
    • Replace File: Discards upload of the currently selected file and allows choosing of another project file from PC.

  4. Click Import Project to confirm project file upload.


Uploading a model (BYOM)

The Bring Your Own Model (BYOM) feature allows users to upload and deploy their own trained AI models to the EdgeBench platform. This is ideal for users who want to integrate custom architectures or domain-specific models that are not available in the ADI Model Zoo. BYOM supports flexible deployment on supported hardware, enabling tailored AI solutions.

Why Use BYOM?
BYOM empowers developers to leverage their own models for specialized tasks, ensuring compatibility with unique data and workflows. This feature also allows users to validate whether their models can be successfully compiled and deployed on target ADI hardware platforms.

Step 1: Prepare Your Model
Refer to the BYOM Models for EdgeBench for instructions on how to prepare and package your custom model.

Step 2: Upload Your Model
Once your model package (ZIP, TAR) is prepared, you can upload it via Workspace.

  1. Navigate to Workspace → Models.
  2. Click Upload Model.
  3. Fill in the required model details:

    a. Model Name: A descriptive name for your model.

    b. Task Type: Select the appropriate task type.

    c. Task: Choose appropriate task from the Task dropdown

    Model Details

  4. Upload your model file:

    a. Drag and drop the archive into the upload area or click Browse to select it manually.

    Upload File

  5. After you upload the model file, the system automatically identifies the Framework. No need to select this manually.

  6. Monitor the upload progress via the progress bar.

    Upload Controls

    • Cancel Upload: Stops the upload and discards the selected file.
    • Replace File: Allows you to discard the current file and select a new one.
  7. Click Add New Model to complete the upload.