Data Processing
The Bring Your Own Model (BYOM) feature requires data processing scripts to ensure that model inputs and outputs are compatible with the model architecture and the target task.
Data processing consists of two script types:
- Pre-processing scripts transform raw input files (for example,
.JPG,.PNG,.WAV) into the input shape and data format expected by the model. - Post-processing scripts transform raw model outputs into human‑readable and task‑appropriate results for presentation and analysis.
This guide provides guidelines on creating custom data processing scripts, which are mandatory for all BYOM workflows.
Script Editor Environment
The script editor operates within a Jupyter-like Python environment, these three imports are mandatory for data processing script files:
- argparse
- numpy
- pathlib
These are the only supported libraries in the runtime environment:
- torch (2.1.2+cpu)
- torchvision (0.16.2+cpu)
- tensorflow-cpu (2.15.0)
- requests (2.32.5)
- pyyaml (6.0.3)
- pandas (2.3.3)
- scipy (1.15.3)
- matplotlib (3.10.8)
- opencv-python (4.11.0.86)
- librosa (0.9.1)
Develop your script outside EdgeBench before uploading it for validation. This environment allows users to test custom post-processing logic directly within the platform.
Creating a Pre-processing Script
When entering the pre‑processing step, the script editor displays a template similar to the following:
import argparse # Standard library for parsing command-line arguments
from pathlib import Path # Cross-platform, safer file path handling
import numpy as np # NumPy for numerical operations and .npy files
# These three imports are mandatory for all postprocessing script files
def preprocess(file_path: str, quant_type: str) -> np.ndarray:
"""
Main preprocess function which applies the preprocessing logic
on the input files
This function should:
1. Load the raw input data from file path
2. Apply domain-specific preprocessing
3. Return a NumPy array ready to send to model for inference
Parameters
----------
1. file_path : str
Absolute Path to the input file.
This may be an audio file, image, or time-series file.
Example: "data/sample.wav" or "images/input.jpg"
2. quant_type: str
Quantization type to use while processing the input files
Example: "int8"
Returns
-------
np.ndarray
Preprocessed data formatted to pass to model for inference.
Notes
-----
Implement task-specific preprocessing logic here, such as:
- Audio: loading waveform, resampling, Mel spectrograms
- Vision: resizing, normalization, channel reordering
- Time series: windowing, smoothing, feature extraction
"""
# TODO: Load file and implement real preprocessing logic
# Example:
# data = load_audio(file_path)
# features = compute_mel_spectrogram(data)
# return features
return # Placeholder return
if __name__ == "__main__":
"""
Script entry point.
Example command-line usage:
---------------------------
python preprocess.py \
--source data/input.wav \
--output_file_path outputs/preprocessed.npy \
--quant_type float32
"""
# Create an argument parser that defines expected CLI inputs
parser = argparse.ArgumentParser(
description="Preprocess an input file and save the result as a NumPy (.npy) array"
)
# Required argument: path to the raw input file
parser.add_argument(
"--source",
required=True,
help=(
"Absolute Path to the input file to be preprocessed."
)
)
# Required argument: output .npy file path (including filename)
parser.add_argument(
"--output_file_path",
required=True,
help=(
"Absolute Path where the preprocessed .npy file will be saved"
)
)
# Required argument: quantization type
parser.add_argument(
"--quant_type",
required=True,
help=(
"Quantization type: int8, int16, float32"
)
)
# Parse command-line arguments into a namespace object
args = parser.parse_args()
# Extract parsed arguments
source_path = args.source
output_file_path = Path(args.output_file_path)
quant_type = args.quant_type
# Run preprocessing on the input file
x = preprocess(source_path, quant_type)
# Save the resulting NumPy array to disk
np.save(output_file_path, x)
# Print helpful confirmation messages
print(f"Processed data shape: {x.shape}")
print(f"Saved preprocessed data to: {output_file_path}")
The core of this template is the preprocess() function, which accepts the following parameters:
- file_path: str - Absolute path to the input file. Supported inputs include image, audio, and time‑series files. An example is
"images/input.jpg". - quant_type: str - Quantization type applied to the processed data. An example is
"int8".
The pre‑processing script must output a NumPy array and write it to a .NPY file for inference.
Pre-processing scripts typically perform the following steps:
- Load raw data from the input file
- Extract task‑specific features
- Transform data to match the model’s input shape
- Apply quantization (if required)
The following discussion uses an image classification pre‑processing script as an example.
Loading Raw Data
Load the raw data from the file_path argument using commonly supported libraries:
- Images (
.PNG,.JPG):PIL.Image.open(file_path) - Audio (
.WAV,.MP3):librosa.load(file_path) - Time series (
.CSV):pandas.read_csv(file_path)
Example for loading an image:
from PIL import Image
p = Path(file_path)
if not p.exists():
raise FileNotFoundError(f"Input file not found: {file_path}")
img = Image.open(p)
Feature Extraction
Extract the desired features from the raw data. Implementation here depends on the task and model training pipeline.
Common operations include:
- For image tasks, resizing, normalization, channel reordering
- For audio tasks, resampling, conversion to mel spectrograms
- For time-series tasks, windowing, smoothing, feature extraction
Example for image classification:
import numpy as np
img = img.convert('L')
img = img.resize((28, 28), Image.BILINEAR)
arr = np.asarray(img).astype(np.float32) / 255.0
Transforming the Data
Processed data must match the exact input shape expected by the model.
Example for an image classification model expecting (1, 1, 28, 28) input shape:
arr = arr[np.newaxis, np.newaxis, :, :]
Quantizing Inputs
If required, quantize data based on quant_type parameter:
q = quant_type.lower()
if q == 'float32':
return arr.astype(np.float32)
elif q == 'int8':
# Map float [-1,1] -> int8 range [-127,127]
out = np.round(arr * 127.0).astype(np.int8)
return out
elif q == 'int16':
# Map float [-1,1] -> int16 range [-32767,32767]
out = np.round(arr * 32767.0).astype(np.int16)
return out
else:
raise ValueError(f"Unsupported quant_type: {quant_type}. Use float32, int8 or int16.")
Validating the Pre-processing Script
To validate your pre-processing script on EdgeBench, go to Adding a Pre-processing Script.
Creating a Post-processing Script
When entering the post-processing step, the script editor displays a template similar to the following:
import argparse # Standard library for parsing command-line arguments
from pathlib import Path # Safer, cross-platform path handling
import numpy as np # Numerical operations and .npy file handling
# These three imports are mandatory for all postprocessing script files
def postprocess(file_path: str,quant_type: str) -> np.ndarray:
"""
Main postprocess function which applies the postprocessing logic
on the model output
This function is expected to:
1. Load a NumPy (.npy) file from path
2. Apply any task-specific transformations
3. Return a NumPy array ready to be passed in the pipeline
Parameters
----------
1. file_path : str
Absolute Path to the input .npy file containing raw model outputs.
Example: "outputs/raw_output.npy"
2. quant_type: str
Quantization type to use while processing the model outputs
Example: "int8"
Returns
-------
np.ndarray
The postprocessed NumPy array.
Notes
-----
Replace the placeholder logic below with real postprocessing steps,
such as:
- Normalization or scaling
- Casting to a specific dtype (e.g., int8, int16, float32)
- Reshaping or filtering values
- Converting logits to probabilities
"""
# TODO: Load file and apply real postprocessing logic
# Example:
# data = np.load(file_path)
# processed = data / np.max(data)
# return processed
return # Placeholder return
if __name__ == "__main__":
"""
Entry point when running this file as a script.
Example command-line usage:
---------------------------
python postprocess.py \
--source outputs/raw_output.npy \
--output_file_path outputs/final_output.npy \
--quant_type float32
"""
# Create the argument parser object
# This defines which command-line arguments the script accepts
parser = argparse.ArgumentParser(
description="Postprocess model outputs and save them as a NumPy (.npy) file"
)
# Required argument: input model output file
parser.add_argument(
"--source",
required=True,
help=(
"Absolute Path to the input .npy file containing raw model outputs."
)
)
# Required argument: output file path (including filename)
parser.add_argument(
"--output_file_path",
required=True,
help=(
"Absolute Path where the postprocessed .npy file will be saved."
)
)
# Required argument: quantization type
parser.add_argument(
"--quant_type",
required=True,
help=(
"Quantization type: int8, int16, float32"
)
)
# Parse arguments provided via the command line
args = parser.parse_args()
# Extract argument values
source_path = args.source
output_file_path = Path(args.output_file_path)
quant_type = args.quant_type
# Run postprocessing on the input file
result = postprocess(source_path, quant_type)
# Print array shape for debugging or validation
print(f"Shape of postprocessed data: {result.shape}")
# Save the final NumPy array to disk
np.save(output_file_path, result)
print(f"Saved postprocessed data to: {output_file_path}")
The core of this template is the postprocess() function, which accepts the following parameters:
- file_path: str - Absolute path to the raw output file. An example is
"outputs/raw_output.npy". - quant_type: str - Quantization type applied to dequantize the data. An example is
"int8".
The post‑processing script must output a NumPy array and write it to a .NPY file for UI presentation.
Pre-processing typically performs the following steps:
- Loading raw model outputs
- Dequantizing values (if applicable)
- Transforming results for task-specific presentation
The following discussion uses an image classification post‑processing script as an example.
Loading Model Outputs
Load the raw model output data from inference using np.load.
import numpy as np
p = Path(file_path)
if not p.exists():
raise FileNotFoundError(f"Model output file not found: {file_path}")
# Load raw model outputs
data = np.load(p)
Dequantizing Outputs
If applicable, dequantize data as shown below:
q = quant_type.lower()
if q == 'float32':
outputs = data.astype(np.float32)
elif q == 'int8':
# int8 was encoded as round(float * 127)
outputs = data.astype(np.float32) / 127.0
elif q == 'int16':
# int16 was encoded as round(float * 32767)
outputs = data.astype(np.float32) / 32767.0
else:
raise ValueError(f"Unsupported quant_type: {quant_type}. Use float32, int8 or int16.")
Transforming Outputs for Display
The post-processing logic to prepare output data for UI display vary by task. The table below shows the expected post-processing output for each task:
| Domain | Task | Expected Output | Structure |
|---|---|---|---|
| Vision | Classification | Probabilities mapped to the model’s labels | np.array([prob_1, prob_2, prob_3])Shape: (1, n), n being the number of classes |
| Vision | Image Segmentation | Two image masks (such as, one for background, one for subject) | np.array([[[val_1, val_2, ...], [val_1, val_2, ...], ...], [[val_1, val_2, ...], [val_1, val_2, ...], ...]])Shape: 2, H, W, corresponds to 2 masks of input image with height H and width W |
| Vision | Object Detection | Array of dictionaries for each detected object specifying bounding box, label, and confidence score | np.array([{"box": box, "label": label, "score": score}])Shape: (n, 1), n being the number of objects detectedBounding box format: (x_ref, x_length, y_ref, y_length) |
| Vision | Visual Wake Word | Probabilities mapped to the model’s labels | np.array([prob_1, prob_2, prob_3])Shape: (1, 2), corresponding to detected or not detected |
| Audio | Denoising | Audio data in NumPy format | np.array([data_1, data_2, data_3...])Shape: (n,), n being the number of audio samples |
| Audio | Genre Identification | Probabilities mapped to the model’s labels | np.array([prob_1, prob_2, prob_3])Shape: (1, n), n being the number of genres |
| Audio | Keyword Spotting | Probabilities mapped to the model’s labels | np.array([prob_1, prob_2, prob_3])Shape: (1, n), n being the number of keywords |
| Time Series | Motor Fault Detection | Time‑series data | np.array([<same shape as input>])Shape: Same shape as the input data. The UI adapter computes Mean Squared Error (MSE) loss between input data and the output reconstructed data, hence, they must have the same shape. |
| Time Series | Anomaly Detection | Time‑series data | np.array([<same shape as input>])Shape: Same shape as the input data. The UI adapter computes Mean Squared Error (MSE) loss between input data and the output reconstructed data, hence, they must have the same shape. |
Example logic for image classification task, converting from logits to probabilities:
exp_shift = np.exp(outputs - np.max(outputs, axis=1, keepdims=True))
probs = exp_shift / np.sum(exp_shift, axis=1, keepdims=True)
return probs
Validating the Post-processing Script
To validate your post-processing script on EdgeBench, go to Adding a Post-processing Script.