User guide

EVAL-AD9434 top view:

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/eval-ad9434-fmc/images/eval_ad9434_top.png

Hardware guide

Hardware configuration - Clock Scheme

There are multiple ways to configure the clock source for AD9434. In this section is presented a guide on how to rework the board to the desired user clock circuitry. Below is a table on what components are needed to install or uninstall on the evaluation board.

Clock Configuration

Install

Uninstall

Ext. Signal Gen.

as it is

as it is

Oscillator

R209, P1(shunt)

—

LVPECL

R208, R307, R308, C300, C311, C304, C305

C209, C210

LVDS

R208, C306, C307

C209, C210, R311

For LVPECL and LVDS configurations, appropriate charge pump filter circuit values are necessary to have an optimized clock buffer performance from AD9517-4.

Warning

On Zedboard, the frequency is set to 463.82MHz, because there is a limitation for BUFG input clock frequency to 464MHz, which is below the maximum sampling rate of the ADC (500MSPS).

Thus the adc_clk period is set to 2.156ns (463.82MHz) on Zedboard.

Power supply

The power supply comes from the FMC connector, given by the FPGA.

The VADJ values can be checked out in the README.md file of each combination with an FPGA, at: projects/ad9434_fmc.

Software guide

The evaluation board is supported with the Libiio library. This library is cross-platform (Windows, Linux, Mac) with language bindings for C, C#, Python, MATLAB, and others. Two easy examples that can be used with it are: