EVAL-ADMX2001 LCR Meter Demo/Evaluation Setup

Note

This page applies to hardware revision B and C, and firmware versions 1.3.1, 1.3.2, and 1.3.3. It may not apply to past or future versions. For firmware update instructions, see Firmware Updates.

The EVAL-ADMX2001 LCR Meter Demo is an evaluation system that is comprised of both the ADMX2001B and the EVAL-ADMX2001EBZ boards.

The ADMX2001B is a high-performance, precision impedance analyzer module.

  • Highly compact, 1.5 inch by 2.5 inch System-on-Module (SOM)

  • Resistance measurements at DC or impedance measurements from 0.2 Hz to 10 MHz

  • 18-bit acquisition channels

  • Operates from a single 3.3V supply

  • Flexible UART and SPI interfaces

  • 18 display mode formats in SI units

The EVAL-ADMX2001EBZ is an easy-to-use evaluation and development breakout board that enables convenient access to the functionality of the ADMX2001B Precision Impedance Analyzer Measurement Module.

  • BNC connectors can interface to common LCR meter test probes and fixtures

  • UART interface can be used with USB-to-UART cables to interface to host PC

  • Trigger and clock synchronization signals are available through SMA connectors that simplify the connection to standard test equipment

  • Arduino-style headers allow the user to develop embedded code with boards like the SDP-K1

  • Power jack accepts various input voltages from ac/dc power adapters that can supply +5V to +12V

EVAL-ADMX2001EBZ Evaluation Kit Contents

  • EVAL-ADMX2001EBZ board

  • UART to USB cable (TTL-232R-RPI)

  • Universal power adapter with 9VDC output

  • LCR meter test clips

Additional Equipment Required

  • ADMX2001B High-Performance Precision Impedance Analyzer Measurement Module

Important

It is critical to purchase both the ADMX2001B High-Performance Precision Impedance Analyzer Measurement Module and the EVAL-ADMX2001EBZ LCR Meter Demonstration Board. These are sold separately.

Optional Equipment

Quick Start

There are five simple steps to start evaluating the ADMX2001:

  • Driver Installation

  • Terminal Emulator Installation

  • Basic hardware setup

  • Open a session through the terminal emulator (e.g. TeraTerm)

  • Perform basic measurements

These steps are explained in detail in the following sections.

1. Driver Installation

Note

The default communication interface to the EVAL-ADMX2001EBZ is via its UART port. When using the UART to USB cable included with the evaluation board (TTL-232R-RPI), FTDI’s Virtual COM Port (VCP) drivers must be downloaded from their website located at https://www.ftdichip.com/Drivers/VCP.htm

Installation steps:

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/dev_mgr_vcp_installed.png

2. Terminal Emulator Installation

To communicate with ADMX2001B via its command-line interface and UART, a terminal emulator like TeraTerm is recommended. Download TeraTerm from the official Github Releases page:

Download and run the latest stable release. Follow the on-screen instructions.

Alternatives like PuTTY can also be used, but some users have had issues with PuTTY where the terminal window does not open. Additionally, some terminals do not support the ANSI Escape Codes which manipulate the cursor position and text color. If the ANSI Escape Codes are not supported, the terminal will render them as boxes. TeraTerm supports these characters.

3. Basic Hardware Setup

The following figure shows the basic connections required for evaluating the EVAL-ADMX2001.

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/eval-admx2001ebz_basic_connections_labeled.png
  • Insert the ADMX2001B module into the EVAL-ADMX2001EBZ board in the location shown above. The connectors are keyed, so they can only be inserted in the orientation shown

  • Set the load select switches to OPEN and GND, as shown below. This is required for the self-test to pass, indicated by the red/green LED on the underside of the ADMX2001B module

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/open_load.png
  • Connect the power adapter to the power jack and to the AC outlet

  • Verify that the self-test light is green (light is on the bottom of the board, but is visible if viewed from the side where the oscillator and FPGA are mounted)

  • Connect the UART to USB cable to the UART terminals TX (orange)–>TX, RX (yellow)–>RX and GND (black)–>GND:

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/uart_to_usb.jpg
  • Ensure that the CLK_SEL jumper cap (located under the UART header) is set to INT (internal clock)

  • Set the load select switches to DUT and GND, as shown below:

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/bnc_load.png
  • Use the test leads to connect to the device under test (DUT):

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/photo_setup_labeled.jpg

The two BNC connectors from the red leads go to the HCUR/HPOT ports, the two BNC connectors from the black leads go to the LPOT/LCUR ports.

Important

Inspect the BNC connectors on the test clips. The housing can become partially unscrewed, allowing the conductor to be pushed back inside and preventing it from making good contact. Additionally, when using the clips in the “open” configuration, each clip should clamp on its own small wire scrap to ensure both sides of the clip are electrically connected.

An example of an unscrewed housing of a test clip:

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/cal_connections_5.jpg

An example of how to use the wire scrap in each of the test clips, when using them in the open configuration:

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/open_config_test_clips_2.png

Self-Test Functionality

When the ADMX2001B powers on, it automatically performs a self-test. The bi-color LED on the underside of the board will turn green if the board boots and passes the self-test, or half-green half-red if the self-test fails. It will turn red if there is a major issue preventing it from booting such as a power issue, missing encryption key, missing firmware or something else. In order to pass the analog component of the self-test, the switches S1 and S2 must be set to OPEN and GND. Alternatively, if S1 and S2 are in the DUT and GND position, the test leads must be connected in the ‘open’ configuration to pass the self-test. The board will still attempt to function without passing the self-test.

The status of the last self-test can be seen by running the command selftest. Using selftest run will rerun the self-test. By default, the self-test only runs on boot.

4. Opening a Session via TeraTerm

After installing TeraTerm, open the program and choose Serial connection. Select the COM port identified earlier in Device Manager. Click OK. Then choose the dropdown labeled Setup, click Serial port, and ensure that the COM port is set, Speed=115200, Data=8 bits, Parity=none, Stop bits=1 bits, Flow control=none. Click New setting. Optionally, choose Setup->Save setup. Save the file to the default directory. Now, when launching TeraTerm, it will automatically try to connect with the saved settings.

Make sure the hardware is properly installed and that power is available to the board via the 12V power adapter. TeraTerm should now be connected to the board. To check:

  • Press ENTER to display the ADMX2001> prompt

  • Type *idn and press ENTER to display the firmware version

  • Type help and press ENTER to see a list of commands supported by ADMX2001B.

Please note that closing the TeraTerm window does not reset the ADMX2001B settings from the last session.

5. Performing Basic Measurements

Upon opening a session with TeraTerm, the ADMX2001B is ready to perform impedance measurements.

Important

The measurements reported by the module will not be accurate unless it has been calibrated. For detailed instructions on how to calibrate the module, please refer to the Calibration Procedure section in this user guide.

By default, the module is set to perform single-point impedance measurements in rectangular coordinates with a 1V pk signal (magnitude = 1) at 1kHz, and no DC offset. To initiate a measurement type the z command at the prompt and press ENTER.

Measurement settings are not always in their base SI form. Frequency is in kHz, delays are in milliseconds. The signal magnitude sets the Vpk value. The peak-to-peak value is twice the signal magnitude, centered around the offset voltage. The DC offset is in volts.

The AC magnitude can be configured anywhere between 0.15V pk and 2.25V pk, but the actual magnitude across the DUT will be be dependent on the DUT impedance, due to the 100Ω source resistance; see Selecting a Measurement Range for details.

Tip

The order in which the settings commands are entered is not important.

Example

Perform a capacitance measurement in parallel with an equivalent resistor (Cp-Rp) at 100kHz with a 1V amplitude (2V pk-pk) sine. Return 5 readings, where each is an average of 10 samples.

ADMX2001> frequency 100
frequency = 100.0000kHz
ADMX2001> display 9
Measurement model: 9 - Capacitance and equivalent parallel resistance (Cp,Rp)
ADMX2001> magnitude 1
magnitude = 1.0000
ADMX2001> average 10
average = 10
ADMX2001> count 5
sampleCount = 5
ADMX2001> z
0,5.677640e-13,8.062763e+07
1,5.668012e-13,8.305672e+07
2,5.675237e-13,8.208995e+07
3,5.673763e-13,8.276912e+07
4,5.683635e-13,8.463327e+07
ADMX2001>

Note

By default, auto-range is selected. To disable the auto-ranging function, use the setgain <ch> <setting> command to select a specific measurement range for the voltage (ch0) or current (ch1) measurement channels.

Using the Help Functionality in the Command-Line Interface

The help command will display all the commands available to the user from the command-line interface (CLI). To get help for any command, simply type

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/help_command_printout_teraterm.png
ADMX2001>help <command>

For example, to get help with how to select different measurement display formats, type

ADMX2001>help display

Which should show a similar screen to the picture shown below

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/help_display_teraterm.png

Useful Hints

Measurement Display Modes

The ADMX2001B returns a result in one of 18 different display modes, shown below. The result is always reported in the base SI unit. For instance, display mode 0 (Cs, Rs) returns the series capacitance in Farads, and the series resistance in Ohms.

Display Mode Number

Mode Name

Form

SI Unit

0

Equivalent series capacitance and resistance

Cs, Rs

Farads, Ohms

1

Equivalent series capacitance and dissipation factor

Cs, D

Farads, Dimensionless

2

Equivalent series capacitance and quality factor

Cs, Q

Farads, Dimensionless

3

Inductance and equivalent series resistance

Ls, Rs

Henries, Ohms

4

Equivalent series inductance and dissipation factor

Ls, D

Henries, Dimensionless

5

Equivalent series inductance and quality factor

Ls, Q

Henries, Dimensionless

6

Impedance in rectangular coordinates (default)

R, X

Ohms, Ohms

7

Impedance in magnitude and phase in degrees

Z, deg

Ohms, Degrees

8

Impedance in magnitude and phase in radians

Z, rad

Ohms, Radians

9

Capacitance and equivalent parallel resistance

Cp, Rp

Farads, Ohms

10

Equivalent parallel capacitance and dissipation factor

Cp, D

Farads, Dimensionless

11

Equivalent parallel capacitance and quality factor

Cp, Q

Farads, Dimensionless

12

Inductance and equivalent parallel resistance

Lp, Rp

Henries, Ohms

13

Equivalent parallel inductance and dissipation factor

Lp, D

Henries, Dimensionless

14

Equivalent parallel inductance and quality factor

Lp, Q

Henries, Dimensionless

15

Admittance in rectangular coordinates

G, B

Siemens, Siemens

16

Admittance in magnitude and phase in degrees

Y, deg

Siemens, Degrees

17

Admittance in magnitude and phase in radians

Y, rad

Siemens, Radians

18

Off

None

None

Selecting a Measurement Range

By default, the ADMX2001B is in auto-ranging mode, which will optimize the measurement gain of the voltage and current measurement channels, depending on the frequency and magnitude of the test signal.

Note

The auto-ranging algorithm will only be applied to the conditions of the first measurement. When performing frequency sweeps, the impedance of the device under test will change and could fall outside of the measurement range selected by the initial measurement conditions.

Additionally, the DC offset control is disabled when using the autorange. Manual gain setting must be employed when using the DC offset. The DC offset will be automatically set to -0.25V to allow the saturation detection to perform as expected when autoranging.

In some cases, the user may want to select a specific measurement range. The measurement range is mostly affected by the transimpedance of channel 1 and the test signal magnitude. It is recommended to select the transimpedance value that is smaller than the expected value of the impedance under test, but larger than the next transimpedance selection.

For example, if the DUT’s expected impedance value is 2kΩ, enter the following in the command line prompt:

ADMX2001> setgain ch0 0
  voltGain = 0
ADMX2001> setgain ch1 1
  currGain = 1

The command setgain ch1 modifies the current measurement range of L_CUR (channel 1). This is done by setting different values for (RTIA) in the feedback loop of the transimpedance amplifier A2. The command setgain ch1 1 sets the transimpedance to 499Ω, appropriate for the 1kΩ-10kΩ range. It is not recommended to use the 10kΩ-100kΩ range for a 2kΩ load since this could exceed the current input channel measurement capabilities and return incorrect readings.

The ADMX2001B uses a balancing bridge architecture. A 100 ohm series resistor Rs protects the source channel. When calculating the current through a DUT or the actual AC magnitude across that DUT, this resistor must be factored in. A transimpedance amplifier is used in measuring the current, and has a 10 ohm input protection resistor RIN. A simplified diagram is shown below. In the diagram, ZX is the DUT (unknown impedance). The transimpedance amplifier holds the connection point to RIN (inverting terminal of the TIA) at 0V. Since RS, ZX and RIN are in series, the DUT current is equal to (magnitude setting Vpk)/(|ZX| + 100Ω + 10Ω).

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/source_and_measurement_channels_v3_renumbered.png

Available current gain settings and the transimpedance values associated with them are listed below.

Ch1 Gain

Max Input Current

Transimpedance

0

25mA

49.9Ω

1

2.5mA

499Ω

2

250uA

4.99kΩ

3

25uA

49.9kΩ

Continuing from the previous example, when the DUT is 2kΩ and the magnitude is set to the maximum setting of 2.25Vpk, the current through the DUT (and into the TIA) is 2.25Vpk/(2kΩ + 110Ω) = 1.06mA. Then selecting ch1 gain to be 1 makes the measurement fit well within the max input current range of 2.5mA.

The command setgain ch0 modifies the input voltage range of channel 0 (between terminals H_POT and L_POT). This is less common, but it can be used to improve measurement sensitivity if the impedance under test is smaller than the lead impedance or less than 100Ω. It can also be used if the magnitude of the test signal is small. This can be the case with sensitive loads, or when the test frequency is high.

Available voltage gain values for channel 0 are listed below.

Ch0 Gain

Max Input Voltage Range

Gain Factor

0

±2.5V

1

1

±1.25V

2

2

±625mV

4

3

±312.5mV

8

The DUT voltage is determined by the set magnitude and the two series protection resistors. The DUT voltage is equal to (magnitude setting Vpk)*(|ZX|)/(|ZX| + 110Ω). For example, to measure a 25Ω DUT with the magnitude set to the maximum setting of 2.25Vpk, the DUT voltage is 2.25Vpk*(25Ω)/(25Ω + 110Ω) = 416.7mVpk, a little under the 625mVpk limit. To utilize the full range, set the ch0 gain = 2.

Voltages across and currents through the DUT that exceed these maximum values for each gain range may result in the ADC saturating, causing the measurement to fail.

Typing the command setgain will display the gain of both input channels and whether or not autoranging is enabled.

ADMX2001> setgain
Autorange enabled
voltGain = 1
currGain = 3
ADMX2001>

To turn autoranging back on after setting a manual range type setgain auto

Even though 16 gain combinations are possible, most measurements can be performed with the 7 combinations shown in the table below.

Ch0 Gain

Ch1 Gain

Impedance Measurement Range

3

0

< 10Ω

2

0

< 25Ω

1

0

< 50Ω

0

0

100Ω to 1kΩ

0

1

1kΩ to 10kΩ

0

2

10kΩ to 100kΩ

0

3

> 100kΩ

These are the same ranges that the autoranging algorithm uses. The previously mentioned procedures can be used to calculate the DUT current and voltage. The following section shows how to estimate the impedance value of the DUT to determine the measurement range. Note that these measurement ranges apply for magnitude = 1 and offset = 0. They may not apply for other settings. To calculate whether the ADC will saturate, use the balancing bridge diagram above. Using the sum of the signal magnitude and offset, calculate what the current through the 110Ω resistors + DUT will be, and choose a gain from the Ch1 gain table. Then, calculate the voltage across the DUT due to this current through it, and choose a voltage gain from the Ch0 gain table.

For a 2kΩ DUT where the sum of the magnitude and offset is 1Vpk, using the two equations we find:

  • DUT current = 1Vpk/(2kΩ + 110Ω) = 0.47mA, select Ch1 Gain = 1.

  • DUT voltage = 1Vpk*2kΩ/(2kΩ + 110Ω) = 948mV, select Ch0 Gain = 0 or 1.

  • The above selection matches the suggested gain combination (0,1) with a given impedance measurement range from 1kΩ to 10kΩ.

Estimating the Impedance and Admittance of Capacitive and Inductive Devices

Impedance is defined as the opposition to the flow of alternating current. Admittance is the reciprocal of impedance, or how easy is for alternating current to flow. Electrical components such as resistors, capacitors and inductors have a direct relationship between their value and the expected impedance (Z):

Z = X = -1/(2πfC) for capacitors Z = X = 2πfL for inductors Z = R for resistors

Where f is the frequency of the signal; C, L, and R are the component values in Farads, Henries and Ohms respectively. R represents resistance and X reactance.

For admittance (Y):

Y = B = 2πfC for capacitors Y = B = -1/(2πfL) for inductors Y = G = 1/R for resistors

Where f is the frequency of the signal; C, L, and R are the component values in Farads, Henries and Ohms respectively. G represents conductivity and B susceptance.

All components, regardless of their construction, will show a combination of resistive (conductive) and reactive (susceptive) properties. These properties can be expressed in the form of ideal electrical components combined either in series or parallel. At any given frequency, impedance/admittance can be expressed as a combination of the reactive element (capacitor or inductor) and a resistive element. The total impedance or admittance magnitude can be obtained by calculating the square-root of the sum of squares (RSS) of the two components or

Z = sqrt(R*R + X*X)

Y = sqrt(G*G + B*B)

To determine the best measurement range for measurement, it is necessary to estimate the impedance or admittance of the device under test at the frequency of measurement using the equations above. A simpler method to obtain an approximate value based on the expected capacitance or inductance value is through the reactance chart shown below.
https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/reactance_chart_labeled.jpg

To find the approximate impedance or admittance value for a capacitor or inductor, find the closest expected value assigned to the diagonal lines and find its equivalent impedance/admittance value on the vertical axis at the frequency of interest (on the horizontal axis). For example, the impedance of a 159fF capacitor, which is represented by the red solid diagonal line in the reactance chart, exhibits |Z|=1MΩ at 1MHz, indicated by the “1M” tick on the vertical axis. This matches the estimated value using equation Z = X = -1/(2πfC). Similarly, for a 15.9nF capacitor, which is shown as blue solid diagonal line in the chart, |Z|=10KΩ at 1kHz.

Reducing Measurement Noise

The average command determines how many samples are averaged for each reading returned. Averaging reduces noise and is helpful in applications that require to detect small changes in a value or when the impedance component of interest is small in comparison to the total impedance magnitude (e.g. ESR of capacitors). The default is set to 1, which means that no averaging is done.

Tip

Averaging increases the time required to return a reading. Values greater than 256 have been observed to have little effect in reducing measurement noise and have a significant impact on measurement speed.

Improving Measurement Precision

To ensure precise and accurate measurements, impedance measurements should be performed with appropriate test fixtures. Measurement leads can introduce additional errors due to parasitic impedances that will vary depending on mechanical configuration.

Tip

The test leads included with the EVAL-ADMX2001EBZ kit can introduce fluctuations of a few picofarads depending on their position. This effect becomes more noticeable with test frequencies higher than 100kHz.

To ensure repeatable and stable measurements, custom-made fixtures that minimize impedance fluctuations due to mechanical configuration are recommended. For example, to test surface-mount components, fixtures like the B+K Precision TL89S1 or the Keysight 16034G are recommended. For a full list of recommended accessories, please refer to the Recommended Accessories Section at the beginning of this user guide.

Performing Parametric Sweeps

The ADMX2001B can automatically perform measurements that sweep different measurement parameters such as

  • Frequency, common in EIS applications (Electrical Impedance Spectroscopy). The frequency increments can be linear or logarithmic.

  • DC bias, common in C-V measurements for semiconductor devices

  • Magnitude

By default, the sweep function is off. To enable parametric sweeps, use the sweep_type command and specify the sweep type. The command also requires the user to enter the start and end points of the sweep. The number of points is determined by the count command.

Example

Perform an 11-point logarithmic frequency sweep from 100kHz to 1MHz.

ADMX2001> count 11
sampleCount = 11
ADMX2001> sweep_type frequency 100 1000
Frequency
sweepStart = +100.0000KHz
sweepEnd = +1000.0000KHz
ADMX2001> sweep_scale log
Sweep scale is log
ADMX2001> z
1.000000e+05,5.683433e-13,8.149236e+07
1.258925e+05,5.704062e-13,4.727518e+07
1.584893e+05,5.674423e-13,2.989029e+07
1.995262e+05,5.652225e-13,1.917354e+07
2.511886e+05,5.622380e-13,1.233886e+07
3.162278e+05,5.577508e-13,8.082886e+06
3.981072e+05,5.490229e-13,5.611289e+06
5.011872e+05,5.421543e-13,3.547964e+06
6.309573e+05,5.299540e-13,2.360688e+06
7.943282e+05,5.136760e-13,1.624230e+06
1.000000e+06,4.798023e-13,1.411488e+06
ADMX2001>

Note

When sweeping parameters, the first value printed will be the swept parameter, followed by the measurement in the display format selected.

Performing DC Resistance Measurements

The DC resistance measurement function can be easily selected by setting the test frequency to zero. In DC mode, since the AC test signal is disabled, the DC offset must be used to generate the test signal. Due to the hardware design, saturation may not be detected if the DC offset is positive; set the DC offset to a negative value to prevent this. DC resistance mode only works in display mode 6, so the display mode must be configured as such.

ADMX2001> frequency 0
DC Resistance mode enabled
ADMX2001> display 6
Measurement model: 6 - Impedance in rectangular coordinates (default) (Rs,Xs)
ADMX2001> offset -1
Offset = -1.0000
ADMX2001> z
0,4.995231e+01
ADMX2001>

In the DC resistance mode, only the DC resistance value is returned.

Plotting Measurement Data

When acquiring multiple measurements or performing sweeps, it is useful to plot the results to observe trends or characteristics of the device under test. TeraTerm allows the user to save a log by going to File->Log, which can then be copy and pasted into a *.csv file that can be opened by spreadsheet applications such as Microsoft Excel®. The log file must be saved BEFORE taking any measurements.

To plot the acquired data in Microsoft Excel, follow the steps below:

  • In TeraTerm, click File, in the dropdown list select Log, and save the log file with any name but make sure to change the default extension from *.log to *.csv

  • Configure the ADMX2001B and run the z command to acquire the desired measurements

  • In a separate TeraTerm window named “TeraTerm:Log”, click close to stop logging data

  • Open the file with Excel

  • Select the data to plot and insert a scatter plot to visualize the data

Optimizing Measurement Timing

This section describes what settings impact the measurement time and how. It also discusses ways to reduce the measurement time down to ~10-12 ms for single measurements (firmware version 1.3.2 only). The measurement time is dependent on a number of factors. Command transmission time, configured delays, source setup time, ADC acquisition time, count setting, averages, etc. Some factors, like the ADC acquisition time, are dependent on the frequency since the ADC needs to capture a minimum of three cycles of the waveform.

Delay Usage and Measurement Sequencing

The commands mdelay (measurement delay) and tdelay (trigger delay) can be used to control the settling time between measurements.

  • The measurement delay or mdelay is observed before each measurement, but not between samples when averaging. The delay is also applied during sweeps and between multiple counts. Both the DC offset and AC test signal are enabled during the delay, but the ADCs do not capture data for the measurement until the delay has elapsed.

  • The ideal measurement delay suitable for different DUTs may vary. When measuring a large capacitor, consider the settling time it requires to charge the DUT; a longer mdelay is preferred to prevent accuracy loss.

  • Trigger delay is only observed after trigger events controlled by the tcount command. This is useful when using the ADMX2001B with external scanning cards or multiplexers, to allow proper debounce and settling time. If configured, the DC offset will be enabled during the trigger delay, but the AC source will only start for the data capture.

To setup mdelay and tdelay, simply enter the command followed by a value in milliseconds.

Below is a demonstration on how each measurement time parameter fits in the measurement sequence. Note that the sinusoidal excitation is turned on during periods marked with blocks in light/dark green. If enabled, the DC offset will turn on during the tdelay blocks. The example measurement uses a 15.8 Ohm resistor as the DUT.

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/command_timing_diagram.png
  1. Single sample measurement. When measuring one count sample, an mdelay is observed before each measurement where the single sample is captured.

ADMX2001> count 1
sampleCount = 1
ADMX2001> average 1
average = 1
ADMX2001> z
0,1.589015e+01,5.979061e-03
  1. Multiple samples averaging. When measuring with average > 1, mdelay is observed only before the first sample, but not between samples.

ADMX2001> count 1
sampleCount = 1
ADMX2001> average 10
average = 10
ADMX2001> z
0,1.588981e+01,5.922471e-03
  1. Multiple counts measurement. When doing multiple counts of single sample measurement, mdelay is observed before each measurement in their individual count.

ADMX2001> count 3
sampleCount = 3
ADMX2001> average 1
average = 1
ADMX2001> z
0,1.588983e+01,6.072280e-03
1,1.589017e+01,6.406131e-03
2,1.588982e+01,6.175226e-03
  1. Multiple triggers measurement. When tcount >1, multiple measurement triggers are enabled. Based on single measurement cycle setting (say count = 3, average = 1), multiple measurement events are triggered. The tdelay defines the delay time between these trigger events.

ADMX2001> count 3
sampleCount = 3
ADMX2001> average 1
average = 1
ADMX2001> tdelay 10
triggerDelay = 10.0000msec
ADMX2001> tcount 3
triggerCount = 3
ADMX2001> z
0,1.588982e+01,6.526160e-03
1,1.589041e+01,5.718554e-03
2,1.589056e+01,6.170146e-03
0,1.588994e+01,6.373706e-03
1,1.589030e+01,5.733064e-03
2,1.589026e+01,5.668341e-03
0,1.589055e+01,5.907189e-03
1,1.588984e+01,5.669621e-03
2,1.588993e+01,6.286668e-03

Optimizing Single Point Measurements

In version 1.3.2, many optimizations were added to reduce the measurement time.

  • The initiate and trigger mode (trigger mode), previously used only for external triggers, is now optimized for faster measurements. See Trigger Input/Output Ports for details on how to use trigger mode (also referred to as the WAIT_FOR_TRIGGER state).

  • When in trigger mode, most commands are disabled. This is because measurement attributes like frequency, gain, magnitude, offset, delays, and others are locked. Locking them means that for each measurement, setup and initialization tasks for those attributes can be skipped because they will always be unchanged. This saves a significant amount of time on each measurement, especially reducing the time between a trigger being received and the measurement acquisition starting.

    • Sweeps do not benefit from this optimization, because the sweep attribute cannot be updated in trigger mode.

    • If enabled, the DC offset is always on in trigger mode. The autorange must be off to enable the DC offset. Keeping the DC offset enabled constantly can be useful when testing with DUTs that need a long DC settling time, as that delay does not need to be repeated for every measurement.

  • The measurement is only reported over the active interface (UART commmand line interface or SPI). The active interface is set based on the most recently sent command. For instance, if the command initiate is sent over UART, and then the command TRIGGER (0x18) is sent over SPI, the result will be readable in the SPI FIFO and not accessible on UART. If INITIATE (0x17) is sent over SPI, and then trigger is sent over UART, the result will print immediately to UART and not be accessible in the SPI FIFO. See ADMX2001B SPI Interface for details on how to operate the SPI interface.

    • The SPI interface is the fastest and can save multiple milliseconds over using the UART (command line) interface.

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/trigger_mode.png

To achieve the fastest single-point measurement time, there are a few points to consider.

  • Interface: The SPI interface should be used to receive the measurement data. Either interface can be used to configure measurement settings, this will not impact the speed of each measurement. The active interface is updated every time a command is sent, to whichever interface sent that command.

  • Trigger source: In trigger mode, there are three options for the trigger source.

    • The trigger command can be sent over the UART (CLI). This is the slowest method, and since trigger will be the most recent command, it will always report the result over the UART (CLI).

    • The TRIGGER (0x18) command can be sent over SPI. This is the preferred method as it is fast, and easy to set up. It also guarantees that the active interface will be set to SPI.

    • A pulse can be applied to the TRIG_IN pin. For this pulse to be registered, external trigger mode must be enabled; see Trigger Input/Output Ports. Measurements initiated with the external trigger can report data over either the UART or SPI interfaces, dependent on where the most recent command was received. For instance, this could be the initiate command in CLI, or INITIATE (0x17) over SPI.

  • Trigger count: when using trigger mode, the trigger count (tcount) sets a condition for automatically exiting trigger mode. It will receive tcount*triggers before returning to the normal operating mode. To continue measuring in trigger mode, the initiate command is needed to re-enter the mode. To exit trigger mode before completing tcount*triggers, the abort command can be used (0x1A) in SPI.

    • There is also support for an “infinite” trigger mode. Run tcount 65536 to enter this mode; the only way to exit trigger mode in this case is with the abort command. Normal z measurements are disabled when tcount is set to 65536.

  • Autorange: The autorange should be disabled for the fastest measurements. The autorange tests the ideal gain by taking multiple measurements with different gain settings, and checking for ADC saturation. Therefore, it can significantly increase the measurement time.

    • When using the autorange with trigger mode, the autorange test is performed when the initiate command runs. See the flow chart above. Leaving and re-entering trigger mode will update the selected gain.

  • Delays: The trigger delay (tdelay) and measurement delay (mdelay) directly impact the measurement time. In trigger mode, the tdelay is applied once per supplied trigger, and the mdelay is supplied once per count (not tcount). Therefore, a typical single measurement will have tdelay+mdelay added on. The default tdelay is 4 ms; this can typically be set to 0 ms with no negative impacts; this is recommended to optimize the measurement time. The default mdelay is 1 ms; at frequencies above 10 kHz, setting this to 0 ms will cause the ADC to capture some data before the AC source has fully turned on. This typically has no impact on the measurement result, allowing 1 ms to be saved per measurement, but it should be tested with each setup.

  • Frequency: the measurement time is highly dependent on the test frequency below ~3 kHz. This is because the system tries to capture a minimum of 3 cycles of the excitation waveform. See the log plot below for the measurement time across frequency.

  • Display mode: the measurement time is also dependent on the display mode. Rectangular formats like display mode 6 (R, X) and 15 (G, B) are the fastest, as they require the least processing. Modes with angle in degrees or radians (polar form) can take 2-3 extra milliseconds; see the chart below.

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/measurement_time.png

*Typical measurement times above are based on the following settings:

  • Interface = SPI, SPI trigger source

  • Mode = trigger mode

  • mdelay = 0

  • tdelay = 0

  • average = 1

  • calibration = on (can save 1-2 ms turning calibration off)

  • autorange = off

Note that measurements taken over the UART will be slower.

Calibration Procedure

A few milliseconds after power up, the ADMX2001B is ready to perform measurements. However, any readings and their units are scaled and assigned using nominal circuit parameters. Measurement accuracy can only be evaluated after performing calibration on the module with an external calibration source with certified traceability. For example, the Keysight E4980A can be used.

There are three basic calibration steps involved in calibrating the module: open calibration, short calibration, and load calibration. The first two correct the module and test lead parasitics. The latter provides traceability to an external source. The calibration steps must be performed in the order open->short->load. Open and load calibration are the most important. Short calibration may need to be skipped in certain gain ranges where the current ADC would saturate. Open calibration may need to be skipped in gain ranges that the voltage ADC would saturate.

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/open_short_load_config.png https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/open_short_load_config_photo.png

Tip

When performing load calibration for a given gain setting and frequency, the optimal load device (usually a resistor) is one with an impedance magnitude close to that of the eventual DUT. The best accuracy at a certain gain and frequency will be with DUTs of a similar impedance to the one used in calibration.

Resistors, capacitors or inductors can be used for calibration. High-quality resistors (e.g. thin film or metal film), air capacitors, and gas-filled capacitors tend to provide the best results. Alternatively, C0G/NP0 type ceramic capacitors can be used as well. The true value of these components must be determined with traceable measurements from another meter, such as the Keysight E4980A.

Each measurement front-end configuration (ch0 and ch1 gain combination) needs to be calibrated separately. If calibration is performed for only one gain combination, calibration needs to be carried out again if the front-end configuration changes. There are a total of 16 possible gain combinations based on the 4 gain and transimpedance ranges for channel 0 and channel 1 respectively.

The autorange will only choose between the 7 gain combinations that have a zero in at least one position. These are shown in the impedance measurement range table within the section Selecting a Measurement Range. If all measurements will be done with the autorange or with these gains, then the other gain settings do not need to be calibrated. In versions 1.2.0 and older, if the user calibrates at a specific gain and frequency, then changes the frequency and calibrates again, the user will overwrite the result of the first calibration. In version 1.2.2, support for calibration over frequency was added. See Calibration Over Frequency for more details.

Important

Each calibration point is for a specific frequency. Measurements taken at a different frequency may be out of tolerance. Always calibrate as near as possible to the intended test frequency.

Calibration Steps

To calibrate the module in a specific gain combination, follow the steps below:

  • Select the desired measurement configuration (gain, frequency, magnitude and offset)

    • Autorange must be disabled during calibration.

  • Set the averaging to at least 200 samples.

  • Ensure the load select switches are in the DUT and GND positions, described in Basic Hardware Setup

  • Connect the H_POT and H_CUR terminal together and the L_POT and L_CUR terminals together to form two separate connection pairs

    • If using the test clips, place them so the alligator clips are separated by the same distance as they will be when the DUT is connected. Each clip should be clipped to a very short scrap of uninsulated wire, which serves to improve the connection between each half of the clip

    • An alternative is to use BNC cables to connect the H_POT/H_CUR pairs and the L_POT/L_CUR pairs.

    • Open calibration at high frequencies and in higher impedance measurement ranges is especially susceptible to error, due to the increased opportunity for coupling into the current measurement path. The test setup is especially important under these conditions

    • For better results, use Keysight 42090A Open Termination

  • Run the calibrate open command

  • Connect all the measurement terminals together

    • Short calibration can be performed only when gain channel 1 is set to 0 or 1. When channel 1 is in gain 1, the magnitude of the source must be less than 0.2Vpk.

    • When measuring extremely tiny impedances (<100mΩ), short calibration becomes extremely important. Many fixtures have a low repeatability under these conditions. Optimizing the repeatability of the fixture is critical to getting a meaningful result, for both calibration and measurement

    • For better results, use Keysight 42091A Short Termination

  • Run the calibrate short command, if possible

  • Connect a known impedance between the measurement leads

  • Run the calibrate rt <value1> xt <value2> command where <value1> is the true value of the resistive component (Ohms) of the calibration impedance and <value 2> is the true value of the reactive component (Ohms)

    • To obtain true values of resistive and reactive components beforehand, use an LCR meter and select Rs and X for the display mode.

    • Scientific notation can be used when entering the rt and xt values

    • For best results, a standard resistor set like the Keysight 42030A can be used

After completing the steps above, calibration coefficients are generated and stored in RAM. These coefficients will be applied to any subsequent measurements, but will be lost after a power cycle or reset of the module. To store the coefficients in non-volatile memory (flash) the command calibration commit <timestamp> must be executed. The timestamp parameter is optional. If supplied, the unix timestamp is the number of seconds elapsed since 01/01/1970. For example:

ADMX2001>calibrate commit 1689959855

This will store the calibration coefficients in the RAM to the flash, and set the date and time stamp of the calibration to 07/21/23 at 05:17 UTC.

Note

To help ensure calibration integrity, the calibration coefficients stored in flash are password protected. The default password is Analog123 and must be entered after running calibrate commit to save the coefficients. The password can be changed with the calibrate password command. Maximum password length is 12 characters.

Calibration Example

Calibrate the gain setting (0, 1) at 100kHz with a resistor of value 1k Ohms. The true resistance Rt from the E4980A at 100kHz was measured as 1000.019 Ohms, and the true reactance Xt was 0.822 Ohms.

ADMX2001> setgain ch0 0
voltGain = 0
ADMX2001> setgain ch1 1
currGain = 1
ADMX2001> frequency 100
frequency = 100.0000kHz
ADMX2001> magnitude 1         <--- 1 Vpk, 2 Vpp
magnitude = 1.0000
ADMX2001> offset 0
Offset = 0.0000
ADMX2001> average 200
average = 200
ADMX2001> tdelay 200
triggerDelay = 200.0000msec
                              <--- Connect open load now
ADMX2001> calibrate open
0,-1.117998e-09,1.162904e-06
Frequency = 100.0000kHz
Cal Temp: 41.4 deg C
open:Done
short:Not Done
load:Not Done
ADMX2001> magnitude 0.2       <--- Need to reduce the magnitude to avoid saturating the current ADC when measuring a short
magnitude = 0.2000
                              <--- Connect short load now
ADMX2001> calibrate short
0,2.075835e-02,1.224807e-02
Frequency = 100.0000kHz
Cal Temp: 41.4 deg C
open:Done
short:Done
load:Not Done
ADMX2001> magnitude 1         <--- Magnitude can be set back to 1 now
magnitude = 1.0000
                              <--- Connect calibration load now (in this case, a 1kΩ resistor)
ADMX2001> calibrate rt 1e+3 xt 0.822
0,1.010381e+03,-1.254483e+01
Frequency = 100.0000kHz
Cal Temp: 41.5 deg C
open:Done
short:Done
load:Done
ADMX2001> calibrate commit 1689959855   <--- The timestamp can be omitted here
PASSWORD> ****
commit : success
ADMX2001> display 6
Measurement model: 6 - Impedance in rectangular coordinates (default) (Rs,Xs)
ADMX2001> z
0,1.000021e+03,8.220137e-01
ADMX2001>

Reading and Writing Calibration Coefficients

Calibration coefficients for each gain can be read to the terminal, and written back to the device. This allows the user to save coefficients for multiple different test setups, conditions, or frequencies. To read the currently loaded coefficients for a certain gain setting, run the command rdcal <vgain> <igain>. This prints the 12 AC and and 2 DC coefficients to the terminal, where they could be saved by an external device. To write coefficients to the device, use the command storecal <vgain> <igain> <coefficient_name> <value>, where coefficient_name is one of the 12 AC or 2 DC coefficients. For example, set Ro to 1e+6 for the gain vgain=0, igain=1:

ADMX2001> storecal 0 1 Ro 1e+6
ADMX2001> rdcal 0 1
Ro = 1.0000000e+06
Xo = -8.5991553e+05
Go = -1.1179984e-09
Bo = 1.1629038e-06
Rs = 2.0758350e-02
Xs = 1.2248066e-02
Gs = 3.5733319e+01
Bs = -2.1083758e+01
Rg = -9.4387458e+03
Xg = 8.5097009e+05
Gg = -3.5847357e+01
Bg = 2.1737716e+01
No calibration coefficients found for the given arguments. The defaults coefficients are ...
Rdg = 1.0000000e+00
Rdo = 0.0000000e+00
ADMX2001>

This process should be repeated for all coefficients for a given gain to be valid. If using other gains, the coefficients will need to be stored for them too. Then, they must be saved using calibrate commit; otherwise, they will be lost if the system reboots.

Calibration Over Frequency

Starting in firmware version 1.2.2, calibration over frequency support is implemented. This means that all 16 gain settings can be fully calibrated at multiple frequency points. The process for calibrating over frequency is the same as single point calibration, except after running calibrate commit for the final gain setting at a given frequency, the user can then change the frequency and repeat the process.

When calibration is enabled, taking a measurement with z will automatically load the calibration coefficients with the nearest frequency from memory. After taking the measurement, running the command calibrate with no arguments will report the frequency of the coefficients that were used. For instance, if calibration was performed at 1 kHz and at 100 kHz, a measurement at 55 kHz would use the coefficients saved for 100 kHz.

There are no restrictions on what frequencies the user can calibrate at. However, there are two hardware revisions of the ADMX2001B module; one has EEPROM for the nonvolatile memory (older) and the other has flash memory. Modules with the EEPROM can store 25 calibration sets at different frequency points before new sets start to overwrite the oldest ones. Modules with the flash can store up to 450 calibration sets. The command selftest run will report whether the module has EEPROM or flash installed.

New commands have been added to facilitate calibration over frequency: resetcal (unchanged) will erase only the currently loaded calibration set from RAM. calibrate reload will load the nearest frequency calibration coefficients from the nonvolatile memory and store them in the RAM (taking a measurement implicitly runs calibrate reload). calibrate erase will permanently delete all saved calibration sets from memory, restoring to the default configuration. This requires the password (default is Analog123) and cannot be undone! calibrate list will report all frequencies that have any calibration data saved (at least one gain setting). calibrate list <freq> will report what gain settings at a given frequency have been calibrated.

The commands for reading and writing calibration coefficients detailed in Reading and Writing Calibration Coefficients apply to the currently selected frequency.

Preloaded Calibration Sets

Version 1.2.2 also adds support for ADMX2001B modules to ship with a set of calibration coefficients intended to help with evaluating the board. Although the firmware supports it, boards that are currently shipping will not have calibration coefficients preloaded. This will be a future development.

Preloaded coefficients may not apply to a given test setup and their accuracy is not guaranteed. If the board came with them pre-loaded, then the below new commands apply: calibrate switch <evalkit/default> choosing evalkit will apply the preloaded coefficients. Choosing default will apply user generated coefficients. Generating calibration coefficients will automatically change the active set to default. calibrate with no arguments will report the active set. The evalkit set cannot be modified or erased. Only the default (user) set should be modified or erased.

Compensation Procedure

Compensation is an additional measurement adjustment function designed to account for changes in the test fixture or leads that were not present during calibration. This feature is in development; currently, it is recommended to recalibrate for each fixture, and use the commands detailed in Reading and Writing Calibration Coefficients to save and load calibration data from a host device.

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/calibration_compensation_boundary_2.png

EVAL-ADMX2001EBZ Terminal Description

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/eval-admx2001ebz_diagram_3.png

Terminal Name

Description

H_CUR

Signal source terminal. It generates the excitation required for measurement. This terminal can source up to +/-5V @ 50mA

H_POT

Voltage sense terminal. Connect to H_CUR at the device under test (DUT)

L_POT

Voltage sense terminal. Connect to L_CUR at the device under test (DUT)

L_CUR

Current sense terminal. Return path for the excitation signal. Connect to the opposite end of the DUT as H_CUR

UART TX

UART transmitter pin. Connect to TX pin on the UART to USB cable. Uses 3.3V logic

UART RX

UART receiver pin. Connect to RX pin on the UART to USB cable. Uses 3.3V logic

UART GND

UART ground. Connect to ground pin on the UART to USB cable

CLK_SEL

Jumper selection of internal or external clock. Set to internal for default operation

TRIG_IN

Trigger input. Use for hardware-timed acquisition only, otherwise leave disconnected

TRIG_OUT

Measurement complete trigger out

CLK_IN

External clock input. Use a LVCMOS 50MHz clock signal and set CLK_SEL to EXT position

CLK_OUT

Clock output. These two terminals have a buffered replica of the 50MHz main clock

PMOD

Controller and Peripheral PMOD terminals for SPI port

Header P6 pins [9-10]

Digital output 0-1

Header P7 pins [1-6]

Digital output 2-7


SPI Interface

The ADMX2001B supports a SPI interface in addition to the UART CLI interface. The SPI bus can be accessed on Header P6 and both PMOD headers of EVAL-ADMX2001EBZ, or pins B14-B17 of the ADMX2001B module. A full command reference for the SPI interface can be found at ADMX2001B SPI Interface.

Trigger Input / Output Ports

The EVAL-ADMX2001EBZ has SMA terminals for the trigger input and output ports. These can be used to synchronize multiple modules or control measurement timing with an external instrument. To use the trigger input, the module must be configured to external trig_mode using the command trig_mode <internal/external>. By default, the board is in internal trig_mode, and ignores pulses on the TRIG_IN port. Next, set the trigger count with tcount <count>. This controls how many external triggers the module will respond to before exiting the WAIT_FOR_TRIGGER state. There is also an “infinite” trigger setting; if the tcount is set to 65536, then it will respond to unlimited triggers and never exit the WAIT_FOR_TRIGGER state automatically. Now, type the command initiate. The module will enter the WAIT_FOR_TRIGGER state. Most commands are disabled in this state. The module will automatically return to the IDLE state after receiving tcount triggers, or immediately if it receives the abort command. While in the WAIT_FOR_TRIGGER state, a software trigger can be provided with the command trigger, in both internal or external trig_mode. If the trig_mode is external, then a 3.3V 15μs pulse (min) to the TRIG_IN port will be registered as a trigger.

When a measurement is initiated from the WAIT_FOR_TRIGGER state, either by an external trigger or software trigger, it will generate a 3.3V 15μs pulse on the TRIG_OUT port.

Immediately after running initiate, the autorange algorithm will run (if the autorange is enabled). The gain chosen by this instance of the autorange will be locked in for subsequent measurements in trigger mode. If the DC offset is enabled, then the DC offset will be applied as soon as the initiate command runs. The DC offset and autorange cannot be used at the same time.

Warning: when the initiate command is run, the board will reload the calibration data automatically from the flash. Any coefficients that were not committed (saved to the flash) will be lost. This process is the same as running the command calibrate reload. Verify that any calibration data that should be applied during trigger mode measurements is saved for it to be applied, and not lost.

PMOD Headers

The EVAL-ADMX2001EBZ features PMOD_IN and PMOD_OUT headers for interfacing with a host over SPI.

Pin Number

Pinout

Note

1

No Connect

2

SDI

3

SDO

4

SCLK

20 MHz max

5

GND

6

VCC

3.3V, PMOD_OUT only. VCC current not limited

7

No Connect

8

No Connect

9

CS

10

No Connect

11

GND

12

VCC

3.3V, PMOD_OUT only. VCC current not limited

Pins 6 and 12 are No Connect on PMOD_IN (P12). On PMOD_OUT (P11), they connect to the 3.3V supply, and there is no current limiting on the board.

Digital Output Pins

The ADMX2001B features eight general purpose digital output pins, intended for controlling external MUXes or other peripherals. Support was added in version 1.2.2. The outputs are broken out on EVAL-ADMX2001EBZ, and can be accessed on pins 9-10 of P6, and pins 1-6 of P7. They can be set with the command gpio_ctrl <N> where N is a decimal from 0-255, and each of the 8 inputs are controlled by the respective bit for that position. Digital output 0 corresponds to the LSB. For instance, configuring gpio_ctrl 133 (1000 0101 in binary) will set high P6 pin 9, and P7 pins 1 and 6.

Header : Pin Number

Bit Number

N Setting

P6 : 9

0

1

P6 : 10

1

2

P7 : 1

2

4

P7 : 2

3

8

P7 : 3

4

16

P7 : 4

5

32

P7 : 5

6

64

P7 : 6

7

128

ADMX2001B Pin Configuration and Function Descriptions

https://media.githubusercontent.com/media/analogdevicesinc/documentation/main/docs/solutions/reference-designs/admx2001_ebz/images/admx2001b_pinout_top.png

Pin Number

Mnemonic

Description

Center Pad

GND

Ground

A1-4, B1-4

VDD

Power supply terminals. Apply +3.3V nominal

A11

VCC

5V rail, not current limited. Leave unconnected.

A18

VEE

-5V rail, not current limited. Leave unconnected.

A23

CLKIN

External clock input. Must connect to 50MHz source or CLKOUT terminal

A25

CLKOUT

Clock output. If using external clock on CLKIN, leave unconnected. Otherwise connect to CLKIN

A22, A24, A26

GND

Ground

B5, B7, B9, B11, B13, B18, B21

GND

Ground

B10

TRIGIN

Measurement trigger input. If unused, leave unconnected

B12

TRIGOUT

Measurement trigger output. If unused, leave unconnected

B14

SCK

Serial data clock input

B15

SDI

Serial data input

B16

SDO

Serial data output

B17

CS

Serial interface port chip select input

B19

TX

UART transmit output. Connect to host’s receiver

B20

RX

UART receive input. Connect to host’s transmitter

B22

JTAG_VCC

JTAG power out.

B23

TCK

JTAG test clock.

B24

TDO

JTAG test data out.

B25

TMS

JTAG test mode select.

B26

TDI

JTAG test data in.

C18-C25

GPIO0-GPIO7

General-purpose digital output terminals

C1, C3, C4, C6, C7, C9, C10, C12-C17, C26

GND

Ground

D1, D3, D4, D6, D7, D9, D10, D12

GND

Ground

C2, D2

HCUR

Source terminal

C5, D5

HPOT

Voltage measurement high terminal. Tie to HCUR at the device under test

C8, D8

LPOT

Voltage measurement low terminal. Tie to LCUR at the device under test

C11, D11

LCUR

Current measurement input

All other pins

NC

Do not connect

| —-

Firmware Updates

The ADMX2001B module firmware is user-updatable. Programming files must be requested by contacting admx-support@analog.com. Make a myAnalog account on (analog.com), by clicking in the top right. Then, email admx-support@analog.com, and mention the email associated with the myAnalog account.

Warning: updating between certain firmware versions can cause saved calibration coefficients to be lost.

Equipment List:

  • EVAL-ADMX2001EBZ board

  • ADMX2001B Impedance Analyzer Measurement Module

  • Intel Altera USB Blaster (Terasic)

  • Universal power adapter with 9VDC output

Software Prerequisites:

  • Python 3.7 or greater

  • Latest Intel Quartus Prime Programmer And Tools

    • Navigate to the downloads page for the latest Quartus Prime Lite Edition, and click the “Additional Software” tab. Alternatively, the full Quartus Prime Lite Edition can be used. Both are free, but the programmer is a smaller download

  • Drivers installed for the Altera USB Blaster

  • Firmware programming folder containing *.pof file (downloaded from Analog.com, request from admx-support@analog.com)

Board Programming Setup

  • Connect the USB Blaster to the computer over USB and verify the driver installation

  • Plug the ADMX2001B module into EVAL-ADMX2001EBZ board

  • Connect the USB blaster to the port labeled “P8 JTAG” on the EVAL-ADMX2001EBZ

  • Connect the EVAL-ADMX2001EBZ to a 9V DC supply

Update Using Installation Script

Versions 1.2.4+ comes bundled with an installation script to simplify the firmware installation process.

This script is the preferred installation method.

  • Follow the steps under Board Programming Setup

  • Ensure that Quartus Prime 18.1 or newer is installed in the following path: C:\intelFPGA_lite\<version_number>\quartus

  • Open a command prompt window

  • Navigate to the Tools folder present in the installation directory of Admx2001Firmware-Relx.y.z, C:\Analog Devices\Admx2001Firmware-Relx.y.z\Tools

    • Here, x, y, & z represents the release number (1.2.4 for example)

  • Run the following command: python admx2001_flash_pof.py --pof "C:\Analog Devices\Admx2001Firmware-Relx.y.z\Firmware\admx_lcr_encrypted.pof"

    • Ensure that x.y.z is replaced with the appropriate release number (1.2.4 for example)

  • Wait until the message “Programming POF completed successfully” is displayed in the terminal. It may take around 20 to 30 seconds for the process to complete.

    • Do not unplug the board or otherwise interrupt the programming process.

  • When the programming is completed (message displayed and prompt appears) close the terminal and unplug the USB blaster. The firmware update is complete.

Update Using Manual Programmer

Versions 1.2.2 and older do not come bundled with an installation script. The Quartus Prime Programmer interface can be used to perform the update. The installation script is the preferred method, as selecting the wrong settings in the manual programming tool can cause the board to no longer boot. It will need to be returned/swapped.

If there are issues preventing the installation script from working to program the board, the manual programmer method can be used. In this case, contact admx-support@analog.com for assistance using the manual programmer.

Firmware Release Highlights

Currently available firmare versions and release highlights:

Version

Status

Release Highlights

1.3.2

Stable

Measurement time optimizations, minor bug fixes

1.3.1

Stable

Substantial measurement noise improvements, bug fixes and more

1.2.4

Stable

Same firmware as 1.2.2. Installation script added to release package

1.2.2

Stable

Adds calibration over frequency, configurable digital outputs, external trigger support, bug fixes and more

1.2.0

Stable

Bug fixes, noise and repeatability improvements. Calibration with complex loads now supported

1.1.1

Legacy

Same fixes as 1.2.0, but not compatible with boards using the flash memory.

1.1.0

Legacy

Added SPI interface and built in self test

1.0.1

Legacy

1.0.0

Legacy

The full release notes are included with each firmware download.

Python Scripting

To facilitate easier measurement optimization on a PC, there is a library of Python functions which make it easy to operate the command-line interface from a Python script. Instead of typing commands over TeraTerm, the library accesses the Serial port directly, and calling the library functions will execute the same commands that are normally typed into the terminal emulator.

These Python libraries are currently accessible by request. First, make a myAnalog account on (analog.com) by clicking in the top right. Then, email admx-support@analog.com, and mention the email associated with the myAnalog account.

The Python script download includes an example measurement sweep script, which shows how to set up the Serial port, configure measurements and begin collecting data. More example scripts are coming in the future. Nearly all functions found in the command-line interface have corresponding Python functions in the library. These functions also perform a certain degree of error checking. This library is for evaluation purposes only.

Version 1.1.0 includes a graphical user interface.

Python Graphical User Interface

Since Python Evaluation Script version 1.1.0, the download package includes a Python based graphical user interface (GUI). The GUI does not yet support all features of the ADMX2001B, but it provides an quicker start and easier experimentation compared to using the UART command-line interface (CLI). The GUI communicates with the board over the UART CLI in the background, so any open terminals connected to the board need to be closed prior to using the GUI.

The GUI requires some 3rd-party Python libraries. The download includes a README.txt file (in the /GUI/ folder) with instructions on how to download these libraries and run the GUI.

Currently, the GUI supports:

  • Continuous or singular measurements

  • Plotting of multiple measurements or sweeps

  • Saving of measurement data

  • 18 display modes in SI units

  • Automatic and manual gain selection

  • Frequency, offset, magnitude and average settings

  • Calibrated measurements (but not the process of calibrating the board)

  • And more!

https://wiki.analog.com/_media/resources/eval/user-guides/admx/updated_admx2001b_python_gui_example.png

The Python GUI is bundled with the latest firmware downloads and available by request. First, make a myAnalog account on (analog.com) by clicking in the top right. Then, email admx-support@analog.com, and mention the email associated with the myAnalog account.

Support

For support, general questions, or firmware update help, reach out to admx-support@analog.com. External Link